KM15 Series Instr Manual Datasheet by TDK-Lambda

Product HANDBOOK KM15 Series TDK-Lambda ENGLISH A READ S A RISK OF E
Product HANDBOOK
KM15 Series
General Safety Instructions:
ENGLISH
READ SAFETY INSTRUCTIONS
Servicing:
These products are not customer serviceable. TDK-Lambda UK LTD. and their authorised agents only are
permitted to carry out repairs.
Critical Components:
These products are not authorised for use as critical components in nuclear control systems, life support
systems or equipment for use in hazardous environments without the express written approval of the
Managing Director of TDK-Lambda EMEA.
Product Usage:
These products are designed for use within a host equipment which restricts access to authorised competent
personnel.
Environmental:
These products are IPX0, and therefore chemicals/solvents, cleaning agents and other liquids must not be
used.
Environment:
This power supply is a switch mode power supply for use in applications within a Pollution Degree 2,
overvoltage category II environment. Material Group IIIb PCB’s are used within it.
Output Loading:
The output power taken from the power supply must not exceed the rating stated on the power supply label,
except as stated in the product limitations in this handbook.
Input Parameters:
This product must be operated within the input parameters stated in the product limitations in this handbook.
End of Life Disposal:
The unit contains components that require special disposal. Make sure that the unit is properly disposed of at
the end of its service life and in accordance with local regulations.
RISK OF ELECTRIC SHOCK
High Voltage Warning:
Dangerous voltages are present within the power supply. The professional installer must protect service
personnel from inadvertent contact with these dangerous voltages in the end equipment.
This product must be reliably earthed and professionally installed in accordance with the prevailing local
electrical wiring regulations and safety standards.
The (+) or (-) output(s) can be earthed or left floating.
An internal fuse protects the unit and must not be replaced by the user. In case of internal defect, the unit
must be returned to TDK-Lambda UK LTD or one of their authorised agents.
Product HANDBOOK KM15 Series TDK-Lambda A
Product HANDBOOK
KM15 Series
HOT SURFACE
External Hot Surfaces:
In accordance with local regulations for Health and Safety at work, manufacturers have an obligation to
protect service engineers as well as users. In order to comply with this, a label must be fitted to these
products which is clearly visible to service personnel accessing the overall equipment, and which legibly
warns that surfaces of these products may be hot and must not be touched when the products are in
operation.
Product HANDBOOK KM15 Series TDK-Lambda DEUTSCH A LESEN S A MIT FRE
Product HANDBOOK
KM15 Series
Allgemeine Sicherheitsvorschriften:
DEUTSCH
LESEN SIE DIE SICHERHEITSVORSCHRIFTEN
Wartung:
Diese Produkte können nicht durch den Kunden gewartet werden. Nur TDK-Lambda UK LTD. und deren
zugelassene Vertriebshändler sind zur Durchführung von Reparaturen berechtigt.
Kritische Komponenten:
Diese Produkte sind nicht für die Verwendung als kritische Komponenten in nuklearen Kontrollsystemen,
Lebenserhaltungssystemen oder Geräten in gefährlichen Umgebungen geeignet, sofern dies nicht
ausdrücklich und in Schriftform durch den Geschäftsführer von TDK-Lambda EMEA genehmigt wurde.
Produktverwendung:
Diese Produkte sind zur Verwendung innerhalb von Host-Anlagen gedacht, die einen auf das Fachpersonal
beschränkten Zugang haben.
Umwelt:
Diese Produkte sind IPX0, aus diesem Grund dürfen keine Chemikalien/Lösungsmittel, Reinigungsmittel und
andere Flüssigkeiten verwendet werden.
Umgebung:
Dieses Netzteil ist ein Schaltnetzteil zur Verwendung in einer Umgebung mit einem Verschmutzungsgrad 2,
Überspannungskategorie II. Materialgruppe IIIb mit darin verwendeten PCBs.
Ausgangsstrom:
Der Ausgangsstrom des Netzteiles darf die Leistung, die auf dem Label des Netzteiles vermerkt ist, nur dann
überschreiten, wenn dies in den Produktgrenzen dieses Handbuches ausgezeichnet ist.
Eingangsparameter:
Dieses Produkt muss innerhalb der Eingangsparameter, die in den Produktgrenzen dieses Handbuches
angegeben sind, betrieben werden.
Entsorgung am Ende der Betriebszeit:
Das Gerät enthält Komponenten die unter Sondermüll fallen. Das Gerät muss am Ende der Betriebszeit
ordnungsgemäß und in Übereinstimmung mit den regionalen Bestimmungen entsorgt werden.
NUR AC-DC PRODUKTE
MIT FREUNDLICHEN GRÜßEN
Hochspannungswarnung:
Innerhalb des Netzteiles gibt es gefährliche Spannungen. Der Elektroinstallateur muss das
Wartungspersonal vor versehentlichem Kontakt mit den gefährlichen Spannungen im Endgerät schützen.
Dies Produkt muss sicher geerdet und von qualifiziertem Personal in Übereinstimmung mit den gültigen
regionalen Bestimmungen zu Verdrahtungen sowie den Sicherheitsstandards installiert werden.
Die (+) oder (-) Ausgänge können geerdet werden oder unangeschlossen bleiben.
Eine interne Sicherung schützt das Gerät und darf durch den Benutzer nicht ausgetauscht werden. Im Fall
von internen Defekten muss das Gerät an TDK-Lambda UK LTD oder einen der autorisierten
Vertriebshändler zurückgeschickt werden.
Product HANDBOOK KM15 Series TDK-Lambda HEISSE
Product HANDBOOK
KM15 Series
HEISSE OBERFLÄCHEN
Äußere heiße Oberflächen:
In Übereinstimmung mit den regionalen Bestimmungen für Gesundheit und Sicherheit bei der Arbeit ist der
Hersteller für den Schutz von Wartungspersonal und Benutzern verantwortlich. Um diesen Bestimmungen
gerecht zu werden, muss auf den Produkten ein Label angebracht werden, das deutlich sichtbar für das
Wartungspersonal mit Zugriff auf die gesamte Anlage ist, und das gut lesbar auf die eventuell heiße
Oberfläche des Gerätes hinweist und das Berühren des Produktes in Betrieb untersagt.
Product HANDBOOK KM15 Series TDK-Lambda FRANQAIS A LIRE LE PRODUITS AC-DC SEULEMENT A RISQUE
Product HANDBOOK
KM15 Series
Consignes de sécurité générale:
FRANÇAIS
LIRE LES CONSIGNES DE SECURITE
Entretien:
Ces produits ne peuvent pas être réparés par le client. Seul, TDK-Lambda UK LTD et ses agents agréés
sont autorisés à effectuer des réparations.
Composants critiques:
Ces produits ne doivent pas être utilisés en tant que composants critiques dans des systèmes de commande
nucléaire, dans des systèmes de sauvetage ou dans des équipements utilisés dans des environnements
dangereux, sans l'autorisation écrite express du directeur général de TDK-Lambda EMEA.
Utilisation du produit:
Ces produits sont conçus pour être utilisés dans un équipement hôte dont l'accès n'est autorisé qu'aux
personnes compétentes.
Environnement:
Ces produits sont IPX0, et donc on ne doit pas utiliser des produits chimiques/solvants, des produits de
nettoyage et d'autres liquides.
Environnement:
Cette alimentation fonctionne en mode commutation pour utilisation dans des applications fonctionnant dans
un environnement avec Pollution Degré 2 et catégorie surtension II. Elle utilise des cartes de circuits
imprimés (PCB) Groupe IIIb.
Intensité soutirée:
L'intensité soutirée de l'alimentation ne doit pas dépasser l'intensité nominale marquée sur la plaque
signalétique, sauf indications contraires dans les limitations du produit dans ce manuel.
Paramètres d'entrée:
Ce paramètre doit être utilisé à l'intérieur des paramètres d'entrée indiqués dans les limitations du produit
dans ce manuel.
Elimination en fin de vie:
L'alimentation contient des composants nécessitant des mesures spéciales pour leur élimination. Vérifiez que
cette alimentation est éliminée correctement en fin de vie utile et conformément aux réglementations locales.
PRODUITS AC-DC SEULEMENT
RISQUE DE CHOC ELECTRIQUE
Attention-Danger haute tension:
Des tensions dangereuses sont présentes dans l'alimentation. L'installateur doit protéger le personnel
d'entretien contre un contact involontaire avec ces tensions dangereuses dans l'équipement final.
Ce produit doit être raccordé à une terre fiable et installé par des professionnels en respectant les
réglementations locales de câblages électriques en vigueur et les normes de sécurité.
Les sorties (+) ou (-) peuvent être raccordées à la terre ou laissées flotttantes.
Un fusible interne protège le module et ne doit pas être remplacé par l'utilisateur. En cas de défaut interne, le
module doit être renvoyé à TDK-Lambda UK LTD ou l'un de ses agents agréés.
Product HANDBOOK KM15 Series TDK-Lambda SURFAC
Product HANDBOOK
KM15 Series
SURFACE CHAUDE
Surfaces chaudes extérieures:
Conformément aux réglementations locales concernant la santé et la sécurité sur les lieux de travail, les
fabricants doivent protéger les techniciens d'entretien et les utilisateurs. Pour cela, une plaque signalétique
doit être installée sur ces produits, et cette plaque doit être bien visible pour les techniciens d'entretien
intervenant sur l'équipement, et elle doit indiquer de manière bien visible que les surfaces de ces produits
peuvent être chaudes et qu'elles ne doivent pas être touchées lorsque les produits fonctionnent.
Product HANDBOOK KM15 Series TDK-Lambda ITALIANO A SI PREG A RISCHIO
Product HANDBOOK
KM15 Series
Norme generali di sicurezza:
ITALIANO
SI PREGA DI LEGGERE LE NORME DI SICUREZZA
Manutenzione:
Il cliente non può eseguire alcuna manutenzione su questi prodotti. L'esecuzione delle eventuali riparazioni è
consentita solo a TDK-Lambda UK LTD e ai suoi agenti autorizzati.
Componenti critici:
Non si autorizza l'uso di questi prodotti come componenti critici all'interno di sistemi di controllo nucleari,
sistemi necessari alla sopravvivenza o apparecchiature destinate all'impiego in ambienti pericolosi, senza
l'esplicita approvazione scritta dell'Amministratore Delegato di TDK-Lambda EMEA.
Uso dei prodotti:
Questi prodotti sono progettati per l'uso all'interno di un'apparecchiatura ospite che limiti l'accesso al solo
personale competente e autorizzato.
Condizioni ambientali:
Questi prodotti sono classificati come IPX0, dunque non devono essere utilizzati sostanze chimiche/solventi,
prodotti per la pulizia o liquidi di altra natura.
Ambiente:
Questo prodotto è un alimentatore a commutazione, destinato all'uso in applicazioni rientranti in ambienti con
le seguenti caratteristiche: Livello inquinamento 2, Categoria sovratensione II. Questo prodotto contiene
schede di circuiti stampati in materiali di Gruppo IIIb.
Carico in uscita:
La potenza in uscita ottenuta dall'alimentatore non deve superare la potenza nominale indicata sulla targhetta
dell'alimentatore, fatto salvo dove indicato nei limiti per i prodotto specificati in questo manuale.
Parametri di alimentazione:
Questo prodotto deve essere utilizzato entro i parametri di alimentazione indicati nei limiti per il prodotto,
specificati in questo manuale.
Smaltimento:
L'unità contiene componenti che richiedono procedure speciali di smaltimento. Accertarsi che l'unità venga
smaltita in modo corretto al termine della vita utile e nel rispetto delle normative locali.
SOLO PER I PRODOTTI A CA-CC
RISCHIO DI SCOSSA ELETTRICA
Avvertimento di alta tensione:
All'interno dell'alimentatore sono presenti tensioni pericolose. Gli installatori professionali devono proteggere
il personale di manutenzione dal rischio di contatto accidentale con queste tensioni pericolose all'interno
dell'apparecchiatura finale.
Questo prodotto deve essere messo a terra in modo affidabile e installato in modo professionale, nel rispetto
delle norme di sicurezza e dei regolamenti vigenti in ambito locale in materia di collegamenti elettrici.
Le uscite (+) o (-) possono essere messa a terra o lasciate isolate.
Un fusibile interno protegge l'unità e non deve essere sostituito dall'utente. Nell'eventualità di un
difetto interno, restituire l'unità a TDK-Lambda UK LTD o a uno dei suoi agenti autorizzati
Product HANDBOOK KM15 Series TDK-Lambda SUPERF
Product HANDBOOK
KM15 Series
SUPERFICIE CALDA
Superfici esterne calde:
Coerentemente con le norme locali in materia di salute & sicurezza professionali, i produttori sono tenuti a
salvaguardare i tecnici di manutenzione, e inoltre gli utenti. Per far fronte a tali obblighi, i prodotti devono
presentare una targhetta, chiaramente visibile al personale di manutenzione che accede all'apparecchiatura
nel complesso e che risulti inoltre leggibile e avverta gli addetti del rischio che le superfici di questi prodotti
possono scottare e non vanno toccate con i prodotti in funzione.
Product HANDBOOK KM15 Series TDK-Lambda ESPANOL A LEA LAS A PELIGR
Product HANDBOOK
KM15 Series
Instrucciones generales de seguridad:
ESPAÑOL
LEA LAS INSTRUCCIONES DE SEGURIDAD
Servicio:
Estos productos no pueden ser reparados por los clientes. TDK-Lambda UK LTD. y sus agentes autorizados
son los únicos que pueden llevar a cabo las reparaciones.
Componentes fundamentales:
Estos productos no pueden ser utilizados como componentes fundamentales en sistemas de control nuclear,
sistemas de soporte vital o equipos a utilizar en entornos peligrosos sin el consentimiento expreso por escrito
del Director General de TDK-Lambda EMEA.
Uso de los productos:
Estos productos han sido diseñados para ser utilizados en un equipo central que restrinja el acceso al
personal cualificado autorizado.
Medioambiental:
Estos productos son IPX0 y, por tanto, no pueden utilizarse sustancias químicas/disolventes, agentes de
limpieza ni otros líquidos.
Medio ambiente:
Esta fuente de alimentación es una fuente de alimentación de modo conmutado a utilizar en aplicaciones
dentro de un entorno con un Grado de contaminación 2 y una Categoría de sobretensión II. En él se utilizan
policloruros de bifenilo del Grupo de materiales IIIb.
Carga de salida:
La potencia de salida tomada de la fuente de alimentación no puede sobrepasar el valor nominal indicado en
la etiqueta de la fuente de alimentación, excepto en los casos indicados en las limitaciones del producto en
este manual.
Parámetros de entrada:
Este producto debe ser utilizado dentro de los parámetros de entrada indicados en las limitaciones del
producto en este manual.
Desecho de la unidad:
La unidad contiene componentes que deben ser desechados de una manera especial. Asegúrese de
desechar correctamente la unidad al final de su vida útil y conforme a las normas locales vigentes.
SÓLO PRODUCTOS CA-CC
PELIGRO DE DESCARGAS ELÉCTRICAS
Advertencia de alta tensión:
En esta fuente de alimentación hay tensiones peligrosas. El instalador profesional debe proteger al personal
de servicio contra cualquier contacto accidental con estas tensiones peligrosas en el equipo final.
Este producto se puede conectar de forma fiable a tierra e instalar profesionalmente de conformidad con las
regulaciones locales para los cableados eléctricos y las normas de seguridad vigentes.
La salida o salidas (+) o (-) pueden conectarse a tierra o se las puede dejar flotando.
Product HANDBOOK KM15 Series TDK-Lambda SUPERF
Product HANDBOOK
KM15 Series
Un fusible interno protege la unidad y este no debe ser nunca reemplazado por el usuario. En caso de existir
algún defecto interno, la unidad debe ser enviada a TDK-Lambda UK LTD o a uno de sus agentes
autorizados.
SUPERFICIE CALIENTE
Superficies externas calientes:
Según las normas locales relativas a la Salud y Seguridad en el trabajo, los fabricantes están obligados a
proteger a los ingenieros de servicio además de a los usuarios. Para que esto se cumpla, debe colocarse
una etiqueta en estos productos que pueda ser vista claramente por el personal de servicio que accede al
equipo general, y con advertencias legibles de que las superficies de estos productos pueden estar calientes
y no deben tocarse cuando los productos se encuentran en funcionamiento.
Product HANDBOOK KM15 Series TDK-Lambda W A A RISCO D
Product HANDBOOK
KM15 Series
Instruções gerais de segurança:
PORTUGUÊS
LEIA AS INSTRUÇÕES DE SEGURANÇA
Manutenção:
Estes produtos não são podem ser submetidos a manutenção por parte do cliente. Apenas a TDK-Lambda
UK LTD e os seus agentes autorizados têm permissão para realizar reparações.
Componentes essenciais:
Não é autorizada a utilização destes produtos como componentes essenciais de sistemas de controlo
nuclear, sistemas de suporte de vida ou equipamento para utilização em ambientes perigosos sem a
expressa autorização por escrito do Director-Geral da TDK-Lambda EMEA.
Utilização do produto:
Estes produtos foram concebidos para utilização dentro de um equipamento de alojamento que apenas
permita o acesso a pessoal qualificado autorizado.
Ambiental:
Estes produtos são IPX0 e, como tal, não se devem utilizar químicos/solventes, agentes de limpeza e outros
líquidos.
Ambiente:
Esta fonte de alimentação é uma fonte de alimentação do modo de comutação para utilização em aplicações
com um Nível de Poluição 2 e ambientes da categoria de sobretensão II. São utilizadas placas de circuitos
impressos do grupo de materiais IIIb.
Carga de saída:
A potência de saída extraída da fonte de alimentação não deve exceder a classificação assinalada na
etiqueta da fonte de alimentação, excepto quando indicado nas limitações do produto neste guia.
Parâmetros de entrada:
Este produto deve ser utilizado dentro dos parâmetros de entrada indicados nas limitações do produto neste
guia.
Eliminação no fim de vida:
A unidade contém componentes que necessitam de procedimentos especiais de eliminação. Certifique-se de
que a unidade é devidamente eliminada no fim da sua vida útil e que tal é feito em conformidade com os
regulamentos locais.
APENAS PRODUTOS CA-CC
RISCO DE CHOQUE ELÉCTRICO
Aviso de alta tensão:
Estão presentes tensões perigosas dentro da fonte de alimentação. O profissional que realizar a instalação
deve proteger o pessoal de assistência contra contactos inadvertidos com estas tensões perigosas do
equipamento final.
Este produto deve ser ligado à terra de forma fiável e instalado por um profissional, de acordo com as
normas de segurança e os regulamentos locais vigentes em relação a cablagens eléctricas.
As saídas (+) e (-) podem ser ligadas à terra ou deixadas soltas.
Existe um fusível interno que protege a unidade e que não deve ser substituído pelo utilizador. Em caso de
defeito interno, a unidade deve ser devolvida à TDK-Lambda UK LTD ou a um dos seus agentes autorizados.
Product HANDBOOK KM15 Series TDK-Lambda SUPERF
Product HANDBOOK
KM15 Series
SUPERFÍCIE QUENTE
Superfícies quentes externas:
Segundo com os regulamentos locais sobre saúde e segurança no local de trabalho, os fabricantes têm a
obrigação de proteger os técnicos de manutenção, bem como os utilizadores. De forma a respeitar este
regulamento, estes produtos deverão ter uma etiqueta que seja facilmente visível ao pessoal de assistência
que aceda ao equipamento em geral, e que alerte, de forma legível, para o facto de as superfícies destes
produtos poderem estar quentes, não devendo ser tocadas quando os produtos estão em funcionamento.
Product HANDBOOK KM15 Series TDK-Lambda Slngle OiP Dual OiP Triple OiP 1 No pin No Pin No Pin 2 A0 (L) AC (L) AC (L) ' 3 AC (N) AC(N) AC(N) Top VleW 4 -DC out Do out GND for +5V 5 No pin GND +5V 6 No pin No pin -DC out 7 +DC out +DC out No pin 3 No pin No pin GND 9 No pin No pin +DC out Use Indoor - Temperature -25°C - +70°C (derating at 2.5%/°C above 50°C) -40°C - +100°C Humidity 20 - 95% RH, non-condensing 20 - 95% RH, non- condensing Altitude ~200m - 3000m ~200m - 5000M Pressure 70kPa - 106kPa 54kPa - 106kPa Orientation ALL Shock <196.1m z(206)="" vibration="" 23.52m/s2="" (10-55hz):="" constant="" sweep="" 1min="" x,="" y,="" z="" for="" 1="" hour="" material="" group="" illb="" pollution="" degree="" 2="" overvoltage="" category="" ii="" class="" ii="">
Product HANDBOOK
KM15 Series
Special Instructions for medical applications (IEC/EN/UL/CSA 60601-1)
These products are designed for continuous operation within an overall enclosure, and must be mounted
such that access to the mains terminals is restricted. See clause 16, IEC60601-1, EN60601-1 and UL/CSA
60601-1.
Input Connection - KMx15 –xx
Pin Single O/P Dual O/P Triple O/P
1 No pin No Pin No Pin
2 AC (L) AC (L) AC (L)
3 AC (N) AC (N) AC (N)
4 -DC out -DC out GND for +5V
5 No pin GND +5V
6 No pin No pin -DC out
7 +DC out +DC out No pin
8 No pin No pin GND
9 No pin No pin +DC out
These products are NOT suitable for use in the presence of flammable anaesthetic mixtures with air or with
oxygen, or with nitrous oxide.
These products are classed as ordinary equipment, type B and have a reinforced barrier between input and
output to IEC60601-1, EN60601-1 and UL/CSA 60601-1. They are NOT protected against the ingress of
water.
Reference should be made to local regulations concerning the disposal of these products at the end of their
useful life.
Environmental Specifications:
Description Operation Storage
Use Indoor -
Temperature -25°C - +70°C (derating at 2.5%/°C above 50°C) -40°C - +100°C
Humidity 20 - 95% RH, non-condensing 20 - 95% RH, non-
condensing
Altitude -200m - 3000m -200m - 5000m
Pressure 70kPa - 106kPa 54kPa - 106kPa
Orientation ALL
Shock <196.1m/s
2
(20G)
Vibration 23.52m/s
2
(10-55Hz): constant sweep 1min X, Y, Z for 1 hour
Material Group IIIb
Pollution Degree 2
Overvoltage Category II
Class II
Product HANDBOOK KM15 Series TDK-Lambda Rated input voltage 100-240 VAC Input voltage range 90 — 264VAC Input frequency range 47 — 63Hz Maximum input current 130mA/ 270mA/ 115/240VAC 0.70mA 0.130mA lnrush current 15W Single O/P 15W Dual O/P 15W Triple O/P (Note 1) 9 12 15 24 +5/-5 +12/-12 +15/-15 +5/+12/-12 +5/+15/-15 2.4 1.8 1.4 0.9 1.5/1 .5 0625/0625 0.5/0.5 2/0.2/0.2 2/0.15/0.15 20A max at 230VAC (25°C celd start) Model Vout(V itput rrent l Max capacttlve loadl (ut 40000 10000 3000 1100 1000 820 4700 560 500 10000/470 10000/600
Product HANDBOOK
KM15 Series
Level of Insulation:
Primary mains circuits to secondary: 4.25 - 4.35kVDC
Safety Approvals:
IEC/UL/EN60601-1, (2
nd
Edition)
UL/cUL60950-1 (2
nd
Edition)
IEC / EN60950-1(2
nd
Edition)
CE marking when applied to any KMx15any product indicates compliance with the Low Voltage Directive
(2006/95/EC) in that it complies with EN60950-1 (2
nd
Edition).
Fusing: Internal fuses (F1): Single fuse in the L line, T2AL, 250V, not Serviceable
External fusing: Recommended 2A/250V slow blow
Input Parameters:
Standard 60950-1
Rated input voltage 100-240 VAC
Input voltage range 90 264VAC
Input frequency range 47 63Hz
Maximum input current
115/240VAC 130mA/
0.70mA 270mA/
0.130mA 400mA/
0.200mA
Inrush current 20A max at 230VAC (25°C cold start)
Output Parameters:
Model Vout (V) Output
current (A) Max
capacitive
load (µ)
3.3 4.4 40000
5 4.4 10000
9 2.4 3000
12 1.8 1100
15 1.4 1000
15W
Single O/P
24 0.9 820
+5/-5 1.5/1.5 4700
+12/-12 0.625/0.625 560
15W
Dual O/P +15/-15 0.5/0.5 500
+5/+12/-12 2/0.2/0.2 10000/470
15W
Triple O/P (Note 1) +5/+15/-15 2/0.15/0.15 10000/600
Note 1: For Triple output modules the main 5V output is isolated from the other ±12V or ±15V outputs (dependant on model). A minimum
load of 25% is required on the ±12V and ±15V outputs.
All outputs are SELV except under the following circumstance: Outputs connected in series are non-SELV if
the total output voltage exceeds 60Vdc
If the total voltage of outputs connected in series exceed the 60Vdc SELV limit then all outputs must be
considered non-SELV.
Non-SELV outputs are hazardous and must not be made user accessible. Consideration must be given to
service engineers making inadvertent contact with the output terminals in the end equipment.
Product HANDBOOK KM15 Series TDK-Lambda INN- m m m E)‘ g 90% IE 4056 m m 10% o ‘0 20 so ‘0 so so 70 an AM Immune l1:
Product HANDBOOK
KM15 Series
Cooling for unit
The KMx15 series are convection cooled, derating for recommended installation shown.
The units are provided with an over temperature protection 10C. Max case temperature 95°C.
Mounting position
Equipment top
The KM15 family of component power supplies is designed for use within other equipment or enclosures
which restrict access to authorised competent personnel only.
Product HANDBOOK KM15 Series TDK-Lambda . 64.0 - - 23‘s »- - . 54‘0 - 5‘0 'i' . 175 ‘ “ 1o 0 1 0 455 2 x A . I . 5‘ 7 5 12 5 10 0 . 5‘ 175 17 5 . y‘ , '8‘ i}, ' ' '9‘ ' {540 60 l - Idelanoetofimm TDK-Lambda TDKrLambda UK L Kingsley Avenue, | Devon, EX34 8E5 Telephone , Sales and Service ead Office and Works +44 (0) ile +44 (0)1271 864894 www.uk.tdk7|ambda.com
Product HANDBOOK
KM15 Series
Mechanical Outline Drawings:
KMx15-xx
(See above for recommended mounting position)
TDK-Lambda UK Ltd
Kingsley Avenue, Ilfracombe
Devon, EX34 8ES
Telephone - Sales and Service +44 (0)1271 856666
Head Office and Works +44 (0)1271 856600
Facsimile +44 (0)1271 864894
WEBSITE: www.uk.tdk-lambda.com