10
Sheet No.: D3-A04901FEN
GP2A25J0000F Series
■Important Notices
· The circuit application examples in this publication
are provided to explain representative applications of
SHARP devices and are not intended to guarantee any
circuit design or license any intellectual property rights.
SHARP takes no responsibility for any problems related
to any intellectual property right of a third party resulting
from the use of SHARP's devices.
· Contact SHARP in order to obtain the latest device
specification sheets before using any SHARP device.
SHARP reserves the right to make changes in the
specifi cations, characteristics, data, materials, structure,
and other contents described herein at any time
without notice in order to improve design or reliability.
Manufacturing locations are also subject to change
without notice.
· Observe the following points when using any devices
in this publication. SHARP takes no responsibility for
damage caused by improper use of the devices which
does not meet the conditions and absolute maximum
ratings to be used specifi ed in the relevant specifi cation
sheet nor meet the following conditions:
(i) The devices in this publication are designed for use
in general electronic equipment designs such as:
--- Personal computers
--- Offi ce automation equipment
--- Telecommunication equipment [terminal]
--- Test and measurement equipment
--- Industrial control
--- Audio visual equipment
--- Consumer electronics
(ii) Measures such as fail-safe function and redundant
design should be taken to ensure reliability and safety
when SHARP devices are used for or in connection
with equipment that requires higher reliability such as:
--- Transportation control and safety equipment (i.e.,
aircraft, trains, automobiles, etc.)
--- Traffi c signals
--- Gas leakage sensor breakers
--- Alarm equipment
--- Various safety devices, etc.
(iii) SHARP devices shall not be used for or in
connection with equipment that requires an extremely
high level of reliability and safety such as:
--- Space applications
--- Telecommunication equipment [trunk lines]
--- Nuclear power control equipment
--- Medical and other life support equipment (e.g.,
scuba).
· If the SHARP devices listed in this publication fall
within the scope of strategic products described in the
Foreign Exchange and Foreign Trade Law of Japan, it
is necessary to obtain approval to export such SHARP
devices.
· This publication is the proprietary product of SHARP
and is copyrighted, with all rights reserved. Under
the copyright laws, no part of this publication may be
reproduced or transmitted in any form or by any means,
electronic or mechanical, for any purpose, in whole or in
part, without the express written permission of SHARP.
Express written permission is also required before any
use of this publication may be made by a third party.
· Contact and consult with a SHARP representative
if there are any questions about the contents of this
publication.
[H174]