SOLDERI NC I RON
SOLDERI NG IRON SLEEP 11 MER
10
5. Set the desired air temperature using buttons A6 and A7.
6. You may start reworking as soon as the desired temperature is reached.
Refer to display panel C3 to verify.
7. When reworking is completed, turn off the “SMD Rework” function
switch. The auto-cooling functionality will commence if the system
detects a temperature higher than 95°C. It will blow at full speed to
accelerate the cooling down of the Hot Air Gun. The auto-cooling
functionality will stop when the temperature of the Hot Air Gun reaches
about 95°C or below, as shown from the actual temperature display
panel, C3. The system will then switch off and display an “OFF”
message from user-defined temperature display panel, C2.
NOTE:
Make sure the smoke absorption functionality is switched OFF when using
the equipment for SMD Rework.
SOLDERING IRON
1. With the unit plugged to the main power source and main power switch
in the ON position, ensure that the Soldering Iron is properly connected
to the receptacle, D1.
2. The Soldering Iron display A2 will show the word “OFF” indicating the
Soldering Iron function is turn off.
3. To use the Soldering Iron turn ON the “Soldering Iron” function
switch, B1.
4. The Soldering Iron display A2 will briefly show the current set
temperature then switch to displaying the actual temperature.
5. When we use the adjustment knob, A3, to set the desired soldering
temperature. The digital display A2 will show the current set
temperature based on the knob position.
OPERATING GUIDELINES
11
5. After a few seconds the digital display A2 will switch to showing the
actual temperature. You may start soldering when the desired
temperature has been reached. The small dot located at the end of the
number displayed in A2 signifies the heater regulation. When the small
dot starts blinking on and off the system has reached the desired set
temperature.
6. After usage turn off the Soldering Iron function switch.
7. If the Soldering Iron tip is still higher than 100 degrees, the Soldering
Iron display will show the word “Hot” indicating the Soldering Iron is
still hot to caution users.
8. When the Soldering Iron tip’s temperature has fallen to manageable
level the display will show the word “OFF”
9. Switch ON the “Smoke Absorber” function switch, B2, to activate
the smoke absorption functionality.
NOTE:
Turn the “Smoke Absorber” ON only after the soldering iron reached the
desired (set) temperature. This is to avoid affecting the temperature increase of the
soldering iron in terms of heating time.
SOLDERING IRON SLEEP TIMER
1. The Soldering Iron has a sleep feature that allows the Soldering Iron to
go into sleep mode depending on user programmed duration.
2. To access and enable the sleep feature of the Soldering Iron:
● Turn Soldering Iron, SMD and Smoke Absorber function switch off.
● Press and hold the hot air temperature increase button A6.
● The Soldering Iron display A2 will turn to “t##” , indicating it is now on
sleep timer adjustment mode.
● Turn the Soldering Iron adjustment knob to select desired sleep time
in minutes.
OPERATING GUIDELINES