T543031
DESCO WEST - 3651 Walnut Avenue, Chino, CA 91710 • (909) 627-8178
DESCO EAST - One Colgate Way, Canton, MA 02021-1407 • (781) 821-8370 • Website: Desco.com
TB-3031 Page 3 of 9 © 2019 DESCO INDUSTRIES INC
Employee Owned
Maintenance
“All ionization devices will require periodic maintenance
for proper operation. Maintenance intervals for ionizers
vary widely depending on the type of ionization
equipment and use environment. Critical clean room
uses will generally require more frequent attention. It
is important to set-up a routine schedule for ionizer
service. Routine service is typically required to meet
quality audit requirements.” (ESD Handbook TR20.20
section 5.3.6.7 Ionizer Maintenance / Cleaning)
EIA-625, recommends checking ionizers every 6
months, but this may not be suitable for many programs
particularly since an out-of-balance may exist for months
before it is checked again. ANSI/ESD S20.20 section
6.1.3.1 Compliance Verification Plan Requirement
states: “Test equipment shall be selected to make
measurements of appropriate properties of the technical
requirements that are incorporated into the ESD
program plan.”
CLEANING THE EMITTER POINTS
Under normal conditions, the ionizer will attract dirt and
dust (especially on the emitter points). To maintain
optimum neutralization efficiency and operation,
cleaning should be performed on a regular basis.
In the event of circuit failure, the unit will enter shutdown
mode.
When the unit enters shutdown mode, ionization will be
stopped, the LED on the front of the unit will illuminate
a constant red, and the audible alarm will continuously
sound. The user must then reset the unit by turning it
OFF and back ON.
The emitter points should be cleaned using the included
Emitter Point Cleaners or a swab dampened with
Isopropyl alcohol.
1. Turn the unit OFF and unplug the power cord.
2. Open the top screen
by loosening the screw
and swinging the grill to
one side.
3. Clean the emitter points
using the included
Emitter Point Cleaners
or a swab dampened
with Isopropyl alcohol.
4. Reattach the top
screen.
5. Plug in the power cord
and turn the unit ON.
6. Verify the performance
of the ionizer by
using a charged plate
monitor, or ionization
test kit.
With normal handling, the emitter points should not
require replacement during the life of the unit. If
necessary, item 60507 Replacement Emitter Points are
available for purchase.
Adjustments and Compliance
Verification
BALANCE OFFSET VOLTAGE ADJUSTMENT
The Chargebuster® Overhead Ionizer is an
auto-balancing unit. However, tuning or manual
adjustment can be accomplished by inserting a small
screwdriver or trimmer adjustment tool into the balance
adjustment hole. To increase the output in a positive
direction, turn the potentiometer clockwise. To increase
the output in a negative direction, turn the potentiometer
counter-clockwise.
INPUT VOLTAGE CONFIGURATION
WARNING - Risk of electric shock
These servicing instructions are for use by qualified
personnel only. Do not perform any servicing of
internal parts unless you are qualified to do so.
NOTE: The AC power cord MUST always be
disconnected before the unit is disassembled.
The input voltage may be verified or reset by opening
the ionizer’s enclosure. This can be accomplished by
removing the 10 screws that secure the cover to the
base.
The ionizer’s input voltage can be configured to 120
VAC or 220 VAC using the JH1 jumpers located on its
PCB. See Figures 7 and 8 for these configurations.
Figure 7. 120 VAC jumper
setting
Figure 8. 220 VAC jumper
setting
If the supply voltage drops from 110 Volts to below 85
Volts or from 200 Volts to below 170 Volts, the unit will
shut down, the audible alarm will beep and the LED will
blink red. The unit will automatically reset when the
minimum voltage is restored.