20 Phone +49(0).551 69 35-0 Fax +49(0).551 69 35-166 www.qioptiq-shop.comsales.qioptiq@excelitas.com
How Do I Apply
Adhesives?
Was muss ich beim
Kleben von Optiken
beachten?
Optics:
Use a bulb blower to remove dust and loose dirt.
Put a lens-cleaning cloth or another soft cotton
cloth (e.g. Opto-WipesTM) on the optics and use a
pipette to apply several drops of alcohol to the
cloth. Make sure the alcohol is chemically pure.
Then drag the cloth slowly over the optics. To
reduce fingerprints or similar impurities, proceed
as described above or soak a cotton swab in
alcohol and wipe it across the optics in an "S"
shaped motion.
Optics holder:
The holder must also be cleaned and freed of dust
and grease. To do this, wipe it with a soft cloth,
using a small amount of a grease-cutting
detergent (such as dishwashing liquid) if
necessary. Wipe again afterwards
with a fresh cloth to remove any residues.
Adhesives:
The type of adhesive you should use depends on
the type of optics you wish to cement. For mirrors,
use an elastic two-component adhesive for a
uniform curing and tension-free hold. For
components such as beamsplitter cubes or plates,
a UV adhesive is ideal. As the name indicates, UV
light is applied to cure the adhesive.
Strips of double-sided tape are commonly used in
research and development laboratories. These are
well-suited for quick experimental setups,
particularly if the optic is removed from the carrier
afterwards. They are not recommended, however,
for long-term use; due to their elasticity and
susceptibility to vibration, it is impossible to ensure
that the position of the optics is maintained.
Tips for cementing optics:
Even if a liquid adhesive is used, the optics can be
removed later if the adhesive is applied in discrete
spots on the edge of the optics only. Affix the optic
holder to your work surface with adhesive strips,
making sure the glue surface is on the horizontal
plane to prevent slippage until the adhesive is
cured. To ensure an even layer of adhesive, lay
two strips of paper as spacers on the optics carrier
and press the optics until the adhesive reaches the
paper. Once the adhesive has cured, you can
remove the paper. This method also prevents the
adhesive from leaking out between the optics and
the holder when the parts are pressed together.
The use of a cotton swab is recommended to
prevent damage when aligning and pressing down
on the optics.
Optik:
Enfernen Sie Staub und losen Schmutz mit einem
kleinen Blasebalg. Legen Sie ein Linsenputztuch
oder weiches Baumwolltuch (z.B. Opto-WipesTM)
auf die Optik und tragen mit einer Pipette einige
Tropfen Alkohol (chem. Reinheit beachten) auf das
Tuch. Abschließend das Tuch langsam über die
Optik ziehen. Bei Fingerabdrücken oder anderen
Verunreinigungen verwenden Sie die o.g.
Materialien oder auch ein mit Alkohol getränktes
Wattestäbchen und wischen in einer leicht
„S“-förmigen Bewegung über die Optik.
Optikhalter:
Auch der Optikhalter ist von Staub und Fett zu
reinigen. Hierfür genügt das Abwischen mit einem
feuchten Tuch, ggf. unter sparsamer Verwendung
eines milden Fettlösers (z.B. Geschirrspülmittel).
Bitte mit neuem Tuch nachwischen, um Rückstände
des Reinigers zu entfernen.
Klebstoffe:
Zum Kleben von Optiken bieten sich je nach Optik
verschiedene Klebstofftypen an. Spiegel sollten mit
einem dauerelastischen Zweikomponenten-Kleb-
stoff fixiert werden. Dieser Klebertyp gewährleistet
eine gleichmäßige Aushärtung und eine
spannungsfreie Verbindung. Für Komponenten wie
Strahlteiler-Würfel oder -Platten ist ein UV-Kleb-
stoff ideal; dabei wird UV-Licht zur Aushärtung der
Klebestelle verwendet.
In Entwicklungslaboren sehr beliebt sind
doppelseitige Klebestreifen. Für schnelle
Versuchsaufbauten sind sie durchaus geeignet,
speziell wenn die Optik anschließend wieder vom
Träger entfernt werden soll. Für den Dauereinsatz
sind sie jedoch nicht zu empfehlen; aufgrund ihrer
Elastizität und Vibrationsanfälligkeit ist eine
Lageänderung der Optik nicht auszuschließen.
Tipps zum Kleben:
Auch bei flüssigen Klebstoffen ist ein späteres
Entfernen der Optik möglich, wenn der Kleber nur
punktuell an der Optikkante aufgetragen wird.
Erleichtern Sie sich das Optikkleben, indem Sie den
Optikhalter auf Ihrer Arbeitsfläche mit Klebestrei-
fen fixieren und lagern Sie den Optikhalter von der
Klebung bis zur Aushärtung waagerecht, um ein
Verrutschen der Optik zu verhindern. Um eine
gleichmäßige Klebstoffschicht zu erhalten, legen
Sie zwei Papierstreifen als Abstandshalter auf den
Optikträger, tragen Sie den Kleber auf und drücken
Sie die Optik bis auf die Papierstreifen an. Nach
dem Aushärten können die Papierstreifen wieder
entfernt werden. Diese Methode verhindert auch,
dass sich der Klebstoff beim Andrücken zwischen
Optik und Halter herausdrückt. Die Verwendung
eines Wattestäbchens zum Ausrichten und
Andrücken der Optik verhindert Beschädigungen.
Applying adhesive in spots between optics and contact
surface of the holder
Positioning paper strips as spacers on a mirror mount
Pressing down and repositioning a mirror on the fixed
mirror mount
Beamsplitter cube illuminated by a UV light source
• To keep the need for cleaning to a
minimum, wear latex gloves or lint-free
cotton gloves when unpacking and setting
up the equipment and make sure all work
surfaces are clean.
Frequently Asked Questions