*5 TEXAS
INSTRUMENTS
SN54LVT8996, SN74LVT8996
3.3-V 10-BIT ADDRESSABLE SCAN PORTS
MULTIDROP-ADDRESSABLE IEEE STD 1149.1 (JTAG) TAP TRANSCEIVERS
SCBS686A – APRIL 1997 – REVISED DECEMBER 1999
5
POST OFFICE BOX 655303 • DALLAS, TEXAS 75265
Terminal Functions
TERMINAL
NAME DESCRIPTION
A9–A0 Address inputs. The ASP compares addresses received via shadow protocol against the value at A9–A0 to determine address
match. The bit order is from most significant to least significant. An internal pullup at each A9–A0 terminal forces the terminal
to a high level if it has no external connection.
BYP Bypass input. A low input at BYP forces the ASP into BYP or BYP/TRST status, depending on PTRST being high or low,
respectively. While BYP is low, shadow protocols are ignored. Otherwise, while BYP is high, the ASP is free to respond to
shadow protocols. An internal pullup forces BYP to a high level if it has no external connection.
CON Connect indicator (output). The ASP indicates secondary-scan-port activity (resulting from BYP, BYP/TRST, MULTICAST, or
ON status) by forcing CON to be low. Inactivity (resulting from OFF, RESET, or TRST status) is indicated when CON is high.
GND Ground
PTCK Primary test clock. PTCK receives the TCK signal required by IEEE Std 1149.1-1990. The ASP always buffers PTCK to STCK.
Shadow protocols are received/acknowledged synchronously to PTCK and connect-status changes invoked by shadow
protocol are made synchronously to PTCK.
PTDI
Primary test data input. PTDI receives the TDI signal required by IEEE Std 1149.1-1990. During appropriate TAP states, the
ASP monitors PTDI for shadow protocols. During shadow protocols, data at PTDI is captured on the rising edge of PTCK. When
a valid shadow protocol is received in this fashion, the ASP compares the received address against the A9–A0 inputs. If the
ASP detects a match, it outputs an acknowledgment and then connects its primary TAP terminals to its secondary TAP
terminals. Under BYP, BYP/TRST, MULTICAST or ON status, the ASP buffers the PTDI signal to STDO. An internal pullup
forces PTDI to a high level if it has no external connection.
PTDO
Primary test data output. PTDO transmits the TDO signal required by IEEE Std 1149.1-1990. During shadow protocols, the
ASP transmits any required acknowledgment via the PTDO. The acknowledgment data output at PTDO changes on the falling
edge of PTCK. Under BYP, BYP/TRST, or ON status, the ASP buffers the PTDO signal from STDI. Under OFF, MULTICAST,
RESET, or TRST status, PTDO is at high impedance.
PTMS
Primary test mode select. PTMS receives the TMS signal required by IEEE Std 1149.1-1990. The ASP monitors the PTMS to
determine the TAP-controller state. During stable TAP states other than Shift-DR or Shift-IR (i.e., Test-Logic-Reset,
Run-Test-Idle, Pause-DR, Pause-IR) the ASP can respond to shadow protocols. Under BYP, MULTICAST, or ON status, the
ASP buffers the PTMS signal to STMS. An internal pullup forces PTMS to a high level if it has no external connection.
PTRST
Primary test reset. PTRST receives the TRST signal allowed by IEEE Std 1149.1-1990. The ASP always buffers PTRST to
STRST. A low input at PTRST forces the ASP to assume TRST or BYP/TRST status, depending on BYP being high or low,
respectively. Such operation also asynchronously resets the internal ASP state to its power-up condition. Otherwise, while
PTRST is high, the ASP is free to respond to shadow protocols. An internal pullup forces PTRST to a high level if it has no
external connection.
STCK Secondary test clock. STCK retransmits the TCK signal required by IEEE Std 1149.1-1990. The ASP always buffers STCK from
PTCK.
STDI Secondary test data input. STDI receives the TDI signal required by IEEE Std 1149.1-1990. Under BYP, BYP/TRST, or ON
status, the ASP buffers STDI to PTDO. An internal pullup forces STDI to a high level if it has no external connection.
STDO Secondary test data output. STDO transmits the TDO signal required by IEEE Std 1149.1-1990. Under BYP, BYP/TRST,
MULTICAST, or ON status, the ASP buffers STDO from PTDI. Under OFF, RESET, or TRST status, STDO is at high impedance.
STMS
Secondary test mode select. STMS retransmits the TMS signal required by IEEE Std 1149.1-1990. Under BYP, MULTICAST,
or ON status, the ASP buffers STMS from PTMS. When disconnected (as a result of OFF status), STMS maintains its last valid
state until the ASP assumes BYP/TRST, RESET, or TRST status (upon which it is forced high) or the ASP again assumes BYP,
MULTICAST, or ON status.
STRST Secondary test reset. STRST retransmits the TRST signal allowed by IEEE Std 1149.1-1990. The ASP always buffers STRST
from PTRST.
VCC Supply voltage