407732 User Manual Datasheet by FLIR Extech

EXTECH“ INSTRUMENTS
USER GUIDE
Digital Sound Level Meter
Model 407732
www.5xtech,cum
407732-en-GB_V1.7 12/14
2
Introduction
Thank you for selecting the Extech Model 407732. This device is shipped fully tested and calibrated
and, with proper use, will provide years of reliable service. Please visit the Extech Instruments website
(www.extech.com) to check for the latest version of this User Guide.
Safety
Read the following safety information carefully before attempting to operate or service the
meter. Use the meter only as specified in this manual; otherwise, the protection provided by
the meter may be impaired.
Environmental Conditions
Altitude up to 2000 meters
Relative Humidity: 90% max.
Operating Temperature: 0 to 40oC (32 to 104oF)
Maintenance and Cleaning
Repair or servicing not covered in this manual should only be performed by qualified
personnel.
Periodically wipe the case with a dry cloth. Do not use abrasives or solvents.
\ m. ‘ soumum mun ‘
407732-en-GB_V1.7 12/14
3
Meter Description
1. Microphone
2. 4-digit LCD Display
3. ON-OFF button
4. LCD Backlight button
5. Frequency weighting selection button
6. Response time selection button
7. Range selector button
8. Max Hold / Data Hold selector button
9. Battery compartment on rear
10. Calibration pots in battery compartment
11. Windscreen
Measurement Considerations
1. Wind blowing across the microphone increases the noise measurement. Use the supplied
windscreen to cover the microphone when applicable.
2. Calibrate the instrument before each use if possible. Especially if the meter has not been used
for a long period of time.
3. Do not store or operate the instrument in areas of high temperature or humidity.
4. Keep meter and microphone dry.
5. Avoid severe vibration.
6. Remove the battery when the meter is to be stored for long periods of time.
Q
407732-en-GB_V1.7 12/14
4
Operation
1. Power the meter by pressing the power button. The meter will begin displaying sound level
readings. If the LCD does not switch on, check the 9V battery located in the rear battery
compartment.
2. Hold the meter in hand facing the microphone toward the source of the sound to be measured.
3. View the measurement on the meter’s LCD. An indication of OVER means that the measurement
is out of range. Toggle the ‘Hi’ (65 to 130dB) and ‘Lo’ (35 to 100dB) measurement ranges using
the HI/LO button. For measurements in the 65 to 100dB region either range can be used.
‘A’ and ‘C’ Frequency Weighting
Use the ‘A/C’ button to select ‘A’ or ‘C’ frequency weighting. With ‘A’ weighting selected, the
frequency response of the meter is similar to the response of the human ear. ‘A’ weighting is
commonly used for environmental or hearing conservation programs such as OSHA regulatory
testing and noise ordinance law enforcement. ‘C’ weighting is a much flatter response and is
suitable for the sound level analysis of machines, engines, etc.
Most noise measurements are performed using 'A' Weighting and SLOW Response.
‘FAST’ and ‘SLOW’ Response Time
Use the ‘F/C’ button to select FAST (125 ms) or SLOW (1 second) response time. Select FAST to
capture noise peaks and noises that occur very quickly. Select the SLOW response to monitor a
sound source that has a consistent noise level or to average quickly changing levels.
Select Slow response for most applications.
‘Hi’ and ‘Lo’ Range Selections
Use the ‘Hi/Lo’ button to select the appropriate range. If the measurement is in the range of 35 to
100 dB, use the ‘Lo’ range. If the measurement is between 65 and 130dB, use the ‘Hi’ range. For
measurements between 65 and 100dB, either range can be used. If the display flashes the OVER
icon, press the range button to toggle the range.
MAX HOLD
In this mode, the meter only updates the LCD when a higher reading than the one presently on the
display is detected. Select MAX HOLD by momentarily pressing the MAX HOLD button. The meter
displays the MAX icon when in the MAX HOLD mode. Press the MAX HOLD button again to exit
this mode (the MAX indicator will switch off).
DATA HOLD
To freeze a displayed reading, press and hold the MAX HOLD button until the MAX and HOLD
display icons appear. To release the display and return to the normal operating mode, press and
hold the MAX HOLD button until the MAX and HOLD icons switch off.
Backlight button
The LCD is equipped with backlighting for easier viewing, especially in dimly lit areas. Press the
backlight button to turn the backlight on. Press again to turn the backlight off. The backlight does not
have an automatic power down function; judicious use will conserve battery life.
9v Baku Quota—o #313,.» um.“ Battery Replacement When the low ballery lCOn EAT appears on the LCD replace the av battery as soon as possmle. The ballery compartment cover rs located on the rear of the meter. Remove the Phillips screw Io loosen the cover Sllde the ballery compartment cover oil, change the ballery‘ and replace the compartment cover. Youl as the end user, are legally bound (Battery ordinancel to return all used banana and accumulators disposal in the household garbage is prohibited! You can hand over your used oatlenes l accumulators al collection points ln your community or wherever batteries / accumulators are soldl — Disposal: Follow the ualrd legal stipulations ln respect ot the disposal of the devrce an end oi its lriecycle 5 407732-en-GfiiV1J 12
407732-en-GB_V1.7 12/14
5
Calibration
To calibrate the 407732, an external calibrator that can provide a 94.0dB signal at 1 kHz is required in
addition to a small screw-driver.
1. Open the battery compartment and locate the two calibration potentiometers behind the 9V
battery (see diagram)
2. Turn the meter ON
3. Put the meter in the ‘C’ weighting mode
4. Put the meter in the ‘FAST’ response mode
5. Place the 407732 microphone into the calibrator. Set the calibrator
to output a 1kHz sine wave @ 94dB
6. Put the meter in the LOW range
7. Adjust the ‘C (Lo)’ potentiometer for a display of 94.0 dB
8. Put the meter in the HIGH range
9. Adjust the ‘C (HI)’ potentiometer for a display of 94.0 dB
Battery Replacement
When the low battery icon BAT appears on the LCD replace the 9V battery as soon as possible.
The battery compartment cover is located on the rear of the meter. Remove the Phillips screw to
loosen the cover. Slide the battery compartment cover off, change the battery, and replace the
compartment cover.
You, as the end user, are legally bound (Battery ordinance) to return all used batteries
and accumulators; disposal in the household garbage is prohibited!
You can hand over your used batteries / accumulators at collection points in your
community or wherever batteries / accumulators are sold!
Disposal: Follow the valid legal stipulations in respect of the disposal of the device at the
end of its lifecycle
CC
407732-en-GB_V1.7 12/14
6
Specifications
Display 4-digit (4000 count) backlit LCD
Display update rate 0.5 seconds
Microphone 0.5” Electret condensor
Measurement Bandwidth 31.5Hz to 8KHz
Dynamic range 65dB
Measurement Range 35 to 130dB (Low: 35 to 100; High: 65 to 130dB)
Frequency weighting ‘A’ and ‘C’ (selectable)
Accuracy / Resolution ± 1.5dB (under reference conditions) / 0.1dB
Standards Meets Type 2 ANSI S1.4-1983, IEC 60651, EN60651
Maximum Hold decay time <1dB / 3min
Response time Fast: 125 milliseconds / Slow: 1 second
Calibration source required 1KHz sine wave @ 94dB
Power 9V Battery
Battery life 50 hours (typical); low battery indicator alerts user
Automatic power off After approx. 15 minutes of inactivity
Operating temperature 0 to 40oC (32 to 104oF)
Operating humidity 10 to 90% RH
Storage temperature -10 to 60oC (14 to 140oF)
Storage humidity 10 to 75% RH
Dimensions/weight 240 x 68 x 25mm (9.45 x 2.68 x 1”) /210g (6.75oz)
9375’ 4
407732-en-GB_V1.7 12/14
7
Typical A-Weighted Sound Levels
50HP Siren (100')
130
120
110
100
90
80
70
60
50
40
30
20
10
140
0
Jet takeoff (200')
dBA
Riveting machine
Chain saw
Subway (20') Boiler r oom
Pneumatic drill (50' ) Freight train (100')
Vacuum cleaner (10') Speech (1')
Large store Large Office
Small office Residence
Night residential area
Whisper (5' 0)
Sound studio
Threshold of hearing
Copyright © 2014 FLIR Systems, Inc.
All rights reserved including the right of reproduction in whole or in part in any form
ISO-9001 Certified
www.extech.com