VE_—:
wiik‘lH [LKKIRONIK
Important Notes
The following conditions apply to all goods within the product range of Würth Elektronik
eiSos GmbH & Co. KG:
1. General Customer Responsibility
Some goods within the product range of Würth Elektronik eiSos GmbH & Co. KG contain statements regarding general suitability for certain
application areas. These statements about suitability are based on our knowledge and experience of typical requirements concerning the
areas, serve as general guidance and cannot be estimated as binding statements about the suitability for a customer application. The
responsibility for the applicability and use in a particular customer design is always solely within the authority of the customer. Due to this
fact it is up to the customer to evaluate, where appropriate to investigate and decide whether the device with the specific product
characteristics described in the product specification is valid and suitable for the respective customer application or not.
2. Customer Responsibility related to Specific, in particular Safety-Relevant Applications
It has to be clearly pointed out that the possibility of a malfunction of electronic components or failure before the end of the usual lifetime
cannot be completely eliminated in the current state of the art, even if the products are operated within the range of the specifications.
In certain customer applications requiring a very high level of safety and especially in customer applications in which the malfunction or
failure of an electronic component could endanger human life or health it must be ensured by most advanced technological aid of suitable
design of the customer application that no injury or damage is caused to third parties in the event of malfunction or failure of an electronic
component. Therefore, customer is cautioned to verify that data sheets are current before placing orders. The current data sheets can be
downloaded at www.we-online.com.
3. Best Care and Attention
Any product-specific notes, cautions and warnings must be strictly observed. Any disregard will result in the loss of warranty.
4. Customer Support for Product Specifications
Some products within the product range may contain substances which are subject to restrictions in certain jurisdictions in order to serve
specific technical requirements. Necessary information is available on request. In this case the field sales engineer or the internal sales
person in charge should be contacted who will be happy to support in this matter.
5. Product R&D
Due to constant product improvement product specifications may change from time to time. As a standard reporting procedure of the
Product Change Notification (PCN) according to the JEDEC-Standard inform about minor and major changes. In case of further queries
regarding the PCN, the field sales engineer or the internal sales person in charge should be contacted. The basic responsibility of the
customer as per Section 1 and 2 remains unaffected.
6. Product Life Cycle
Due to technical progress and economical evaluation we also reserve the right to discontinue production and delivery of products. As a
standard reporting procedure of the Product Termination Notification (PTN) according to the JEDEC-Standard we will inform at an early stage
about inevitable product discontinuance. According to this we cannot guarantee that all products within our product range will always be
available. Therefore it needs to be verified with the field sales engineer or the internal sales person in charge about the current product
availability expectancy before or when the product for application design-in disposal is considered. The approach named above does not
apply in the case of individual agreements deviating from the foregoing for customer-specific products.
7. Property Rights
All the rights for contractual products produced by Würth Elektronik eiSos GmbH & Co. KG on the basis of ideas, development contracts as
well as models or templates that are subject to copyright, patent or commercial protection supplied to the customer will remain with Würth
Elektronik eiSos GmbH & Co. KG. Würth Elektronik eiSos GmbH & Co. KG does not warrant or represent that any license, either expressed or
implied, is granted under any patent right, copyright, mask work right, or other intellectual property right relating to any combination,
application, or process in which Würth Elektronik eiSos GmbH & Co. KG components or services are used.
8. General Terms and Conditions
Unless otherwise agreed in individual contracts, all orders are subject to the current version of the “General Terms and Conditions of Würth
Elektronik eiSos Group”, last version available at www.we-online.com.
Würth Elektronik eiSos GmbH & Co. KG
EMC & Inductive Solutions
Max-Eyth-Str. 1
74638 Waldenburg
Germany
Tel. +49 (0) 79 42 945 - 0
www.we-online.com
eiSos@we-online.com
CREATED CHECKED GENERAL TOLERANCE PROJECTION
METHOD
DaMa SKl DIN ISO 2768-1m
DESCRIPTION
Plastic Caps for USB Connectors
WA-PCCA ORDER CODE
726 144 001
REVISION STATUS DATE BUSINESS UNIT PAGE
001.000 Valid 2016-11-29 eiCan 2/2
This electronic component has been designed and developed for usage in general electronic equipment only. This product is not authorized for use in equipment where a higher safety standard and reliability standard is especially required or where a failure of the product is reasonably expected to cause severe personal injury or death, unless the parties have executed an agreement specifically governing such use. Moreover Würth Elektronik eiSos GmbH
& Co KG products are neither designed nor intended for use in areas such as military, aerospace, aviation, nuclear control, submarine, transportation (automotive control, train control, ship control), transportation signal, disaster prevention, medical, public information network etc.. Würth Elektronik eiSos GmbH & Co KG must be informed about the intent of such usage before the design-in stage. In addition, sufficient reliability evaluation checks for safety
must be performed on every electronic component which is used in electrical circuits that require high safety and reliability functions or performance.