45 ‘35?
mm .m
WURTH ELEK'I'RONIK
Cautions and Warnings:
The following conditions apply to all goods within the product series of WE-LQS of Würth
Elektronik eiSos GmbH & Co. KG:
General:
• This electronic component is designed and manufactured for use in general electronic equipment.
• Würth Elektronik must be asked for written approval (following the PPAP procedure) before incorporating the components into any
equipment in fields such as military, aerospace, aviation, nuclear control, submarine, transportation (automotive control, train control,
ship control), transportation signal, disaster prevention, medical, public information network etc. where higher safety and reliability are
especially required and/or if there is the possibility of direct damage or human injury.
• Electronic components that will be used in safety-critical or high-reliability applications, should be pre-evaluated by the customer.
• The component is designed and manufactured to be used within the datasheet specified values. If the usage and operation conditions
specified in the datasheet are not met, the wire insulation may be damaged or dissolved.
• Do not drop or impact the components, the component may be damaged.
• Würth Elektronik products are qualified according to international standards, which are listed in each product reliability report. Würth
Elektronik does not warrant any customer qualified product characteristics beyond Würth Elektroniks’ specifications, for its validity and
sustainability over time.
• The responsibility for the applicability of the customer specific products and use in a particular customer design is always within the
authority of the customer. All technical specifications for standard products also apply to customer specific products.
Product specific:
Soldering:
• The solder profile must comply with the technical product specifications. All other profiles will void the warranty.
• All other soldering methods are at the customers’ own risk.
• Strong forces which may affect the coplanarity of the components’ electrical connection with the PCB (i.e. pins), can damage the part,
resulting in avoid of the warranty.
Cleaning and Washing:
• Washing agents used during the production to clean the customer application might damage or change the characteristics of the wire
insulation, marking or plating. Washing agents may have a negative effect on the long-term functionality of the product.
• Using a brush during the cleaning process may break the wire due to its small diameter. Therefore, we do not recommend using a brush
during the PCB cleaning process.
Potting:
• If the product is potted in the customer application, the potting material may shrink or expand during and after hardening. Shrinking
could lead to an incomplete seal, allowing contaminants into the core. Expansion could damage the components. We recommend a
manual inspection after potting to avoid these effects.
Storage Conditions:
• A storage of Würth Elektronik products for longer than 12 months is not recommended. Within other effects, the terminals may suffer
degradation, resulting in bad solderability. Therefore, all products shall be used within the period of 12 months based on the day of
shipment.
• Do not expose the components to direct sunlight.
• The storage conditions in the original packaging are defined according to DIN EN 61760-2.
• The storage conditions stated in the original packaging apply to the storage time and not to the transportation time of the components.
Packaging:
• The packaging specifications apply only to purchase orders comprising whole packaging units. If the ordered quantity exceeds or is
lower than the specified packaging unit, packaging in accordance with the packaging specifications cannot be ensured.
Handling:
• Violation of the technical product specifications such as exceeding the nominal rated current will void the warranty.
• Applying currents with audio-frequency signals may result in audible noise due to the magnetostrictive material properties.
• The temperature rise of the component must be taken into consideration. The operating temperature is comprised of ambient
temperature and temperature rise of the component.The operating temperature of the component shall not exceed the maximum
temperature specified.
These cautions and warnings comply with the state of the scientific and technical knowledge and are believed to be accurate and reliable.
However, no responsibility is assumed for inaccuracies or incompleteness.
Würth Elektronik eiSos GmbH & Co. KG
EMC & Inductive Solutions
Max-Eyth-Str. 1
74638 Waldenburg
Germany
Tel. +49 (0) 79 42 945 - 0
www.we-online.com
eiSos@we-online.com
CHECKED REVISION DATE (YYYY-MM-DD) GENERAL TOLERANCE PROJECTION
METHOD
ChriB 001.006 2019-11-26 DIN ISO 2768-1m
DESCRIPTION
WE-LQS SMT Semi-Shielded
Power Inductor ORDER CODE
74404042101
SIZE/TYPE BUSINESS UNIT STATUS PAGE
4018 eiSos Valid 5/6
This electronic component has been designed and developed for usage in general electronic equipment only. This product is not authorized for use in equipment where a higher safety standard and reliability standard is especially required or where a failure of the product is reasonably expected to cause severe personal injury or death, unless the parties have executed an agreement specifically governing such use. Moreover Würth Elektronik eiSos GmbH
& Co KG products are neither designed nor intended for use in areas such as military, aerospace, aviation, nuclear control, submarine, transportation (automotive control, train control, ship control), transportation signal, disaster prevention, medical, public information network etc.. Würth Elektronik eiSos GmbH & Co KG must be informed about the intent of such usage before the design-in stage. In addition, sufficient reliability evaluation checks for safety
must be performed on every electronic component which is used in electrical circuits that require high safety and reliability functions or performance.