SA-9 Owners Manual Datasheet by Jonard Tools

@ JONARDTDDLSE on \ Fax 914 793 A527 \ Jonard com JONARDTDOLSQ @ %W@ €94
SA-9-115 SA-9-E-115
P/N 15183 REV .G
INSTRUCTIONS:
How to change filter
Location and mounting
Maintenance
CAUTIONS
1 Carefully lift out the filter keeping disruption to a minimum.
2 Insert used filter into a plastic bag or box and dispose of properly.
3 Slide new filter into the top of the unit until the fan is fully covered.
1 Mount unit on a stable work surface equipped with an ac power
supply.
2 Locate unit 6” to 8” (152 to 203mm) from work area.
1 Unplug unit.
2 Remove filter from unit carefully.
3 Using a small brush clean fan and housing, being careful not to breath
in the dust.
4 Make sure that the fan blades spin freely.
This equipment is for industrial/laboratory use.
Indoor use only.
Altitude up to 6561 FT (2000 meters).
Maximum RH of 80% up to 88°F (31°C) decreasing 50% RH at 104°F (40°C).
Pollution degree 2 in accordance with IEC644.
Installation category II.
Temperature range 41°F (5°C) to 104°F (40°C)
The user must be aware that if the equipment is used in a manner not
specified by the mounfacturer, safety may be impaired.
If the supply cord is damaged, or servicing is required, this work must be
carried out by the manufacturer or its service agent or a similarly qualified
person in order to avoid a hazard.