Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Concerto System Agenda Slide 3

Shown here is a high level view of the clocking, power and resets on the F28M35x device. This presentation will begin by looking at the clock input source, the system PLL configuration, and the configuration of the clock to the Master, Control and Analog subsystems in more detail. One thing to notice is that the USB and the CAN modules have special clocking options. Next the Missing Clock detection, the Digital Voltage Regulator and the Analog Voltage Regulator will be reviewed. Finally, this presentation will explain the different types of resets on a Concerto device such as the Analog Reset, Device System Reset and the Control System Reset.

PTM Published on: 2012-07-31