Intel® has engaged with several partners to bring the full video surveillance solution to market. The premier partner offering all of the sensor processing IP is Apical (acquired by Arm®). There are also three partners offering highly-optimized H.264 encoders for the FPGA; Ocean Logic, and Jointwave. Additionally, Intel® partners with Sensity, which provides a high-performance analytics engine for the FPGA that operates at full 1080p30 frame rates. Finally, there are the partners that provide graphics rendering cores (for on-screen display), storage interface cores (for local camera storage) and standard interface IP cores (e.g. USB, etc.).