Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
MSP430FR5969 LaunchPad Part 4 Slide 7

Next the debug perspective. CCStudio's integrated debugger has several capabilities to simplify development. Options related to actively debugging code such as run, halt, step over and step into are provided in the top left corner of the CCS window shown here. Select a number of options from the Window tab using the Show View option such as watch variables, memory browser, registers and console. Stepping through the code and analyzing the various input / output expressions is made easy using the debug view.

PTM Published on: 2014-06-24