To create a new project select file new and CCS project. Enter the name of the project and select the project location. At this time, select the target MSP430 configuration, the designer will be working with the MSP430FR5969 device. Also use the connection option to specify the debug. To create a new project select file new and CCS project. Enter the name of the project and select the project location. At this time, select the target MSP430 configuration, the designer will be working with the MSP430FR5969 device. Also use the connection option to specify the debug.