Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
MSP430FR5969 LaunchPad Part 4 Slide 19

When double clicking on the project folder in the project navigator window, one can see that all of the DriverLib files are included in the DriverLib folder. The project is also prepopulated with a main .c file that includes the necessary header files. Change the project properties to select the FR5969 device and the project is now enabled with DriverLib.

PTM Published on: 2014-06-24