Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Product List
This slide highlights ST’s low profile packages, including the classic PowerFLAT 5x6 and the dual island 5x6. The term dual indicates that there are two islands, allowing two identical dies inside. It also shows the asymmetric dual island 5x6, which can be used for example in DC/DC buck configurations where it does not require the low RDS(on) in one of the two MOSFETs. Also shown on this slide are smaller packages such as the PowerFLAT 3.3x3.3 and 2x2.
PTM Published on: 2015-03-24