Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Slide 28
Slide 29
Slide 30
Slide 31
Slide 32
Slide 33
Slide 34
Slide 35
Slide 36
Slide 37
Slide 38
Slide 39
Slide 40
Slide 41
Slide 42
Slide 43
Slide 44
Slide 45
Slide 46
Slide 47
Slide 48
Slide 49
Slide 50
Slide 51
Slide 52
Slide 53
Slide 54
Slide 55
Slide 56
Slide 57
Slide 58
Product List
The LPC1700 is pin-to-pin compatible with the popular ARM7-based NXP LPC2300 series, which allows for a smooth migration for ARM7 customers to move on to Cortex-M3. The NXP implementation of Cortex-M3 has the following key implementations: an MPU (Memory Protection Unit), which can be a great complement for an RTOS based application; a NVIC (Nested Vectored Interrupt Controller) that offers defined interrupt latency; and a WIC (Wakeup Interrupt controller) that allows fast wakeup from power down modes. The Flash Accelerator in the NXP Cortex-M3 allows the devices to execute out of Flash with zero-wait states. The LPC1700 also has excellent DMA support that fully enables the high end serial interfaces like USB, Ethernet and CAN. With 15 serial interfaces, this device is tailored for communication. The LPC1700 is more power efficient in active mode and it would consume less than 1uA in Deep Power down mode. Also, the LPC1700 is currently the industry’s fastest running Cortex-M3 processor at 100MHz.
PTM Published on: 2011-11-02