Wireless Fidelity, or Wi-Fi, is a global wireless protocol. It has had many improvements and iterations over the years. As Wi-Fi 6 and 6E are being rolled out to the public on a global scale, there are some unique issues with interference from existing wireless protocols and other technologies that make each geographic location a custom rollout. Because of the technologies already in place, one needs to make sure that whatever is added to the wireless congestion does not interfere with existing technologies and that the existing technologies do not interfere with the wireless network. ECS has developed ten different filters that are used in pairs to meet the challenges in each geographical area. These filters are covering the full band from 5,925MHz to 7,125MHz. The illustration here shows where each has been adopted. The customer can see that North America and some areas of South America and Saudi Arabia have adopted the slightly narrower band of 5,925MHz to 7,125MHz, while Europe and Australia have adopted the 5,925MHz to 6,425MHz. The ECS dielectric ceramic filters give the customer the flexibility to deploy the Wi-Fi 6 and 6E globally.