Digi-Key Corporation Announces Expansion of CUI Medical Power Supply Offering
THIEF RIVER FALLS, Minnesota, USA - 2012 年 02 月 08 日
Electronic components distributor Digi-Key Corporation, recognized by design engineers as having the industry's largest selection of electronic components available for immediate shipment, today announced the addition of 20 W, 40 W, and 60 W open frame medical power supplies from CUI, further expanding its high density, high efficiency VMS series product portfolio.
The series is designed to be used in a wide variety of medical and dental applications, carrying UL/cUL and TUV 60601-1 safety certifications and EN55011 class B EMI compliance. Featuring no-load power draw of less than 0.5 W and efficiency up to 90 percent, the series is designed for applications seeking to reduce stand-by and overall power consumption.
These high efficiency power supplies offer universal input (90-264 VAC) and are available in seven output voltage models ranging from 3.3 to 48 VDC. The series can operate from 0° to 50°C at full load, derating linearly to 50 percent load at 70°C. Features of the VMS series include over-voltage and short circuit protections.
CUI’s VMS series’ new, compact 20 W, 40 W, and 60 W power supplies, along with the entire VMS portfolio, are available for purchase now on Digi-Key's global websites.
About CUI
Headquartered in Tualatin, OR, CUI Inc. is a technology company dedicated to the development, commercialization, and distribution of new, innovative electro-mechanical products. Broad power, motion control, and component product portfolios allow customers to address design challenges across a range of industries and applications. Built on a solid foundation of core operating principals, CUI seeks to maximize value customers through engineering, manufacturing, and supply chain capabilities. As an industry leader, they will continue to invest in the future through new technologies, talented employees, expanded manufacturing capabilities, and a growing global reach.
About Digi-Key Corporation
Digi-Key Corporation, based in Thief River Falls, Minn., is a global, full-service provider of both prototype/design and production quantities of electronic components, offering more than three million products from over 650 quality name-brand manufacturers. With over one million products in stock and an impressive selection of online resources, Digi-Key is committed to stocking the broadest range of electronic components in the industry and providing the best service possible to its customers. Additional information and access to Digi-Key's broad product offering is available on the Digi-Key website.
- Editorial Contact
- Laura Stengrim
- DigiKey
- (218) 681-8000 ext. 14489
- laura.stengrim@digikey.com