Maker.io main logo

Beginner's Guide to KiCad

1,756

2017-12-19 | By SparkFun Electronics

License: See Original Project

Courtesy of SparkFun

Introduction

If you're like me and you've decided to take the plunge from EAGLE PCB to KiCad it can be really jarring. EAGLE had many quirks and rough edges that I'm sure I cursed when I first learned it back in 2005. Since then EAGLE has become a second language to me and I've forgotten all the hard bits. So, as you migrate to KiCad remember to take breaks and breathe (and say 'Key-CAD' in your head). You'll be dreaming in KiCad in no time!

This tutorial will walk you through a KiCad example project from schematic capture to PCB layout. We'll also touch on library linking, editing, and creation. We'll also export our PCB to gerbers so the board can be fabricated.

While this tutorial is aimed at beginners I am going to use terms such as 'schematic components' and 'polygon pours'. If something doesn't make sense that's ok, just take a moment to do a quick search. If you really get stuck please use the comments section on the right. We always want to improve our tutorials to make them easier.

KiCad Project Window

Download and Install KiCad

Note: This tutorial was written using KiCad 4.0.6 on Windows 10.

Let's get started! Head over to KiCad's download page and download the latest version of the software for your specific platform:

DOWNLOAD KICAD FOR YOUR OPERATING SYSTEM/DISTRIBUTION

Run KiCad

Once installed, run KiCad. The main navigation window will display where you will be able to open all the periphery programs like schematic capture and PCB layout.

Click the image for a closer look

The KiCad project window looks quite empty and sad. Let's open an example!

Setting Up a Project

The ZOPT2201 UV sensor designed originally in SparkX is a great I2C UV Index sensor and will serve as our starting example for this tutorial. Download the ZOPT220x UV Sensor Breakout designs for KiCad and unzip the four files into a local directory:

ZOPT220X UV SENSOR BREAKOUT KICAD BOARD FILES

Note: I operate extensively out of a ...\Dropbox/Projects folder so you'll see that file structure in many of the images. This setup allows my laptop and work computer to sync without hassle.

Once the four files are located in a local directory (try looking in your downloads folder for …\ZOPT220x_UV_Sensor_Breakout-Tutorial), click File -> Open Project and open the ZOPT220x UV Sensor Breakout.pro file.

open the ZOPT220x UV Sensor Breakout.pro file.

What are all these files?

  • *.pro - Main project file to keep track of the file structure.

  • *.cmp - Defines which footprints go with which schematic components.

  • *.kicad_pcb - The PCB layout.

  • *.sch - The schematic.

These four files are all you need to share a KiCad design with a fellow collaborator. You may also need to share a footprint file, which will be explained more later-on in this tutorial.

You may have had your first critical-judgment-eye-squint. Why is there a file to define which footprints go with which schematic components? This is fundamental to KiCad and is very different from how EAGLE works. It's not a bad thing, just different.

Setting Up Schematic Component Libraries

Double click on the schematic file with Kicad's Eeschema schematic editor. You'll probably get an error:

Double click on schematic file with Kicad’s Eeschema

Ignore this for now. Click 'Close'.

Click ‘Close’.

The schematic will load with lots of components with question marks (i.e.??). KiCad is missing the link to the devices within this schematic. Let's get them linked!

Linking Component Libraries w/ Eeschema

From within EeSchema, click on Preferences -> Component Libraries. This will open a new window. In the image below you can see that the project file contains information about where it should look for "Component library files". Each project has its own connections to different file structures. We need to tell this project where to find the symbols for this schematic.

file contains info about “Component library files”

We will need the SparkFun_SchematicComponents.lib file. Download and store it in a local directory:

DOWNLOAD "SPARKFUN_SCHEMATICCOMPONENTS.LIB"

From the KiCad window, click the top 'Add' button. We'll show you how to create your own schematic symbols in a bit.

click the top ‘Add’ button

Navigate to the directory where you stored the SparkFun_SchematicComponents.lib file and click 'Open'. This file contains all the schematic components.

Once you've added the SparkFun schematic components library file, you should see it added to the list.

you should see it added to the list

The astute will note the slightly different directory structure in the window:

Copy Code
C:\Users\Nathan\...

and

Copy Code
C:\Users\nathan.seidle\...

That's the difference between my home PC and my work PC. To avoid future errors when opening this schematic, let's remove the entry from the active library files. Highlight the C:\Users\Nathan... entry from the list and click on the 'Remove' button.

Click on 'OK' to close out the Component Libraries manager. Now close and re-open the schematic to refresh.

close and re-open the schematic to refresh

Congrats! No more ?? boxes. For more information about using schematic component libraries across multiple computers, check the next subsection about the "user-defined search path." Otherwise, let's start editing the schematic!

User Defined Search Path: Using Component Libraries on Multiple Computers

The schematic component libraries are assigned using KiCad's Component Library Manager. If you're like me and have schematic libraries shared across multiple computers, adding a "User defined search path" is helpful:

adding a “User defined search path” is helpful

In the image, I have "..\..\SparkFun-KiCad-Libraries" defined. This is the local relative path to a Dropbox folder. These component library paths are specific to this project and *.pro file. When I open this project on my laptop, it will first look for the files in the "C:\Users\nathan.seidle..." location. It will fail and then search the relative path of "..\SparkFun-KiCad-Libraries" and find the files. It allows me to share libs between computers and between GitHub repos without having to reassign the libraries every time I open the project on a different computer.

For now, you should continue with the tutorial. In the future, you may want to revisit this if you use KiCad across multiple computers.

Editing a Schematic

If I get you to do nothing else, I will get you to learn the keyboard shortcuts! Yes, you can click on the equivalent buttons. However, the speed and efficiency of KiCad really shines when muscle memory kicks in so start memorizing. Here are the keyboard shortcuts in KiCad's Eeschema that we will be using frequently in this tutorial:

  • a - To add component.

  • c - Copy a component when the cursor is over another component.

  • w - To wire components.

  • v - Edit component value.

  • Esc - Escape mode or whatever command in progress and return to normal pointer mode.

  • ctrl+z - Undo. Use liberally to undo any mistakes.

  • ctrl+s - To save. Make sure to save often!

Note: To view or edit the list of all the hotkeys, go to Preferences -> Hotkeys.

This breakout board needs a larger 4.7uF decoupling cap (because I say so). Let's add it!

Adding Component to Schematic

Press 'a' to add a device to the schematic then click on the schematic:

Press ‘a’ to add a device to schematic

There are hundreds of components (668 items according to the title bar). Feel free to dig around but to quickly find what we need type 'cap' into the field Filter:. Select the device labeled as C_Small from the device library. Then hit enter or click 'OK'.

Select device labeled as C_Small from device library

Place it on the schematic next to the 0.1uF cap.

Place it on the schematic next to the 0.1uF cap

After you place the capacitor, you'll notice you're still in placement mode. Hit the 'Esc' button on your keyboard to return to normal pointer mode. I find myself hitting escape twice a lot just to be sure I'm back in the default state.

Copying Component

Once in default state put your mouse pointer on top of the 3.3V marker on the 0.1uF cap. Press 'c' to copy that device and place it above the new capacitor.

Press ‘c’ to copy that device/place it above new cap

Do the same for the ground marker. Press 'ctrl+s' to save your work.

Wiring Components

Now let's wire them together. You guessed it, press 'w' but here's the catch: have your mouse pointer over one of the bubbles before you press 'w'.

press ‘w’: have your pointer over one of the bubbles

Move your mouse to the other bubble and left click on the mouse to complete the wiring for GND. Remember if you mess up, press 'Esc' once or twice to return to default. Then move your mouse pointer to the bubble you want to connect and press 'w' and begin wiring 3.3V. The shortcut 'w' stands for wire.

Did something go wrong? Use 'ctrl+z' liberally to undo any mistakes.

Use

Power and ground are now connected to our capacitor.

Changing a Component Value

Let's change the value from C_Small to 4.7uF. Hover the mouse pointer over C_Small and press 'v' (for value change). Change C_Small in the Text field by typing 4.7uF. Then hit enter or click 'OK'.

Change C_Small in the Text field by typing 4.7uF

Congrats! You've just wired up your first schematic component. Press ctrl+s to save your work.

Annotate Schematic Components

But what about the C? designator?! Don't worry about it! One of the many benefits of KiCad is the ability to auto-annotate a schematic.

KiCad has ability to auto-annotate a schematic

Click on the Annotate schematic components button.

Click on the Annotate schematic components button

Use the default settings and simply click on Annotate button to confirm. KiCad will ask you if you're sure, simply press return or click 'OK' again.

Use default settings and click on Annotate button

A capacitor with correct value and designator! We are all set. Time to edit the PCB.

Editing a PCB Layout

Before we start editing the PCB, here are the keyboard shortcuts in KiCad's Pcbnew that we will be using frequently in this tutorial:

  • + - Press to switch next layer.

  • - - Press to switch to the previous layer.

  • m - Move item.

  • b - Update ground polygon pours.

  • Delete - Remove a trace or component.

  • x - Route new track.

  • v - Add through via.

  • n - Next grid size. Use with caution. There will be tears if you use a grid outside of 50mils or 25 mils.

  • Page Up - Return to the top copper layer.

  • Esc - Escape mode or whatever command in progress and return to normal pointer mode.

  • ctrl+z - Undo. Use liberally to undo any mistakes.

  • ctrl+s - To save. Make sure to save often!

Note: To view or edit the list of all the hotkeys, go to Preferences -> Hotkeys.

Generate Netlist

We've got our schematic, now let's get the new 4.7uF cap placed on the board. From the schematic, click on the 'Generate netlist' button.

From schematic, click on ‘Generate netlist’ button

You'll see the following window:

You

KiCad is powerful. And with this power, comes an overwhelming number of options. Lucky for us, we are just scraping the surface so we don't need to fiddle with any of these options. Simply press enter or click 'Generate' to confirm this screen. KiCad will ask you where you want to save the netlist as a *.net file with the default location being the project folder. Again, press enter or click 'Save' to confirm.

Configuring Layer Colors

Return to the main project window and double-click the *.kicad_pcb file.

double-click the *.kicad_pcb file

Welcome to PCB editing. Of all the differences between EAGLE and KiCad, it was the look within PCB layout that threw me off the most. Under the View menu you will find three other views: Default, OpenGL, and Cairo. I prefer OpenGL. Let's switch Canvas to OpenGL for now.

Your mouse wheel does what you expect: Zoom In/Out and Pan by Clicking.

I don't like the layer colors! Yeah, me either. To change the layer colors, on the right side menu use your mouse wheel to click on the green square next to B.Cu (bottom copper layer). I prefer the following layer colors:

  • Red 2 (Default) for F.Cu (Top Copper)

  • Blue 4 for B.Cu (Bottom Copper)

  • White for F.SilkS (Front Silk Screen)

  • Yellow 3 for B.SilkS (Bottom Silk Screen)

  • Gray 3 for Edge.Cuts (a.k.a board outline or dimensional layer in EAGLE)

  • Gray 2 (Default) for F.CrtYd (Denotes the total board space required on the top layer for the component)

I don

Pressing '+' and '-' will switch between top and bottom copper layers. This is useful when you need to view a certain layer.

This is useful when you need to view a certain layer

It's all cosmetic but these layer colors make it easier for me to see what's going on.

Be sure to poke around the Render tab (next to the Layer tab), namely the Values and References check boxes.

poke around the Render tab (next to the Layer tab)

I find the Values and References extremely distracting when turned on so I leave them OFF. Many designers live and die by these values, so use as needed.

Adding a Footprint

Aren't we here to add a 4.7uF cap to the board? Where is it? It's nowhere, sorry.

What's going on? We failed to assign a footprint to the capacitor we added in the schematic. Remember, KiCad does not link schematic components to footprints the same way EAGLE does. We have to specifically connect a footprint to each schematic component that was added.

Navigate back to schematic and click on the 'Run CvPcb' button to associate components and footprints:

Navigate to schematic and click on ‘Run CvPcb’ button

If this is the first time you've run CvPcb you'll get this warning:

the first time you run CvPcb you’ll get this warning

Simply click through it.

Simply click through it

Depending on how many libraries you have installed, this may take up to 30 seconds. We will make this better later in the tutorial but for now, be patient.

In the left column is all the footprint libraries that KiCad ships with. In the middle is the list of components in your schematic. On the right is any footprint that may work with the highlighted component in the middle. Your job is to double-click on the footprint on the right that goes with the component in the middle.

To make life easier click on the 'View selected footprint' button.

click on the ‘View selected footprint’ button

Now you can preview the footprint as you click down the list in the right.

preview footprint as you click down list in the right

In Windows, I press and hold the Windows button and press the left arrow and release. This will lock the CvPcb window on one side. Then select and lock the Footprint Preview Window to the right. This allows us to flip through footprints in the left window while seeing the preview on the right.

Highlight C2 in the middle column. Then double-click the Capacitors_SMD:C_0603 in the right column. C2 should now be assigned a footprint.

double-click Capacitors_SMD:C_0603 in right column

Re-Generate Netlist

Close the CvPcb window and click 'Save and Exit'. We need to re-export the Netlist. Remember how to do that? Click the 'Generate netlist' button again, press enter twice. Open to the PCB editor either from the schematic or from the project window.

Click ‘Generate netlist’ button, press enter twice

Hey! It's still missing! We changed things, so we need to import the netlist! Remember how? Click on the 'Read netlist' button and you should see this window:

Click ‘Read netlist’ button and you should see this

Click 'Read Current Netlist' and 'YES' to confirm. You can also hit enter twice. You should see the new capacitor near the board.

You should see the new capacitor near the board

This is a decoupling cap so let's put it next to the 0.1uF cap that is already there. Start by hovering over the new cap and press 'm' for move.

Start by hovering over new cap and press

Left click to place the capacitor. Now press 'm' over the 0.1uF cap in the way by moving it to the left.

Now press

Press 'b' to update the GND polygon pours.

Press ‘b’ to update the GND polygon pours.

We've got some traces to fix but this isn't too bad. Hover over the bits of traces that you want to remove and press 'Delete'. Let's delete the trace and via that is under the capacitor's +3v3 terminal. If your pointer is over multiple items (as shown in the image below with the cursor over both the trace and capacitor), KiCad will pop up a menu to clarify your selection. This is basically asking you to pick which one you want to operate on.

cursor over both the trace and capacitor

If you ever run into a problem press 'Esc' to return to default pointer mode. If you ever delete something wrong press 'ctrl+z'.

If a problem occurs press ‘Esc’ to return to pointer

Once you've removed most of the offending traces, you can begin routing by pressing 'x'.

Why doesn't the 0603 footprint I added match the one on the board? SparkFun has tweaked its PCB footprints over many years to fit our manufacturing processes. This includes pick and place and automated optical inspection. There's nothing magical about it; we've found our slightly larger 0603 footprint works best for our setup. We use a mixture of footprints that ship with KiCad and our own set of footprints. For the purposes of this tutorial, don't fret about it. This footprint will work just fine.

Single click on the pad that has the gray air-wire and drag it to the pad that it needs to connect to. Single click again to lock the wire in place. Press 'b' to update the polygons.

Press ‘b’ to update the polygons

In the image below, KiCad is trying to route this trace in an odd way. If we place the trace here it will create an acute angle which is generally bad (read up on "acid traps"). We want the trace to be a T intersection. We need to change the grid.

Well that

Well that's annoying!

Press 'n' to go to the next grid size. I needed to hit 'n' only once to go to the 0.25mil grid to get this nice intersection, you may need to get to a finer grid. You can also find this in the menu options under "Grid: 0.0635mm (2.5mils)."

I highly recommend you do not use a grid other than 50 mils or 25 mils. Otherwise, there will be tears later. All your components, vias, traces and board outlines must be on a 50 or 25 mil grid. (Silkscreen is a different story)

Nice T intersection!

Nice T intersection!

In the image below, I am routing the GND air wires. This is not really needed because the polygon pour connects the two pads but it does illustrate how good the 'magnetic' routing assistance is in KiCad. It's very quick and easy to go from pad to pad.

I am routing the GND air wires

We have two air-wires left. To get these we'll need to place vias down to the bottom layer. Start by pressing 'x' and clicking on the start of the capacitor's air wire for GND again.

We have two air-wires left

Bring the trace out.

Bring the trace out.

When you've reached open ground press 'v' to create a via. Single click to place the via and KiCad will automatically start routing on the bottom layer. Press 'Esc' to stop laying down traces; the polygon pour will take it from here. Pressing 'Page Up' will take you back to the top layer.

One air wire left!

One air wire left!

To get this last air wire, you can try clicking on the GND pad of the 0.1uF cap but annoyingly KiCad won't start routing?! Why?! It's actually a good thing: the SDA trace is too close (overlapping actually) to the GND pad on the 0.1uF cap. By not letting you start routing KiCad is saying that trying to put a trace here would violate the DRC rules. What to do? Rip up the SCL and SDA lines to make some room.

Rip up the SCL and SDA lines to make some room

Aha! Much better. Press 'x', click on the capacitor's GND terminal, bring the trace out, and press 'v' to drop a via in this area. Hit escape to stop routing (let the polygon take care of it). Finally, press 'Page Up' to return to the top layer view.

Finally, press ‘Page Up’ to return to top layer view

Use the 'Delete' and 'x' buttons to re-route the SDA and SCL lines to finish up this board. Then press 'b' to update the polygons. The board should look similar to the image below.

Routed with no air wires!

Routed with no air wires!

Congrats! We have finished routing the footprints. Now let's run the DRC to see if we're legal.

How to Remove a Component's Footprint from a PCB Layout

Before we continue let's go over the process for modifying or removing a component from a PCB layout. For example, let's say that you wanted to remove an extra capacitor or resistor from a design. You would do all the regular steps:

  1. Delete device from the schematic.

  2. Export the netlist by clicking the generate netlist button.

  3. Import the netlist into PCB Layout by clicking on the read netlist button.

The difference is a few import settings:

The difference is a few import settings

During the netlist import, the default settings are to 'Keep' exchange footprint and to 'Keep' extra footprints.

Here, we need to change two things:

  • Exchange Footprint -> Change: This will allow footprints to change

  • Extra Footprints -> Delete: This will remove any extra footprints that remain

You may also want to 'Delete' unconnected tracks to clean up any left over tracks from the component you removed.

Running Design Rule Check

Click on the ladybug with the green check mark on it to open the Design Rule Check (DRC) window.

open the Design Rule Check (DRC) window

Note: All the DRC settings are in millimeters. If you'd prefer to see the settings in inches, close this window. On the left tool menu of the PCB layout window, click on the 'in' button. This will change all the units to inches. Re-open the DRC window and you can now change the settings using imperial units.

Let's take a moment to talk trace width, trace spacing, and vias. In general, SparkFun designs boards with:

  • 10mil trace width

  • 10mil trace spacing

  • 20mil vias

We go smaller than this on many designs but if you're designing your first PCB, do not design it with 4mil traces and 8mil vias. You shouldn't need to go that small on your first board.

Why design in 10mil trace/space when a fab house allows 8mil or smaller for the same price?

Making PCBs is tricky and for each increment of tolerance, you remove you increase the chances that the PCB (proto or not) will be fabricated with an error. And those errors can be hard to identify. We design with 10mil trace/space in order to insure and reduce the probability that we'll see PCBs with errors on the production floor. There's nothing worse than troubleshooting a faulty product and asking yourself: "I've tried every rework and soldering trick in the book, is it the PCB that's bad?"

That stated, we are seeing many PCB fab houses charge low prices for 7mil trace/space and 12mil vias. If you've got a complex board with tight layout challenges, it's better to use the smaller trace/space and vias. Save yourself the layout time and rely on the PCB fab house to correctly fabricate your board.

We generally use the KiCad defaults of:

  • Clearance: By Netclass

  • Min Track Width: 0.2mm = 0.0079mil

  • Min Via Size: 0.4mm = 0.0157mil

Press enter again to run the DRC with the default settings.

ErrType(): Via near track

Aw shucks! What's wrong with my board? The vias marked with red arrows are too close to the traces nearby. The error message will show up in the window as an error indicating: "Via near track." Fix them by ripping up (press 'Delete') any traces near the vias and re-route them (press 'x').

Fix by ripping up any traces near vias and re-routing

After adjusting the traces causing the issues, re-run the DRC. These three flags should disappear.

DRC markers have been cleared

DRC markers have been cleared

Congrats! You've fixed those "Via near track" issues.

ErrType(): Pad near pad

But wait, we are not done yet! There are still two DRC error arrows left with the error indicating: "Pad near pad". KiCad is trying to tell us the pads on this solder jumper are too close together. SparkFun has used this footprint for years and is comfortable with the design so let's change the Netclass clearance constraint.

let

Open the DRC rules from the Design Rules menu.

Open the DRC rules from the Design Rules menu

Here is where you can create specific rules for specific traces and classes of traces. The problem that we are running into is the Default Clearance is 0.079mil (0.2mm). If we decrease this to 7mil (0.01778mm), click 'OK', and re-run the DRC…

click ‘OK’, and re-run the DRC…

DRC errors resolved! Now reducing the DRC clearances in order to get your board to pass DRC is not an ideal solution. We want the pads on the solder jumper to be close enough to be easily jumpered with solder so increasing the distance between the pads on the footprint would be counterproductive. In general, you should set your DRC rules and stick to them.

you should set your DRC rules and stick to them

Watch Your Airwires!

One last note about DRC: Leaving airwires on your PCB is a sure fire way to generate coasters (bad, unusable PCBs).

Leaving airwires on your PCB can generate coasters

From the DRC window, there is a 'List Unconnected' button. This will show you the location of any unconnected traces (I had to rip up the SDA trace on the bottom right side of the PCB to show this error). It's very important that you check for airwires before ordering your PCBs. As you progress through your layout, I recommend focusing on the 'Unconnected' count at the bottom of the screen (circled in pink). If you think you are done routing a board but still show a few unconnected wires that you can't find, the DRC window will help you locate them.

Press 'ctrl+s' to save your work.

Well done. You've made it through design rule checking! Now it's time to order boards.

Exporting Gerbers

We added a component to the schematic, we modified the PCB layout, and we checked for errors. Now we are confident and ready to have our boards made! Time to export the gerber files.

Generate Drill and Gerber Files

Gerber files are the 'artwork' or the layers that the PCB fabrication house will use to construct the board. We've got a great tutorial on the different layers of a PCB so be sure to read up if all this is new to you.

Click on the 'Plot' button next to the printer icon in the top bar to open the 'Plot' window.

Click on ‘Plot’ button next to printer icon

In general, there are 8x layers you need to have a PCB fabricated:

  • Top Copper (F.Cu)+ Soldermask (F.Mask) + Silkscreen (F.SilkS)

  • Bottom Copper (B.Cu) + Soldermask (B.Mask) + Silkscreen (B.SilkS)

  • Board outline (Edge.Cuts)

  • Drill file

In the Plot window with the Plot format set for Gerber, be sure these Layers are checked:

  • ☑ F.Cu

  • ☑ B.Cu

  • ☑ B.SilkS

  • ☑ F.SilkS

  • ☑ B.Mask

  • ☑ F.Mask

  • ☑ Edge.Cuts

Additionally, click on 'Generate Drill File' button. You can use the defaults here as well. More on the PTH vs. NPTH check box in a minute. For now, just click 'Drill File' or press enter to generate the drill file.

click ‘Drill File’/press enter to generate drill file

Click on 'Close' in the 'Drill Files Generation' window.

Click 'Plot' to generate the gerber files for the layers and then click 'Close'.

Time to Review Your Gerbers

This is the last chance to catch any errors before paying real money. Reviewing the gerber layers often shows you potential errors or problems before you send them off to fab.

Reviewing gerber layers shows errors/problems

Return to the main KiCad project window and open up GerbView by clicking on the button.

Note: There are many gerber viewers available. I enjoy using Gerbv but the built-in viewer to KiCad works well so that's the one we will discuss.

Once KiCad's GerbView is open, click on File -> Load Gerber File. Select all the files shown and click Open.

click on File -> Load Gerber File

Next, click File -> Load EXCELLON Drill File. Load your drill files by selecting the all the drill files shown and click 'Open'. They should be in the same directory.

click File -> Load EXCELLON Drill File

The layout looks very different but this is a good thing. You've been staring at your design for hours and it's hard for your brain to see issues. I generally do not change the layer colors unless I have to. I want the gerber review to be jarring and different from my layout practices so that I'm more likely to catch issues.

From this view, turn off all the layers but the Top Copper (layer 5). Additionally, from the Render menu, turn off the Grid and DCodes. This will make the review less cluttered.

This will make the review less cluttered

Now step through the different layers by toggling them on and off. You're looking for irregularities and things that look out of place. Here are some things I look for:

  • Do any traces have weird routing that could be improved?

  • Do the vias line up with the top copper where they should?

  • Does the top solder mask make sense with the SMD IC's footprint?

  • Are the via's covered in solder mask (also called 'tented vias') or are they exposed?

  • Does the top silkscreen look good? Make sense? Everything aligned the way I want it? Are pin 1 indicators clear?

looking for irregularities

Now turn everything off and repeat for the bottom layers.

Did you catch it? There are a handful of things wrong with this example.

  1. The bottom silkscreen is missing the GND indicator.

  2. The top GND silkscreen indicator is in italics.

  3. There are two drill files for some reason.

Leaving a silkscreen indicator off won't break your board but it's small defects like this that the gerber review is meant to catch.

Whoops! Bottom silkscreen for GND is missing!

Whoops! Bottom silkscreen for GND is missing!

Homework:

Take a moment and return to the PCB layout window to edit the make these corrections.

  • Add a silkscreen to the bottom layer for GND. To do this, select the bottom silk layer (B.SilkS) in Pcbnew. Click on Place -> Text, type "GND" in the Text: field, and click 'OK'. You can also copy text on the bottom silkscreen layer by right-clicking it, selecting Duplicate, and placing text next to the GND pad. Make sure to change text to GND by right-clicking the text, selecting Properties, changing the text, and clicking 'OK'.

  • Change the top GND indicator so it's not italics. To do this, edit the text properties and change the Style: to Normal.

  • Plot new gerber files.

  • Review your work in GerbView to verify the fixes.

Now, we need to deal with the two drill files.

PTH vs NPTH

When generating the drill file for this design two files where generated:

  • *.drl - The standard EXCELLON drill file you need to send to PCB fab house.

  • *-NPTH.drl - The non-plated through hole drill file.

Non-plated through holes are holes on your PCB that do not have copper covering the vertical walls of the hole. This is sometimes required for advanced designs where thorough electrical isolation is needed. However, it is rare. While plated through holes (PTH) are common and cheap, NPTH requires an extra step in the PCB fabrication process and will often cost extra.

We don't need NPTH for this design, so what happened? The 'STAND-OFF' footprint (i.e. used for the drill holes top of the board for mounting holes) was imported from the SparkFun Eagle library and KiCad seems to think it is a non-plated hole for some reason.

To correct this go back to the PCB layout, click on the Plotter, click 'Generate Drill File' and select the box that says 'Merge PTH and NPTH holes into one file'. In a later section, we'll go over how to edit the 'STAND-OFF' footprint to use a regular PTH hole.

Solder Paste Stencils

Are you doing SMD reflow? Need to order a stencil to apply the solder paste to your board? Turn on F.Paste in the Plot window to generate the top paste layer.

This *.gtp file is sent to a stencil fabricator to create the stainless steel or mylar solder paste stencil. If you're unfamiliar with stenciling solder paste we have a fabulous tutorial.

We use OSHStencils for our proto stencils. The top paste layer is not needed to fabricate a PCB.

Order Your Board!

If you're happy with your layout, let's order some PCBs! Every fab house understands and works with gerber files, so navigate to the directory on your computer where your KiCad project resides.

let’s order some PCBs

Select and zip the following 8x files:

  • *.drl - Drill file

  • *.gbl - Gerber Bottom Layer

  • *.gbs - Gerber Bottom Soldermask

  • *.gbo - Gerber Bottom Silkscreen (Overlay)

  • *.Edge.Cuts.gm1 - Board Outline (Gerber Mechanical 1)

  • *.gtl - Gerber Top Layer

  • *.gts - Gerber Top Soldermask

  • *.gto - Gerber Top Silkscreen (Overlay)

You could zip all the files in the directory and send them off to your fab house but I don't recommend it. There are a tremendous number of PCB layout software packages generating all sorts of different file names and formats. It's often difficult to tell if *.cmp is a gerber file or something else. Does the customer care about the *.gtp file or is that just extra? It's better to give the fab house only what you want fabricated.

The final step? Order your boards! The gerbers are the universal way to communicate with a PCB vendor. There are hundreds if not thousands of PCB vendors out there. Shop around!

In addition to your gerbers, you'll need to specify via email or the PCB vendor's website various elements of the PCB:

  • What thickness PCB? 1.6mm is standard but 0.8mm is just as rigid and may help with 50 ohm trace impedance matching.

  • What color solder mask? Green is default but red looks awesome.

  • What color silkscreen? White is most common but other colors are available.

  • How many layers? This example is a 2x layer board meaning there is just a top copper and bottom copper. However, some designs need to have 4x, 10x, and even 16x layers to route the board. Additional layers increase the cost significantly.

The Solder mask Looks Big

If you had a look at the solder mask on this PCB and wondered why it looked odd, you're not alone. Let's compare the PCB's solder mask for KiCad (as shown in green) and Eagle (as shown in pink). You should notice two things:

  1. In the KiCad design, I have a pad on the main sensor that looks like it's slightly misplaced. Pad 1 doesn't line up with the other pads. Weird. It's a problem that needs to be fixed, but the error won't kill the board.

  2. More importantly, the solder mask on the Eagle design has gaps between the pins on the connector and the sensor IC. This will help reduce solder bridging between pins. In the KiCad version, the mask apertures look too big.

KiCad Solder mask

KiCad Solder mask

Eagle Solder mask

Eagle Solder mask

In the image below, we can see the SMD Qwiic connector within Eagle. The default solder mask clearance is 0.1mm per side in Eagle.

the SMD Qwiic connector within Eagle

In KiCad's Pcbnew, open the ZOPT220x Breakout and click on Dimensions -> Pads Mask Clearance. KiCad's solder mask clearance has a default of 0.2mm per side. We recommend you change this value to 0.1mm. Most fab houses will use 0.1mm as their default as well. You will then need to re-export your gerbers and load them back into GerbView.

click on Dimensions -> Pads Mask Clearance

Making the clearance smaller than 0.1mm will cause difficulties for the fab house to get the registration correct.

What is registration? It's the alignment of different layers. If the soldermask layer is shifted 2mm away from the copper layer, then the SMD pads you need to solder to will be covered up by soldermask. The fab house has to get these layers aligned with high precision to make a functional board. Reducing the clearance below 0.1mm makes the fab house have less room for error and can lead to delays or increased fabrication costs.

Creating a Custom KiCad Footprint Library

This section will show you how to create your own local custom footprints so that you can use them and connect them to schematic components using CvPcb. We're going to assume you've already been through the previous sections of this tutorial; you should have KiCad downloaded and installed.

Open KiCad's project manager and then click on the PCB footprint editor button.

Open KiCad

You may get the warning. That's ok, just click through it. This is KiCad's way of telling you it's going to create the default table of libraries that link to KiCad's extensive GitHub repos.

Click Preferences -> Footprint Libraries Manager

Click Preferences -> Footprint Libraries Manager. This will open the list of all the footprint libraries now accessible to you.

Click Preferences -> Footprint Libraries Manager

This is a tremendous list of libraries! Click 'OK' to close the manager.

Click ‘OK’ to close the manager

Let's poke around these libraries. Click on 'Load footprint from library' button and then 'Select by Browser'. This is a handy tool for perusing the available footprints.

This is a handy tool for viewing available footprints

Navigate to the LEDs -> LED_CREE-XHP50_12V footprint. Here is an example footprint in LEDs library. Double click on this footprint to open it up in the editor.

Navigate to the LEDs -> LED_CREE-XHP50_12V footprint

Note the title bar of the editor window has changed. The active library is now LEDs and it is read-only. Obviously, KiCad wants to control their libraries; not just anyone can save to their repos. If we want to edit this footprint we need our own local copy.

Note the title bar of the editor window has changed

Let's create a local directory to keep all our local footprints. For this tutorial, please create a local folder called 'C:\KiCadLibs\' (or your platform's equivalent).

Now click on File->Save Footprint in New Library.

Now click on File->Save Footprint in New Library

I recommend using different directory names for different sets of footprints (resistors, connectors, LEDs, etc). Select the 'KiCadLibs' folder that was created and then type '\LEDs'. KiCad will create the new 'LEDs.pretty' directory with a file 'C:\KiCadLibs\LEDs.pretty\LED_CREE-XHP50_12V.kicad_mod'. And we're off to the races. Except, not quite yet.

we

Notice the title bar in the Footprint Editor still states the active library is LEDs and is read-only. We need to switch the active directory to our local folder. I'm going to head you off: File->Set Active Directory doesn't work as it only gives you the list of libraries that KiCad ships with. Oh KiCad!

Before we can set our new footprint directory as active, we need to make KiCad aware of it. Re-open the Preferences -> Footprint Libraries Manager.

Re-open the Preferences -> Footprint Libraries Manager

Click on the 'Append with Wizard' button. You'll be asked to locate the directory you want to add. In this case, we want to add the 'Files on my computer'. Click on the 'Next >' button, select the directory we created (i.e. 'C:\KiCadLibs\LEDs.pretty'. Click on 'Next >' a few times. When prompted 'Where do you wish the new libraries to be added', select 'To Global library configuration (visible to all projects)' and click 'Finish'.

KiCad may throw an error because the 'LEDs' nickname is used twice. I renamed mine to 'LEDs-Custom' then click on 'OK' to close out the Footprint Libraries Manager.

click on ‘OK’ to close out Footprint Libraries Manager

If you inspect the Footprint Editor toolbar again, you'll see the LEDs library is still active and read-only. Now we can click on 'File->Set Active Library'. Here is where KiCad shines - the Filter works well. Type LED and select the LEDs-Custom library.

Type LED and select the LEDs-Custom library

At last! We have an active local library. Now when you click 'Save footprint in local library' or press 'ctrl+s' KiCad will prompt you with a Save Footprint window with Name (annoyingly every time). Press enter and your modifications will be saved.

Warning: KiCad doesn't give you an overwrite warning. So if you already have a footprint called '1206 LED' but create a new footprint and save it as '1206 LED,' KiCad will overwrite the old footprint without a peep.

Now you can explore creating and editing footprints using the Footprint Editor.

After you've created your first footprint or two be sure to read KiCad's KiCad Library Conventions (KLC). It's a well documented system for creating community share-able footprints. Left to our own devices we will all create things a little differently; the KLC tries to get us all on the same page and SparkFun follows it.

In the future, if you're creating a lot of footprints consider using git repo to manage the changes. At SparkFun, we use the following structure:

  • \SparkFun-KiCad-Libraries - A git repo directory containing all KiCad schematic component files (*.lib)

  • \SparkFun-KiCad-Libraries\Footprints - Contains directories of footprints

  • \SparkFun-KiCad-Libraries\Footprints\LEDs.pretty - Directory containing all the LED footprints (*.kicad_mod)

  • \SparkFun-KiCad-Libraries\Footprints\Sensors.pretty - Directory containing all the sensor footprints (*.kicad_mod)

  • etc.

By using a git repo, SparkFun engineers and our users can contribute schematic components and footprints.

Paring Down the KiCad Libraries

When opening CvPcb to assign footprints to the schematic components, it can take a very long time to load. This is because KiCad is pinging all the KiCad GitHub repos and pulling down 93 libraries. To make this faster, we recommend removing the libraries that are either deprecated or libraries that you will never use.

Remove libraries that are deprecated/you won

It's quick and easy to remove a library: select a row in the Footprint Libraries Manager and click the 'Remove Library' button. If something goes wrong, don't panic! Simply click 'Cancel' in the manager window and the library manager will close without saving changes. If things go really wrong, you can always delete the 'fp-lib-table' file and restart KiCad. This will cause it to create the footprint table with the KiCad defaults.

The footprint libraries table file (on Windows 10) is located in your AppData. It should look similar to: 'C:\Users\Nathan\AppData\Roaming\kicad\fp-lib-table'.

Note: AppData is a hidden directory so you'll need to make hidden folders visible.

The contents of

The contents of 'fp-lib-table'

Removing the deprecated libraries brings the default count down to 75 and CvPcb still takes an annoyingly long time to load. This is where you'll have to make some tough decisions. Do you plan to ever need the 'Shielding-Cabinets' library? Perhaps. Perhaps not. If I ever do need an RF shield for a design, it will most likely be a custom part or a part that is not in the library. So that one gets the toss.

SparkFun is taking a blended approach. We're becoming very familiar with the default KiCad libraries and using their footprints wherever it makes sense. When we find or use a package we like, we copy it over to the SparkFun-KiCad-Libraries GitHub repo. At the same time, we're continuing to leverage all our custom Eagle footprints that we've been using and creating for over a decade. We know and trust these footprints. I have had many PCBs ruined because I trusted someone else's footprint so I tend to be very paranoid. Use the community where you can but be very rigorous about checking them for correctness.

If you're needing a generic 2x5 pin male header, check the KiCad libraries. It should work fine. However, if you're using a more eclectic part, you may be better off creating the footprint from scratch. Even if the KiCad libraries contain the part, you'll want to check it against the datasheet very closely and do a one to one test print.

Using Eagle Footprints in KiCad

If you're familiar with Eagle, it can be scary to think all the time spent creating footprints will be lost when switching to KiCad. Don't fear! KiCad inherently reads Eagle footprints! Yep, it's built right in. Now don't get too excited. KiCad can't read your Eagle schematic components but we have a solution for that in a later section.

KiCad can

The approach we are taking at SparkFun is to link to a local copy of all our classic Eagle Librarie Anytime we need one of the Eagle footprints, we copy and paste it into a modern KiCad library. We don't have to re-create the footprint but by moving it over to a KiCad library. We are able to then edit the footprint as needed. Furthermore, any new footprints are created from scratch and saved to the appropriate SparkFun KiCad library.

You should have already opened the PCB Footprint Editor at least once by now. This will have created a 'fp-lib-table' file that we will be editing shortly. Now to get started, be sure that KiCad is closed.

Download the SparkFun Eagle Libraries from GitHub.

SPARKFUN EAGLE LIBRARY GITHUB REPOSITORY

Unzip them into a local directory of your choice. I store our Eagle libraries in a DropBox folder so both my desktop and laptop can access the same set of files.

You could use the Footprint Libraries Manager located in the footprint editor but adding or removing many libraries becomes tedious; it's easier to edit the table file directly.

The contents of fp-lib-table

The contents of fp-lib-table

The 'fp-lib-table' tells KiCad where to find all the various libraries and what types of libraries they are (KiCad, GitHub, EAGLE, etc).

We are going to edit this file to add in the SparkFun libraries as well as remove the deprecated libraries and libraries that SparkFun doesn't use.

Here are the files of importance:

  • original fp-lib-table - This is what KiCad creates by default. You don't really need to download it. It's just for reference.

  • sparkfun fp-lib-table - The list of SparkFun libraries. You don't need to download it, just for reference.

  • combined fp-lib-table - This is the combination of the original table, with extraneous libraries removed and SparkFun libraries added.

Download the 'combined fp-lib-table' to a local folder. Rename it to 'fp-lib-table'. Now move the file to where KiCad expects it. The footprint libraries table file (on Windows 10) is located in the AppData folder similar to: 'C:\Users\Nathan\AppData\Roaming\kicad\fp-lib-table'. You'll want to overwrite the file that is there.

Note: AppData is a hidden directory so you'll need to make hidden folders visible.

Once the file is in place, re-open KiCad, open the PCB footprint editor, and finally the Footprint Libraries Manager. You should see a long list of libraries including the new SparkFun libraries.

long list of libraries including SparkFun libraries

The last step is to tell KiCad the local path to the SparkFun libraries. Currently it's a variable called SFE_LOCAL. We need to assign this to something. Close the Library Manager window, click on Preferences -> Configuration Paths. Click the 'Add' button. Edit the Name and Path fields.

In the image below, you can see I've set the 'SFE_LOCAL' variable to a local path of 'C:\Users\nathan.seidle\Dropbox\Projects\SparkFun-Eagle-Libraries\'. Set this variable to wherever you locally stored the SparkFun Eagle Libraries.

set the ‘SFE_LOCAL’ variable to a local path

Congratulations! You can now see, use, and copy all the SparkFun Eagle libraries.

See/use/copy all the SparkFun Eagle libraries

Creating Custom KiCad Schematic Components

Once you've learned to create your own schematic parts and custom footprints, you become unlimited by what technologies you can play with. Let's get started!

From the main project window start the Schematic library editor.

Start the Schematic library editor

This process is similar to how we started a custom footprint library. First, let's find a schematic symbol we want to start our custom library with. The photocell is just as common as it gets. Let's pull in the 'R_PHOTO' schematic component from the device library and use it to start our new custom schematic component library.

Start by clicking on the 'Selecting working library' (i.e. book) icon located in the upper left corner. Then select 'device' to set the working library.

select ‘device’ to set the working library

Click on the 'Load component to edit from current library' button and type r_photo in the filter to quickly locate the photoresistor component. When located, click 'OK'.

When located, click ‘OK’

Click on 'Save current component to new library' button.

Click on ‘Save current component to new library’

I recommend you store this *.lib file in the same 'C:\KiCadLibs\' directory we stored the footprint library within. I called my lib file 'CustomComponents.lib' so that I know these are mine.

lib file ‘CustomComponents.lib’

Once you click 'Save', a warning will pop up. This is just KiCad's polite way of letting you know that you can't access your library until you link to it. So let's do that.

Once you click ‘Save’, a warning will pop up

Click on Preferences -> Component Libraries to view the current set of libraries. In the image below, we can see the stock schematic component libraries that ship with KiCad. Next to the 'Component library files', click 'Add'.

Next to the ‘Component library files,’ click ‘Add’

Navigate to your 'C:\KiCadLibs' directory and then open 'CustomComponents.lib'. It should now appear at the bottom of the Component library files list. Click 'OK' to return to the library editor.

Again, click on the 'Select working library' button but this time either scroll to your custom list or type 'Custom' to find the 'CustomComponents' library. Click 'OK'.

find the

Then click on 'Load component to edit from the current library' button and we should see only the photoresistor schematic component. Double click on R_PHOTO to begin editing it.

Double click on R_PHOTO to begin editing it

Now at this point, we can add new symbols from scratch to our library and we can also copy from one library to another.

How to Copy a Component to Your Custom KiCad Library

KiCad is always changing and they've made leaps and bounds improvements but copying a schematic component from one library to another is still a bit wild.

For example, let's copy the CP2104 from the silabs library into our custom library. Start by setting the active library to the one that contains the part you want to copy by clicking on the 'Select working library' button. In our example, we want to set silabs as the active library.

we want to set silabs as the active library

Load the CP2104 component by clicking on the 'Load component to edit from the current library' button.

Now set the active library to the library we want to copy the CP2104 into. For this example, that means that we need to click on the 'Select working library' button and set the active library to 'CustomComponents'.

click ‘Select working library’ and set active library

Click on the 'Update current component in current library' button to save the component in CustomComponents.lib. The 'Save current library to disk' button will become enabled and you can save this component to your custom library.

‘Save current library to disk’ will become enabled

To verify it's now in the library click on the 'Load component to edit from the current library' button. You should see your new shiny CP2104 in the list.

How to Delete a Component from Your Custom KiCad Library

Bad CP2104! Bad component.

To remove a component, be sure you've set your custom library as the active one. Let's try removing the component that we just added in our custom library CustomComponents.lib. If you have not already, click on 'Select working library' to set the active library to CustomComponents. Click on the 'Delete component in current library' (i.e. the trash can) button. You'll be prompted for which component you want to remove. Select CP2104 from the list.

Select CP2104 from the list

Click 'OK' and then 'Yes' to delete the component from the library. Click the 'Current library to disk' button and 'Yes' to save.

Shout out to Joan_Sparky! He is the best! (No relation)

KiCad Library Convention

Be sure to check KiCad's KiCad Library Convention once you get comfortable creating components. These conventions take into account a heap of industry specialized knowledge that we can all benefit from.

Resources and Going Further

Congratulations! That was a big tutorial and you made it through.

For more information related to KiCad, check out the resources below:

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.