Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Topic 4 Control Subsystem Slide 19

In summary the Concerto device family is a dual core architecture which combines three basic systems in a single device. First the Master System, this is the Cortex-M3 based CPU system, which contains multiple communication ports and is the primary application processor. Second is the control system, the C28x FPU based system and it contains multiple control peripherals such as the PWMs, captures, encoders and serial interfaces for advanced control and baseband signaling processing applications. Third is the analog subsystem it contains the integrated analog components such as a high performance ADC and the analog comparators. Again, the architecture is really designed so that the master and control system are relatively independent as if one were working with two separate devices plus the analog system, except it is all in one chip.

PTM Published on: 2012-06-20