Typically, address pins are only used on I²C devices to allow multiple devices with the same base slave address to be on the same bus. The SPI devices also have address pins to allow multiple devices on the same bus while using one chip select.
所订产品一般在 7-10个工作日 内送达中国,具体时间取决于收货地点。
最低订购金额为人民币 300 元,顺丰快递免运费配送。
当用人民币下单时,按照国际贸易条款 DDP(DigiKey 支付关税、海关费用和当地税款)方式结算。
电汇预付
![]()
![]()
![]()
更多来自全授权合作伙伴的产品
下单后,从合作伙伴发货平均需要时间 1-3 天,也可能产生额外运费。可能另外收取运费。 实际发货时间请留意产品详情页、购物车和结账页面上的说明。
国际贸易结算方式:CPT(交货时支付关税、海关费用和适用 VAT/应付税金)
有关详情,请访问帮助和支持
Typically, address pins are only used on I²C devices to allow multiple devices with the same base slave address to be on the same bus. The SPI devices also have address pins to allow multiple devices on the same bus while using one chip select.
谢谢!
敬请关注收件箱中的 DigiKey 新闻与更新!
请输入电子邮件地址