Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Product List
The software provides easy configuration of PIXI components through the Property Pallet. Each PIXI component has a set of Properties that could be different from other components. The Property Pallet shows properties of the selected component only. All the settings in properties pallet, for each component, are reflected in the register map generated by the software. Each component has a set of properties and default values for sub parameters. This example represents a single-ended ADC on input pin 1. The parameters which may be selected are as follows: Average # Samples – the default is 1 but the designer can select a range from 1 to 128. Reference Voltage – the default is internal reference but the designer can select internal or external reference source. Voltage Range – the default is 0 to 10 V but the designer can select 0 to 10 V, or -5 to 5 V, or -10 to 0 V, or 0 to 2.5 V.
PTM Published on: 2014-10-23