Maker.io main logo

Understanding RTL and HDL: Part 2 of our Verilog Journey

1,656

2023-12-29 | By DWARAKAN RAMANATHAN

What is RTL?

RTL stands for "Register-Transfer Level," and it is a level of abstraction used in digital design and hardware description languages (HDLs) like Verilog and VHDL. RTL is a critical step in the process of designing digital circuits and systems. Here's what RTL represents and its significance:

Abstraction Level: RTL is an intermediate abstraction level between high-level system behavior and low-level hardware implementation.

  • Registers and Data Paths: RTL focuses on registers (temporary data storage) and data paths (connections between registers.)
  • Clock Cycles: Operations in RTL are synchronized with clock cycles, defining discrete time steps.
  • Data Transfer: RTL specifies how data moves between registers, often involving combinational logic elements.
  • Hardware Description: RTL is described using hardware description languages (HDLs) and is crucial for simulation, verification, and synthesis in digital design.

What is Hardware Description Language?

A Hardware Description Language (HDL) is a specialized programming language used for describing the behavior and structure of digital circuits and systems. HDLs are primarily employed in the field of digital electronics and integrated circuit (IC) design. These languages allow engineers and designers to create models of digital hardware, simulate their behavior, and synthesize them into actual hardware.

Key characteristics and uses of Hardware Description Languages (HDLs) include:

  • Digital Circuit Description: HDLs enable engineers to describe digital circuits at various levels of abstraction, ranging from high-level behavior to low-level hardware details.
  • Behavioral Modeling: Engineers can specify the desired functionality of a digital system without defining the specific implementation details. This is known as behavioral modeling and allows for rapid system-level design.
  • Structural Modeling: HDLs also support structural modeling, where designers specify the interconnections of hardware components such as gates, flip-flops, and multiplexers.
  • Hierarchy: HDLs support hierarchical design, allowing complex systems to be divided into smaller, more manageable modules with well-defined interfaces. This promotes modularity and design reusability.
  • Simulation: HDL models can be used for simulating digital circuits. Engineers can test the behavior of a design under various conditions and verify its correctness before physical implementation.
  • Verification: Verification is a critical phase in hardware design. HDLs facilitate the creation of test benches and test cases to verify that a design meets its specifications.
  • Synthesis: HDL code can be synthesized into a netlist, which represents the hardware structure of a design. This netlist can then be implemented on hardware platforms such as FPGAs (Field-Programmable Gate Arrays) or ASICs (Application-Specific Integrated Circuits.)
  • Timing Constraints: Designers can specify timing constraints in HDLs to ensure that circuits meet required performance criteria, such as clock frequency and timing requirements.

Two of the most commonly used Hardware Description Languages are:

  • Verilog: Verilog is widely adopted in the semiconductor industry and is used for both design and verification of digital circuits. It has evolved into SystemVerilog, which includes advanced features for verification.
  • VHDL (VHSIC Hardware Description Language): VHDL is another popular HDL, especially in aerospace, defense, and European markets. It is known for its strong typing and rigorous design verification capabilities.

Sections of Verilog Code:

Copy Code
module and_gate ( 
‎    input wire a, 
‎    input wire b, 
‎    output wire y 
‎); 
assign y = a & b; 
end module
  • module and_gate: This line begins the module definition, named "and_gate." In Verilog, modules are used to encapsulate and describe digital components or blocks of logic within a larger design. In this case, we are defining an AND gate as a module.
  • input wire a, input wire b: These lines declare two input ports for the module. The keywords "input" specify that these ports receive data from external sources. "Wire" indicates that these signals are single-bit and continuous, meaning they can change value continuously. a and b are the names of the input ports, which represent the two inputs to the AND gate.
  • output wire y: This line declares an output port for the module. Similar to the input ports, it's defined as a single-bit continuous signal. y is the name of the output port, representing the output of the AND gate.
  • assign y = a & b: This line assigns the value of the output signal y based on the logical AND operation of input signals a and b. Here's how it works; a and b represent the two input signals of the AND gate. & is the bitwise AND operator in Verilog, used for performing logical AND between the bits of two signals. y is assigned the result of the logical AND operation of a and b. If both a and b are logic '1' (high), then y will be '1'; otherwise, it will be '0'.

Designing vs. Verification in Verilog:

Designing and verification are two distinct phases in the development of digital circuits using Verilog or any hardware description language (HDL). Let's explore the differences between designing and verification using examples in Verilog.

Designing with Verilog:

  • Purpose: In the design phase, you create the actual functionality of the digital circuit. You specify how the circuit should behave and its architecture.

Example: Designing a 4-bit adder that takes two 4-bit binary numbers as input and produces a 4-bit sum as output.

  • Code Focus: Design Verilog code describes the logic and structure of the circuit. It includes details about how components are interconnected and how data flows within the circuit.
Copy Code
module four_bit_adder ( 
‎    input [3:0] A, 
‎    input [3:0] B, 
‎    output [3:0] SUM 
‎); 
‎ 
assign SUM = A + B; 
‎ 
endmodule

Verification with Verilog:

  • Purpose: Verification ensures that the designed digital circuit behaves correctly and meets its specifications. It involves testing and validating the design to catch errors and ensure it works as intended.

Example: Verifying the 4-bit adder designed earlier to confirm that it correctly adds two 4-bit binary numbers.

  • Code Focus: Verification Verilog code focuses on creating test benches and test cases that exercise the design. It simulates the behavior of the circuit under various conditions and inputs.
Copy Code
module test_four_bit_adder; 
‎ 
reg [3:0] A, B; 
wire [3:0] SUM; 
‎ 
four_bit_adder DUT ( 
‎    .A(A), 
‎    .B(B), 
‎    .SUM(SUM) 
‎); 
‎ 
initial begin 
‎    // Test cases and stimulus generation 
‎    A = 4'b0011; 
‎    B = 4'b0101; 
‎ 
‎    // Delay for a few time units 
‎    #10; 
‎ 
‎    // Check the output SUM 
‎    if (SUM === 4'b1000) 
‎        $display("Test PASSED"); 
‎    else 
‎        $display("Test FAILED"); 
‎ 
‎    // More test cases... 
end 
‎ 
endmodule
  • Goal: The primary goal of verification is to ensure that the design operates correctly under various scenarios. Verification code creates tests, monitors the design's response, and reports any discrepancies or errors.

In summary, designing with Verilog involves creating the actual digital circuit, and defining its logic and architecture. Verification with Verilog involves testing and validating the design to ensure it meets specifications and functions correctly. Both phases are essential for the successful development of digital systems.

The link to the first part of this blog is Here

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.