Maker.io main logo

Pro Micro RP2040 Hookup Guide

1,106

2025-06-03 | By SparkFun Electronics

License: See Original Project Qwiic Raspberry Pi MCU

Courtesy of SparkFun

Guide by bboyho

Introduction

The Pro Micro RP2040 is a low-cost, high-performance board with flexible digital interfaces ‎featuring the Raspberry Pi Foundation's RP2040 microcontroller. The board uses well ‎known Pro Micro footprint with castellated mounting holes.‎

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need ‎everything though depending on what you have. Add it to your cart, read through the guide, ‎and adjust the cart, as necessary.‎

Tools

You will need a soldering iron, solder, and general soldering accessories for a secure ‎connection when using the plated through hole pads.‎

Prototyping Accessories

Depending on your setup, you may want to use IC hooks for a temporary connection. ‎However, you will want to solder header pins to connect devices to the plated through holes ‎for a secure connection.‎

For those that want to take advantage of the Qwiic enabled devices, you'll want to grab a ‎Qwiic cable.‎

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview if ‎you decide to take advantage of the Qwiic connector.‎

qwiic_1

Qwiic Connect System

We would also recommend taking a look at the following tutorials if you aren't familiar with ‎them.‎

  • How to Solder: Through-Hole Soldering: This tutorial covers everything you need to know ‎about through-hole soldering.‎

  • Serial Communication: Asynchronous serial communication concepts: packets, signal ‎levels, baud rates, UARTs and more!‎

  • Serial Peripheral Interface (SPI): SPI is commonly used to connect microcontrollers to ‎peripherals such as sensors, shift registers, and SD cards.‎

  • Pulse Width Modulation: An introduction to the concept of Pulse Width Modulation.‎

  • Logic Levels: Learn the difference between 3.3V and 5V devices and logic levels.‎

  • I2C: An introduction to I2C, one of the main embedded communications protocols in use ‎today.‎

  • Analog vs. Digital: This tutorial covers the concept of analog and digital signals, as they ‎relate to electronics.‎

Hardware Overview

Old School to New School

The Pro Micro RP2040 design uses the original Pro Micro and Qwiic Pro Micro USB C's ‎footprint.‎

older_2

Older Pro Micro with ATmega32U4‎

newer_3

Newer Qwiic Pro Micro USB C with RP2040‎

The Pinout

All of the Pro Micro RP2040's GPIO and power pins are broken out to two, parallel headers. ‎Some pins are for power input or output; other pins are dedicated GPIO pins. Further, the ‎GPIO pins can have special function depending on how they are multiplexed Here's a map ‎of which pin is where and what special hardware functions it may have.‎

pinout_4

Note: For more information on the multiplexed pins, check out "section 1.4.3 GPIO ‎Functions"of the RP2040 datasheet.

RP2040 Datasheet (31.2MB)‎

Power

There are a variety of power and power-related nets broken out to connectors and through ‎hole pads. Each pad has a castellated edge. The back of the board also has the USB pins ‎broken out for power.

power_5

power_6

These nets consist of the following:‎

  • V is the voltage provided from the USB connector.‎

  • + is the raw, unregulated voltage input for the Pro Micro RP2040. If the board is ‎powered via USB (i.e., V), the voltage at this pin will be about 4.8V (USB's 5V minus a ‎Schottky diode drop). On the other hand, if the board is powered externally, through ‎this pin, the applied voltage can be up to 5.3V.‎

  • ‎3.3V is the voltage supplied to the on-board RP2040. We suggest using regulated ‎‎3.3V when connecting to this pin. If the board is powered through the raw "+" pin, ‎this pin can be used as an output to supply 3.3V other devices.‎

  • rst can be used to restart the Pro Micro RP2040. There is a built-in reset button to ‎reset the board. However, the pin is broken out if you need to access this pin ‎externally. This pin is pulled high by a 10kΩ resistor on the board, and is active-low, ‎so it must be connected to ground to initiate a reset. The Qwiic Pro Micro will remain ‎‎"off" until the reset line is pulled back to high.‎

  • GND, of course, is the common, ground voltage (0V reference) for the system.‎

USB Pins

On the back of the board, you can access the USB data pins and power for either USB 1.1 ‎Host or Device.‎

usb_7

GPIO Pins

The Pro Micro RP2040 breaks out the GPIO pins to plated through holes pads on the edge of ‎the board. Each pad is castellated as well.‎

pin_8

Top of Board with Edge PTH Pads

pin_9

Bottom of Board with Edge PTH Pads

The Pro Micro's GPIO pins — 20 in all — (if you include the two pins on the Qwiic connector ‎as well) are multi-talented. Every pin can be used as a digital input or output, for blinking ‎LEDs or reading button presses. These pins are referenced via an integer value between 0 ‎and 29.‎

Four pins feature analog to digital converters (ADCs) and can be used as analog inputs. ‎These are useful for reading potentiometers or other analog devices.‎

Note: There is an additional ADC pin that is not broken out on the RP2040. It is connected ‎to the internal temperature sensor. While it is not broken out on the board, you can access ‎the temperature sensor readings using examples from either the C/C++ or MicroPython ‎SDK.

All pins can be set with the pulse width modulation (PWM) functionality, which allows for a ‎form of analog output. The RP2040 can only provide a total of up to 16 controllable PWM ‎outputs.‎

There are hardware UART (serial), I2C, and SPI pins available as well. These can be used to ‎interface with digital devices like serial LCDs, XBees, IMUs, and other serial sensors.‎

The RP2040 has 26 external interrupts, which allow you to instantly trigger a function when ‎a pin goes either high, low, or changes state.‎

Qwiic Connector

The board includes a Qwiic connector to easily connect Qwiic enabled I2C devices to the ‎board. SCL is connected to GPIO17 while SDA is connected to GPIO16.‎

board_10

Note: If you decide not to use the I2C port with a Qwiic-enabled device, you can technically ‎use the Qwiic cable with either male or female jumpers as GPIO pins.

On-Board LEDs

There are two LEDs on the Pro Micro RP2040. The red LED indicates whether power is ‎present. The other is the addressable WS2812 RGB LED. The addressable LED is connected ‎to GPIO25. You'll to define functions or use the WS2812 library to control that LED.‎

ledboard_11

There is a pad on the back of the board that is connected to the WS2812's DO pin. If you ‎decide to daisy chain more LEDs, you'll want to solder to this pad.‎

pad_12

External Flash Memory

The Pro Micro RP2040 includes a W25Q128JVPIM, which adds 128Mb (16MB) of flash ‎memory externally.

external_13

Boot Button

The boot button is connected to the external flash memory. Pressing this button forces USB ‎boot mode so that the board shows up as a USB mass storage device.‎

boot_14

Reset Button

As explained earlier, there is a reset button to reset the RP2040. This adds the option of ‎forcing the RP2040 into bootloader mode without needing to unplug/replug the board back ‎into your USB port. To keep the board size at a minimum, the buttons are not labeled. To ‎distinguish between the two buttons, just remember that the reset button is on the same ‎side of the board as the reset pin.‎

reset_15

SWD Pins

For advanced users, there are two pins (i.e., D for data/SWDIO and C for clock/SWCLK) on ‎the back broken out for SWD programming on the back of the board. You'll need to solder ‎wire to connect to these pins.‎

swd_16

Board Dimensions

The board measures 1.3" x 0.7". Keep in mind that the USB-C connector is not flush with ‎the board and will protrude about 0.05" from the edge of the board. Not included in the ‎image below is the PCB thickness, which is 0.8mm. This is thinner than a majority of PCBs ‎used for SparkFun original designs.‎

dimensions_17

Hardware Hookup

Header pins were left off the Pro Micro RP2040 to allow users the flexibility of connecting ‎any type of 0.1" header to the board. For temporary connections to the I/O pins, you could ‎use IC hooks to test out the pins. However, you'll need to solder headers or wires of your ‎choice to the board for a secure connection. For advanced users, you could also design a ‎PCB to take advantage of the castellated edges for a lower profile. Here are a few tutorials to ‎connect to the pads depending on your personal preference.‎

solder_18

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.‎

wire_19

Working with Wire

How to strip, crimp, and work with wire.‎

holes_20

How to Solder: Castellated Mounting Holes

Tutorial showing how to solder castellated holes (or castellations). This might come in ‎handy if you need to solder a module or PCB to another PCB. These castellations are ‎becoming popular with integrated WiFi and Bluetooth modules.‎

Note: For advanced users taking advantage of the castellated edges, you can design a ‎board with the Qwiic Pro Micro Eagle footprint.

GitHub SparkFun Eagle Library: SparkFun-Boards.lbr

In order to power and upload to the board, you will simply need a USB C cable connected to ‎your computer.‎

connect_21

Connecting to GPIO

There a few methods of connecting to the GPIO. For a temporary connection when ‎prototyping, you can use IC hooks to connect your circuit to a breadboard. Below is an ‎example of a basic 5mm LED connected to a 330Ω current limiting resistor on a ‎breadboard.‎

breadboard_22

For a secure connection to the Pro Micro RP2040's GPIO, it is recommended to solder ‎header pins. If you designed the board using the footprint, you can also solder the board ‎using the castellated headers. In this case, two 1x12 male header pins are being soldered ‎to the board with the help of a breadboard.‎

header_23

While originally intended to connect Qwiic-enabled devices, you can also use the SDA and ‎SCL pins as a quick, visible test to see if the board is working. In this case, the SCL pin was ‎used as a GPIO pin. Similar to the circuit with the IC hooks, the pin was connected to a ‎basic 5mm LED and a 330Ω current limiting resistor on a breadboard.‎

test_24

Qwiic Enabled Device

You can also easily connect a Qwiic enabled device to the Qwiic connector. Below is an ‎example of the Qwiic VL53L1X distance sensor and Qwiic Micro OLED connected to the ‎Qwiic Pro Micro.‎

device_25

UF2 Bootloader

The Pro Micro 2040 is easy to program, thanks the UF2 bootloader. With this bootloader, ‎the board shows up on your computer as a USB storage device without having to install ‎drivers for Windows 10, Mac, and Linux!‎

What is UF2?‎

UF2 stands for USB Flashing Format, which was developed by Microsoft for PXT (now ‎known as MakeCode) for flashing microcontrollers over the Mass Storage Class (MSC), just ‎like a removable flash drive. The file format is unique, so unfortunately, you cannot simply ‎drag and drop a compiled binary or hex file onto the board. Instead, the format of the file ‎has extra information to tell the processor where the data goes, in addition to the data itself. ‎For more information about UF2, you can read more from the MakeCode blog, as well as ‎the UF2 file format specification.‎

Software Overview

There are two methods of programming the RP2040. You can use MicroPython or ‎C/C++ depending on your personal preference. The documentation is written for the ‎Raspberry Pi's Pico development board but will apply for any board with the RP2040. Just ‎make sure to adjust the pin definition depending on what GPIO is broken out.‎

Getting Started with the Raspberry Pi Pico

Examples (MicroPython)‎

The Raspberry Pi foundation has provided the necessary tools, documentation, and ‎examples to get started with the RP2040. If you haven't already, check out the ‎documentation on the Pico. We'll use this as a reference when using the chip on other ‎development boards to fit your needs in this tutorial.‎

Raspberry Pi: Pico Python SDK (PDF)‎

We'll be using the MicroPython examples from this repo using Thonny IDE.‎

GitHub: raspberrypi/pico-micropython-examples

Installing MicroPython on the RP2040‎

Note: Interested in going further? The Raspberry Pi Foundation also released a book to get ‎started with the Pico's RP2040: "Get Started with MicroPython on Raspberry Pi Pico."‎

  • ‎Get Started with MicroPython on Raspberry Pi Pico

To install MicroPython on the RP2040, users can download the firmware for Raspberry Pi ‎Pico. Head over to the Raspberry Pi Foundation's RP2040 documentation. Click on the tab ‎for the "MicroPython", scroll down to the Drag-and-Drop MicroPython section, and click ‎the download link for the Raspberry Pi Pico.‎

Firmware for the Raspberry Pi Pico

Note: Since this tutorial was written, MicroPython has built and released new firmware ‎specifically for the RP2040 Pro Micro. The *.uf2 firmware file can be download from the ‎MicroPython website, by clicking the button below:‎

Download the latest firmware release for the RP2040 Pro Micro from MicroPython

Press and hold the boot button down with one hand.‎

press_26

Press the reset button momentarily.‎

press_27

press_28

Release the boot button. The board should appear as a removable drive called RPI-RP2.‎

release_29

Draw and drop the UF2 file into the "removable drive". The board will automatically reboot. ‎Below is an image highlighting the UF2 file being moved to the removeable drive on a ‎Raspberry Pi.‎

draw_30

Configuring Thonny IDE

Note: If you are using a Raspberry Pi, make sure that you are using the latest Raspberry Pi ‎image. Enter the following command in the LXTerminal to download and install the latest ‎packages. The && combines the two commands into a single line and the -y answers "yes" ‎to any prompts.

Copy Code
sudo apt update && sudo apt full-upgrade -y

Check to make sure that you are using Thonny v3.3.3 and above. If you are using a ‎Raspberry Pi, type the following command to check the version:

Copy Code
thonny -v

You should get a result similar to the output below. If you have a version that is equal or ‎higher, you should be good to go!

Copy Code
INFO    thonny:Thonny version: 3.3.3

If you are using a different operating system, you can also download the Thonny IDE.

Open Thonny up from the start menu: Raspberry Pi Start Menu > Programming > Thonny ‎Python IDE

menu_31

Set Thonny's interpreter for the RP2040. The "Raspberry Pi Pico" will work for the RP2040. ‎Head to the menu and select: Run > Select Interpreter....‎

set_32

This will open a new window for the Thonny options. In the Interpreter tab, ‎select MicroPython (Raspberry Pi Pico) as the interpreter.‎

window_33

Note: You can also click on the bottom right to Configure Interpreter... and follow the ‎same steps outlined above.

note_34

In the same window, make sure to select the option to have Thonny automatically detect ‎the COM port for the board: Port > < Try to detect port automatically >‎

auto_35

Note: If you are on Linux based OS like the Raspberry Pi, the COM port may show up ‎as tty(AMA0 (/dev/ttyAMA0).‎

Hello World!‎

To check if this is working open the Thonny IDE, type the following into the editor. Feel free to ‎adjust the message to whatever you prefer.‎

Copy Code
print("Hello world!")

Hit the "Run current script" button. In the Shell, you will see the following output. Sweet!‎

Copy Code
>>> %Run -c %EDITOR_CONTENT
Hello world!

script_36

Note: To save the file and have it run every time the board is powered up, simply ‎select File > Save As... from the menu.

save_37

When a window pops up, select Raspberry Pi Pico.

popup_38

‎Then save the file as main.py

main_39

‎Just make sure to save any code that was edited on your computer (e.g., Save as... > This ‎computer) before closing Thonny.

save_40

Note: If you are using a terminal window and REPL, you will need to type the functions into ‎the terminal window. While you can copy and paste, the terminal window will not recognize ‎indents for loops or custom defined subroutines. As a result, the pasted code will not be ‎interpreted correctly by REPL. You'll want to make sure that you are using the Thonny editor ‎to avoid this error.‎

Blink

If you have the MicroPython examples saved, head to the following folder in your ‎downloads .../pico-micropython-examples/blink/blink.py. Your code should look like the ‎following. Of course, you can also copy and paste the code provided after the next ‎paragraph as well.‎

Once you open it in Thonny, adjust the pin number to the GPIO that the LED is connected to. ‎Since we are using the example that was written specifically for the Pico as opposed to the ‎Pro Micro RP2040, we'll need to adjust the pin. In this case, we'll use the ‎RP2040's GPIO17 that is connected to the Qwiic connector so that we do not have to solder ‎pins to the board. This is assuming that we are connecting a current limiting resistor and an ‎LED between the GPIO17 and GND.‎

Copy Code
# ========== DESCRIPTION==========
# The following code was originally written by 
# the Raspberry Pi Foundation. You can find this
# example on GitHub.
#
#     https://github.com/raspberrypi/pico-micropython-examples/blob/master/blink/blink.py
#
# Note that the GPIO for the LED was adjusted
# for the Pro Micro RP2040. Make sure to use 
# a current limiting resistor with the LED.

from machine import Pin, Timer

led = Pin(17, Pin.OUT)
tim = Timer()
def tick(timer):
    global led
    led.toggle()

tim.init(freq=2.5, mode=Timer.PERIODIC, callback=tick)

Hit the "Run current script" button. Once the code runs, you will see the LED blink. If you ‎want the board to run blink every time the board is powered up, just follow the note provided ‎at the end the previous example.‎

run_41

WS2812‎

If you have the MicroPython examples saved, head to the following folder in your ‎downloads .../pico-micropython-examples/pio/neopixel_ring/neopixel_ring.py . Your ‎code should look like the following. Of course, you can also copy and paste the code ‎provided after the next paragraph as well.‎

Once you open it in Thonny, adjust the pin number to the GPIO that the LED is connected to ‎for PIN_NUM. Since we are using the example that was written specifically for the Pico as ‎opposed to the Pro Micro 2040, we'll need to adjust the pin. In this case, we'll use the ‎RP2040's GPIO25 that is connected to the WS2812. We will also adjust the NUM_LEDs ‎to 1.‎

Copy Code
# ========== DESCRIPTION==========
# Example using PIO to drive a set of WS2812 LEDs.
#
# The following code was originally written by
# the Raspberry Pi Foundation. You can find this 
# example on GitHub.
#
#    https://github.com/raspberrypi/pico-micropython-examples/blob/master/pio/neopixel_ring/neopixel_ring.py
#
# Note that the 'NUM_LEDs' was adjusted to 1. Also
# the GPIO for the addressable WS2812 RGB LED called
# `PIN_NUM` was adjusted for the Pro Micro RP2040. 

import array, time
from machine import Pin
import rp2

# Configure the number of WS2812 LEDs.
NUM_LEDS = 1
PIN_NUM = 25
brightness = 0.2

@rp2.asm_pio(sideset_init=rp2.PIO.OUT_LOW, out_shiftdir=rp2.PIO.SHIFT_LEFT, autopull=True, pull_thresh=24)
def ws2812():
    T1 = 2
    T2 = 5
    T3 = 3
    wrap_target()
    label("bitloop")
    out(x, 1)               .side(0)    [T3 - 1]
    jmp(not_x, "do_zero")   .side(1)    [T1 - 1]
    jmp("bitloop")          .side(1)    [T2 - 1]
    label("do_zero")
    nop()                   .side(0)    [T2 - 1]
    wrap()


# Create the StateMachine with the ws2812 program, outputting on pin
sm = rp2.StateMachine(0, ws2812, freq=8_000_000, sideset_base=Pin(PIN_NUM))

# Start the StateMachine, it will wait for data on its FIFO.
sm.active(1)

# Display a pattern on the LEDs via an array of LED RGB values.
ar = array.array("I", [0 for _ in range(NUM_LEDS)])

##########################################################################
def pixels_show():
    dimmer_ar = array.array("I", [0 for _ in range(NUM_LEDS)])
    for i,c in enumerate(ar):
        r = int(((c >> 8) & 0xFF) * brightness)
        g = int(((c >> 16) & 0xFF) * brightness)
        b = int((c & 0xFF) * brightness)
        dimmer_ar[i] = (g<<16) + (r<<8) + b
    sm.put(dimmer_ar, 8)
    time.sleep_ms(10)

def pixels_set(i, color):
    ar[i] = (color[1]<<16) + (color[0]<<8) + color[2]

def pixels_fill(color):
    for i in range(len(ar)):
        pixels_set(i, color)

def color_chase(color, wait):
    for i in range(NUM_LEDS):
        pixels_set(i, color)
        time.sleep(wait)
        pixels_show()
    time.sleep(0.2)

def wheel(pos):
    # Input a value 0 to 255 to get a color value.
    # The colours are a transition r - g - b - back to r.
    if pos < 0 or pos > 255:
        return (0, 0, 0)
    if pos < 85:
        return (255 - pos * 3, pos * 3, 0)
    if pos < 170:
        pos -= 85
        return (0, 255 - pos * 3, pos * 3)
    pos -= 170
    return (pos * 3, 0, 255 - pos * 3)


def rainbow_cycle(wait):
    for j in range(255):
        for i in range(NUM_LEDS):
            rc_index = (i * 256 // NUM_LEDS) + j
            pixels_set(i, wheel(rc_index & 255))
        pixels_show()
        time.sleep(wait)

BLACK = (0, 0, 0)
RED = (255, 0, 0)
YELLOW = (255, 150, 0)
GREEN = (0, 255, 0)
CYAN = (0, 255, 255)
BLUE = (0, 0, 255)
PURPLE = (180, 0, 255)
WHITE = (255, 255, 255)
COLORS = (BLACK, RED, YELLOW, GREEN, CYAN, BLUE, PURPLE, WHITE)

print("fills")
for color in COLORS:       
    pixels_fill(color)
    pixels_show()
    time.sleep(0.2)

print("chases")
for color in COLORS:       
    color_chase(color, 0.01)

while True:
    print("rainbow")
    rainbow_cycle(0)

Hit the "Run current script" button. Once the code runs, it will display each color at "0.2" ‎brightness. The LED will then animate. Since there is only one LED attached, it will look like ‎it will be blinking through the colors. Once the board jumps into the while loop, the LED will ‎begin cycling between colors smoothly. Remember, you can have the board run the ‎example every time the board is powered up by following the note provided in an earlier ‎example.‎

Pro_Micro_RP2040_WS2812_RGB_Rainbow

If you are looking to simplify the code, you can also use the library written for the WS2812. ‎This saves some of the functions in a separate file. Just make sure to adjust the GPIO to ‎connect to the WS2812(s) and the number of LEDs.‎

GitHub: pico_python_ws2812b Library

Resources and Going Further

For more information, check out the resources below:‎

制造商零件编号 18288
PRO MICRO RP2040
SparkFun Electronics
制造商零件编号 12002
BREADBOARD - SELF-ADHESIVE (WHIT
SparkFun Electronics
制造商零件编号 09741
TEST LEAD HOOK TO TIP PLUG 2.5"
SparkFun Electronics
制造商零件编号 14322
PHOTON STACKABLE HEADER - 12 PIN
SparkFun Electronics
制造商零件编号 15081
QWIIC CABLE KIT
SparkFun Electronics
制造商零件编号 14427
QWIIC CABLE - 100MM
SparkFun Electronics
制造商零件编号 14425
QWIIC CABLE - BREADBOARD JUMPER
SparkFun Electronics
制造商零件编号 17257
FLEXIBLE QWIIC CABLE - 500MM
SparkFun Electronics
制造商零件编号 17261
FLEXIBLE QWIIC CABLE - FEMALE JU
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.