How to Control Linear Actuator Using a Capacitive Touch Button and Ardui
2026-05-20 | By Ron Cutts
License: GNU Lesser General Public License Microcontrollers Touch Motors Arduino
In this project, we will learn how easy it is to control a linear actuator with Arduino using a capacitive touch button and Visuino.
Watch the video!
Learn more about Visuino: What is Visuino
What You Will Need
Arduino UNO (Or any other Arduino)
Visuino program: Download Visuino






The Circuit
Connect the power supply (batteries) pin (gnd) to the motor driver controller pin (gnd)
Connect the power supply (batteries) pin (+) to motor driver controller pin (+)
Connect the power supply (batteries) pin (+) to the Arduino pin (VIN)
Connect GND from the Arduino to the motor driver controller pin (gnd)
Connect digital pin(6) from Arduino to motor driver pin (IN1)
Connect digital pin(8) from Arduino to motor driver pin (IN2)
Connect the linear actuator to the motor driver, as you can see on the schematic
Connect the Capacitive Touch button pin (SIG) to Arduino digital pin (2)
Connect the Capacitive Touch button pin (VCC) to the Arduino pin (5V)
Connect the Capacitive Touch button pin (GND) to the Arduino pin (GND)

Start Visuino, and Select the Arduino UNO Board Type
Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2


In Visuino Add & Set Components
Add "Debounce Button" component
Add "Toggle(T) Flip-Flop" component
Add "Speed and Direction To Speed" component
Add "L298N" component
Select "SpeedAndDirectionToSpeed1" and in the properties window set "Initial Speed" to 1





In Visuino Connect Components
Connect Arduino digital pin [2] to "Button1" pin [In]
Connect "Button1" pin [Out] to "TFlipFlop1" pin [Clock]
Connect "TFlipFlop1" pin [Out] to "SpeedAndDirectionToSpeed1" pin [Reversed]
Connect "SpeedAndDirectionToSpeed1" pin [Out] to "DualMotorDriver1" > Motors [0] Pin [In]
Connect ""DualMotorDriver1" > Motors [0] Pin [Direction]" to Arduino digital pin[8]
Connect ""DualMotorDriver1" > Motors [0] Pin [Speed]" to Arduino digital pin Analog PWM[6]


Generate, Compile, and Upload the Arduino Code
In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Play
If you power the Arduino module and press the touch button, the linear actuator will start to move in one direction, and if you press the touch button again, it will reverse.
Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this. You can download it here and open it in Visuino: https://www.visuino.eu