Melexis Technologies NV 的 DVK90109 Dev Kit 规格书
MeleXIe
Mlcroekachonlc Integrated eyelema
«m mm
m
DVK90109
125kHz RFID Development Kit
User Manual
390129010902 Page 1 of 13 Development Kit
Rev. 002 Apr-2008
Features and Benefits
Standard ISO communications
User interface software
RS232 serial communication
Dedicated instruction set
6 to 9Volts supply compliant
Ordering Information
Part No.
DVK90109
General Description
The development kit DVK90109 has been developed by Melexis to create specific applications using 125 kHz
protocols and to evaluate the advantages of the MLX90109 transceiver IC.
The DVK90109 results of the combination of the development board DVKRFID and the evaluation board
EVB90109. The EVB90109 is plugged on the DVKRFID through a 10 pins connector (including Coil, VCC and
Ground) and controlled by the microcontroller ATMEGA128.
A set of commands has been elaborated by Melexis to define the communication between the Computer and the
evaluation board EVB90109.
MeleXIe
Microelectronlc Integrated eyelems
DVK90109
125kHz RFID Development Kit
User Manual
390129010902 Page 2 of 13 Development Kit
Rev. 002 Apr-2008
Table of Contents
1 UNPACKING THE SYSTEM .....................................................................................3
2 CONNECTING THE SYSTEM...................................................................................3
3 DIGITAL COMMUNICATION EVB90109 - DVKRFID.................................................4
4 DIGITAL COMMUNICATION DVKRFID – PC............................................................5
4.1 Protocol assignment................................................................................................................ 5
4.2 List of instructions .................................................................................................................. 5
4.3 Error Instruction......................................................................................................................6
4.4 Instructions set ........................................................................................................................ 6
4.4.1
Version (VER) ..........................................................................................................................................6
4.4.2
Set Field (STF)..........................................................................................................................................6
4.4.3
Configuration of the MLX90109 (CFG)...................................................................................................7
4.4.4
HEA : HEAder..........................................................................................................................................7
4.4.5
REA : REAd .............................................................................................................................................7
4.4.6
WRI : Write Q5 tag...................................................................................................................................8
4.4.7
SEL : Select tag Hitag1.............................................................................................................................9
4.4.8
RDH : Read Hitag1 memory.....................................................................................................................9
4.4.9
WRH : Write Hitag1 memory...................................................................................................................9
5 MELEXIS RS232 INTERFACE PROGRAM ...............................................................11
5.1 Start RS232 interface:............................................................................................................. 11
5.2 Select serial communication port COM.................................................................................. 11
5.3 Open serial communication port............................................................................................. 11
5.4 Generates commands file........................................................................................................ 11
5.5 Select commands file .............................................................................................................. 12
5.6 Send a command..................................................................................................................... 12
6 DISCLAIMER............................................................................................................13
Mlcroeiechonlc Integrated eyelama
DVK90109
125kHz RFID Development Kit
User Manual
390129010902 Page 3 of 13 Development Kit
Rev. 002 Apr-2008
1 Unpacking the system
The DVK90109 board is delivered with all components to build a complete RFID setup.
Contents of the box:
1) Development kit 125 kHz
o Development kit RFID (DVKRFID)
o Evaluation board MLX90109 (EVB90109)
o Alimentation block 3 to 12V
o 125 KHz Transponder in credit card format
2) Compact Disc (Software and documentation)
o EVB90109 documentation
o DVK90109 User Guide
o RS232 PC interface software
2 Connecting the system
1) The EVB90109 is plugged through a 10 pins connector (DIL10) on a 14 pins connector (DIL14) on the
DVKRFID (EVB90109 AREA). The following pictures show how to connect the EVB90109 on the
DVKRFID board.
Figure 1:EVB90109 connector on the DVKRFID Figure2:EVB90109
2) Connect the board DVK90109 to the COM-port of your computer, with a RS232 cable. This allows
communication between the DVK90109 and your computer.
3) Connect the power supply of the DVK90109.
Important Note: The supply must be between 6 to 9 Volts DC. Higher voltage may damage permanently the
DVK90109 circuit.
Microelectronlc Integrated eyelems
DVK90109
125kHz RFID Development Kit
User Manual
390129010902 Page 4 of 13 Development Kit
Rev. 002 Apr-2008
3 Digital communication EVB90109 - DVKRFID
The microcontroller on the DVKRFID board communicates with the EVB90109 through a 10 pins connector.
Transponder EVB90109
CONNECTOR
DVKRFID
(microcontroller)
RS232
DVK90109
RFID
The picture and the table below describe all connections between the EVB90109 and the DVKRFID board.
{
EVB90109 DVKRFID
10 pins
connector
Vcc
Ground
Coil
Speed
Mode
Modu
ModuR2
ModuR3
DataIn
ClockIn
Name Function Direction Comment
Vcc Supply voltage for the EVB90109 DVK -> EVB
GND Ground connection for the EVB90109 DVK -> EVB
Speed Data rate selection: GND = 4kBaud, Vcc = 2kBaud DVK -> EVB
Mode Decoding selection: GND = Biphase, Vcc = Manchester DVK -> EVB
Modu Power down mode DVK -> EVB NOT USED
ModuR2 Antenna voltage control: GND = Field ON, Vcc = Field OFF DVK -> EVB
ModuR3 - DVK -> EVB NOT USED
DataIn Data Ouput EVB -> DVK
ClockIn Clock Ouput EVB -> DVK
DataIn and ClockIn will be
internally pulled-up by the
microcontroller.
Coil Oscillator output EVB -> DVK
Microelectronlc Integrated eyelems
DVK90109
125kHz RFID Development Kit
User Manual
390129010902 Page 5 of 13 Development Kit
Rev. 002 Apr-2008
4 Digital communication DVKRFID – PC
The DVK90109 board communicates with a PC through a serial interface RS232.
Transponder EVB90109
CONNECTOR
DVKRFID
(microcontroller)
RS232
DVK90109
RFID
This part specifies a dedicated set of commands useful for the operation with the MLX90109 RFID transceiver
IC.
This instruction set is defined for the development kit DVK90109.
The microcontroller ensures the following functions:
o Control and configure the MLX90109 transceiver
o Read the data information from the MLX90109 transceiver (on-chip decoding)
o Communicate with a PC through the serial connection RS232.
4.1 Protocol assignment
The different commands are based on a Mnemonic assignment defined by three ASCII characters forming the
Operation Code, followed by a specific number of ASCII or Hexadecimal parameters, depending on the type of
the command.
OP CODE : 3 ASCII characters
PARAMETERS : ASCII characters or
Hexadecimal characters
The syntax of a command is typically: OpCode<Parameter1>,<Parameter2>,<Parameter3>,…
Each parameter should be separated by a comma.
4.2 List of instructions
Operation Syntax Function
VERsion VER↵ Get the firmware version for the microcontroller
SeT Field STF<On/Off>↵ Set the field ON or OFF
ConFiGuration CFG<Encoding>,<Datarate>↵ Set the type of current transponder with the encoding method and the data
rate used by the Transponder
HEAder HEA<Header>,<Nbr Significant bit>↵ Define the header to read the Identification code (ID)
REAd Tag REA<Op mode>↵ Perform a read operation and decode data with the encoding method of
the transponder defined with the <Op mode> parameter
WRIte Tag WRI,<data>,<address>↵ Perform a write operation with 100% modulation for Q5 tag
SELect Tag SEL↵ Select a Hitag1 tag by sending an UID request then a select command.
Return UID and configuration page
ReaD Hitag1 RDH,<command>,<address>↵ Perform a read operation and decode data with the encoding method of
the transponder Hitag1
MeleXIe
Microelectronlc Integrated eyelems
DVK90109
125kHz RFID Development Kit
User Manual
390129010902 Page 6 of 13 Development Kit
Rev. 002 Apr-2008
WRite Hitag1 WRH,<command>,<address>,<data>↵ Perform a write operation for Hiatg1 tag with the data defined in the <data>
parameter
Note: Be careful that a value is necessary in all fields defined by the instruction. The default value defined in the
following instruction set is only the value set by the program during the initialization phase. This means that if the
CFG instruction is not sent, the <Encoding> and <Baudrate> fields will take default values being respectively
biphase and 4kbit/s.
4.3 Error Instruction
No Name Meaning Message
0 Instruction error If the Opcode syntax is not correct or not defined.
err0↵
1 Definition error If the definition syntax is not correct.
err1↵
2 No tag detected If no transponder has been detected.
err2↵
3 Header not found If the header cannot be found in the read code.
err3
5 Read operation failed If the calculated CRC or parity check doesn’t correspond to the read value. err5↵
6 Others error err6↵
8 Measure Frequency Antenna If a problem occurs during antenna frequency measurement (value too high, no
signal …)
err8↵
4.4 Instructions set
4.4.1 Version (VER)
Get the firmware version.
This command can be used to control the serial connection RS232.
Syntax VER↵
Return Melexis RFID <Development kit> V<Version>
Example VER↵
Reply: Melexis RFID DVK90109 V2.0
4.4.2 Set Field (STF)
Set the magnetic field ON or OFF.
Syntax STF<on/off>↵
<on/off> = Characters defining the current state of the field (<on> to put the field ON and <off> to put the field OFF).
Default value: <on>.
Return Ok
Example STFon↵
Reply: Ok
MeleXIe
Microelectronlc Integrated eyelems
Example:
0019—9099
DVK90109
125kHz RFID Development Kit
User Manual
390129010902 Page 7 of 13 Development Kit
Rev. 002 Apr-2008
4.4.3 Configuration of the MLX90109 (CFG)
Set the configuration of the transceiver to decode data information from a transponder (encoding mode and data
rate).
Syntax CFG<Encoding>,<Datarate>↵
<Encoding> = ASCII letter specifying the encoding method used by the Transponder (<M> for Manchester and <B> for
Biphase). Default value: <B>.
<Datarate> = ASCII number specifying the data rate used by the transponder (<2> for 2kbits/s, <4> for 4kbits/s). Default
value: <4>.
Return Ok
Example CFGB,4↵
Reply: Ok
4.4.4 HEA : HEAder
Specify the header of the data sent by the transponder.
The program will search for the header in the data read from the transponder and display the data with the
header first.
The header is a number of bits that cannot be reproduced in the rest of the ID. For example in the standard norm
ISO11784, the first 11 bits of the ID code will be used as the header and fixed to “0000 0000 001”.
Syntax HEA<Header>,<Nbr significant bit>↵
<Header> = Hexadecimal number defining the header.
<Nbr unused bit> = Hexadecimal number defining the number of Header bits to be removed (mustn’t be higher than 7).
Return Ok <Header in binary>
Example HEA0020,5↵
Reply: Ok 00000000001
HEA002010,7↵
Reply: Ok 00000000001000000
Example: The header is calculated with two parameters. <Header> defining the header in hexadecimal (an entire
number of byte is necessary) and <Nbr Of Unused bit> a decimal number defining the number of bits which are
to be removed from the given Header to form the new Header. Thus, it is possible to define a length of header
different of a power of 2.
HEA0020,5 = 0000 0000 0010 0000 = 0000 0000 001
4.4.5 REA : REAd
Read, decode and return data from a transponder.
If a problem occurs during operation (no header found, no transponder), an error message will be displayed as
referenced in the table 1.3 Error Instruction.
Syntax REA<Opmode>,<Nbr of bit>↵
<Opmode> = Number defining the programmed decoding method used.
o <1> Searches for the header, decodes ISO11784 mode, controls CRC value and displays the decoded data.
MeleXIe
Microelectronlc Integrated eyelems
07d
DVK90109
125kHz RFID Development Kit
User Manual
390129010902 Page 8 of 13 Development Kit
Rev. 002 Apr-2008
o <2> Searches for the header, decodes Melexis 88bits mode, controls CRC value and displays decoded data.
o <3> Searches for the header and displays the data read.
o <4> Only displays the data read (no decoding, no search for the header).
<Nbr of bit> = ASCII number specifying the number of bit read. <064>, <128>, <144> and <256> are implemented.
Return <data>
err2 (no tag detected)
err3 (no header found)
err5 (read failed)
Example REA1,128↵
Read 128bits, searches for the header and decodes the ID read according to the standard norm ISO11784. Checks the
CRC and returns corresponding message (data read or error).
REA2,128↵
Read 128bits, searches for the header and decodes the ID read according to the Melexis 88 bits encoding method.
Checks the CRC and returns corresponding message (data read or error).
REA3,064↵
Read 64bits, searches for the header and returns corresponding message (data read or error).
REA4,256↵
Reads and displays 256bits.
Note: The ISO11784/85 standard norm and the Melexis 88bits encoding method will be only performed on 128
bits read. So in these two mode (opmode <1> and <2>) the field <Nbr of bit> will be ignored and 128bits will be
always read.
Note: REA command will not set the field of the EVB90109. Before performing a read operation, the field must
be ON by using the STFon command.
4.4.6 WRI : Write Q5 tag
Write data in the Q5 tag memory.
This function will use the 100% modulation (please refer to the application note “100% modulation (On-Off
Keying)”) to write data according to Q5 tag communication protocol.
An “Ok” will confirm the success of the operation.
Syntax WRI,<data>,<address>↵
<data> = 4 bytes data (hexadecimal value) <MSB…LSB>.
<address> = 1 bytes address of the Q5 memory (hexadecimal value).
Return Ok
Err2↵ (no tag detected)
Example WRI,00AA00BB,07↵
Write data 0x00, 0xAA, 0x00 and 0xBB into the block 7 of the Q5 memory
Ok>
Note: WRI command will not set the field of the EVB90109. Before performing a read operation, the field must be
ON by using the STFon command.
MeleXIe
Microelectronlc Integrated eyelems
Lfi-l
10d
DVK90109
125kHz RFID Development Kit
User Manual
390129010902 Page 9 of 13 Development Kit
Rev. 002 Apr-2008
4.4.7 SEL : Select tag Hitag1
Select the tag Hitag1 in the field by sending a Set_CC and a SELECT command.
This function will use the 100% modulation (please refer to the application note “100% modulation (On-Off
Keying)”) to select the tag according to Hitag1 communication protocol. The tag answer with its UID and its
configuration page
The command SEL will return the UID and the configuration page in case of success of the operation.
Syntax SEL↵
Return UID: Unique tag identifier
Configuration page: configuration of the tag (encoding, data rate, security features…)
Err2↵ (no tag detected)
Example SEL↵
UID = 7972C535 / Configuration page = FF370000>
Note: SEL command will not set the field of the EVB90109. Before performing a read operation, the field must be
ON by using the STFon command.
4.4.8 RDH : Read Hitag1 memory
Read an area of the Hitag1 memory.
This function will use the 100% modulation (please refer to the application note “100% modulation (On-Off
Keying)”) to send the selected command and will decode the data sent by the tag according to the Hitag1
communication protocol.
The command RDH will return the data requested in case of success of the operation.
Syntax RDH,<command>,<address>↵
<command> = 4 bits (binary value) corresponding to the command (refer to Hitag1 specification).
<address> = 1 byte address (hexadecimal value)
Return Data : size depends of the type of command and the address used
Err2↵ (no tag detected)
Example RDH,1101,10↵
Data received = AABBCCDD……..>
Note: SEL command has to be sent before performing a read operation.
4.4.9 WRH : Write Hitag1 memory
Write an area of the Hitag1 memory.
This function will use the 100% modulation (please refer to the application note “100% modulation (On-Off
Keying)”) to send the selected command and the selected data according to the Hitag1 communication protocol.
The command WRH will return a confirmation sentence in case of success of the operation.
Syntax RDH,<command>,<address>,<data>↵
<command> = 4 bits (binary value) corresponding to the command (refer to Hitag1 specification).
<address> = 1 byte address (hexadecimal value)
<data> = 4 bytes data to write in the Hitag1 memory
Return Confirmation sentence
MeleXIe
Microelectronlc Integrated eyelems
DVK90109
125kHz RFID Development Kit
User Manual
390129010902 Page 10 of 13 Development Kit
Rev. 002 Apr-2008
Err2↵ (no tag detected)
Example WRH,1000,10,AAABBCCDD↵
4 bytes data AABBCCDD written at address 10>
Note: SEL command has to be sent before performing a read operation.
MeleXIe
Mlcroelectronlc Integrated eyelems
DVK90109
125kHz RFID Development Kit
User Manual
390129010902 Page 11 of 13 Development Kit
Rev. 002 Apr-2008
5 Melexis RS232 interface program
The RS232 interface program is a easy-to-use windows software developed by Melexis to send
commands through the RS232 interface of a Pc.
The RS232 interface program uses text files to generate the set of commands and is able to control
the COM port of the Pc (COM 1 or 2 can be chosen) and to send the corresponding commands
through it.
5.1 Start RS232 interface:
Double click on RS232.exe file. The following interface window will be displayed.
5.2 Select serial communication port COM
Click on “setupcom” button. On the new window displayed, choose “br9600” on COM1-2. Close the
new window by clicking on the top right corner. The speed communication is now validated at 9600
bit/s.
5.3 Open serial communication port
Click on “OpenCom1” button. This will open the corresponding communication port (COM1-2).
5.4 Generates commands file
The RS 232 program uses a text file which contains all commands. All commands must be defined
like specified below.
Baud rate selection
Open/Close serial communication
Select commands file
To close the interface window
Toggle between a single execution and repetitive command
execution (click in the command column
after toggling)
Reply
window
(reply from the
DVK90109 will be displayed in
this window)
Error message window
Main window (command list and
comments will be displayed in this
window)
MeleXIe
Mlcroelectronlc Integrated eyelems
devkltiznnmiandesxxt , NntEDad
van vers'lun /
srm : Set Hem on
SI'FF Sgt 1‘1er UFf
Melex
Mmmnsmmm n Bnmn, mu; ‘
Mmmnscmmm n um... 2m
Mwmnscmmm‘ m an»; mm
mm mm.
sum and umunm
smukmum m
ammmsmmm mum
mm .. mn‘
damn "m hg‘
mm mm rum
Hemnummmu
DVK90109
125kHz RFID Development Kit
User Manual
390129010902 Page 12 of 13 Development Kit
Rev. 002 Apr-2008
5.5 Select commands file
Click on “ReadFilecom1” button. On the new displayed windows, find the text file which contains the
command list (MLX-Programmer.txt is available together with RS232.exe) and double click on it.
This file will be displayed on the left table of the interface window. On the left column, several lines of
commands are displayed with some comments on the right column like shown in the picture below.
5.6 Send a command
To send a command, double click on it and the response will be displayed in the “ResultCom” window.
Command Some spaces character
:
introduce a comment line. It must be always
followed by a space character.
MeleXIe
Mlcroelectronlc Integrated eyelems
DVK90109
125kHz RFID Development Kit
User Manual
390129010902 Page 13 of 13 Development Kit
Rev. 002 Apr-2008
6 Disclaimer
Devices sold by Melexis are covered by the warranty and patent indemnification provisions appearing
in its Term of Sale. Melexis makes no warranty, express, statutory, implied, or by description regarding
the information set forth herein or regarding the freedom of the described devices from patent
infringement. Melexis reserves the right to change specifications and prices at any time and without
notice. Therefore, prior to designing this product into a system, it is necessary to check with Melexis for
current information. This product is intended for use in normal commercial applications. Applications
requiring extended temperature range, unusual environmental requirements, or high reliability
applications, such as military, medical life-support or life-sustaining equipment are specifically not
recommended without additional processing by Melexis for each application.
The information furnished by Melexis is believed to be correct and accurate. However, Melexis shall
not be liable to recipient or any third party for any damages, including but not limited to personal injury,
property damage, loss of profits, loss of use, interrupt of business or indirect, special incidental or
consequential damages, of any kind, in connection with or arising out of the furnishing, performance or
use of the technical data herein. No obligation or liability to recipient or any third party shall arise or
flow out of Melexis’ rendering of technical or other services.
© 2004 Melexis NV. All rights reserved.
For the latest version of this document, go to our website at
www.melexis.com
Or for additional information contact Melexis Direct:
Europe and Japan: All other locations:
Phone: +32 1367 0495 Phone: +1 603 223 2362
E-mail: sales_europe@melexis.com E-mail: sales_usa@melexis.com
ISO/TS 16949 and ISO14001 Certified