Microchip Technology 的 PIC24F04KA20x Prog Spec 规格书
6‘
MICROCHIP
2010 Microchip Technology Inc. DS39991A-page 1
PIC24FXXKA2XX
1.0 DEVICE OVERVIEW
This document defines the programming specifications
for the PIC24FXXKA2XX family of 16-bit micro-
controller devices. This is required only for developing
programming support for the PIC24FXXKA2XX family.
Users of any one of these devices should use the
development tools that are already supporting the
device programming.
The programming specifications are specific to the
following devices:
• PIC24F04KA200
• PIC24F04KA201
2.0 PROGRAMMING OVERVIEW
OF THE PIC24FXXKA2XX
FAMILY
PIC24FXXKA2XX family devices are programmed
exclusively using In-Circuit Serial Programming™
(ICSP™). This method provides native, low-level pro-
gramming capability to erase, program and verify the
device. Section 3.0 “ICSP Programming” describes
the ICSP method.
2.1 Power Requirements
All devices in the PIC24FXXKA2XX family are
3.3V supply designs. The core, the peripherals and the
I/O pins operate at 3.3V. The device can operate from
1.8V to 3.6V.
Table 2-1 provides the pins that are required for
programming, which are indicated in Figure 2-1. Refer
to the device data sheet for complete pin descriptions.
TABLE 2-1: PIN DESCRIPTIONS (DURING PROGRAMMING)
Note: Unlike other PIC24F devices,
PIC24FXXKA2XX devices do not support
Enhanced ICSP programming. These
devices also do not support in-circuit
debugging over the ICSP interface.
Pin Name During Programming
Pin Name Pin Type Pin Description
MCLR/VPP MCLR/VPP P Programming Enable
VDD VDD P Power Supply
VSS VSS PGround
PGCx PGC I Programming Pin Pair: Serial Clock
PGDx PGD I/O Programming Pin Pair: Serial Data
Legend: I = Input, O = Output, P = Power
PIC24FXXKA2XX Flash Programming Specifications
jjjjjjj
333333333]
EEEEEEE
EEEEEEEEEE
PIC24FXXKA2XX
DS39991A-page 2 2010 Microchip Technology Inc.
FIGURE 2-1: PIC24FXXKA2XX PIN DIAGRAMS
PIC24XXKA201
1
2
3
4
5
6
7
8
9
10
20
19
18
17
16
15
14
13
12
11
20-Pin SPDIP, SOIC
MCLR/VPP
PGC2
PGD2
PGC3
PGD3
VDD
VSS
1
2
3
4
5
6
7
14
13
12
11
10
9
8
14-Pin SPDIP, SOIC
MCLR/VPP
PGC2
PGD2
PGC3
PGD3
VDD
VSS
PIC24F04KA200
89
2
3
1
12
13
14
15
106
11
1617181920
7
PIC24F04KA201
5
4
MCLR/VPP
PGC2
PGD2
VDD
VSS
PGC3
PGD3
20-Pin QFN
2010 Microchip Technology Inc. DS39991A-page 3
PIC24FXXKA2XX
2.2 Memory Map
The program memory map extends from 000000h to
FFFFFEh. Code storage is located at the base of the
memory map, and supports up to about 1.38 K words
of instructions (about 4 Kbytes). Figure 2-2 depicts the
memory map.
Table 2-2 provides the program memory size and
number of program memory rows present in each
device variant.
The erase operation can be done on one word, half of
a row or one row at a time. The program operation can
be done only one word at a time.
The device Configuration registers are implemented
from location, F80000h to F80010h, and can be erased
or programmed one register at a time. Table 2-3 pro-
vides the implemented Configuration registers and
their locations.
Locations, FF0000h and FF0002h, are reserved for the
Device ID registers. These bits can be used by the
programmer to identify the device type that is being
programmed. See Section 4.0 “Device ID” for more
information. The Device ID registers read out normally
even after code protection is applied.
TABLE 2-2: PROGRAM MEMORY SIZES
TABLE 2-3: CONFIGURATION REGISTER
LOCATIONS
FIGURE 2-2: PROGRAM MEMORY MAP
Device Program Memory
Upper Address
(Instruction Words) Rows
PIC24F04KA200 AFEh (1.375K) 44
PIC24F04KA201
Configuration Register Address
FGS F80004
FOSCSEL F80006
FOSC F80008
FWDT F8000A
FPOR F8000C
FICD F8000E
FDS F80010
000000h
Code Memory
Configuration Memory
Space
(2816 x 24-bit)
800000h
Device ID FEFFFEh
FF0000h
FFFFFEh
Reserved
Reserved
8007F0h
FF0002h
FF0004h
Reserved
(2 x 16-bit)
User Flash
8007EEh
Configuration Registers F80010h
F80000h
Diagnostic Words
800800h
8007FEh
000AFEh
User Memory
Space
Reserved
PIC24FXXKA2XX
DS39991A-page 4 2010 Microchip Technology Inc.
3.0 ICSP PROGRAMMING
The ICSP method is a special programming protocol
that allows reading and writing to the PIC24FXXKA2XX
device family memory. This is accomplished by apply-
ing control codes and instructions, serially to the
device, using PGCx and PGDx pins.
In ICSP mode, the system clock is taken from the
PGCx pin, regardless of the device‘s oscillator
Configuration bits. All of the instructions are shifted
serially to an internal buffer, loaded into the Instruction
Register (IR) and then executed. No program is fetched
from the internal memory. Instructions are fed in 24 bits
at a time. PGDx is used to shift data in, and PGCx is
used as both the serial shift clock and the CPU
execution clock.
3.1 Overview of the Programming
Process
Figure 3-1 illustrates the high-level overview of the
programming process.
After entering the ICSP mode, perform the following:
1. Bulk Erase the device.
2. Program and verify the code memory.
3. Program and verify the device configuration.
4. Program the code-protect Configuration bits if
required.
3.2 ICSP Operation
Upon entry into ICSP mode, the CPU is Idle. An
internal state machine governs the execution of the
CPU. A 4-bit control code is clocked in, using PGCx
and PGDx, and this control code is used to command
the CPU (see Table 3-1).
The SIX control code is used to send instructions to the
CPU for execution, and the REGOUT control code is
used to read data out of the device via the VISI register.
FIGURE 3-1: HIGH–LEVEL ICSP™
PROGRAMMING FLOW
TABLE 3-1: CPU CONTROL CODES IN
ICSP™ MODE
Note: During ICSP operation, the operating
frequency of PGCx should not exceed
8MHz.
4-Bit
Control Code Mnemonic Description
0000 SIX Shift in 24-bit instruction
and execute.
0001 REGOUT Shift out the VISI
(0784h) register.
0010-1111 N/A This is reserved.
Start
Perform Bulk
Erase
Program Memory
Verify Program
End
Enter ICSP™ Mode
Program Configuration Bits
Verify Configuration Bits
Exit ICSP Mode
2010 Microchip Technology Inc. DS39991A-page 5
PIC24FXXKA2XX
3.2.1 SIX SERIAL INSTRUCTION
EXECUTION
The SIX control code allows execution of
PIC24FXXKA2XX family assembly instructions. When
the SIX code is received, the CPU is suspended for
24 clock cycles as the instruction is then clocked into the
internal buffer. Once the instruction is shifted in, the state
machine allows it to be executed over the next four PGC
clock cycles. While the received instruction is executed,
the state machine simultaneously shifts in the next 4-bit
command (see Figure 3-2).
Coming out of Reset, the first 4-bit control code is
always forced to SIX and a forced NOP instruction is
executed by the CPU. Five additional PGCx clocks are
needed on start-up; thereby, resulting in a 9-bit SIX
command, instead of the normal 4-bit SIX command.
After the forced SIX is clocked in, the ICSP operation
resumes to normal. That is, the next 24 clock cycles
load the first instruction word to the CPU.
3.2.1.1 Differences Between SIX Instruction
Execution and Normal Instruction
Execution
There are some differences between executing
instructions using the SIX ICSP command and normal
device instruction execution. As a result, the code
examples in this specification might not match those
required to perform the same operations during normal
device operation.
The differences are:
• Two-word instructions require 2 SIX operations to
clock in all the necessary data.
Examples of two-word instructions are: GOTO and
CALL.
• Two-cycle instructions require 2 SIX operations to
complete. The first SIX operation shifts in the
instruction and begins to execute it. A second SIX
operation, which should shift in a NOP to avoid
losing data, allows the CPU clocks required to
finish executing the instruction.
Examples of two-cycle instructions are table read
and table write instructions.
• The CPU does not automatically stall to account
for pipeline changes. A CPU stall occurs when an
instruction modifies a register, which is used by
the instruction immediately following the CPU stall
for Indirect Addressing. During normal operation,
the CPU forces a NOP while the new data is read.
To account for this, while using ICSP, any indirect
references to a recently modified register should
be proceeded with a NOP.
For example, MOV #0x0,W0 followed by MOV
[W0],W1 must have a NOP inserted in between.
If a two-cycle instruction modifies a register, which
is used indirectly, it requires two following NOPs;
one to execute the second half of the instruction
and the other to stall the CPU to correct the
pipeline.
For example, TBLWTL [W0++],[W1] should be
followed by 2 NOPs.
• The device Program Counter (PC) continues to
automatically increment during the ICSP
instruction execution, even though the Flash
memory is not being used. As a result, it is
possible for the PC to be incremented so that it
points to invalid memory locations.
Examples of invalid memory spaces are
unimplemented Flash addresses or the vector
space (location 0x0 to 0x1FF).
If the PC ever points to these locations, it causes
the device to reset, possibly interrupting the ICSP
operation. To prevent this, instructions should be
periodically executed to reset the PC to a safe
space. The optimal method of achieving this is to
perform a “GOTO 0x200”.
3.2.2 REGOUT SERIAL INSTRUCTION
EXECUTION
The REGOUT control code allows for the data to be
extracted from the device in the ICSP mode. It is used
to clock the contents of the VISI register out of the
device over the PGDx pin. After the REGOUT control
code is received, the CPU is held Idle for 8 cycles. After
this, an additional 16 cycles are required to clock the
data out (see Figure 3-3).
The REGOUT code is unique as the PGDx pin is an input
when the control code is transmitted to the device.
However, after the control code is processed, the
PGDx pin becomes an output as the VISI register is
shifted out.
Note: To account for this forced NOP, all example
codes in this specification begin with a
NOP to ensure that no data is lost.
Note 1: After the contents of VISI are shifted out,
the PIC24FXXKA2XX devices maintain
PGDx as an output until the first rising
edge of the next clock is received.
2: Data changes on the falling edge and
latches on the rising edge of PGCx. For
all data transmissions, the Least
Significant bit (LSb) is transmitted first.
“PAA‘
PIC24FXXKA2XX
DS39991A-page 6 2010 Microchip Technology Inc.
FIGURE 3-2: SIX SERIAL EXECUTION
FIGURE 3-3: REGOUT SERIAL EXECUTION
P4
23 123 2324 1 2 3 4
P1
PGCx
P4A
PGDx
24-Bit Instruction Fetch
Execute PC – 1,
16
0000
Fetch SIX
456 78 181920212217
LSB X X X X X X X X X X X X X X MSB
PGDx = Input
P2
P3
P1B
P1A
78 9
0000000
Only for
Program
Memory Entry
Control Code
4 5
Execute 24-Bit
Instruction, Fetch
Next Control Code
00
1234 1278
PGCx
P4
PGDx
PGDx = Input
Execute Previous Instruction, CPU Held in Idle Shift Out VISI Register<15:0>
P5
PGDx = Output
123 1234
P4A
11 13 15 161412
No Execution Takes Place,
Fetch Next Control Code
00000
PGDx = Input
MSb
1234
1
456
LSb
141312
... 11100
Fetch REGOUT Control Code
0
2010 Microchip Technology Inc. DS39991A-page 7
PIC24FXXKA2XX
3.3 Entering ICSP Mode
3.3.1 LOW-VOLTAGE ICSP ENTRY
As illustrated in Figure 3-4, the following processes are
involved in entering ICSP Program/Verify mode using
MCLR:
1. MCLR is briefly driven high, then low.
2. A 32-bit key sequence is clocked into PGDx.
3. MCLR is then driven high within a specified
period of time and held.
The programming voltage, VIH, is applied to MCLR; this
is VDD in the case of PIC24FXXKA2XX devices. There
is no minimum time requirement for holding at VIH.
After VIH is removed, an interval of at least P18 must
elapse before presenting the key sequence on PGDx.
The key sequence is a specific 32-bit pattern:
‘0100 1101 0100 0011 0100 1000 0101
0001‘ (more easily remembered as 4D434851h in
hexadecimal). The device will enter Program/Verify
mode only if the sequence is valid. The Most Significant
bit (MSb) of the most significant nibble must be shifted in
first.
Once the key sequence is complete, VIH must be
applied to MCLR and held at that level for as long as
the Program/Verify mode is to be maintained. An
interval of at least P19 and P7 must elapse before
presenting data on PGDx. Signals appearing on PGCx
before P7 has elapsed would not be interpreted as
valid.
3.3.2 HIGH-VOLTAGE ICSP ENTRY
Entering the ICSP Program/Verify mode, using the VPP
pin is the same as entering the mode using MCLR. The
only difference is the programming voltage applied to
VPP is VIHH, and before presenting the key sequence
on PGDx, an interval of at least P18 should elapse (see
Figure 3-5).
Once the key sequence is complete, an interval of at
least P7 should elapse, and the voltage should remain
at VIHH. The voltage, VIHH, must be held at that level for
as long as the Program/Verify mode is to be main-
tained. An interval of at least P7 must elapse before
presenting the data on PGDx.
Signals appearing on PGDx before P7 has elapsed will
not be interpreted as valid.
Upon a successful entry, the program memory can be
accessed and programmed in serial fashion. While in
ICSP mode, all unused I/Os are placed in a
high-impedance state.
FIGURE 3-4: ENTERING ICSP™ MODE USING LOW-VOLTAGE ENTRY
FIGURE 3-5: ENTERING ICSP™ MODE USING HIGH-VOLTAGE ENTRY
MCLR
PGDx
PGCx
VDD
P6 P14
b31 b30 b29 b28 b27 b2 b1 b0b3
...
Program/Verify Entry Code = 4D434851h
P1A
P1B
P18
P19
0100 0 0
P7
VIH VIH
1
0
1
VPP
PGDx
PGCx
VDD
P6
b31 b30 b29 b28 b27 b2 b1 b0b3
...
Program/Verify Entry Code = 4D434851h
P1A
P1B
P18
0100 0 01
0
1
VIHH
VIH
P7
PIC24FXXKA2XX
DS39991A-page 8 2010 Microchip Technology Inc.
3.4 Flash Memory Programming in
ICSP Mode
3.4.1 PROGRAMMING OPERATIONS
The NVMCON register controls the Flash memory write
and erase operations. To program the device, set the
NVMCON register to select the type of erase operation
(see Table 3-2) or write operation (see Table 3-3). Set
the WR control bit (NVMCON<15>) to initiate the
program.
In ICSP mode, all programming operations are
self-timed. There is an internal delay between setting and
automatic clearing of the WR control bit when the
programming operation is complete. Refer to
Section 5.0 “AC/DC Characteristics and Timing
Requirements” for information on the delays associated
with various programming operations.
3.4.2 STARTING AND STOPPING A
PROGRAMMING CYCLE
The WR bit (NVMCON<15>) is used to start an erase
or write cycle. Initiate the programming cycle by setting
the WR bit.
All erase and write cycles are self-timed. The WR bit
should be polled to determine if the erase or write cycle
is completed. Start a programming cycle as follows:
BSET NVMCON, #WR
TABLE 3-3: NVMCON VALUES FOR
WRITE OPERATIONS
TABLE 3-2: NVMCON VALUES FOR
ERASE OPERATIONS
NVMCON
Value Erase Operation
4064h Erase the code memory and
Configuration registers (does not erase
programming executive code and
Device ID registers).
404Ch Erase the general segment and
Configuration bits associated with it.
4068h Erase the boot segment and
Configuration bits associated with it.
405Ah(1) Erase four rows of code memory.
4059h(1) Erase two rows of code memory.
4058h(1) Erase a row of code memory.
4054h Erase all the Configuration registers
(except the code-protect fuses).
4058h(1) Erase Configuration registers except
FBS and FGS.
Note 1: The destination address decides the
region (code memory or Configuration
register) of the erased rows/words.
NVMCON
Value Write Operation
4004h(1) Write one Configuration register.
4004h(1) Program one row (32 instruction words)
of code memory or executive memory.
Note 1: The destination address decides the
region (code memory or Configuration
register) of the erased rows/words.
2010 Microchip Technology Inc. DS39991A-page 9
PIC24FXXKA2XX
3.5 Erasing Program Memory
To erase the program memory (all of code memory,
data memory and Configuration bits, including the
code-protect bits), set the NVMCON to 4064h and then
execute the programming cycle.
Figure 3-6 illustrates the ICSP programming process
for Bulk Erase. This process includes the ICSP
command code, which must be transmitted (for each
instruction), LSB first, using the PGCx and PGDx pins
(see Figure 3-2).
Table 3-4 provides the steps for executing serial
instruction for the Bulk Erase mode.
FIGURE 3-6: BULK ERASE FLOW
TABLE 3-4: SERIAL INSTRUCTION EXECUTION FOR CHIP ERASE
Note: Program memory must be erased before
writing any data to program memory.
End
Set the WR bit to Initiate Erase
Write 4064h to NVMCON SFR
Delay P11 + P10 Time
Start
Command
(Binary) Data
(Hex) Description
Step 1: Exit the Reset vector.
0000
0000
0000
000000
040200
000000
NOP
GOTO 0x200
NOP
Step 2: Set the NVMCON to erase the entire program memory.
0000
0000
24064A
883B0A
MOV #0x4064, W10
MOV W10, NVMCON
Step 3: Set the TBLPAG and perform dummy table write to select the erased memory.
0000
0000
0000
0000
0000
0000
200000
880190
200000
BB0800
000000
000000
MOV #<PAGEVAL>, W0
MOV W0, TBLPAG
MOV #0x0000, W0
TBLWTL W0, [W0]
NOP
NOP
Step 4: Initiate the erase cycle.
0000
0000
0000
A8E761
000000
000000
BSET NVMCON, #WR
NOP
NOP
Step 5: Repeat this step to poll the WR bit (bit 15 of NVMCON) until it is cleared by the hardware.
0000
0000
0000
0000
0000
0000
0001
0000
000000
040200
000000
803B02
883C22
000000
<VISI>
000000
NOP
GOTO 0x200
NOP
MOV NVMCON, W2
MOV W2, VISI
NOP
Clock out the contents of the VISI register.
NOP
PIC24FXXKA2XX
DS39991A-page 10 2010 Microchip Technology Inc.
3.6 Writing Code Memory
The procedure for writing code memory is the same as
writing the Configuration registers. The difference is
that the 32 instruction words are programmed one at a
time. To facilitate this operation, working registers,
W0:W5, are used as temporary holding registers for the
data to be programmed. Figure 3-8 illustrates the code
memory writing flow.
Table 3-5 provides the ICSP programming details,
including the serial pattern with the ICSP command
code, which must be transmitted, LSB first, using the
PGCx and PGDx pins (see Figure 3-2).
In Step 1 of Table 3-5, the Reset vector is exited. In
Step 2, the NVMCON register is initialized for
programming a full row of code memory. In Step 3, the
24-bit starting destination address for programming is
loaded into the TBLPAG register and W7 register. The
upper byte of the starting destination address is stored
in TBLPAG and the lower 16 bits of the destination
address are stored in W7.
To minimize the programming time, a packed
instruction format is used (see Figure 3-7).
In Step 4 of Table 3-5, four packed instruction words
are stored in working registers, W0:W5, using the MOV
instruction; the Read Pointer, W6, is initialized.
Figure 3-7 illustrates the contents of W0:W5 holding
the packed instruction word data. In Step 5, eight
TBLWT instructions are used to copy the data from
W0:W5 to the write latches of the code memory. Since
code memory is programmed 32 instruction words at a
time, Steps 3 to 5 are repeated eight times to load all
the write latches (see Step 6).
After the write latches are loaded, initiate programming
by writing to the NVMCON register in Steps 7 and 8. In
Step 9, the internal PC is reset to 200h. This is a
precautionary measure to prevent the PC from
incrementing to unimplemented memory when large
devices are being programmed. Finally, in Step 10,
repeat Steps 3 through 9 until all of the code memory is
programmed.
FIGURE 3-7: PACKED INSTRUCTION
WORDS IN W0:W5
15 8 7 0
W0 LSW0
W1 MSB1 MSB0
W2 LSW1
W3 LSW2
W4 MSB3 MSB2
W5 LSW3
TABLE 3-5: SERIAL INSTRUCTION EXECUTION FOR WRITING CODE MEMORY
Command
(Binary) Data
(Hex) Description
Step 1: Exit the Reset vector.
0000
0000
0000
000000
040200
000000
NOP
GOTO 0x200
NOP
Step 2: Set the NVMCON to program 32 instruction words.
0000
0000
24004A
883B0A
MOV #0x4004, W10
MOV W10, NVMCON
Step 3: Initialize the Write Pointer (W7) for TBLWT instruction.
0000
0000
0000
200xx0
880190
2xxxx7
MOV #<DestinationAddress23:16>, W0
MOV W0, TBLPAG
MOV #<DestinationAddress15:0>, W7
2010 Microchip Technology Inc. DS39991A-page 11
PIC24FXXKA2XX
Step 4: Load W0:W5 with the next 4 instruction words to program.
0000
0000
0000
0000
0000
0000
2xxxx0
2xxxx1
2xxxx2
2xxxx3
2xxxx4
2xxxx5
MOV #<LSW0>, W0
MOV #<MSB1:MSB0>, W1
MOV #<LSW1>, W2
MOV #<LSW2>, W3
MOV #<MSB3:MSB2>, W4
MOV #<LSW3>, W5
Step 5: Set the Read Pointer (W6) and load the (next set of) write latches.
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
0000
EB0300
000000
BB0BB6
000000
000000
BBDBB6
000000
000000
BBEBB6
000000
000000
BB1BB6
000000
000000
BB0BB6
000000
000000
BBDBB6
000000
000000
BBEBB6
000000
000000
BB1BB6
000000
000000
CLR W6
NOP
TBLWTL [W6++], [W7]
NOP
NOP
TBLWTH.B [W6++], [W7++]
NOP
NOP
TBLWTH.B [W6++], [++W7]
NOP
NOP
TBLWTL [W6++], [W7++]
NOP
NOP
TBLWTL [W6++], [W7]
NOP
NOP
TBLWTH.B [W6++], [W7++]
NOP
NOP
TBLWTH.B [W6++], [++W7]
NOP
NOP
TBLWTL [W6++], [W7++]
NOP
NOP
Step 6: Repeat Steps 3 though 5, eight times, to load the write latches for 32 instructions.
Step 7: Initiate the write cycle.
0000
0000
0000
A8E761
000000
000000
BSET NVMCON, #WR
NOP
NOP
Step 8: Repeat this step to poll the WR bit (bit 15 of NVMCON) until it is cleared by the hardware.
0000
0000
0000
0000
0000
0001
0000
040200
000000
803B02
883C22
000000
<VISI>
000000
GOTO 0x200
NOP
MOV NVMCON, W2
MOV W2, VISI
NOP
Clock out contents of the VISI register.
NOP
Step 9: Reset device internal PC.
0000
0000
040200
000000
GOTO 0x200
NOP
Step 10: Repeat Steps 3 through 9 until the entire code memory is programmed.
TABLE 3-5: SERIAL INSTRUCTION EXECUTION FOR WRITING CODE MEMORY (CONTINUED)
Command
(Binary) Data
(Hex) Description
PIC24FXXKA2XX
DS39991A-page 12 2010 Microchip Technology Inc.
FIGURE 3-8: PROGRAM CODE MEMORY FLOW
Start Write Sequence
All
locations
done?
No
End
Start
Yes
Load 2 Bytes
to Write
Buffer at <Addr>
All
bytes
written?
No
Yes
and Poll for WR bit
to be Cleared
N = 1
LoopCount = 0
Configure
Device for
Writes
N = 1
LoopCount =
LoopCount + 1
N = N + 1
2010 Microchip Technology Inc. DS39991A-page 13
PIC24FXXKA2XX
3.7 Writing Configuration Registers
The procedure for writing the Configuration registers is
the same as for writing code memory. The only differ-
ence is that only one word is programmed in each
operation. When writing Configuration registers, one
word is programmed during each operation. Only work-
ing register, W0, is used as a temporary holding register
for the data to be programmed.
Table 3-6 provides the default values of the
Configuration registers.
Table 3-6 provides the ICSP programming details for
programming the Configuration registers, including the
serial pattern with the ICSP command code, which
must be transmitted, LSB first, using the PGCx and
PGDx pins (see Figure 3-2). In Step 1 of Table 3-7, the
Reset vector is exited. In Step 2, the NVMCON register
is initialized for programming code memory. In Step 3,
the 24-bit starting destination address for programming
is loaded into the TBLPAG register and W7 register.
TABLE 3-6: DEFAULT VALUES FOR
CONFIGURATION REGISTER
SERIAL INSTRUCTION
Note: The TBLPAG register is hard-coded to
0xF8 (the upper byte address of all
locations of the Configuration registers).
Note: The TBLPAG register must be loaded with
F8h.
Configuration
Registers Value
FGS 03h
FOSCSEL 87h
FOSC FFh
FWDT DFh
FPOR FBh
FICD(1) C3h
FDS FFh
Note 1: The Configuration register, FICD, is a
reserved location and should be
programmed with the default value given
above.
PIC24FXXKA2XX
DS39991A-page 14 2010 Microchip Technology Inc.
TABLE 3-7: SERIAL INSTRUCTION EXECUTION FOR WRITING CONFIGURATION REGISTERS
Command
(Binary) Data
(Hex) Command
(Binary)
Step 1: Exit the Reset vector.
0000
0000
0000
000000
040200
000000
NOP
GOTO 0x200
NOP
Step 2: Initialize the Write Pointer (W7) for the TBLWT instruction.
0000 200007 MOV #0x0000, W7
Step 3: Set the NVMCON register to program Configuration registers.
0000
0000
24004A
883B0A
MOV #0x4004, W10
MOV W10, NVMCON
Step 4: Initialize the TBLPAG register.
0000
0000
200F80
880190
MOV #0xF8, W6
MOV W0, TBLPAG
Step 5: Load the Configuration register data to W6.
0000 2xxxx6 MOV #<FBS_VALUE>, W6
Step 6: Write the Configuration register data to the write latch and increment the Write Pointer.
0000
0000
0000
0000
000000
BB1B86
000000
000000
NOP
TBLWTL W6, [W7++]
NOP
NOP
Step 7: Initiate the write cycle.
0000
0000
0000
A8E761
000000
000000
BSET NVMCON, #WR
NOP
NOP
Step 8: Repeat this step to poll the WR bit (bit 15 of NVMCON) until it is cleared by the hardware.
0000
0000
0000
0000
0000
0001
0000
040200
000000
803B02
883C22
000000
<VISI>
000000
GOTO 0x200
NOP
MOV NVMCON, W2
MOV W2, VISI
NOP
Clock out contents of the VISI register.
NOP
Step 9: Reset device internal PC.
0000
0000
040200
000000
GOTO 0x200
NOP
Step 10: Repeat Steps 5 through 9 to write other fuses, Load W6 with their respective values and W7 with their
respective addresses.
2010 Microchip Technology Inc. DS39991A-page 15
PIC24FXXKA2XX
TABLE 3-8: PIC24FXXKA2XX FAMILY CONFIGURATION BITS DESCRIPTION
Bit Field Register Description
BOREN<1:0> FPOR<1:0> Brown-out Reset Enable bits
11 = Brown-out Reset is enabled in hardware; SBOREN bit is disabled
10 = Brown-out Reset is enabled only while device is active and disabled in
Sleep; SBOREN bit is disabled
01 = Brown-out Reset controlled with the SBOREN bit setting
00 = Brown-out Reset is disabled in hardware; SBOREN bit is disabled
BORV<1:0> FPOR<6:5> Brown-out Reset Voltage bits
11 = VBOR set to 1.8V min
10 = VBOR set to 2.0V min
01 = VBOR set to 2.7V min
00 = Downside protection on POR enabled – “Zero-power” selected
DSWDTEN FDS<7> Deep Sleep Watchdog Timer Enable bit
1 = DSWDT is enabled
0 = DSWDT is disabled
DSWDTPS<3:0> FDS<3:0> Deep Sleep Watchdog Timer Postscale Select bits
The DSWDT prescaler is 32; this creates an approximate base time unit of
1ms.
1111 = 1:2,147,483,648 (25.7 days)
1110 = 1:536,870,912 (6.4 days)
1101 = 1:134,217,728 (38.5 hours)
1100 = 1:33,554,432 (9.6 hours)
1011 = 1:8,388,608 (2.4 hours)
1010 = 1:2,097,152 (36 minutes)
1001 = 1:524,288 (9 minutes)
1000 = 1:131,072 (135 seconds)
0111 = 1:32,768 (34 seconds)
0110 = 1:8,192 (8.5 seconds)
0101 = 1:2,048 (2.1 seconds)
0100 = 1:512 (528 ms)
0011 = 1:128 (132 ms)
0010 = 1:32 (33 ms)
0001 = 1:8 (8.3 ms)
0000 = 1:2 (2.1 ms)
DSZPBOR FDS<6> Deep Sleep Zero-Power BOR Enable bit
1 = Zero-Power BOR is enabled in Deep Sleep
0 = Zero-Power BOR is disabled in Deep Sleep (does not affect operation in
non Deep Sleep modes)
FCKSM<1:0> FOSC<7:6> Clock Switching and Monitor Selection Configuration bits
1x = Clock switching is disabled, Fail-Safe Clock Monitor is disabled
01 = Clock switching is enabled, Fail-Safe Clock Monitor is disabled
00 = Clock switching is enabled, Fail-Safe Clock Monitor is enabled
FNOSC<2:0> FOSCSEL<2:0> Oscillator Selection bits
000 = Fast RC Oscillator (FRC)
001 = Fast RC Oscillator with divide-by-N with PLL module (FRCDIV+PLL)
010 = Primary Oscillator (XT, HS, EC)
011 = Primary Oscillator with PLL module (HS+PLL, EC+PLL)
100 = Secondary Oscillator (SOSC)
101 = Low-Power RC Oscillator (LPRC)
110 = Reserved; do not use
111 = Fast RC Oscillator with divide-by-N (FRCDIV)
Note 1: The MCLRE fuse can only be changed when using the VPP-Based Test mode entry. This prevents a user
from accidentally locking out the device from low-voltage test entry.
PIC24FXXKA2XX
DS39991A-page 16 2010 Microchip Technology Inc.
FWPSA FWDT<4> WDT Prescaler
1 = WDT prescaler ratio of 1:128
0 = WDT prescaler ratio of 1:32
FWDTEN FWDT<7> Watchdog Timer Enable bit
1 = WDT is enabled
0 = WDT is disabled (control is placed on the SWDTEN bit)
GSS0 FGS<1> General Segment Code Flash Code Protection bit
1 = No protection
0 = Standard security is enabled
GWRP FGS<0> General Segment Code Flash Write Protection bit
1 = General segment may be written
0 = General segment is write-protected
ICS<1:0> FICD<1:0> ICD Pin Placement Select bit
11 = Reserved; do not use
10 = PGEC2/PGED2 are used for ICSP programming
01 = PGEC3/PGED3 are used for ICSP programming
00 = Reserved; do not use
IESO FOSCSEL<7> Internal External Switchover bit
1 = Internal External Switchover mode is enabled (Two-Speed Start-up
enabled)
0 = Internal External Switchover mode is disabled (Two-Speed Start-up disabled)
MCLRE(1) FPOR<7> MCLR Pin Enable bit(1)
1 = MCLR pin is enabled; RA5 input pin is disabled
0 = RA5 input pin is enabled; MCLR is disabled
OSCIOFNC FOSC<2> CLKO Enable Configuration bit
1 = CLKO output signal is active on the OSCO pin; primary oscillator must be
disabled or configured for the External Clock mode (EC) for the CLKO to
be active (POSCMD<1:0> = 11 or 00)
0 = CLKO output is disabled
POSCMD<1:0> FOSC<1:0> Primary Oscillator Configuration bits
11 = Primary oscillator disabled
10 = HS Oscillator mode selected (4 MHz-25 MHz)
01 = XT Oscillator mode selected (100 kHz-4 MHz)
00 = External Clock mode selected
POSCFREQ<1:0> FOSC<4:3> Primary Oscillator Frequency Range Configuration bits
11 = Primary oscillator/external clock input frequency is greater than 8 MHz
10 = Primary oscillator/external clock input frequency is between 100 kHz and
8MHz
01 = Primary oscillator/external clock input frequency is less than 100 kHz
00 = Reserved; do not use
PWRTEN FPOR<3> Power-up Timer Enable bit
0 = PWRT is disabled
1 = PWRT is enabled
SOSCSEL FOSC<5> Secondary Oscillator Select bit
1 = Secondary oscillator is configured for high-power operation
0 = Secondary oscillator is configured for low-power operation
TABLE 3-8: PIC24FXXKA2XX FAMILY CONFIGURATION BITS DESCRIPTION (CONTINUED)
Bit Field Register Description
Note 1: The MCLRE fuse can only be changed when using the VPP-Based Test mode entry. This prevents a user
from accidentally locking out the device from low-voltage test entry.
2010 Microchip Technology Inc. DS39991A-page 17
PIC24FXXKA2XX
WDTPS<3:0> FWDT<3:0> Watchdog Timer Postscale Select bits
1111 = 1:32,768
1110 = 1:16,384
•
•
•
0001 =1:2
0000 =1:1
WINDIS FWDT<6> Windowed Watchdog Timer Disable bit
1 = Standard WDT selected; windowed WDT is disabled
0 = Windowed WDT is enabled
TABLE 3-8: PIC24FXXKA2XX FAMILY CONFIGURATION BITS DESCRIPTION (CONTINUED)
Bit Field Register Description
Note 1: The MCLRE fuse can only be changed when using the VPP-Based Test mode entry. This prevents a user
from accidentally locking out the device from low-voltage test entry.
PIC24FXXKA2XX
DS39991A-page 18 2010 Microchip Technology Inc.
3.8 Reading Code Memory
To read the code memory, execute a series of TBLRD
instructions and clock out the data using the REGOUT
command.
Table 3-9 provides the ICSP programming details for
reading code memory. In Step 1, the Reset vector is
exited. In Step 2, the 24-bit starting source address for
reading is loaded into the TBLPAG register and the W6
register. The upper byte of the starting source address
is stored in TBLPAG, and the lower 16 bits of the source
address are stored in W6.
To minimize the reading time, the packed instruction
word format, which was used for writing, is also used
for reading (see Figure 3-7). In Step 3, the Write
Pointer, W7, is initialized. In Step 4, two instruction
words are read from code memory, and clocked out of
the device through the VISI register, using the REGOUT
command. Step 4 is repeated until the required amount
of code memory is read.
TABLE 3-9: SERIAL INSTRUCTION EXECUTION FOR READING CODE MEMORY
Command
(Binary) Data
(Hex) Description
Step 1: Exit Reset vector.
0000
0000
0000
000000
040200
000000
NOP
GOTO 0x200
NOP
Step 2: Initialize TBLPAG and the Read Pointer (W6) for TBLRD instruction.
0000
0000
0000
200xx0
880190
2xxxx6
MOV #<SourceAddress23:16>, W0
MOV W0, TBLPAG
MOV #<SourceAddress15:0>, W6
Step 3: Initialize the Write Pointer (W7) to point to the VISI register.
0000
0000
207847
000000
MOV #VISI, W7
NOP
Step 4: Read and clock out the contents of the next two locations of code memory through the VISI register using
the REGOUT command.
0000
0000
0000
0001
0000
0000
0000
0000
0000
0000
0000
0001
0000
0000
0000
0000
0001
0000
BA1B96
000000
000000
<VISI>
000000
BADBB6
000000
000000
BAD3D6
000000
000000
<VISI>
000000
BA0BB6
000000
000000
<VISI>
000000
TBLRDL [W6], [W7]
NOP
NOP
Clock out contents of VISI register.
NOP
TBLRDH [W6++], [W7]
NOP
NOP
TBLRDH.B [++W6], [W7--]
NOP
NOP
Clock out contents of VISI register.
NOP
TBLRDL [W6++], [W7]
NOP
NOP
Clock out contents of VISI register.
NOP
Step 5: Reset device internal PC.
0000
0000
040200
000000
GOTO 0x200
NOP
Step 6: Repeat Steps 4 and 5 until the required code memory is read.
2010 Microchip Technology Inc. DS39991A-page 19
PIC24FXXKA2XX
3.9 Reading Configuration Memory
The procedure for reading a Configuration register is
the same as reading the code memory. The only
difference is that the 16-bit data words are read (with
the upper byte read being all ‘0‘s) instead of the 24-bit
words. There are eight Configuration registers and they
are read, one register at a time.
Table 3-10 provides the ICSP programming details for
reading all of the Configuration registers.
Note: The TBLPAG register should be
hard-coded to 0xF8 (the upper byte
address of the Configuration register) and
the Read Pointer, W6, is initialized to
0x00h.
TABLE 3-10: SERIAL INSTRUCTION EXECUTION FOR READING ALL THE CONFIGURATION
REGISTERS
Command
(Binary) Data
(Hex) Description
Step 1: Exit Reset vector.
0000
0000
0000
000000
040200
000000
NOP
GOTO 0x200
NOP
Step 2: Initialize TBLPAG, the Read Pointer (W6) and the Write Pointer (W7) for TBLRD instruction.
0000
0000
0000
0000
0000
200F80
880190
200007
207847
000000
MOV #0xF8, W0
MOV W0, TBLPAG
MOV #0x0000,W6
MOV #VISI, W7
NOP
Step 3: Read the Configuration register and write it to the VISI register (located at 784h), and clock out the
VISI register using the REGOUT command.
0000
0000
0000
0001
BA0BB6
000000
000000
<VISI>
TBLRDL [W6++], [W7]
NOP
NOP
Clock out contents of VISI register.
Step 4: Repeat Step 3 to read other fuses. Load W6 with their respective address.
Step 5: Reset device internal PC.
0000
0000
040200
000000
GOTO 0x200
NOP
PIC24FXXKA2XX
DS39991A-page 20 2010 Microchip Technology Inc.
3.10 Verifying Code Memory and
Configuration Registers
To verify the code memory, read the code memory
space and compare it with the copy held in the
programmer’s buffer. Figure 3-9 illustrates the verify
process flowchart. Memory reads occur 1 byte at a
time, hence 2 bytes must be read to compare with the
word in the programmer’s buffer. Refer to Section 3.8
“Reading Code Memory” for implementation details
of reading code memory. On the same lines, the data
EEPROM and Configuration registers can be verified.
FIGURE 3-9: VERIFY CODE MEMORY
FLOW
3.11 Exiting ICSP Mode
Exit the Program/Verify mode by removing VIH from
MCLR/VPP as illustrated in Figure 3-10. The only
requirement to exit is that an interval of P16 should
elapse between the last clock and the program signals
on PGCx and PGDx before removing VIH.
FIGURE 3-10: EXITING ICSP™ MODE
Note: Code memory should be verified
immediately after writing if code protection
is enabled. Since Configuration registers
include the device code protection bit, the
device will not be readable or verifiable if a
device Reset occurs after the code-protect
bits are set (value = 0).
Read Low Byte
Read High Byte
Does
Word = Expect
Data?
All
code memory
verified?
No
Yes
No
Set TBLPTR = 0
Start
Yes
End
with Post-Increment
with Post-Increment
Failure
Report Error
MCLR/VPP
P16
PGDx
PGD = Input
PGCx
VDD
VIH/VIHH
VIH
P17
Description
2010 Microchip Technology Inc. DS39991A-page 21
PIC24FXXKA2XX
4.0 DEVICE ID
The Device ID region of memory can be used to
determine the mask, variant and manufacturing
information about the device. The Device ID region is
2 x 16 bits and it can be read using the READC
command. This region of memory is read-only and can
also be read when code protection is enabled.
Table 4-1 provides the Device ID for each device;
Table 4-2 provides the Device ID registers; Table 4-3
describes the bit field of each register.
TABLE 4-1: DEVICE IDs
4.1 Checksums
4.1.1 CHECKSUM COMPUTATION
Checksums for the PIC24FXXKA2XX family are
16 bits. The checksum is calculated by summing the
following:
• Contents of the code memory locations
• Contents of the Configuration registers
Table 4-4 describes how to calculate the checksum for
each device.
All memory locations are summed, one byte at a time,
using only their native data size. More specifically,
Configuration registers are summed by adding the
lower two bytes of these locations (the upper byte is
ignored) while the code memory is summed by adding
all three bytes of the code memory.
TABLE 4-2: PIC24FXXKA2XX DEVICE ID REGISTERS
Device ID DEVID
PIC24F04KA200 0D02h
PIC24F04KA201 0D00h
Address Name Bit
15 14131211109876543210
FF0000h DEVID FAMID<7:0> DEV<7:0>
FF0002h DEVREV — REV<3:0>
TABLE 4-3: DEVICE ID BITS DESCRIPTION
Bit Field Register Description
FAMID<7:0> DEVID Encodes the family ID of the device.
DEV<7:0> DEVID Encodes the individual ID of the device.
REV<3:0> DEVREV Encodes the revision number of the device.
TABLE 4-4: CHECKSUM COMPUTATION
Device Read Code Protection Checksum Computation Erased
Checksum
Value
Chip Checksum with
0xAAAAAA at 0x00
Location and
at Last Location
PIC24F04KAXXX Disabled CFGB + SUM (0:000AFE) 0x74B4 0x72B6
Enabled 0 0x0000 0x0000
Legend: Item Description
SUM[a:b] = Byte sum of locations, a to b inclusive (all 3 bytes of code memory)
CFGB = Configuration Block (masked),
Byte sum of (FGS & 0x0003 + FOSCSEL & 0x0087 + FOSC & 0x00DF + FWDT & 0x00DF +
FPOR & 0x00FB + FICD & 0x00C3 + FDS & 0x00FF)
PIC24FXXKA2XX
DS39991A-page 22 2010 Microchip Technology Inc.
5.0 AC/DC CHARACTERISTICS AND TIMING REQUIREMENTS
TABLE 5-1: STANDARD OPERATING CONDITIONS
Standard Operating Conditions
Operating Temperature: 0C to +70C and programming: +25C is recommended.
Param
No. Symbol Characteristic Min Max Units Conditions
D111 VDD Supply Voltage During Programming VDDCORE 3.60 V Normal programming
D112 IPP Programming Current on MCLR —50A—
D113 IDDP Supply Current During Programming — 2 mA —
D031 VIL Input Low Voltage VSS 0.2 VDD V—
D041 VIH Input High Voltage 0.8 VDD VDD V—
D042 VIHH Programing Voltage on VPP VDD +1.5 9 V —
D080 VOL Output Low Voltage — 0.4 V IOL = 8.5 mA @ 3.6V
D090 VOH Output High Voltage 1.4 — V IOH = -3.0 mA @ 3.6V
D012 CIO Capacitive Loading on I/O Pin (PGDx) — 50 pF To meet AC specifications
P1 TPGC Serial Clock (PGCx) Period 125 — ns —
P1A TPGCL Serial Clock (PGCx) Low Time 50 — ns —
P1B TPGCH Serial Clock (PGCx) High Time 50 — ns —
P2 TSET1 Input Data Setup Time to Serial Clock 15 — ns —
P3 THLD1 Input Data Hold Time from PGCx 15 — ns —
P4 TDLY1 Delay Between 4-Bit Command and
Command Operand
40 — ns —
P4A TDLY1ADelay Between 4-Bit Command Operand
and the Next 4-Bit Command
40 — ns —
P5 TDLY2 Delay Between Last PGCx of Command
Byte and First PGCx of Read of Data
Word
20 — ns —
P6 TSET2VDD Setup Time to MCLR 100 — ns —
P7 THLD2 Input Data Hold Time from MCLR VPP
(from VIHH to VIH)
25 — ms —
P10 TDLY6 PGCx Low Time After Programming 400 — ns —
P11 TDLY7 Chip Erase Time 5 — ms —
P12 TDLY10 Page (4 rows) Erase Time 5 — ms —
P13 TDLY9 Row Programming Time 2 — ms —
P14 TRMCLR Rise Time to Enter ICSP™ mode — 1.0 s—
P15 TVALID Data Out Valid from PGCx 10 — ns —
P16 TDLY10 Delay Between Last PGCx and MCLR 0—s —
P17 THLD3MCLR to VDD —100ns —
P18 TKEY1 Delay Between First MCLR and First
PGCx for Key Sequence on PGDx
1—ms —
P19 TKEY2 Delay Between Last PGCx for Key
Sequence on PGDx and Second MCLR
1—ms —
Rev A Documenl 9/2010
2010 Microchip Technology Inc. DS39991A-page 23
PIC24FXXKA2XX
APPENDIX A: REVISION HISTORY
Rev A Document (9/2010)
Original version of this document; takes all information
specific to PIC24XXKA20X family devices, originally
found in DS39919, and created a new specification. No
technical information regarding the devices or their
programming has changed.
PIC24FXXKA2XX
DS39991A-page 24 2010 Microchip Technology Inc.
NOTES:
QUALITY MANAGEMENT SYSTEM
CERTIFIED BY DNV
= ISO/TS “5949:2002 =
2010 Microchip Technology Inc. DS39991A-page 25
Information contained in this publication regarding device
applications and the like is provided only for your convenience
and may be superseded by updates. It is your responsibility to
ensure that your application meets with your specifications.
MICROCHIP MAKES NO REPRESENTATIONS OR
WARRANTIES OF ANY KIND WHETHER EXPRESS OR
IMPLIED, WRITTEN OR ORAL, STATUTORY OR
OTHERWISE, RELATED TO THE INFORMATION,
INCLUDING BUT NOT LIMITED TO ITS CONDITION,
QUALITY, PERFORMANCE, MERCHANTABILITY OR
FITNESS FOR PURPOSE. Microchip disclaims all liability
arising from this information and its use. Use of Microchip
devices in life support and/or safety applications is entirely at
the buyer’s risk, and the buyer agrees to defend, indemnify and
hold harmless Microchip from any and all damages, claims,
suits, or expenses resulting from such use. No licenses are
conveyed, implicitly or otherwise, under any Microchip
intellectual property rights.
Trademarks
The Microchip name and logo, the Microchip logo, dsPIC,
KEELOQ, KEELOQ logo, MPLAB, PIC, PICmicro, PICSTART,
PIC32 logo, rfPIC and UNI/O are registered trademarks of
Microchip Technology Incorporated in the U.S.A. and other
countries.
FilterLab, Hampshire, HI-TECH C, Linear Active Thermistor,
MXDEV, MXLAB, SEEVAL and The Embedded Control
Solutions Company are registered trademarks of Microchip
Technology Incorporated in the U.S.A.
Analog-for-the-Digital Age, Application Maestro, CodeGuard,
dsPICDEM, dsPICDEM.net, dsPICworks, dsSPEAK, ECAN,
ECONOMONITOR, FanSense, HI-TIDE, In-Circuit Serial
Programming, ICSP, Mindi, MiWi, MPASM, MPLAB Certified
logo, MPLIB, MPLINK, mTouch, Omniscient Code
Generation, PICC, PICC-18, PICDEM, PICDEM.net, PICkit,
PICtail, REAL ICE, rfLAB, Select Mode, Total Endurance,
TSHARC, UniWinDriver, WiperLock and ZENA are
trademarks of Microchip Technology Incorporated in the
U.S.A. and other countries.
SQTP is a service mark of Microchip Technology Incorporated
in the U.S.A.
All other trademarks mentioned herein are property of their
respective companies.
© 2010, Microchip Technology Incorporated, Printed in the
U.S.A., All Rights Reserved.
Printed on recycled paper.
ISBN: 978-1-60932-604-3
Note the following details of the code protection feature on Microchip devices:
• Microchip products meet the specification contained in their particular Microchip Data Sheet.
• Microchip believes that its family of products is one of the most secure families of its kind on the market today, when used in the
intended manner and under normal conditions.
• There are dishonest and possibly illegal methods used to breach the code protection feature. All of these methods, to our
knowledge, require using the Microchip products in a manner outside the operating specifications contained in Microchip’s Data
Sheets. Most likely, the person doing so is engaged in theft of intellectual property.
• Microchip is willing to work with the customer who is concerned about the integrity of their code.
• Neither Microchip nor any other semiconductor manufacturer can guarantee the security of their code. Code protection does not
mean that we are guaranteeing the product as “unbreakable.”
Code protection is constantly evolving. We at Microchip are committed to continuously improving the code protection features of our
products. Attempts to break Microchip’s code protection feature may be a violation of the Digital Millennium Copyright Act. If such acts
allow unauthorized access to your software or other copyrighted work, you may have a right to sue for relief under that Act.
Microchip received ISO/TS-16949:2002 certification for its worldwide
headquarters, design and wafer fabrication facilities in Chandler and
Tempe, Arizona; Gresham, Oregon and design centers in California
and India. The Company’s quality system processes and procedures
are for its PIC® MCUs and dsPIC® DSCs, KEELOQ® code hopping
devices, Serial EEPROMs, microperipherals, nonvolatile memory and
analog products. In addition, Microchip’s quality system for the design
and manufacture of development systems is ISO 9001:2000 certified.
6‘
‘MICRDCHIP
DS39991A-page 26 2010 Microchip Technology Inc.
AMERICAS
Corporate Office
2355 West Chandler Blvd.
Chandler, AZ 85224-6199
Tel: 480-792-7200
Fax: 480-792-7277
Technical Support:
http://support.microchip.com
Web Address:
www.microchip.com
Atlanta
Duluth, GA
Tel: 678-957-9614
Fax: 678-957-1455
Boston
Westborough, MA
Tel: 774-760-0087
Fax: 774-760-0088
Chicago
Itasca, IL
Tel: 630-285-0071
Fax: 630-285-0075
Cleveland
Independence, OH
Tel: 216-447-0464
Fax: 216-447-0643
Dallas
Addison, TX
Tel: 972-818-7423
Fax: 972-818-2924
Detroit
Farmington Hills, MI
Tel: 248-538-2250
Fax: 248-538-2260
Kokomo
Kokomo, IN
Tel: 765-864-8360
Fax: 765-864-8387
Los Angeles
Mission Viejo, CA
Tel: 949-462-9523
Fax: 949-462-9608
Santa Clara
Santa Clara, CA
Tel: 408-961-6444
Fax: 408-961-6445
Toronto
Mississauga, Ontario,
Canada
Tel: 905-673-0699
Fax: 905-673-6509
ASIA/PACIFIC
Asia Pacific Office
Suites 3707-14, 37th Floor
Tower 6, The Gateway
Harbour City, Kowloon
Hong Kong
Tel: 852-2401-1200
Fax: 852-2401-3431
Australia - Sydney
Tel: 61-2-9868-6733
Fax: 61-2-9868-6755
China - Beijing
Tel: 86-10-8528-2100
Fax: 86-10-8528-2104
China - Chengdu
Tel: 86-28-8665-5511
Fax: 86-28-8665-7889
China - Chongqing
Tel: 86-23-8980-9588
Fax: 86-23-8980-9500
China - Hong Kong SAR
Tel: 852-2401-1200
Fax: 852-2401-3431
China - Nanjing
Tel: 86-25-8473-2460
Fax: 86-25-8473-2470
China - Qingdao
Tel: 86-532-8502-7355
Fax: 86-532-8502-7205
China - Shanghai
Tel: 86-21-5407-5533
Fax: 86-21-5407-5066
China - Shenyang
Tel: 86-24-2334-2829
Fax: 86-24-2334-2393
China - Shenzhen
Tel: 86-755-8203-2660
Fax: 86-755-8203-1760
China - Wuhan
Tel: 86-27-5980-5300
Fax: 86-27-5980-5118
China - Xian
Tel: 86-29-8833-7252
Fax: 86-29-8833-7256
China - Xiamen
Tel: 86-592-2388138
Fax: 86-592-2388130
China - Zhuhai
Tel: 86-756-3210040
Fax: 86-756-3210049
ASIA/PACIFIC
India - Bangalore
Tel: 91-80-3090-4444
Fax: 91-80-3090-4123
India - New Delhi
Tel: 91-11-4160-8631
Fax: 91-11-4160-8632
India - Pune
Tel: 91-20-2566-1512
Fax: 91-20-2566-1513
Japan - Yokohama
Tel: 81-45-471- 6166
Fax: 81-45-471-6122
Korea - Daegu
Tel: 82-53-744-4301
Fax: 82-53-744-4302
Korea - Seoul
Tel: 82-2-554-7200
Fax: 82-2-558-5932 or
82-2-558-5934
Malaysia - Kuala Lumpur
Tel: 60-3-6201-9857
Fax: 60-3-6201-9859
Malaysia - Penang
Tel: 60-4-227-8870
Fax: 60-4-227-4068
Philippines - Manila
Tel: 63-2-634-9065
Fax: 63-2-634-9069
Singapore
Tel: 65-6334-8870
Fax: 65-6334-8850
Taiwan - Hsin Chu
Tel: 886-3-6578-300
Fax: 886-3-6578-370
Taiwan - Kaohsiung
Tel: 886-7-213-7830
Fax: 886-7-330-9305
Taiwan - Taipei
Tel: 886-2-2500-6610
Fax: 886-2-2508-0102
Thailand - Bangkok
Tel: 66-2-694-1351
Fax: 66-2-694-1350
EUROPE
Austria - Wels
Tel: 43-7242-2244-39
Fax: 43-7242-2244-393
Denmark - Copenhagen
Tel: 45-4450-2828
Fax: 45-4485-2829
France - Paris
Tel: 33-1-69-53-63-20
Fax: 33-1-69-30-90-79
Germany - Munich
Tel: 49-89-627-144-0
Fax: 49-89-627-144-44
Italy - Milan
Tel: 39-0331-742611
Fax: 39-0331-466781
Netherlands - Drunen
Tel: 31-416-690399
Fax: 31-416-690340
Spain - Madrid
Tel: 34-91-708-08-90
Fax: 34-91-708-08-91
UK - Wokingham
Tel: 44-118-921-5869
Fax: 44-118-921-5820
Worldwide Sales and Service
08/04/10