0011030003 Instr Sheet 规格书
HT1884 Exlraclor Too‘
KN®
molex
\_/
Products
HT1884 Extractor Tool
Doc No: ATS-011030003 Release Date: 01-31-02 UNCONTROLLED COPY Page 1 of 2
Revision: E Revision Date: 09-29-09
Extractor Tool
Instruction Sheet
Order No. 11-03-0003
Engineering No. (HT1884)
FEATURES
This tool is designed to extract different terminal series from various plug and receptacle housings. See Chart
below.
SCOPE
Products: KK 3.96mm (.156 in) pitch Crimp Terminals
Terminal
Series No
Description Housings
Series No Terminal Order No.
08-01-0101
08-01-0102
08-01-0105
08-01-0106
08-01-0121
08-01-0122
08-01-0123
08-01-0124
08-03-0101
08-03-0102
08-05-0103
08-05-0104
08-05-0105
08-06-0101
08-06-0102
08-06-0105
1797 KK 3.96mm (.156 in) pitch
Bifurcated Terminals 1796
08-06-0106
08-07-0101
08-07-0102
08-30-0109
08-30-0110
08-34-0105
08-34-0106
1799 KK 3.96mm (.156 in) pitch
Right Angle Terminal
2139, 41696,
52213 and 52266
08-34-0109
08-35-0105
08-35-0106
08-03-0303
08-03-0304
08-05-0301
08-05-0302
4366 KK 3.96mm (.156 in) pitch
Straight- On Dualcon TM Terminals
4338 08-05-0305
40-01-1194
50-36-1873
08-03-0305
08-03-0306
08-05-0303
08-05-0304
4573 KK 3.96mm (.156 in) pitch
Cantilever Straight-On Terminals 4338 50-36-2431
50-36-2432
OPERATION:
1. Push the terminal forward in the arrow direction before
using the Extractor Tool as shown in Figure 1. Insert
the Extractor Tool into the slot on the bottom or top of
the connector housing.
EXTRACTOR
TOOL
EXTRACTOR
TOOL
HOUSING
WIRE
Figure 1
LOCKING
TAB
HOUSING
TERMINAL
HT1884 Exlraclor Too‘
HT1884 Extractor Tool
Doc No: ATS-011030003 Release Date: 01-31-02 UNCONTROLLED COPY Page 2 of 2
Revision: E Revision Date: 09-29-09
2. Depress the terminal locking tabs, push the terminal back through the Connector slot and pull the
terminated wire out in the arrow direction as shown in Figure 2.
CAUTION: Molex specifications are valid only when used with Molex terminals, applicators and tooling.
Molex does not offer repair parts for Extraction Tools due to the inexpensive nature of the tool.
Contact Information
For more information on Molex application tooling please contact your nearest Molex location shown below.
Americas Headquarters
Lisle, Illinois 60532 U.S.A.
1-800-78MOLEX
amerinfo@molex.com
Far East North Headquarters
Yamato, Kanagawa, Japan
81-462-65-2324
feninfo@molex.com
Far East South Headquarters
Jurong, Singapore
65-6-268-6868
fesinfo@molex.com
European Headquarters
Munich, Germany
49-89-413092-0
eurinfo@molex.com
Corporate Headquarters
2222 Wellington Ct.
Lisle, IL 60532 U.S.A.
630-969-4550
Fax: 630-969-1352
Visit our Web site at http://www.molex.com
Figure 2
EXTRACTOR
TOOL
EXTRACTOR
TOOL
HOUSING
WIRE
LOCKING
TAB
LOCKING
TAB
T
ERMINAL
TERMINAL