B&K Precision 的 570A Manual 规格书
ALJ‘
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
MODEL 570A HANDHELD
LINEAR IC TESTER
OPERATOR’S MANUAL
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
CONTENTS
1. introduction .............................................................................. 2
2. DC input ................................................................................... 2
3. battery eliminator..................................................................... 3
4. switching on.............................................................................. 3
5. operating modes....................................................................... 4
6. entering test numbers............................................................... 4
7. testing the IC ............................................................................ 5
8. test results................................................................................. 6
9. testing further ICs...................................................................... 8
10. continuous testing ................................................................. 8
11. search mode.......................................................................... 9
12. self test mode...................................................................... 10
13. CompactLink mode ............................................................. 10
14. specifications....................................................................... 11
15. IC support list....................................................................... 12
introduction................................................................................ 12
15.2. operational amplifiers................................................... 12
15.3. comparators.................................................................. 15
15.4. switches and multiplexers............................................. 16
15.5. regulators, references and virtual grounds..................... 16
15.6. opto couplers and isolators........................................... 17
15.7. miscellaneous............................................................... 18
16. Service Information............................................................. 19
17. Limited One-Year Warranty................................................. 20
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
1. introduction
Thank you for purchasing the B & K
Precision Model 570A Hand Held
Linear IC Tester.
The basic function of the B & K Model
570A Linear IC Tester is to test a linear
IC for correct logical functioning as
described in the manufacturer’s IC data
sheets. The B & K Model 570A applies the necessary analogue
signals to the inputs of the IC, monitoring the outputs at each stage
and comparing them with the expected voltages. Any discrepancy
results in a FAIL indication and the faulty pins are shown on the
integral display. Additional facilities are also provided, amongst
them test loops that can be used for goods inwards inspection,
detecting intermittent faults or simply providing a rapid method of
exercising any IC for demonstration or educational purposes. Since
the B & K Model 570A contains an extensive IC library, it is not
necessary to program the unit yourself other than to key in the IC
number. It is also capable of identifying an unknown IC using the
SEARCH mode - this is a feature that many users will find extremely
valuable.
The B & K Model 570A is provided with an RS-232 interface
enabling it to be connected to a companion software package
called CompactLink running on a PC. CompactLink allows test
programs for ICs not included in the internal library to be developed
and downloaded into the B & K Model 570A memory to enhance
the library according to your wishes.
2. DC input
The B & K Model 570A is powered by four AA batteries or by the
use of the battery eliminator input at the rear of the case. To insert
the batteries, turn the unit upside down and remove the battery
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
cover by removing the two cross head screws holding it in place.
The batteries must be inserted in the correct orientation, as
indicated by the drawing within the battery compartment. Incorrect
insertion of batteries will not allow the unit to operate. Replace the
battery cover and insert the screws. If the battery voltage falls too
low, a low battery warning symbol will be displayed at the top left
hand cell of the display in normal operating mode. A low battery
warning will also be displayed during a result display. Test results
may be inconsistent under these conditions.
3. battery eliminator
An external battery eliminator is available for prolonged use of the
B & K Model 570A. Some ICs consume a significant amount of
current when powered up, and battery life can be conserved by
using the eliminator. There is no need to remove the batteries prior
to inserting the battery eliminator. However, please note that during
prolonged periods of non-use batteries are prone to leakage and
should be removed. Note that to avoid damage to the unit we
strongly advise that you only use the recommended battery
eliminator that is available by contacting your distributor. Note that
using an incorrect battery eliminator voltage may damage the unit
and invalidate the warranty.
4. switching on
To switch the unit on, simply press the 'ON' key. To preserve battery
life, the unit powers itself off after approximately three minutes of
non-use or when “Sw Off” is selected from the main menu. When
the unit is switched on, it first performs a self-diagnosis test.
Therefore, before switching on, check that the test socket is empty to
prevent interference with the diagnostics. If the unit passes the self-
test, a pass result will be displayed on the screen. Press a key to
enter the main operating mode - the display will be as follows:
NO:
MODE:Single :RDY
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
When this initial display is obtained the B & K Model 570A is ready
for use. If, however, the message SELF-TEST FAIL: is displayed
along with a fault message, this indicates that a self-test diagnostic
fault has been detected. Any detected faults will be displayed one
at a time. Pressing the TEST/EXEC key will then revert to the
opening menu as above, but of course operation of the unit will
then be suspect. Before contacting your distributor, check that the
test socket is completely empty.
5. operating modes
The B & K Model 570A has a number of test modes that are
selected using the MODE/CLEAR key from the initial screen. The
test modes are as follows:
Single - execute a single test on the IC in the socket.
Loop - execute test repeatedly, regardless of the result.
P Loop - execute test repeatedly, provided the result was PASS.
F Loop - execute test repeatedly, provided the result was FAIL.
Search - identify the number of the IC in the socket.
Diags - execute the diagnostic self-test.
CmLink - enter remote mode for CompactLink software.
Sw Off - turn off the unit
6. entering test numbers
Press the MODE/CLEAR key until the desired test mode is displayed.
Enter the number of the IC you wish to test. Pressing the
MODE/CLEAR key will clear the last digit from the display if a
mistake is made.
Note: The NUMERIC information only is entered, leav ing out the
manufacturers prefixes and suffixes and IC family information.
As an example, all the following linear ICs should be entered as
7, 4, 1 on the keypad:
e.g. uA741CP, uA741M, uA741C etc
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
Some ICs are available in different pin outs or package types, and
also there may be several different types of IC with the same
numerical part number. In these cases the B & K Model 570A will
automatically determine which test to perform. If however the IC is
faulty the unit may not be able to determine the correct IC type - if
this happens a warning message will be displayed. A complete list
of all ICs supported by the B & K Model 570A is contained in the IC
SUPPORT LIST at the end of this manual together with notes on
any special requirements for certain ICs.
Note that if you have stored a user library using CompactLink, an IC
in the user library with the same number as one in the internal
library will take precedence. This allows a new test to be written for
an existing IC. If you wish both tests to be available, use a different
number for your user test.
7. testing the IC
The test socket is a 24 pin shell with 16 active pins. Insert the IC to
be tested in the front of the 24 pin Zero Insertion Force socket with
pin 1 towards the display as shown below:
For 3 pin TO220 or TO92 packages, insert the IC in pins 6, 7 and 8
(lower left) of the socket with the metal tab or flat side facing to the
right.
Ensure that the operating lever on the socket is in the open (i.e. up)
position before inserting the IC. Close the socket by lowering the
lever, making sure that the IC is firmly seated in the socket and
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
making good contact. Press the TEST/EXEC key to activate the test
sequence for the IC. If an invalid IC type number was entered, or if
the IC you have requested is not supported the message "Unknown"
will be displayed. Simply entering another IC type number will
automatically clear this error message. If a valid type number was
entered, the IC test will begin and the message "BUSY" will be
displayed while the test proceeds. Many of the tests, however,
execute so quickly that this message is not noticeable.
8. test results
A pre-determined sequence of signals is applied to the inputs of the
IC under test and the output voltages are measured prior to
comparing with the correct values. The exact nature of the test
depends on the function of the IC, but as an example the
operational amplifier tests include both open and closed loop
testing over a range of input voltages and gain settings. If all the
outputs respond correctly, the result PASS will be displayed at the
top right of the display. A scrolling message will contain the IC
function and power pin information.
If a short circuit between the power pins of the IC is detected, a
warning ‘SHT!' will appear on the top right of the display and, since
no valid test is then possible, the result will FAIL. If the IC under test
takes an excessive amount of current when power is applied, a
warning 'ICC!' will appear. Press the TEST/EXEC key to continue
with the test, or MODE/CLEAR to abandon. Depending on the
condition of the batteries there may also be a ‘BAT!’ warning which
indicates that the batteries are incapable of supplying the current
required by the IC under test. You can continue with the test by
pressing the TEST/EXEC key, but the unit may malfunction because
of a drop in battery voltage. To avoid this, change the batteries or
use a battery eliminator. Note that a faulty IC may demand more
operating current and therefore will quickly drain the batteries.
Some ICs require external components to be fitted prior to the test -
in these cases the message EXT or CAP will be displayed at the top
right of the display. Please refer to the IC lists at the end of this
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
manual for details of the component(s) required. After fitting the
component the test can be carried out by a further press of the
TEST key. If you wish you can abandon the test by pressing the
CLEAR key.
In the case of a FAIL result, the error conditions at all the non-
functional pins of the IC will be scrolled on the display, and the IC
function will be shown. The various failure conditions that can be
displayed are as follows:
V<< - the voltage on the pin was lower than
expected.
V>> - the voltage on the pin was higher than expected.
D<< - the diode drop voltage was lower than expected.
D>> - the diode drop voltage was higher than expected.
LOAD - the input cannot be driven.
In some cases, the scrolling test results may include one or more
WARNING indications. These warnings indicate conditions that may
result in an incorrect test result, and are as follows:
D/F - result may be invalid because last self-test failed.
BAT - battery voltage too low during test
ICC - large current taken by IC under test
Some ICs are available in various packages, and also there are
some ICs in the library which have the same numerical part number
even though the IC functions are different. In these cases the B & K
Model 570A will automatically determine the IC type prior to the
test, provided that the IC is functional. If the IC is faulty, the
following warning will appear after the test:
WARNING: All Part Types FAIL
This indicates that the IC is faulty, but the pin information cannot be
displayed since the exact part type cannot be identified.
Before discarding a failed IC check that the correct IC type number
was entered and also check that the IC pins are clean and making
good contact with the test socket. Note that there is no way of
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
stopping a test once it has commenced, but see the description of
loop functions later in this manual.
9. testing further ICs
After a test is completed, the test result will be displayed. To test
another IC of the same type, simply insert the next IC and press the
TEST/EXEC key again. To test a different IC, enter the new IC type
number in the usual way, noticing that pressing the first digit of the
new number automatically clears the previous number from the
display. Remember that the MODE/CLEAR key can be used if an
error is made during the entry of the IC type number.
10. continuous testing
It is possible to test the same IC repeatedly to detect intermittent or
temperature-related faults, or to rapidly test a batch of identical ICs.
There are three types of test loop modes:
Loop - execute a test repeatedly, regardless of the result.
P Loop - execute a test repeatedly, provided the result is PASS.
F Loop - execute a test repeatedly, provided the result was
FAIL.
The B & K Model 570A is configured into one of the loop modes
using the MODE/CLEAR key as described earlier. Insert the IC and
press TEST/EXEC in the usual way to start the continuous test
process. The result of each test is displayed as PASS or FAIL on the
top right of the display. In LOOP mode, this allows a large batch of
identical ICs to be tested, without any action on the part of the
operator other than inserting the IC. When the IC is inserted,
sufficient time must be allowed for the test to take place before the
result status is updated, so if in doubt the IC should be tested in
single mode so that the approximate test time can be determined.
It will be found that high throughput can be obtained using this
mode.
To stop any of the test loops, press MODE/CLEAR, but note that the
test in progress is completed before the command is obeyed. The
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
effect of this is usually unnoticeable, but where the test takes a
reasonable time to execute there will be a delay before the
instrument responds to the MODE/CLEAR key.
Note: Testing high current ICs in loop mode will drain the
batteries quickly, and it is recommended that a battery eliminator
is used if you wish to perform loop tests.
11. search mode
This feature allows the type number of an unknown IC to be
determined, provided the IC is actually contained in the B & K
Model 570A library, and it is a correctly functioning IC. This facility
is useful when the IC type number is illegible or has been removed.
Use the MODE/CLEAR key to choose SEARCH mode, insert the
unknown IC into the socket and press the TEST/EXEC key. You will
be prompted to choose the number of pins of the IC you wish to
identify - use the MODE/CLEAR key to select from 3 to 16 pins or
'QUIT' to abandon this mode. Press the TEST/EXEC key again to
start the SEARCH or to quit as required.
During the identification process the display will indicate the
number of ICs identified (IDENT:) and will show graphically how far
through the library the SEARCH has progressed. At the end of the
SEARCH, a list of all the similar ICs will be scrolled onto the display.
The list may be scrolled again by pressing the TEST/EXEC key.
If the IC cannot be identified the message "Not in Library" will be
displayed. This means either that the IC is not in the library or it is
non-functional. Note that if the B & K Model 570A detects
excessive supply current (ICC! or BAT! warnings), the IC will not be
identified during the SEARCH, but can still be tested in SINGLE
mode.
If you have a user library present the search will extend to user ICs in
that library also. However, CompactLink contains a facility for
excluding ICs from the search if required.
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
12. self test mode
This feature allows you to check the integrity of the unit, including
the pin drivers and receivers, power supplies and other internal
hardware. The test executes automatically at switch on, but you can
if you wish perform a self-test at any time by selecting Self-Test
(DIAGS) mode using the MODE/CLEAR key and pressing
TEST/EXEC.
If a fault is discovered a brief description will be displayed which will
help our engineers to locate and rectify the fault. This message
should be noted and quoted in any correspondence relating to a
unit fault. Contact your distributor in the event of a self-test fail, but
first of all ensure that the socket was empty when the diagnostics
were run.
13. CompactLink mode
The B & K Model 570A is provided with an RS-232 interface to
connect to a PC with a serial COM port or using a USB to RS-232
converter. A companion software package CompactLink is available
which provides library management, test development and
debugging and user library update facilities. You can also use
CompactLink to update the software of your B & K Model 570A
without replacing the internal memory or opening the case.
To enter CompactLink mode, user the MODE/CLEAR key to enter
CMLINK mode, then press TEST/EXEC. Press TEST/EXEC again
to confirm that you wish to enter CompactLink mode, and the
display will show “Not Connected”. Run the CompactLink software
on your PC, connect the serial cable and follow the CompactLink
manual instructions to connect to the B & K Model 570A.
For comprehensive instructions on using CompactLink please refer
to the manual and built-in help supplied with the software.
Note that in CompactLink mode, including waiting for a connection,
the normal power down timeout is disabled and the unit will remain
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
on for ever. We recommend using a battery eliminator when using
CompactLink mode to develop test programs.
14. specifications
SPECIFICATIONS
Batteries: 4 X AA size
DC input: 6V, 850mA max, center positive, regulated.
Power consumption: Power off 10A max
Standby 30mA max
Testing IC dependent
Test parameters: Supplyvoltage 2V to 10V IC dependant
Op amp gains open loop, 1,2,11,46
Stimulus 0 - 10V, 8 bits, 330R source
Sense 0 to 10.5V, 12 bit, >1M load
RS-232 settings 38400 baud, 8 data bits, 1 stop bit, no parity
Dimensions: 200mm X 100mm X 55mm approx.
LibraryICs: Op amps, comparators, optos, regulators, references,
switches, miscellaneous
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
15. IC support list
15.1. introduction
This section is a complete list of the ICs supported by the B & K
Model 570A. If there are any special requirements necessary for a
particular IC, this will be indicated in the comments column in the
table. Always consult this list before testing an IC you have not
tested before, particularly when there is a comment present.
15.2. operational amplifiers
IC Number Comments
AD546 546
AD548 548
AD645 645
AD648 648
AD711 711
AD712 712
AD713 713
AMP03 03
CA1458 1458
CA3080 3080
CA3130 3130
CA3140 3140
CA3160 3160
CA3240 3240
CA3260 3260
CA5130 5130
CA5160 5160
CA5260 5260
HA3-2840-5 328405
ICL7611 7611
ICL7612 7612
ICL7621 7621
ICL7641 7641
ICL7642 7642
L272 1272
LF147 147
LF155 155
LF156 156
Software Version No.
BK570A 2.03
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
LF157 157
LF255 255
LF256 256
LF257 257
LF347 347
LF351 351
LF353 353
LF355 355
LF356 356
LF357 357
LF411 411
LF412 412
LM101 101
LM107 107
LM108 108
LM11 11
LM118 118 Add 47nF capacitor between IC pins 1 and 6
LM124 124
LM148 148
LM158 158
LM201 201
LM207 207
LM208 208
LM218 218 Add 47nF capacitor between IC pins 1 and 6
LM224 224
LM248 248
LM258 258
LM2900 2900
LM2902 2902
LM2904 2904
LM2924 2924
LM301 301
LM307 307
LM308 308
LM318 318 Add 47nF capacitor between IC pins 1 and 6
LM324 324
LM348 348
LM358 358
LM3900 3900
LM392 392
LMC6032 6032
LMC6042 6042
LMC660 660
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
LT1013 1013
LT1014 1014
MAX407 407
MAX427 427
MC3303 3303
MC33171 33171
MC33172 33172
MC33174 33174
MC3403 3403
NE531 531
NE5532 5532
NE5534 5534
OP-07 07
OP200 200
OP-27 27
OP-282 282
OP290 290
OP-37 37
OP-42 42
OP482 482
OP490 490
OP-77 77
OP-90 90
OP-97 97
OPA121 121
OPA606 606
OPA620 620
RC4458 4458
TL061 061
TL062 062
TL064 064
TL071 071
TL072 072
TL074 074
TL081 081
TL082 082
TL084 084
TLC1079 1079
TLC2272 2272
TLC271 271
TLC272 272
TLC274 274
TLC277 277
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
TLC279 279
TLC2872 2872
TLE2061 2061
TLE2062 2062
TLE2064 2064
TLE2071 2071
TLE2072 2072
TLE2074 2074
TLE2081 2081
TLE2082 2082
TLE2084 2084
TLE2161 2161
UA709-14 709
UA709-8 709
UA741-14 741
UA741-8 741
UA747 747
UA748 748
15.3. comparators
IC Number Comments
CMP04 04
LM111 111
LM119 119
LM139 139
LM193 193
LM211 211
LM219 219
LM239 239
LM2901 2901
LM2903 2903
LM293 293
LM311 311
LM319 319
LM3302 3302
LM339 339
LM393 393
LP111 111
LP211 211
LP239 239
LP265 265
LP2901 2901
LP311 311
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
LP339 339
LP365 365
LT1016 1016
TLC339 339
TLC3702 3702
TLC3704 3704
TLC372 372
TLC393 393
15.4. switches and multiplexers
IC Number Comments
4016 4016
4051 4051
4052 4052
4066 4066
4529 4529
DG201 201
DG202 202
DG211 211
DG212 212
DG308 308
DG309 309
DG411 411
DG412 412
DG413 413
DG417 417
DG418 418
DG419 419
DG508 508
LF13201 13201
LF13202 13202
LF13508 13508
15.5. regulators, references and virtual grounds
IC Number Comment
LM2930-5 29305 Add 100uF between IC pins 2 (-) and 3 (+)
LM2931-5 29315 Add 100uF between IC pins 2 (-) and 3 (+)
LM340T5 3405
LM7805 7805
LM7806 7806
LM7808 7808
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
LM7905 7905 Mayneed 10uF between IC pins 2 (-) and 3 (+)
MAX667 667 Mayneed 10uF between IC pins 4 (-) and 2 (+)
MAX872 872
MAX874 874
REF02 02
REF03 03
REF05 05
REF43 43
TLE2425 2425
TLE2426 2426
15.6. opto couplers and isolators
IC Number Comments
4N25 425
4N26 426
4N27 427
4N28 428
4N29 429
4N30 430
4N31 431
4N32 432
4N33 433
4N35 435
4N36 436
4N37 437
6N135 6135
6N136 6136
H11A1 111
H11A2 112
H11A3 113
H11A4 114
H11A5 115
HCPL2503 2502
HCPL2530 2530
HCPL2531 2531
HCPL4502 4502
HCPL4503 4503
ILCT6 6
ILD74 74
ISD74 74
LD428 428
MCT2 2
MCT210 210
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
MCT2200 2200
MCT2201 2201
MCT2202 2202
MCT271 271
MOC8030 8030
MOC8050 8050
TIL197 197
TIL198 198
TIL199 199
TLP250 250
TLP521 521
TLP521-2 5212
TLP521-4 5214
TLP559 559
TLP621 621
TLP621-2 6212
TLP621-4 6214
15.7. miscellaneous
IC Number Comment
AD7524 7524
DAC08 08
NE555 555
NE556 556
ULN2001 2001
ULN2002 2002
ULN2003 2003
ULN2004 2004
ULN2064 2064
ULN2065 2065
ULN2066 2066
ULN2067 2067
ULN2068 2068
ULN2069 2069
ULN2070 2070
ULN2071 2071
ULN2074 2074
ULN2075 2075
ULN2076 2076
ULN2077 2077
Protected bvlhe manmaclurer’s comiaht laws. All ria his reserved.
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
16. Service Information
Contact B&K Precision to receive a repair Return Authorization
tracking number. This number must be clearly written on the
exterior of the shipping carton and will assist us with the processing
of your return. Return all merchandise to B&K Precision Corp. with
pre-paid shipping. The flat-rate repair charge includes return
shipping to locations in North America. For overnight shipments
and non-North America shipping fees contact B&K Precision Corp.
Warranty Service: Please return the product in the original
packaging with proof of purchase to the below address. Clearly state
in writing the performance problem and return any leads, connectors
and accessories that you are using with the device.
Non-Warranty Service: Return the product in the original packaging
to the below address. Clearly state in writing the performance
problem and return any leads, connectors and accessories that you
are using with the device. Customers not on open account must
include payment in the form of a money order or credit card. For the
most current repair charges contact the factory before shipping the
product.
B&K Precision Corp. Phone: 714- 921-9095
22820 Savi Ranch Parkway Facsimile: 714-921-6422
Yorba Linda
CA 92887-4604
Include with the instrument your complete return shipping address,
contact name, phone number and description of problem.
Protected bythe manufacturer’s copyright laws. All rights reserved.
Model 570A Linear IC Tester
Copyright 1993-2007 B&K Precision Corp.
17. Limited One-Year Warranty
B&K Precision Corp. warrants to the original purchaser that its
product and the component parts thereof, will be free from defects
in workmanship and materials for a period of one year from the date
of purchase. B&K Precision Corp. will, without charge, repair or
replace, at its’ option, defective product or component parts.
Returned product must be accompanied by proof of the purchase
date in the form a sales receipt.
To obtain warranty coverage in the U.S.A., this product must be
registered by completing and mailing the enclosed warranty card to:
B&K Precision Corp., 22820 Savi Ranch Parkway, Yorba Linda, CA
92887 - 4604 within fifteen (15) days from proof of purchase.
Exclusions: This warranty does not apply in the event of misuse or
abuse of the product or as a result of unauthorized alterations or
repairs. It is void if the serial number is altered, defaced or
removed.
B&K Precision Corp. shall not be liable for any consequential
damages, including without limitation damages resulting from loss
of use. Some states do not allow limitation of incidental or
consequential damages, so the above limitation or exclusion may
not apply to you. This warranty gives you specific rights and you
may have other rights, which vary from state-to-state.
Model Number: _______________________
Date Purchased: _______________________
B&K Precision Corp. Phone: 714- 921-9095
22820 Savi Ranch Parkway Facsimile: 714-921-6422
Yorba Linda
CA 92887-4604