Microchip Technology 的 AT88SC018 Summary 规格书
.1 mg
Features
• Companion Chip to CryptoRF® and CryptoMemory®
⎯ Securely implements host algorithms
⎯ Securely stores host secrets
⎯ Verifies Host Firmware Digests
• High Security Features in Hardware
⎯ CryptoMemory and CryptoRF F2 Algorithm
⎯ SHA-1 Standard Cryptographic Algorithm
⎯ 64-bit Mutual Authentication Protocol (Under License of ELVA)
⎯ Permanently Coded Serial Numbers
⎯ High Quality Random Number Generator (RNG)
⎯ Metal Shield Over Memory
⎯ Data Scrambling in Nonvolatile Memory
⎯ Delay Penalties to prevent Systematic Attacks
⎯ Reset Locking to prevent Illegal Power Cycling
⎯ Voltage and Frequency Monitors
• Host-side Crypto Functions
⎯ Authentication Challenge Generation
⎯ Device Challenge Response
⎯ Message Authentication Codes (MAC) Generation
⎯ Data Encryption and Decryption
⎯ Secure Authentication Key Management
• Secure Storage and Key Management
⎯ Up to 16 sets of 64-bits Diversified Host Keys
⎯ Eight Sets of Two 24-bit Passwords
⎯ Secure and Custom Personalization
⎯ Up to 232-Byte Read/Write Configurable User Data Area
• Nonvolatile Up Counters
⎯ Four sets Unidirectional Counters
⎯ 6.4 Million Maximum Counts Per Counter
• Application Features
⎯ Low Voltage Supply: 2.7V – 3.6V
⎯ 2-Wire Serial Interface (TWI, 5V Compatible)
⎯ Standard 8-lead SOIC Plastic Package, Green compliant (exceeds RoHS)
• High Reliability
⎯ Endurance : 100,000 Cycles
⎯ Data Retention : 10 years
⎯ ESD Protection : 3,000 V min. HBM
CryptoCompanion™
Chip for
CryptoMemory and
CryptoRF
AT88SC018
Summary
5277DS–CryptoCompanion–9/09
hugJ/www.\Il.msl.gov/hgsgubs/fi9180-1 htm
E‘
2 CryptoCompanion™ Chip
5277DS–CryptoCompanion–9/09
1. Product Overview
The CryptoCompanion™ Chip is designed as the mate to Atmel’s CryptoRF and CryptoMemory chips, collectively
referred to in the remainder of this document as CRF.
CryptoCompanion makes extensive use of the SHA-1 hash algorithm as specified in
http://www.itl.nist.gov/fipspubs/fip180-1.htm and elsewhere. In this document, the nomenclature SHA-1(a, b, c) means
to concatenate a, b & c in that order and then pad them to a block size of 64 bytes before computing the digest.
CryptoCompanion generates SHA-1 digests of single round datasets at a time.
1.1. General Operation
The CRF chip contains secrets that must be known or derived by a host system in order to establish a trusted link
between the two and permit communications to happen. CryptoCompanion stores these secrets in an obscured way in
nonvolatile memory and contains all the circuitry necessary to perform the authentication, password and
encryption/decryption functions specified in the CRF datasheet. In this manner, the secrets do not ever need to be
revealed.
The general cryptographic strategy is as follows:
• Each CRF chip has a serial or identification number (ID) and authentication secret Gi stored in EEPROM. ID is
freely readable while Gi can never be read and is unique for all tags.
• CryptoCompanion contains an EEPROM that holds a set of common secrets (Fn). CryptoCompanion combines Fn
with ID and KID to compute a value of G that is expected to match that in the CRF chip. Specifically, G = SHA-1(Fn,
ID, KID)
• G is further diversified by the inclusion of a number (KID) generated by the host system in a manner of its choosing.
Typically, it will be the result of a cryptographic operation on the CRF ID value calculated using other data, secrets
and/or algorithms external to CryptoCompanion. This permits scenarios that offer varying degrees of additional
security.
• CryptoCompanion includes a general purpose cryptographic quality random number generator which is used to
seed a mutual authentication process between CryptoCompanion and CRF. If the CRF confirms the
CryptoCompanion challenge, and the CryptoCompanion confirms the CRF response, then the host system
proceeds with CRF operations. In this way the host system may use the CRF without knowing the CRF's secrets
directly.
1.2. CryptoCompanion Benefits
The following is a partial list of the benefits of using this chip versus storing the algorithms and secrets in standard
FLASH system memory.
• Keep confidential those core secrets that are used to authenticate with and communicate to/from CRF.
(Store them in EEPROM, use them on-chip)
• Flexible system implementation – multiple secrets and policies for different CRF locations within the system.
Multiple manufacturer setup options.
• Hardware encryption engines, avoids algorithm disclosure from reverse-compilation of system operating code.
• Full hardware security implementation makes it harder for an attacker (even with lab equipment) to get secrets
stored on CryptoCompanion.
• Global secrets are protected using strong security, standard algorithm (SHA-1).
• Robust random number generation avoids accidental replay for all cryptographic operations using the system, not
just with respect to CRF.
• Secure EEPROM storage for configuration information, etc. May permit reduction in the total BOM for the system.
• Easy to use – little programming required; no knowledge of security algorithms or protocols, fast time to market.
A lllEl‘
CryptoCompanion™ Chip
3
5277DS–CryptoCompanion–9/09
1.3. Package, Pin Definition & IO
1.3.1. Pin Definition
1.3.1.1. VCC , Gnd
Power supply is 2.7 – 3.6V. Supply current less than 5 mA.
CryptoCompanion will be available to accept commands 60 ms after the later of VCC rising above 2.7V or Reset being
driven high if CryptoCompanion is in a security delay then this interval is significantly longer.
During Power Up, VCC must exhibit a monotonic ramp at a minimum rate of 50 mV/mS until VCC has crossed the 2.7V
level. During Power Down, VCC must exhibit a monotonic ramp at a minimum rate of 50 mV/mS once it has dropped
below the 2.5V boundary. CryptoCompanion does not support hot swapping or hot plugging.
VCC must be bypassed with high quality surface mount capacitors that are properly located on the board. Atmel
recommends two capacitors connected in parallel having a value of 1μF and 0.01μF. The capacitors should be
manufactured using X5R or X7R dielectric material. These capacitors should be connected to CryptoCompanion using
a total of no more than 1cm PC board traces. Atmel recommends the use of a ground plane and a trace length of less
than 0.5cm between the capacitors and the VCC pin. Failure to follow these recommendations may result in improper
operation.
1.3.1.2. SDA
Two wire interface data pin, 5 V compatible. Minimum data setup time = 0.1 μs, and minimum data hold time = 0 μs min.
The system board must include an external pull-up resistor.
1.3.1.3. SCL
Two wire interface clock pin, 5 V compatible. Maximum SCL rate is 400KHz, minimum TLOW = 1.2 μs, minimum
THIGH = 0.6 μs. The system board must include an external pull-up resistor.
1.3.1.4. Reset (RST)
This active low input will reset all states within CryptoCompanion. Honored regardless of the state of PowerDown.
1.3.1.5. PowerDown (PDN)
When held low, the part operates normally. When held high the part will go to sleep and ignore all transitions on SDA
and SCL, power consumption will drop to less than 10 μA. There is a 50 ms delay between this pin falling and the first
transition on SDA or SCL that will be accepted by the chip.
m‘
4 CryptoCompanion™ Chip
5277DS–CryptoCompanion–9/09
1.3.2. Package
CryptoCompanion is packaged in an 8 lead SOIC package with the following pin definition:
Table 1. 8 lead SOIC package pin definition
Pin Number Pin Name
1 VCC
5 Gnd
7 SDA
8 SCL
4 RST
3 PDN
2,6 NC
Pins 2 & 6 are not internally connected and should be connected to ground on the PC board.
1.3.3. Connection Diagram
Figure 1. Connection Diagram
2.7v - 5.5v
2.7v - 3.6v
SDA
SCL
Microprocessor CryptoCompanion
1.3.4. Environmental
CryptoCompanion is guaranteed to operate over the industrial temperature range of -40° to 85° C. ESD is rated at 3KV,
Human Body Model.
1.3.5. TWI Input/Output Operation
CryptoCompanion communicates to the system using a two wire interface (TWI), which is similar to SMBus. The chip
operates as a slave and does not support clock stretching. This two wire protocol is identical to that supported by the
Atmel AT24C16B serial EEPROM chips. Please see that datasheet on the Atmel web site for detailed timing and
protocol information.
A “El.
CryptoCompanion™ Chip
5
5277DS–CryptoCompanion–9/09
The system processor is expected to properly format commands for CryptoCompanion (which may include information
from the CRF chip), and then process the outputs of CryptoCompanion (which may include sending some of the
outputs to the CRF chip).
CryptoCompanion cannot directly communicate with CRF chips. Both CRF and CryptoCompanion are slave devices.
The bus master may use one or two busses to communicate with them. Separate TWI addresses must be used if both
chips are on the same bus.
1.4. Memory Locking
When this initialization is complete the Lock command should be executed which limits access to the memory per the
restrictions listed later in this section. The system can determine the current lock value by using the
ReadManufacturingID command to read out the ManufacturingID value (MfrID) and the lock byte.
The table below describes the encoding of the least significant two bits of the Lock byte. On shipment from Atmel,
Lock[1:0] will have a value of either 10 or 00, depending on the part number ordered. An AT88SC018 in either of these
two states is considered ‘unlocked’. It is not possible to change from one of these unlocked states to the other.
After the Lock command has been executed, the Lock byte will have the value 0xFF. Subsequent changes to the Lock
byte are impossible.
Table 2. Memory Locking
LockBit 1 Lock Bit 0 (LSB) Meaning
1 1 Locked. ReadMemory & WriteMemory enabled, subject to the restrictions in this
section. WriteMemoryEncrypted and ReadMemoryDigest disabled.
1 0 Unlocked/Confidential. ReadMemoryDigest, WriteMemory and
WriteMemoryEncrypted enabled. ReadMemory disabled.
0 0 Unlocked. ReadMemory & WriteMemory enabled. WriteMemoryEncrypted and
ReadMemoryDigest disabled.
2. AC & DC Characteristics
Table 3. DC Characteristics (1)
Applicable over recommended operating range from VCC = +2.7 to 3.6 V,
TAC = -40o C to 85o C (unless otherwise noted)
Symbol Parameter Test Condition Min Typ Max Units
VCC Supply Voltage 2.7 3.6 V
ICC Supply Current 400kHz 5 mA
ISB Standby Current VIN = VCC or GND 15 μA
VIL SDA Input Low Voltage -0.3 VCC x 0.3 V
VIL CLK Input Low Voltage -0.3 VCC x 0.3 V
VIL RST Input Low Voltage -0.3 VCC x 0.3 V
VIL PDN Input Low Voltage -0.3 VCC x 0.3 V
VIH SDA Input High Voltage VCC x 0.7 5.25 V
VIH SCL Input High Voltage VCC x 0.7 5.25 V
VIH RST Input High Voltage VCC x 0.7 5.25 V
A “El.
6 CryptoCompanion™ Chip
5277DS–CryptoCompanion–9/09
VIH PDN Input High Voltage VCC x 0.7 5.25 V
IIL SDA Input Low Current 0 < VIL < VCC x 0.15 -10 10 μA
IIL SCL Input Low Current 0 < VIL < VCC x 0.15 -10 10 μA
IIL RST Input Low Current 0 < VIL < VCC x 0.15 -10 10 μA
IIL PDN Input Low Current 0 < VIL < VCC x 0.15 -10 10 μA
IIH SDA Input High Current VCC x 0.7 < VIH < VCC -10 10 μA
IIH SCL Input High Current VCC x 0.7 < VIH < VCC -10 10 μA
IIH RST Input High Current VCC x 0.7 < VIH < VCC -10 10 μA
IIH PDN Input High Current VCC x 0.7 < VIH < VCC -10 10 μA
VOH SDA Output High Voltage 20k Ohm external
Pull-up VCC x 0.8 V
VOL SDA Output Low Voltage IOL = 1mA 0.4 V
Note: 1. Typical values at 25° C. Maximum values are characterized values and not test limits in production.
SCL
tsu STA
SDA \N
‘m H
IF 5
‘—>
1Low
'HDsTA 1M: DAT
‘Low
‘—’ ‘BUF
SDA OUT
A lllEl‘
CryptoCompanion™ Chip
7
5277DS–CryptoCompanion–9/09
Table 4. AC Characteristics (1)
Applicable over recommended operating range from VCC = +2.7 to 3.6 V,
TAC = -40o C to 85o C, CL = 30pF (unless otherwise noted)
Symbol Parameter Min Max Units
fCLK Clock Frequency 0 400 kHz
Clock Duty cycle (2) 40 60 %
tR Rise Time - SDA, RST, PDN (2) 300 nS
tF Fall Time - SDA, RST, PDN (2) 300 nS
tR Rise Time - SCL (2) 300 nS
tF Fall Time - SCL (2) 300 nS
tAA Clock Low to Data Out Valid 900 nS
tHD.STA Start Hold Time 600 nS
tSU.STA Start Set-up Time 600 nS
tHD.DAT Data In Hold Time 100 nS
tSU.DAT Data In Set-up Time 100 nS
tSU.STO Stop Set-up Time 600 nS
tDH Data Out Hold Time 50 900 nS
Note: 1. Typical values at 25° C. Maximum values are characterized values and not test limits in production.
2. This parameter is not tested. Values are based on characterization and/or simulation data.
Figure 2. SCL: Serial Clock, SDA: Serial Data I/O®
A “El.
8 CryptoCompanion™ Chip
5277DS–CryptoCompanion–9/09
3. Ordering Codes
Table 5. Ordering Codes
Ordering Code Package Voltage
Range
Memory Locking
(see
Section 1.4 for Lock Definitions) Temperature Range
AT88SC018-SU-CM 8S1 2.7V – 3.6V 00 (Unlocked) Green compliant (exceeds
RoHS), Industrial (-400 C – 850
C), Bulk
AT88SC018-SU-CM-T 8S1 2.7V – 3.6V 00 (Unlocked) Green compliant (exceeds
RoHS), Industrial (-400 C – 850
C), Tape and Reel
AT88SC018-SU-CN 8S1 2.7V – 3.6V 10 (Unlocked/Confidential)
Green compliant (exceeds
RoHS), Industrial (-400 C – 850
C), Bulk
AT88SC018-SU-CN-T 8S1 2.7V – 3.6V 10 (Unlocked/Confidential)
Green compliant (exceeds
RoHS), Industrial (-400 C – 850
C), Tape and Reel
Table 6. Package Type
Package Type Description
8S1 8-lead, 0.150” Wide, Plastic Gull Wing Small Outline Package (JEDEC SOIC)
BW‘
WEE
L
1,
TOP VIEW
END VIEW
El —<—> —> h
A COMMON DIMENSIONS
{um 01 Measuva = mm)
[ \ A1 SVMBOL MIN NOM MAX NOTE
A 1.35 7 I 75
H: j * A‘ 0.10 7 0.25
' 4 b 0.31 7 o 51
c 0.17 7 o 25
D 4.30 7 5 05
El 3 a1 7 3 99
E 5 79 7 6 20
SIDE VIEW 8 1.27Bsc
L 0 I‘D - I 27
a n‘ 7 a‘
Non These draw/mus are In: uenam mmnuauan onw R2121 1a JEDEC Drawmu M5»u121vanzm7n AA 1m Dmperdlmensmns \olemnces, damms. 21c
3/17/05
TITLE DRAWING N0. REV.
m 1150 E Cheyenne Mm, Blvd. 551‘ B-lead (0.150" Wwde Body), Plastic Gun Wing 531 c
_ Colorado Spr1ngs,CO 80906 Small Oulllne (JEDEC SOIC)
A IIIEI.“
—>
CryptoCompanion™ Chip
9
5277DS–CryptoCompanion–9/09
4. Package Drawing
Figure 3. 8S1 – SOIC
A lllEl‘
10 CryptoCompanion™ Chip
5277DS–CryptoCompanion–9/09
5. Revision History
Doc. Rev. Date Comments
5277DS 09/2009 Finalized AC & DC Charateristics. Updated Counter information.
5277CS 02/2009 Document updated.
5277BS 12/2008 Document updated.
A IIIEL
5277DS–CryptoCompanion–09/09
Headquarters International
Atmel Corporation
2325 Orchard Parkway
San Jose, CA 95131
USA
Tel: 1(408) 441-0311
Fax: 1(408) 487-2600
Atmel Asia
Room 1219
Chinachem Golden Plaza
77 Mody Road Tsimshatsui
East Kowloon
Hong Kong
Tel: (852) 2721-9778
Fax: (852) 2722-1369
Atmel Europe
Le Krebs
8, Rue Jean-Pierre Timbaud
BP 309
78054 Saint-Quentin-en-
Yvelines Cedex
France
Tel: (33) 1-30-60-70-00
Fax: (33) 1-30-60-71-11
Atmel Japan
9F, Tonetsu Shinkawa Bldg.
1-24-8 Shinkawa
Chuo-ku, Tokyo 104-0033
Japan
Tel: (81) 3-3523-3551
Fax: (81) 3-3523-7581
Product Contact
Web Site
www.atmel.com
Technical Support
CryptoMemory@atmel.com
CryptoRF@atmel.com
Sales Contact
www.atmel.com/contacts
Literature Requests
www.atmel.com/literature
Disclaimer: The information in this document is provided in connection with Atmel products. No license, express or implied, by estoppel or otherwise, to any
intellectual property right is granted by this document or in connection with the sale of Atmel products. EXCEPT AS SET FORTH IN ATMEL’S TERMS AND
CONDITIONS OF SALE LOCATED ON ATMEL’S WEB SITE, ATMEL ASSUMES NO LIABILITY WHATSOEVER AND DISCLAIMS ANY EXPRESS, IMPLIED OR
STATUTORY WARRANTY RELATING TO ITS PRODUCTS INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTY OF MERCHANTABILITY, FITNESS
FOR A PARTICULAR PURPOSE, OR NON-INFRINGEMENT. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, CONSEQUENTIAL,
PUNITIVE, SPECIAL OR INCIDEN-TAL DAMAGES (INCLUDING, WITHOUT LIMITATION, DAMAGES FOR LOSS OF PROFITS, BUSINESS INTERRUPTION,
OR LOSS OF INFORMATION) ARISING OUT OF THE USE OR INABILITY TO USE THIS DOCUMENT, EVEN IF ATMEL HAS BEEN ADVISED OF THE
POSSIBILITY OF SUCH DAMAGES. Atmel makes no representations or warranties with respect to the accuracy or completeness of the contents of this document
and reserves the right to make changes to specifications and product descriptions at any time without notice. Atmel does not make any commitment to update the
information contained herein. Unless specifically provided otherwise, Atmel products are not suitable for, and shall not be used in, automotive applications. Atmel’s
products are not intended, authorized, or warranted for use as components in applications intended to support or sustain life.
© 2009 Atmel Corporation. All rights reserved. Atmel®, Atmel logo and combinations thereof, CryptoMemory®, CryptoRF®, and others are registered trademarks,
CryptoCompanion™, and others are trademarks of Atmel Corporation or its subsidiaries. Other terms and product names may be trademarks of others.