u-blox 的 EVK-ANNA-B112 Quick Start 规格书
Software installation
The EVK-ANNA-B112 software and doc-
umentation is available at www.u-blox.
com/evk-search. Supported Windows
operating systems are Vista, 7, 8, and 10.
1. Download latest s-center software; run
the executable following instructions.
2. When the installation is complete, find
the s-center menu under Windows
Start button, All Programs > u-blox
3. In the s-center menu, you will find the
s-center application, user guide and
uninstall options.
Refer to the EVK-ANNA-B112 User
Guide for a comprehensive description of
the evaluation kit.
Quick Start EVK-ANNA-B112
Copyright © 2019, u-blox AGUBX-18019809 - R03
ANNA-B112
module
U.FL
connector
UART LEDs: DS1, DS2,
DS5, DS6, DS7, DS8
USB connector
RESET button
(SW0)
Restore button
(SW1)
Power RGB
LED DS9
Kit includes
• EVK-ANNA-B112 board
• NFC antenna
• USB cable
• 2.4 GHz external antenna*
* EVK-ANNA-B112U only
More information
This evaluation kit is also used as an
open CPU platform to develop custom
applications. See the ANNA-B112
System Integration Manual.
For more information regarding
EVK-ANNA-B112, contact your nearest
u-blox support:
www.u-blox.com/support
Driver installation
1. Connect the EVK-ANNA-B112 board to
your PC using the included USB cable.
2. Verify that the USB drivers are in-
stalled successfully.
NOTE: In case the drivers are not in-
stalled automatically, refer to the
EVK-ANNA-B112 User Guide.
3. Once the drivers are installed, a COM
port is enabled in Windows. Use the
Windows Device Manager to view the
port number (COM #) for the USB
serial port.
For EVK-ANNA-B112U, attach the
antenna to the U.FL connector. The
EVK-ANNA-B112C has an internal
antenna.
UBX-18019809 - R03