Octavo Systems LLC 的 OSD335x-SM Power Application Note 规格书
Figure 1
"555217: maasx
pm: mule scum:
svs vow
pm: mm mm. fills
Emmzl anpnnzvllx
mam vulIago mus
mm mmmnnl nus
sqpauznmnm
HIIIII
\‘ymflmv
|
svsjnmjpzv
svsynnyw
1
srs_vnn3_spsv
svsynnzjvav
Isvs_vn D_mv
vsAvnuLstv
haw
i
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
1 Introduction
This application note is intended for engineers to understand the power management system of
OSD335x-SM. It is also intended to aid in power budgeting for systems using the OSD335x-SM. It
provides an overview of the power management system inside the OSD335x-SM and runs through an
example application power budgeting procedure.
The OSD335x-SM contains the TPS65217C Power Management Integrated Circuit(PMIC) and the TL5209
Low Drop-Out(LDO) regulator as well as all associated passives for power management. The PMIC is
responsible for powering the AM335x processor and the DDR3 as well as provide output power for other
system needs. It provides configurable power-up and power-down sequencing required by the
processor and monitors the processor input voltage levels. The PMIC contains 3 DC-DC power
converters, 2 LDOs and 2 load switches that can be configured as LDOs that can be used as power
supplies. It can be powered by any combination of a 5V AC adapter, USB port, or Single Cell Li-Ion
battery. Figure 1 shows the power system of OSD335x-SM including connections between the PMIC and
various power domains of the processor.
Figure 1: Power connections inside OSD335x-SM
The OSD335x-SM allows the I/O voltage domains (VDDSHVx) of the AM335x to be set to either 1.8V or 3.3V.
The VDDSHVx pins of the OSD335x-SM (ie VDDSHV1 thru VDDSHV6), which can be found in Table 5.5, must be
connected to either a 1.8V or 3.3V power source in order to provide power to the I/Os. Recommendations on
how to connect the I/O voltage domain pins is in the OSD335x-SM Layout Guide in the Reference Documents
section. See the AM335x datasheet in the Reference Documents section for more information on the pins
associated with each I/O voltage domain.
1
P.
.w
T
2
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
Table 1 shows the voltage output levels of each of the voltage sources. Each of the output voltages can
be changed dynamically using I2C commands when the PMIC is in active mode.
Table 1 PMIC voltage outputs
TPS65217C Voltage Source
OSD335x Voltage rail
Voltage (V)
DCDC1
VDDS_DDR
1.5
DCDC2
VDD_MPU
1.1
DCDC3
VDD_CORE
1.1
LDO1
SYS_RTC_1P8V
1.8
LDO2
SYS_VDD2_3P3V
3.3
LDO3
SYS_VDD_1P8V
1.8
LDO4
SYS_VDD3_3P3V
3.3
on
3
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
Table of Contents
1 Introduction ............................................................................................................................................ 1
2 Revision History ...................................................................................................................................... 4
3 Power Up Sequence ............................................................................................................................... 5
3.1 Additional functions of the PMIC ............................................................................................................ 6
4 Power Budgeting: How to Approach it? ................................................................................................. 6
4.1 Step 1: Creating a Power Diagram .................................................................................................. 6
4.2 Step 2: Creating a Power Budget ..................................................................................................... 8
4.2.1 Maximum Power ...................................................................................................................... 8
4.2.2 Refining the Power Budget ..................................................................................................... 14
4.3 Step 3: Tally Up .............................................................................................................................. 16
5 Conclusion ............................................................................................................................................ 17
6 Reference Documents .......................................................................................................................... 17
4
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
2 Revision History
Revision Number
Revision Date
Changes
Author
1
10/24/2017
Initial Release
Neeraj Dantu
Notice: The information provided within this document is for informational use only. Octavo Systems
provides no guarantees or warranty to the information contained.
s P, I E ..
Figure 2,
I I DLVI I DLYZ I DLY3 I DLV4 I
I Ims 5ms 1ms 1ms
svsivom \ I I I I I
—‘ I | I |
PMICiNWAKEUP | | I | | I I
PWRiEN | I I I I o
I | I |
SYS_RTC_1P8V I I I I I o
SYS_VDD2_3P3V I I I I o
I I I I
VDDsiDDR | | I I 0
VDD_MPU I I I I I ' o
| | | | I
VDD CORE
7 I I I I I o
SYSivDDilPBV | | ‘—I—|—I_ o
I | I—I—
svsivomiapav I 0
PGDLV
PMIC70UT7PGOOD I I I I I I' 20“ I o
I
LDO_PGOOD '
5
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
3 Power Up Sequence
The power-up sequence of the processor is shown below in Figure 2, with the numbers in red
representing the order in which they come up, and the main power up events are described below:
Figure 2: AM335x + PMIC power up sequence for OSD335x-SM
1. SYS_RTC_1P8V is activated.
2. PMIC_OUT_LDO_PGOOD rail which is connected externally to the processor’s RTC_PWRONRSTN
(Power on reset of RTC domain) is pulled high to indicate presence of right voltages for the RTC
domain of the processor to power-up.
3. RTC circuitry in the processor comes up and pulls the PMIC_IN_PWR_EN signal high instructing
the PMIC to start power-up sequence. The output of DCDC1 (VDDS_DDR) which powers the DDR
memory is also activated.
4. Output of LDO3 (SYS_VDD_1P8V) is activated
5. Output of LDO2 (SYS_VDD2_3P3V) is activated
6. Output of LDO4 (SYS_VDD3_3P3V) is activated
7. Outputs of DCDC2 (VDD_MPU) and DCDC3 (VDD_CORE) are activated
8. PMIC_OUT_PGOOD which is connected externally to the processor’s PWRONRSTN (Power on
reset of AM335x) of the processor is pulled high releasing the processor from reset.
datasheet
6
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
This power up sequence and delays between each step of the sequence are already programmed
into the PMIC inside the OSD335x so you don’t need to worry about it. The power-down sequence
follows the reverse order of the power-up sequence.
3.1 Additional functions of the PMIC
The PMIC also performs some tertiary functions. A few of the key functions are listed below. For a
complete explanation of all the functions provided by the TPS65217C PMIC refer to the datasheet.
1. The PMIC retrieves the processor from OFF or SLEEP mode upon detecting a falling edge on
PMIC_IN_PB_IN. It also power cycles the processor if PMIC_IN_PB_IN is held low for more than
8 seconds.
2. It provides an active low wake up signal (PMIC_OUT_NWAKEUP) which is de-asserted when a
wakeup event is detected.
3. The PMIC has an interrupt pin (PMIC_OUT_NINT) to signal an event or fault condition to the
processor. The pin is released when the processor reads the INT register.
4. PMIC provides a linear charger for Single Cell Li-Ion batteries and allows charging of the battery
and powering of the system at the same More information can be obtained from the datasheet.
5. The TPS65217C provides protection to the AM335x and itself in the event of catastrophic
situations like an unexpected short or excessive current leakage.
6. It monitors the functioning of a battery if one is connected and charges the battery when
possible.
Now that the function and of the PMIC and its relationship with the processor is clear, the process of
power budgeting discussed below can be better understood.
4 Power Budgeting: How to Approach it?
It is a good practice to make a power budget for your product/design at the beginning of the project.
Good power budgeting contributes to circuit robustness, increased product life and reduced cost of the
product. A power budget should include the availability of power, operating temperature, amount of
data collected, communication, and operation modes of the processor.
4.1 Step 1: Creating a Power Diagram
The first step in making a power budget is to have a power diagram that shows all the power paths of
the system. Start with all the available power sources for the system. For OSD335x, this would include
power rails that are described in the datasheet as output power supplies. There are six output power
rails on the OSD335x including a 2.75V – 5.5 output (SYS_VOUT), three 3.3V outputs (SYS_VDD1_3P3V,
SYS_VDD2_3P3V and SYS_VDD3_3P3V) and three 1.8V outputs (SYS_RTC_1P8V, SYS_VDD_1P8V and
SYS_ADC_1P8V).
Perk:
Range of SYS_VOUT is determined by input power supply voltage. For example, if the SiP is being powered
through a battery (VIN_BAT), SYS_VOUT can be 2.75 V – 5.5 V depending on the battery voltage. Due to the
dropout behavior of the LDO TL5209, its output voltage rail SYS_VDD1_3P3V should not be used when the
OSD335x is being powered through VIN_BAT. Please refer to the TL5209 datasheet for details.
Figure 3
IvaIH-ur
mu mnmhmm
use S‘ave
Lonnenar
mum II‘M/hMHl (m)
“MM-HIM mum,
5V5 VDDl 3P3V 3.3 V
mm,» \rmm
Wh‘ x
mm m SN7-men7m'um)
mam 1y nmwm [H]
mum
MM \Hme
I
I
I
I
I
I
I
I
I
I
I
I
I
wmvnmnm m 1‘ m) I
I
I
I
I
I
I
I
I
I
I
I
I
I
~-_-____-_—
7
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
Next, put in the power consuming components and connect them to the appropriate power rail. The
connection should be based on the voltage input level for the component. Current supply capacities of
the power rails and ease of use can also be factors for choosing the best power rail for the component.
In order to understand this process, let us use the OSD3358-SM-RED Platform. The board provides
access to many peripherals of OSD335x-SM and has a number of external components powered by the
OSD335x-SM. Figure 3 shows the completed power system diagram for the design. It shows most of the
components that draw at least a nominal amount of power.
The diagram not only shows the power rail for a particular component but also lists all the components
that are being powered by a power rail. In addition to helping with the power budgeting, this allows you
to identify power issues early in the design process and make necessary adjustments.
Figure 3: OSD3358-SM-RED power system diagram
Table 2
datasheet
datasheet
8
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
4.2 Step 2: Creating a Power Budget
The next step involves making a power budget to estimate power consumption of each component and
thus the total power consumption of the board.
4.2.1 Maximum Power
There are several challenges involved in accurately estimating the power consumption of each
component. For example, it is difficult to estimate how much current, the AM3358 processor and the
DDR Memory draw since that is highly application specific. Power consumption will also depend on the
presence of a USB device or a Micro SD card. To account for all situations, we can start out by assuming
maximum power consumption for all the components. Table 2 shows the power budget table for
OSD3358-SM-RED assuming maximum power consumption for each component.
Table 2: Power budget table with maximum power consumption
Part Name
Part Number
Max Current (mA)
Supply voltage
rail Voltage
(V)
Max Power (mW)
AM3358
U1
307.8
Internal
5
1539
TPS65217C
U1
< 1
Internal
5
<5
TL5209
U1
25
Internal
5
125
DDR RAM
U1
339
Internal
1.5
508.5
TPS2051
U15
< 1
SYS_VOUT
5
< 5
USB Connectors
X4, X5
< 500
SYS_VOUT
5
< 2500
24LC32AT
U1
3
Internal
3.3
15
APX811
U4
20
SYS_VDD1_3P3V
3.3
66
USB2534-1080AEN
U8
80
SYS_VDD1_3P3V
3.3
264
ASDMB-12.000MHZ
Y3
15
SYS_VDD1_3P3V
3.3
49.5
ASDMB-24.576MHz
Y5
15
SYS_VDD1_3P3V
3.3
75
DM3BT-DSF-PEJS
X3
200
SYS_VDD1_3P3V
3.3
1000
SDIN8DE2-16G
U7
80
SYS_VDD1_3P3V
3.3
400
SN74LVC1G07DCK
U3
24
SYS_VDD1_3P3V
3.3
120
SN74LVC2G241DCUR
U6
24
SYS_VDD1_3P3V
3.3
120
AR8035-AL1A
U9
128
SYS_VDD1_3P3V
3.3
422.4
TDA19988BHN
U10
77
SYS_VDD_1P8V
1.8
385
MPU-9250
U23
3.7
SYS_VDD1_3P3V
3.3
12.21
TMP468
U17
10
SYS_VDD1_3P3V
3.3
33
BMP280
U22
1
SYS_VDD1_3P3V
3.3
3.3
S25FL127S
U21
50
SYS_VDD1_3P3V
3.3
165
AT97SC3205T
U16
25
SYS_VDD1_3p3V
3.3
82.5
Total
~7895
**SDIN8DE2-16G datasheet is not available on the internet. So, an equivalent datasheet was used to
determine current consumption
**AT97SC3205T datasheet does not specify current consumption. So, an equivalent datasheet was used
Maximum current consumption values can be found from the component datasheets for most devices.
However, there is no deterministic way of calculating the current consumed by the AM335x and the
DDR3 as they are highly application specific. The next two sections will explore how to use tools
provided by TI and Micron to estimate the max power used by the AM335x and DDR.
AM335x Power Estimation Tool
htt :
www.U.com too‘ owerest
Device Revision P621
DDR Type DDRBL
DDR Loading 1
Junction Temperature ('C) 40
Power Estimation Mode Max
Sman Reflex 01f
VDDSHV1 Voltage [V] 3.3
VDDSHV2 Voltage [V] 3.3
VDDSHV3 Voltage [V] 3.3
VDDSHV4 Voltage [V] 3.3
VDDSHV5 Voltage [V] 3.3
VDDSHV6 Voltage [V] 3.3
9
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
4.2.1.1 Using Power Estimation Tool for estimating AM3358 power consumption
Texas Instruments provides access to a power estimation tool that can calculate the internal power
consumption of AM3358 including individual power domains of the processor. The process involves
filling out a spreadsheet and submitting it to a webpage. The detailed procedure is described in the wiki
page “AM335x Power Estimation Tool”. A short overview of the process with notes on usage with the
OSD335x is given below. The inputs shown in the screenshots were put in to calculate the maximum
power consumption of AM335x.
1. Download either the simplified or the advanced spreadsheet for AM335x from
http://www.ti.com/tool/powerest
2. In section A, among other inputs, set the device revision to PG2.1, DDR type to , DDR loading to
1, and all the VDDSHVx voltages to 3.3. The power modes of AM335x are discussed later in this
document.
Figure 4: System configuration in power estimation spreadsheet
OPP Slot 0
CORE OPP 0PP100
MPU OPP NI'I'RO
MPU Frequency (Mill) 1000
Slot 0
ARM Sub—system Utilization %
ConexAB 1M
ConexAB NEON 1W
SGX Sub—system (For SGX- Slot 0
enabled devices only) Utilization 56
SGX 1W
10
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
3. Set the Operational Performance Point (OPP), MPU frequency and Utilization percentages in
Section B.
Figure 5: Processor options and utilization in power estimation spreadsheet
4. Input Utilization percentages for peripheral usage of AM335x in section C.
Slol 0
Module Name Utilization 56
EDMA 1M
EMIF 1M
GPMC 1W
OCMC—RAM 1M
LCDC 1“
USB 1“
Ethernet MAC 1”
PRUSS 1W
McASP1 1W
McASPZ 1N
MMC1 1M
MMCZ 1N
MMC3 1M
Misc. Peripherals (UART, SPI,
I26, CAN, GPIO, eHRPWM, eQEP, 1M
RTC etc)
Module Name Slot 0
ADC
11
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
Figure 6: Peripheral utilization in power estimation spreadsheet
5. Enable/Disable analog modules in Section D
Figure 7: ADC module usage in power estimation spreadsheet
6. Click on the submit button in the spreadsheet. This will open a webpage to which the edited
spreadsheet can be uploaded to. This requires logging in to TI’s website.
7. A power analysis report will be emailed to the email address attached to the user account
logged into.
m
T
sstEus
AM335x Power Estimation Report
mm m. um. mmleflD‘lJmns
ammo" rump-11mm): 40
mu. mm mm
AM can in. mm] mmououm
I I I
VDIla 01V) Currant“)
mm max Laalaga Acllva
VDD MPU 1.33 1.30 0.020 0.010
VDD CORE 1.10 1.10 0.010 0.411
VDDS DPLL 1.00 1.00 0.000 0.010
V008 SMM 1.00 1 .00 0.000 0.000 0.00007
VDDS DDR 1.” 1 .00 0.000 0.000 0.000 0.00010
VDDS 1P5 1.00 1 .00 0.000 0.000 0.000 0.01 000
VDDS SF! 0.00 0.00 0.000 0.000 0.000 0.01770
V00“ PUV USN/1 VDDA ADC 1.00 1.00 0.000 0.000 0.000 0.00000
VDDA! PSV US$011 0.00 0.00 0.000 0.000 0.000 0.00000
final 1 .00001
Nohl :
VDDB_DPLL Incum- VDD$_PLL_MPU. VDDS_PLL_CDRE_LCD and VDD$_PLL_DDR pow" suppllon
vuns_snm Includu vnos_sRAM_conE_aa and vuns_amu_mu_aa pawn luppflu
vnos_1n lncludu vans, vnns_mc, vnns_osc ma 1,: v VDDSNVX pow-r Inwllu
V008 0F: lncllld'l 0.0 V VDUSflVl pow" Iuppllol
Processor SDK Linux kernel gerformance guide
AM335x gower consumption summam
sgreadsheet
12
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
Figure 8: Power estimation result
The worst-case current consumption can be obtained by maximizing the inputs to the spreadsheet.
Other relevant resources that help estimation of AM335x power usage are given below:
1. Processor SDK Linux kernel performance guide
2. AM335x power consumption summary
4.2.1.2 Estimating Power for the DDR3
Like the AM335x spreadsheet, Micron provides a spreadsheet to estimate DDR3L power consumption.
Though the exact power consumption depends on the part number of the memory, the spreadsheet
serves as a ball park estimation tool. A brief use case of the spreadsheet is shown below.
1. Download the spreadsheet available for the DDR3L memory on Micron’s website.
.
m
DRAM Density
Number 01 DO: per DRAM
Speed Grade
Mode Register bit 12: Precharge PD Exit Mode
{{{4
quRD DORS SDQAM mm weer Der MNldual DO
mmsmuwmwnuosnunmlsnw
quwfi DDR3 SDRAM termination power per mammal
DO uumg WRITEs m Ims new
Pompom DDR3 seam Ierlnmahon power per numeual
DO aumg READS 1mm mner DRAM
POQWRMH DOES SDMM lemunahon power per mwual
DO dumg WRITES to «he! DRAM
The percentage mm Ina! an banks on me
DRAM file In a precnarged SIM!
The percemage at me all bank manage line
for which cxz rs new Low
The manage mm: at Ieasl one bank acllve
nm: to: much CKE I: held LOW
Page VIII late
RDSCME The percentage o'clock cyclesmlch are
mmtmg read data rmm me DRAM
Wflscms mpememage onlock cyclesvmxn are
unpunmg m dale lo the DRAM
IennRDunx The manage onlockcyclesumxn are
lemma} 3 read data In ”lame! DRAM
Ingrmwnsum The managemuocuyclesmxn are
\ terminal: . me data m anomer DRAM
amps“. Tne average lune between ACT commands lo 5 u as
[Ills OW (Includes ACT losame or dlflefefll
Dam In me same DRAM Genet
13
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
2. Input SDRAM configuration inputs in the “DDR3 Config” The screenshot shows inputs specific to
DDR3 memory used in OSD335x.
Figure 9: DDR3 configuration in power estimation spreadsheet
3. Input DRAM usage conditions in “System Config” These inputs may vary based on use case. The
inputs shown below are for estimating worst case power consumption of the RAM.
Figure 10: DDR3 system configuration in power estimation spreadsheet
m
Psys Power Consumption Summary
Total Background Power
Total DDR3 SDRAM Power
TERM 2nd rank
ACT 182.1 mW
Total Activate Power 182.1 mW
RD 0.0 mW
WR 70.3 mW
READ IIO 0.0 mW
Write ODT 207.6 mW
—
ACT STBY 40.9 mW
PRE STBY 0 0 mW
ACT PDN O 0 mW
PRE PDN 0 0 mW
REF 7 6 mW
14
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
4. The “Summary” page will show the power consumption summary for previously entered inputs.
Figure 11: DDR3 power consumption summary
From the results, the worst case current consumption was calculated to be 339 mA with 1.5 V input
4.2.2 Refining the Power Budget
Some of the current consumption numbers are highly unrealistic. No system uses all the processor cores
and peripherals at a 100% utilization. The DDR current consumption is calculated assuming 100% of the
time is spent writing to the memory with lowest ACT command interval. So, while it is safe to use these
figures to assume worst case load, the system would be vastly over-designed. It is better to build a
second power budget table with typical current consumptions and a more application specific scenario
while keeping the previous version in mind.
Table 3
Tab|e4
Tab‘e 3.
15
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
Table 3 Application specific power budget table
Part Name
Part Number
Max Current (mA)
Supply voltage
rail
Voltage
(V)
Max Power (mW)
AM3358
U1
186.4
Internal
5
932
TPS65217C
U1
< 1
Internal
5
<5
TL5209
U1
8
Internal
5
125
DDR RAM
U1
206
Internal
1.5
309
TPS2051
U8
< 1
SYS_VOUT
5
< 5
USB2534-1080AEN
U8
45
SYS_VDD1_3P3V
3.3
148.5
USB Connector
X4, X5
< 500
SYS_VOUT
5
< 2500
24LC32AT
U1
1
Intenal
3.3
5
DM3BT-DSF-PEJS
X3
100
SYS_VDD1_3P3V
3.3
500
SDIN8DE2-16G
U7
80
SYS_VDD1_3P3V
3.3
400
SN74LVC1G07DCK
U3
16
SYS_VDD1_3P3V
3.3
80
SN74LVC2G241DCUR
U6
16
SYS_VDD1_3P3V
3.3
80
AR8035-AL1A
U9
33.9
SYS_VDD1_3P3V
3.3
111.8
MPU-9250
U23
3.2
SYS_VDD1_3P3V
3.3
10.6
S25FL127S
U21
24
SYS_VDD1_3P3V
3.3
79.2
Total
5291
Table 3 shows an application specific power budget table in which the processor is operated in
conditions described in Table 4. All the other peripherals and features are assumed to be disabled in this
scenario and ‘typical’ current consumption values from component datasheets are used rather than
‘maximum’ current consumption values.
Table 4 AM335x application specific operating conditions
Feature/peripheral
Utilization (%)
Cortex A8
70
Cortex A8 NEON
70
CORE OPP
OPP100
MPU OPP
NITRO
MPU Frequency
1 GHz
EMIF
70
OCMC RAM
70
USB
70
Ethernet MAC
70
MMC1
70
Miscellaneous Peripherals
50
ADC
OFF
Note that the utilization percentages of each feature/peripheral of the AM335x processor are still high.
This is done to leave ourselves some head room if the board runs into an unexpected scenario. Similarly,
the RAM usage is also safely assumed to have a 20% page hit rate, a 10ns interval between ACT
commands, 30% of the time spent reading from RAM and 30% of the time writing to the RAM. Also,
observe that several components of the board are not in use and so are left out of Table 3.
Tab‘e 5,
Table 5,
16
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
4.3 Step 3: Tally Up
Thus, we have an extreme scenario and an application specific application scenario for our power
budget. The usage scenarios should now be stacked up to the supply capacities of output power rails of
OSD335x that we outlined in step 1 to make sure everything checks out. Given below are the conditions
that need to be verified and corresponding usage on the OSD3358 SBC reference design from the
datasheet:
Table 5 Current limitations from OSD335x datasheet
Condition
Limitation
Extreme
Application
VIN_AC input current
2.0 A
1.58 A
1.05 A
VIN_USB input current* (See below)
1.3 A
1.58 A
1.05 A
VIN_BAT input current (5V battery)
2.0 A
1.58 A
1.05 A
SYS_VOUT output current
500 mA
500mA
500mA
SYS_VDD1_3P3V (VDD_3V3B) output current
500 mA
752.7mA
318.1mA
SYS_VDD2_3P3V (VDD_3V3AUX) output current
150 mA
–
–
SYS_RTC_1P8V (VDD_RTC) output current
100 mA
–
–
SYS_VDD_1P8V (VDD_1V8) output current
250 mA
77mA
–
SYS_ADC_1P8V (VDD_ADC) output current
25 mA
–
–
From Table 5, although SYS_VOUT current consumption looks like it touches the maximum
recommended output current, it is highly unlikely to have a USB device that would draw 500mA in the
application. The extreme condition input current exceeds the USB input current limit. But, there are
alternative input power paths(AC and BAT) that can mitigate this issue even though the scenario will
never occur. The load current for the SYS_VDD1_3P3V voltage rail also exceeds the output current limit
in the extreme scenario. So, that voltage rail may fail if components begin to draw maximum specified
currents. But, the application specific current draws taken into account while designing the board are
significantly lower than the limits. More weight was placed on the application scenario vs theoretical
maximum current consumptions during the design. As can be seen from Table 5, there is enough room
for the board to be able to deal with most unexpected situations of high current consumption in an
application scenario.
While this board presents no problems in power analysis for an application, there might be situations
where the current draws are close or exceed the power rail limits in a design. In this case, alternative
approaches to design can solve the problem. The OSD335x has multiple rails of 1.8V and 3.3V. So,
spreading out the total current consumption of all the parts among the available power rails can be a
Perk:
By default, VIN_USB is limited to 500mA. A current limiting register in the PMIC needs to be modified
to allow current greater than 500mA. Another important thing to keep in mind is the type of
components used for power supply. While the MPU domain, CORE domain and the DDR memory are
powered by efficient DC to DC converters, all the other power rails come from LDOs. So, current
consumption of the components powered by LDOs is a direct addition to the overall current
consumption irrespective of the level of the voltage rail.
Software Power Management with the OSD335X Family
TP865217C datasheet
TL5209 LDO datasheet
AM335X datasheet
Powering the AM335X with TP565217C
Using Power Estimation Tool to estimate power consumption of AM335x
Processor SDK Linux kernel gerformance guide
AM335X power consumgtion summafl
Sgreadsheet for DDR3 power consumgtion estimation
AM335X Power Management User Guide
Linux Core Power Management User’s guide
AM335X Power Management User Guide
AM335X Power Management Standby User’s Guide
17
OSD335x-SM Power Application Note
Rev.1 10/24/2017
Octavo Systems LLC
Copyright 2018
first approach. If that does not resolve the issue, alternative power paths need to be designed. This
might involve using more regulators and/or using AC/BAT input instead of the current limiting USB
input.
5 Conclusion
This document discussed the power management system of OSD335x-SM and presented a power
budgeting procedure that helps in efficient product design. Most of the above discussion centers around
hardware. However, software also plays an important role in power management. Some aspects of
software power management and a case study on its advantages are presented in the application note:
Software Power Management with the OSD335x Family.
6 Reference Documents
1. TPS65217C datasheet
2. TL5209 LDO datasheet
3. AM335x datasheet
4. Powering the AM335x with TPS65217C
5. Using Power Estimation Tool to estimate power consumption of AM335x
6. Processor SDK Linux kernel performance guide
7. AM335x power consumption summary
8. Spreadsheet for DDR3 power consumption estimation
9. AM335x Power Management User Guide
10. Linux Core Power Management User’s guide
11. AM335x Power Management User Guide
12. AM335x Power Management Standby User’s Guide