Octavo Systems LLC 的 Bare Metal Appl on OSD335x using U-Boot 规格书
httgrflbeagleboard‘orgflatest-images)
Bare Metal Applications on OSD335x using U-Boot
Rev.1 3/26/18
Octavo Systems LLC
Copyright 2018
1 Introduction
Be it for performance, complexity or ability to audit, at times embedded developers will find themselves
in a situation where running a bare metal application directly on OSD335x without Linux is needed. One
common scenario for this is in time sensitive or real-time applications when better control is needed
over every aspect of program execution. Another scenario would be if an application developer felt the
need to eliminate the OS on the processor and of any overhead associated with it. However, Linux does
provide a number of benefits that can aid in program development, so careful evaluation should be
completed when determining whether to create a bare metal application. Regardless, the OSD335x
Family of devices can run bare metal applications easily. This application note will show you how to
load an application from an external SD Card (or eMMC or TFTP) to the DDR3 of the OSD335x and run it.
For this application note, you will need a Host Computer running Ubuntu and an OSD335x Family based
development or prototype board, such as the Beagleboard.org® BeagleBone® Black Wireless,
PocketBeagle® or OSD3358-SM-RED board. This development board should be running a Debian
BeagleBone® image (http://beagleboard.org/latest-images) in order to leverage the U-Boot bootloader
to load your bare metal application (the Linux portion of the image will not be used and may be
removed).
Notice: The information provided within this document is for informational use only. Octavo Systems
provides no guarantees or warranty to the information contained.
2
Bare Metal Applications on OSD335x using U-Boot
Rev.1 3/26/18
Octavo Systems LLC
Copyright 2018
Table of Contents
1 Introduction .......................................................................................................................................... 1
2 Revision History .................................................................................................................................... 3
3 Installing StarterWare for AM335x ....................................................................................................... 4
4 Installing Linaro GCC Compiler .............................................................................................................. 5
5 Building StarterWare Example .............................................................................................................. 6
6 Running Demo Application on OSD335x using SD Card or eMMC ....................................................... 7
7 Running Demo Application on OSD335x using TFTP ............................................................................ 9
8 Booting Bare Metal Applications ........................................................................................................ 11
9 References .......................................................................................................................................... 11
3
Bare Metal Applications on OSD335x using U-Boot
Rev.1 3/26/18
Octavo Systems LLC
Copyright 2018
2 Revision History
Revision Number
Revision Date
Changes
Author
1
3/26/2018
Initial Release
Eshtaartha Basu
OSD335875M7RED
htt
4
Bare Metal Applications on OSD335x using U-Boot
Rev.1 3/26/18
Octavo Systems LLC
Copyright 2018
3 Installing StarterWare for AM335x
First, we will need to install the development environment for creating and building a bare metal
application on the AM335x, StarterWare.
NOTE: All instructions given in this article were tested using a host machine running Ubuntu 16.04 and
the OSD3358-SM-RED Reference, Evaluation, Development Board for the OSD335x-SM SiP Products
running BeagleBone Debian 9.3 (U-Boot version: U-Boot 2017.01-00006-gb2bbabfe41)
You can download StarterWare installer for AM335x (v2.00.xx.xx) and BeagleBone Black patch
(Starterware_BBB_support) from http://www.ti.com/tool/starterware-sitara. You will be asked to create
a TI account and enter contact details to download all the files.
1. On the host Ubuntu Machine, open a Terminal (
Ctrl + Alt + T
on the keyboard)
2. Create a directory named bareMetal to hold the StarterWare files:
$ mkdir ~/bareMetal
3. Move the downloaded StarterWare installer file to the bareMetal directory:
$ mv ~/Downloads/AM335x_Starterware_02_00_01_01_Setup.bin ~/bareMetal
4. Make the StarterWare installer executable:
$ cd ~/bareMetal
$ chmod +x AM335X_StarterWare_02_00_01_01_Setup.bin
5. Install the dependencies to install StarterWare:
$ sudo apt-get update
$ sudo apt-get install zlib1g-dev libncurses5-dev
6. Run the installer:
$ ./AM335X_StarterWare_02_00_01_01_Setup.bin
7. During the installation, change the install path to
~/bareMetal/AM335X_StarterWare_02_00_01_01
and Installation Type to
Typical
.
8. Given we are running our bare metal application on a variant of the BeagleBone Black, we need to
install the BeagleBone Black patch. To do this simply move the downloaded
StarterWare_BBB_support.tar.gz
to
AM335X_StarterWare_02_00_01_01
folder and
extract it:
htt 5: launch ad.net ccVarmr
embedded[4.7[4.7720127g47ma'or
5
Bare Metal Applications on OSD335x using U-Boot
Rev.1 3/26/18
Octavo Systems LLC
Copyright 2018
$ mv ~/Downloads/StarterWare_BBB_support.tar.gz
~/bareMetal/AM335X_StarterWare_02_00_01_01
$ cd ~/bareMetal/AM335X_StarterWare_02_00_01_01
$ tar xvfz StarterWare_BBB_support.tar.gz
At this point, StarterWare should be successfully installed on your host Ubuntu system.
4 Installing Linaro GCC Compiler
Next, we need to install a cross compiler that will allow us to build AM335x applications on our host
Ubuntu system.
Download the Linux Installation Tarball (version: 4.7-2012q4) from https://launchpad.net/gcc-arm-
embedded/4.7/4.7-2012-q4-major There are always improvements being made to GCC, so while a
specific version is reference and tested in this app note, this procedure should be similar for future
versions of the compiler.
1. Make a folder for compiler and move the downloaded file into it:
$ mkdir ~/bareMetal/linaro-gcc
$ mv ~/Downloads/gcc-arm-none-eabi-4_7-2012q4-20121208-linux.tar.bz2
~/bareMetal/linaro-gcc
2. Extract the compiler:
$ cd ~/bareMetal/linaro-gcc
$ tar xvfj gcc-arm-none-eabi-4_7-2012q4-20121208-linux.tar.bz2
3. Add the compiler location to StarterWare Makefile using your favorite editor (we used gedit):
$ gedit ~/bareMetal/AM335X_StarterWare_02_00_01_01/build/armv7a/gcc/makedefs
4. Modify the “PREFIX” variable with the following:
ifndef PREFIX
PREFIX=${LIB_PATH}/bin/arm-none-eabi-
endif
5. Setup path to toolchain:
$ export LIB_PATH=${HOME}/bareMetal/linaro-gcc/gcc-arm-none-eabi-4_7-2012q4
We now have StarterWare installed and a cross compiler that will allow us to build the StarterWare code
for the AM335x.
http: infocenterarmxom help Index.jsp?topic: com.arm.doc.ddi0344h BCGFFBFD.htm|
http: infocenterarmxom help Index.jsp?topic: com.arm.doc.ddi0344f ngciiaf.htm\
6
Bare Metal Applications on OSD335x using U-Boot
Rev.1 3/26/18
Octavo Systems LLC
Copyright 2018
5 Building StarterWare Example
Now, we will use the tools from Sections 3 and 4 to build a StarterWare application.
For the StarterWare examples, we will disable the MMU, instruction and data caches, and some
exception handling in the initialization assembly file (init.S for gcc) to avoid any unexpected behavior.
Depending on your application, you may need to enable some or all of these features. If you do, then
please update the initialization file appropriately.
1. Open init.S using your favorite editor (again we use gedit):
$ gedit ~/bareMetal/AM335X_StarterWare_02_00_01_01/system_config/armv7a/gcc/init.S
2. Add the following after “Entry:” at line ~88 (“Entry” is the Reset handler in StarterWare. It is used to
set the stack pointers and initialize hardware registers before “main()” function is called and is the
best place to make this modification):
SUB r0, r0, r0
MCR p15, 0, r0, c1, c0, 0
To learn more about the above two lines of assembly instructions, refer:
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0344h/BCGFFBFD.html
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0344f/Bgbciiaf.html
3. Save the file and close it.
4. Build StarterWare demo examples:
$ cd
~/bareMetal/AM335X_StarterWare_02_00_01_01/build/armv7a/gcc/am335x/beaglebone
$ make
5. Once the build process is complete, check if the build was successful by navigating to:
$ ls -lA
~/bareMetal/AM335X_StarterWare_02_00_01_01/binary/armv7a/gcc/am335x/beaglebone/
gpio/Release
You should be able to see
gpioLedBlink.bin
file.
At this point, you now have a binary application file that can be loaded into the DDR memory of the
OSD335x / OSD335x-SM device and run. For your bare metal application, you should copy and extend
the structure and build process defined in StarterWare. The build process outlined above should be
similar for your application.
7
Bare Metal Applications on OSD335x using U-Boot
Rev.1 3/26/18
Octavo Systems LLC
Copyright 2018
6 Running Demo Application on OSD335x using SD Card or eMMC
Next, we need to run the binary application that was built in Section 5 to the OSD335x / OSD335x-SM
device. One method to do this is to use non-volatile storage such as an SD Card or eMMC attached to
the OSD335x / OSD335x-SM to store the binary application so that it can be loaded from U-Boot.
NOTE: For simplicities sake, we are leveraging the fact that the SD card / eMMC has a valid Linux image
with a file system that we can use to read and write our binary image. In a production scenario where
you want to leverage the size savings of using bare metal, you will need the MLO and U-Boot portions of
the image and then will need a file system to store the binary application.
First, we need to transfer the image to the OSD335x / OSD335x-SM development board.
1. Make sure that the development board has fully booted Linux; is connected to the host computer
via a USB cable and login to the board from the host computer through SSH:
$ sudo ssh 192.168.7.2 -l debian
The default password for all BeagleBoard images is
temppwd
. Enter it when prompted.
2. Copy
gpioLEDBlink.bin
file from Host Ubuntu Computer to OSD335x board using SCP:
$ cd
~/bareMetal/AM335X_StarterWare_02_00_01_01/binary/armv7a/gcc/am335x/beaglebone/
gpio/Release
$ sudo scp gpioLedBlink.bin debian@192.168.7.2:/home/debian
Next, we need to access the U-Boot console to load and boot the application. In BeagleBone images,
the console defaults to the UART0 peripheral. It is straight forward to access UART0 in most
development boards (see individual board documentation for the port / pins to access UART0).
NOTE: For instructional purposes, we are demonstrating the interactive way to load and boot the bare
metal application. In a production scenario, you would need to modify the “bootcmd” variable within
the U-Boot environment to automatically load and boot the bare metal application.
1. Connect a
UART to USB cable
between UART0 pins of OSD335x and Host Computer. Use a free
Serial Client like
Putty
to open a serial terminal and observe boot messages on boot up.
2. Set the terminal to
115200 Baud Rate (8N1).
3. When the development board boots, U-Boot messages are shown on the serial terminal. To load
and run a bare metal application from either an SD Card or eMMC, we must prevent U-Boot from
§COM35 , PuTTV
8
Bare Metal Applications on OSD335x using U-Boot
Rev.1 3/26/18
Octavo Systems LLC
Copyright 2018
automatically booting Linux. To do so, hit the
Enter
on the keyboard
within first 2 seconds of
OSD335x boot
.
Once Linux Boot is interrupted, U-Boot command line prompt can be seen as shown in Figure 1
Figure 1 U-Boot Command Line
To load and run the bare metal application from either the SD Card or eMMC, we need to understand
the correct device and partition where the bare metal application is stored. In the OSD3358-SM-RED
development board, the SD Card is on MMC0 and the eMMC is on MMC1 and in the default BeagleBone
image, the Linux filesystem is on partition 1.
4. To load and run the application from an SD Card:
load mmc 0:1 0x80000000 <path to your .bin file; e.g. /home/Debian/gpioLedBlink.bin>
go 0x80000000
Similarly, to load and run the application from eMMC:
load mmc 1:1 0x80000000 <path to your .bin file; e.g. /home/Debian/gpioLedBlink.bin>
go 0x80000000
w“
m“
Cv
Os
9
Bare Metal Applications on OSD335x using U-Boot
Rev.1 3/26/18
Octavo Systems LLC
Copyright 2018
7 Running Demo Application on OSD335x using TFTP
Another way, we can load and run the binary application that was built in Section 5 on the OSD335x /
OSD335x-SM device is to use TFTP to transfer the image directly to U-Boot so that it can load and run
the application.
Before we can use TFTP with U-Boot, you’ll have to configure the host Ubuntu machine with a TFTP
server.
1. Install TFTP server:
$ sudo apt-get install tftpd-hpa
2. Install TFTP client:
$ sudo apt-get install tftp
3. Configure TFTP parameters using your favorite editor:
$ sudo gedit /etc/default/tftpd-hpa
4. Modify the contents of the file:
TFTP_USERNAME="tftp"
TFTP_ADDRESS="0.0.0.0:69"
TFTP_OPTIONS="--create --listen --verbose /home/userName/cmpt433/public"
RUN_DAEMON="yes"
In the above block of code, make sure to replace
userName
with the username of your system.
5. Verify if TFTP is running:
$ netstat -a | grep tftp
You should see something like this:
udp 0 0 *:tftp
6. Restart the server
$ sudo service tftpd-hpa restart
Now, we need to test if TFTP is working. To do this, we can just use the Ubuntu host machine to
perform a loopback test.
1. Create a test directory and test file to transfer:
10
Bare Metal Applications on OSD335x using U-Boot
Rev.1 3/26/18
Octavo Systems LLC
Copyright 2018
$ mkdir ~/bareMetal/TFTP
$ echo ‘Testing TFTP successful’ > ~/bareMetal/TFTP/testTFTP.txt
2. Verify TFTP file transfer by transferring a file from Ubuntu host to itself:
$ tftp
tftp> connect 127.0.0.1
tftp> get home/ubuntu/bareMetal/TFTP/testTFTP.txt
Received 17 bytes in 0.0 seconds
tftp> quit
Note: In the above command, replace
ubuntu
with the username of your Host Machine.
3. Verify the contents of the transferred file:
$ cat test_tftp.txt
Testing TFTP successful
At this point we are ready to use TFTP within U-Boot to get the bare metal application so that it can be
loaded and run on the development board.
NOTE: Again, the steps shown below are how to interactively load and run the bare metal application.
In a production scenario, the U-Boot environment will need to be modified to automatically load and
run the application.
1. Both host Ubuntu machine and OSD335x / OSD335x-SM development board should be connected to
the same local area network. This can be done over Ethernet or over USB using the RNDIS gadget
framework that allows the development board to do IP transfers over USB.
2. Use Steps 1, 2 and 3 of Section 6 to get to a U-Boot command prompt on the development board.
3. Using a single command on the U-Boot command line, load and run the app using TFTP:
=> setenv ipaddr <board ip>;setenv loadaddr 0x80000000; setenv serverip <server
ip>;setenv tftproot /home/userNameOfHostMachine/bareMetal/TFTP;setenv bootfile
${tftproot}/gpioLedBlink.bin;tftp ${loadaddr} ${bootfile};echo -----Booting and loading
BareMetal App through TFTP-----;go ${loadaddr};
htt 5: octaves stems.c0m forums )
https://www.cs.sfu.ca/CourseCentraI/433/bfraser/other/BareMetalGuide. pdf
https://www.cs.sfu.ca/CourseCentraI/433/bfraser/other/DriverCreationGuide.pdf
11
Bare Metal Applications on OSD335x using U-Boot
Rev.1 3/26/18
Octavo Systems LLC
Copyright 2018
8 Booting Bare Metal Applications
At this point, you are now able to create, compile, load and run bare metal applications on the OSD335x
Family of devices using either non-volatile storage such as an SD Card or eMMC, or over the network
using TFPT. If you get any errors, please check that all the paths are configured correctly. Also, you can
post questions or comments on our forum (https://octavosystems.com/forums/)
9 References
For more information, please refer to the following links:
• Bare Metal on the BeagleBone, Simon Fraser University, 2017
https://www.cs.sfu.ca/CourseCentral/433/bfraser/other/BareMetalGuide.pdf
• Driver Creation Guide for BeagleBone, Simon Fraser University, 2017
https://www.cs.sfu.ca/CourseCentral/433/bfraser/other/DriverCreationGuide.pdf