Silicon Labs 的 LTE-M Expansion Kit Quick-Start Guide 规格书
($9
SILICEIN LABS
QSG156: LTE-M Expansion Kit Quick-Start
Guide
The LTE-M Expansion Kit is an excellent way to explore and
evaluate the Digi XBee3™ LTE-M cellular module which allows
you to add low-power long range wireless connectivity to your
EFM32/EFR32 embedded application.
The Digi XBee3™ LTE-M cellular module is an easy to use cellular module. The LTE-M
Expansion Kit easily integrates and brings LTE-M connectivity to compatible Silicon
Labs Wireless and MCU Starter Kits through the expansion header.
Software examples for the LTE-M Expansion Kit for the EFM32GG11 Giant Gecko STK
(SLSTK3701A) are available in Simplicity Studio™. This guide demonstrates how to
download and run one of these examples.
LTE-M Expansion Kit Contents
• Expansion board with Digi XBee3™
wireless module socket
• Digi XBee3™ LTE-M cellular module
• Hologram SIM card
• Cellular patch antenna
• Quick Start card
silabs.com | Building a more connected world. Rev. 0.1
..~ LaumlurrSwwmySmdm
m: m Navigate Search
Sign!" v {3 3. f
a _<> mm»
o No Dawns
‘31:
0 Salmon;
Em :vodun Ham:
Jumlogggdln
~ @Eim
ijxi Run mm Htlp
Seavzh
pm Canflgumm
=u
“'5 Welcome to Simplicity Studio
To virw mm. mm a m 01 :Oan m m: 0mm v :w m Salmons virw
Getting Staned Documemation Compatible Tools Resources
E = E Demos E Sallwar. xamples E Documents
Srlxia m. mam vigw mm. 3:54.; Hi who-audio m comm“ mm. kil a! mum viuummem
Chang: Mum: snK Chang: Mam: sDK Chang: PldemdSDK
Change Pldeiled IDE
0.ka for m“ updaia vs; a 2017 mm Labs
1. Getting Started
Introduction
The Digi XBee3™ LTE-M cellular module is capable of sending and receiving SMS messages. This guide will walk through the steps
necessary to run the Xbee SMS demo in Simplicity Studio, which demonstrates this capability.
Note: An EFM32GG11 Giant Gecko STK (SLSTK3701A) is required for this demo. Please see the following guide for instructions on
how to get started with the EFM32GG11 kit:
QSG149: EFM32GG11-SLSTK3701A Quick-Start Guide
Install Simplicity Studio
Simplicity Studio is a free software suite needed to start developing your application. Download the latest version of Simplicity Studio
from the Silicon Labs website:
http://www.silabs.com/simplicity-studio
QSG156: LTE-M Expansion Kit Quick-Start Guide
Getting Started
silabs.com | Building a more connected world. Rev. 0.1 | 2
Activate the included SIM card
The included Hologram SIM card must be activated before it can be used with the Digi XBee3™ LTE-M cellular module. This can be
done by following these instructions:
1. In a browser, navigate to https://hologram.io/ and create a new account.
2. Once your account has been activated, navigate to https://dashboard.hologram.io/activate and follow the instructions to complete
the activation of your SIM card.
Note: The activation process will ask you to configure the SIM's APN to "hologram" with username and password empty. This will
be done by automatically by the demo on the EFM32GG11 STK.
3. If desired, purchase a phone number for the SIM card on the dashboard in the card's Configuration page. Instructions for this step
can be found here: https://help.hologram.io/getting-started-with-hologram/how-can-i-get-a-phone-number-to-send-sms-messages-
to-my-sim
Note: Purchasing a phone number is not necessary, as you can still send and receive SMS messages through the Hologram dash-
board without one.
Assemble the Expansion Board
1. Place the Digi XBee3™ LTE-M cellular module into the socket on the expansion board.
2. Insert the Hologram SIM card into the SIM card slot on the module.
3. Connect the included patch antenna to the module's u.FL connector labeled 'CELL'. The completed assembly is shown in the figure
below.
QSG156: LTE-M Expansion Kit Quick-Start Guide
Getting Started
silabs.com | Building a more connected world. Rev. 0.1 | 3
wmummsvsu rirzn is rum as m ,
oooooooooooo
oooooo
W‘SS 2.52m“. 1.
:p ' as s :
flmm IIIIIIHIIIllllllllllll” gm“
' ” oobkioa‘é'oodoooéoa“
coo
mcflafiufififififlfifififimmufm lulu!“-
oouuooouuooooo
5mm us: H
m IHIIIIIIHIIIIIIIIllHll
“ oo‘ué‘o’uu‘ooaoo
neooooooaao
"'1 “WWW H.“ MM,
0-»
5‘
goo
f 9'”:
I!!!
"mm”
6
Download and Run the SMS Demo
The LTE-M Expansion Kit has several demos available for it that run on an EFM32GG11 Giant Gecko STK. To download and run the
Xbee SMS demo:
1. Once the expansion board is assembled, connect it to the expansion header of an EFM32GG11 STK, as shown below.
2. Once the expansion board is connected, the EFM32GG11 STK can then be powered by connecting the USB connector on the left
and setting the switch to the AEM position.
QSG156: LTE-M Expansion Kit Quick-Start Guide
Getting Started
silabs.com | Building a more connected world. Rev. 0.1 | 4
.- |aunrmvryilxmeAJmmgms/w/mmmr s‘mmuwsmmo ‘
We can Wm Search men m. mm m
54W . a 5. ; Wm :
r e. mm 0 SlmpumleE mm; 4 [Army mum u (mhgmmu
“Mn-1mm ‘ . . .
J-Llnk Slllcon Labs (440096711)
5, x 1: x 0 . ,
“ "WWW “m“m’“) Pvcicrmd snx Gr, m snK 9mm :1 w.” 5 a r. n Mmm 05 mm m n
m M m Hymn—“m [)I-fl—vw
v mezammamcxmsamrflns
wxmu mummy“ m
”my man man gum
Mapmrl’wmwamvcmnn wmarms Chang:
W. ‘ mm mm W ,, .
Gemngsmned Documentation CompatiblcTools Resources
Demni - + m Samar! Eumpks - + a sax Dncumrnlalmn - +
mmmmma am. 5) A
V ‘ ‘1 smn‘luu M90 films a
mm , my h ‘ W
h u ‘ um
mmmn m m: me
’( a; V 1,
m y , r m
m, u w L
SISYKS1H1AII< m:="" ‘="" h="" “="" smummkemnum="" i.="" nahum="" m="" mm“="" cznmsmmn="" an:="" slstk3701a7ite7xhee75ms="" (9="" mm="" exan‘ple="" dfoje‘ci="" uses="" .="" dim="" xbee="" medu‘e="" n:="">
3. Launch the demo in Simplicity Studio by finding the [SLSTK3701_lte_xbee_sms] demo under [Getting Started] in the Launcher,
under [Demos].
4. Follow the initialization sequence on the LCD.
Note: The initialization sequence, including finding a cell signal, may take up to one minute. If this process takes longer than a
minute, try to find a location with a stronger cell signal.
QSG156: LTE-M Expansion Kit Quick-Start Guide
Getting Started
silabs.com | Building a more connected world. Rev. 0.1 | 5
Pilot (28390)
7 Q None
| Messaging
5m (-1 name
mmumw
mu eq ‘ (mm W
Hume M, m
Rue;
2: ms
Acton“
A|| aulvily r ‘ ‘7
5m mmam nivlci UNK
39b45fllfill‘76‘2839fl '“ "7
‘8D627 Mibflfl
V CB . We
lasx inn/2 15 minutes in»
an MST Momllly "
Send a ms-ssage
n4 ‘\ m mu vIaSMS
Helln Wurld‘
mm“ o
(m’mvn: w: rnoM
WW , iwawzsssn‘od
mmnm ‘9 __ /
:\ Lnarr‘ mmunmmszgwg
Send and Receive SMS messages
If you have purchased a phone number for your Hologram SIM card, you may now send SMS messages to this phone number.
If you haven't purchased a phone number, you can send SMS messages through the Hologram dashboard instead.
The SMS message will be received and displayed on the EFM32GG11 STK's LCD, along with the sender's phone number. The demo
will automatically respond back with the message "You are linked to this Xbee" to this phone number. Pressing BTN0 on the
EFM32GG11 STK will also send a message stating the number of messages the demo has received so far.
Note: Sending and receiving SMS messages may take over a minute.
Note: The Hologram SIM card will cause the SMS response from the module to be from a different phone number than the one as-
signed to the SIM card. This response will be from a +88 number, and some carriers block these numbers automatically. If you receive
no responses from the kit during this demo, you may contact your carrier and request that they allow messages from +88 numbers.
Note: The SMS demo will configure the Digi XBee3™ LTE-M cellular module to search for and use the strongest carrier, between Veri-
zon and AT&T. The module also has the option to be configured to use a specific carrier, if desired.
QSG156: LTE-M Expansion Kit Quick-Start Guide
Getting Started
silabs.com | Building a more connected world. Rev. 0.1 | 6
2. Additional Resources
Additional Software Examples
Two additional software examples for the EFM32GG11 Giant Gecko STK are available within Simplicity Studio. These can be accessed
from the [Launcher] perspective under [Software Examples] with the kit selected.
1. Digi XBee Device Cloud example: This example project uses a Digi XBee module to communicate via LTE-M. It transmits tempera-
ture data to the Digi Device Cloud and allows a Cloud user to modify LED's on the board.
2. Digi XBee Time Server example: This example project uses a Digi XBee module to receive the current time from an online timer
server and displays the time on the LCD.
Additional Documentation
For more information, please review the following:
•UG310: LTE-M Expansion Kit User's Guide
•https://www.digi.com/xbee
•https://hologram.io/
QSG156: LTE-M Expansion Kit Quick-Start Guide
Additional Resources
silabs.com | Building a more connected world. Rev. 0.1 | 7
Q
SILICON LABS
http://www.silabs.com
Silicon Laboratories Inc.
400 West Cesar Chavez
Austin, TX 78701
USA
Simplicity Studio
One-click access to MCU and
wireless tools, documentation,
software, source code libraries &
more. Available for Windows,
Mac and Linux!
IoT Portfolio
www.silabs.com/IoT
SW/HW
www.silabs.com/simplicity
Quality
www.silabs.com/quality
Support and Community
community.silabs.com
Disclaimer
Silicon Labs intends to provide customers with the latest, accurate, and in-depth documentation of all peripherals and modules available for system and software implementers using or
intending to use the Silicon Labs products. Characterization data, available modules and peripherals, memory sizes and memory addresses refer to each specific device, and "Typical"
parameters provided can and do vary in different applications. Application examples described herein are for illustrative purposes only. Silicon Labs reserves the right to make changes
without further notice and limitation to product information, specifications, and descriptions herein, and does not give warranties as to the accuracy or completeness of the included
information. Silicon Labs shall have no liability for the consequences of use of the information supplied herein. This document does not imply or express copyright licenses granted
hereunder to design or fabricate any integrated circuits. The products are not designed or authorized to be used within any Life Support System without the specific written consent of
Silicon Labs. A "Life Support System" is any product or system intended to support or sustain life and/or health, which, if it fails, can be reasonably expected to result in significant personal
injury or death. Silicon Labs products are not designed or authorized for military applications. Silicon Labs products shall under no circumstances be used in weapons of mass
destruction including (but not limited to) nuclear, biological or chemical weapons, or missiles capable of delivering such weapons.
Trademark Information
Silicon Laboratories Inc.® , Silicon Laboratories®, Silicon Labs®, SiLabs® and the Silicon Labs logo®, Bluegiga®, Bluegiga Logo®, Clockbuilder®, CMEMS®, DSPLL®, EFM®, EFM32®,
EFR, Ember®, Energy Micro, Energy Micro logo and combinations thereof, "the world’s most energy friendly microcontrollers", Ember®, EZLink®, EZRadio®, EZRadioPRO®,
Gecko®, ISOmodem®, Micrium, Precision32®, ProSLIC®, Simplicity Studio®, SiPHY®, Telegesis, the Telegesis Logo®, USBXpress®, Zentri, Z-Wave, and others are trademarks or
registered trademarks of Silicon Labs. ARM, CORTEX, Cortex-M3 and THUMB are trademarks or registered trademarks of ARM Holdings. Keil is a registered trademark of ARM
Limited. All other products or brand names mentioned herein are trademarks of their respective holders.