Kitronik Ltd. 的 Electro-Fashion 规格书
Electro-Fashion
Textiles & Craft
SEWABLE LED KITS
ELECTRO-FASHION KITS WITH FLAT LEDS
ELECTRO-FASHION - 60 STUDENT BULK PACK
Kits are packed ready for student use and include a coin cell
holder, a coin cell, 2m of conductive thread and either two
flashing LEDs or one colour changing LED. They allow lighting
effects to be added to textiles designs without soldering.
These kits are ready-packed with all of the parts needed for
students to make a simple E-Textiles circuit. The kit includes
two flat LEDs that are marked up with + and – markings,
making them smaller and easier to use than LEDs with leads.
As well as the two flat LEDs, the kit also includes a 2m t-shirt
of conductive thread, a sewable coin cell holder and coin cell.
The bulk pack offers great value for teaching larger groups
of students.
Description
Description
Description
Code
Code
Code
Flashing blue sewable LED kit
Sewable LED kit with blue flat LEDs
Sewable LED - 60 student bulk pack
Flashing green sewable LED kit
Sewable LED kit with green flat LEDs
Flashing red sewable LED kit
Sewable LED kit with red flat LEDs
Flashing yellow sewable LED kit
Sewable LED kit with white flat LEDs
Colour changing sewable LED kit
2702
2735
2707
2703
2736
2704
2737
2705
2738
2706
1+
1+
10+
1+
Pack includes: 60 x sewable coin cell holders.
60 x CR2032 coin cell batteries.
180m of conductive thread, 3m per student.
10 x colour changing LEDs.
25 x each of blue, red, yellow
and green flashing LEDs.
Project Example
Project Example
(requires extra LEDs)
(@619
Electro-Fashion
Textiles & Craft
ELECTRO-FASHION CAT KIT
This cat kit contains all the items you need to
make the cat (except for a pair of scissors and a
needle). To make the cat the felt is cut into three
pieces following the lines marked on the pre-
printed design. The LED eyes, battery holder and
a switch are sewn on to a piece of felt following
the stitch lines. The cat is then sewn together and
stuffed with wadding. Pop the battery in and when
the cat’s ear is pressed the eyes will light.
PROJECT EXAMPLES - ELECTRO-FASHION SEWABLE LEDs
Kit contents:
- 1 x Printed felt.
- 2 x Sewable green slim LEDs.
- 1 x Sewable push button switch.
- 1 x Sewable coin cell holder.
- 1 x CR2032 coin cell.
- 2 x Conductive thread.
- 8m Embroidery thread.
- Wadding.
www.kitronik.co.uk/cat
Code
2725
1+
Examples of conductive fabric used on the hands of puppets.
When these are touched together, the circuit is completed and the LED lights up.
KiIEiik
Electro-Fashion
Textiles & Craft
ELECTRO-FASHION FLASHER
CONTROLLER, LEDS & THREAD
This unit offers a simple way of adding ‘flashing’ white LEDs to a textiles
project. The unit is programmed with a number of flashing patterns that
are selected by a push button on the main PCB. Pressing this button cycles
through the following patterns: all LEDs constantly on, slow flash (all on, all
off), fast flash (each in turn), and turned off. The device features auto off, which
turns the unit off after 30 minutes to preserve battery life. Depending upon
flash pattern the battery lasts for approximately two days of constant use.
This kit is supplied ‘pre-built’ so requires no soldering. Each kit comprises
three small PCB’s. The largest of the three PCB’s holds an LED plus the control
electronics, battery and a push button. On both of the remaining PCB’s there is
an LED, which are connected to the main board with conductive thread.
This board allows LEDs to be turned on automatically when it is dark. On one
side of the board is the coin cell holder, which takes a CR2032 coin cell as well
as a small on off slide switch. On the other side of the board is the light sensor.
The design means that it is possible to cut a small hole in the front of the
product for the light sensor to detect the light level, whilst also being able
to get to the back of the board to change the battery and turn the board
off. When turned off any connected LEDs will be off. When turned on the
connected LEDs will be off in day light but come on in the dark.
Description
Description
Description
Code
Code
Code
Flasher controller and LEDs
Electro-Fashion - Light sensor
Magnetic switch & magnet
2719
2721
2720
1+
1+
1+
10+
10+
10+
Includes approximately 2m of conductive thread.
Dimensions: L34 x W20 x H9mm. Includes a CR2032 battery.
ELECTRO-FASHION MAGNETIC SWITCH & MAGNET
ELECTRO-FASHION LIGHT SENSOR
This magnetic switch can turn on LEDs when the magnet is placed near the switch.
Accepts CRznaz battery
0
OD
Tms two posmon mtmature sttde O
o e Dimensluns L217 xWb.5 x H7mm
Electro-Fashion
Textiles & Craft
This specially designed coin cell holder has large
connection points for the conductive thread. These
are clearly marked to show the battery polarity. The
unit also has a small power
switch so that you can turn
the power on and off.
This specially designed coin cell holder has large
connection points for the conductive thread. These
are clearly marked to show
the battery polarity.
This push button switch will
allow LEDs to light whilst
the switch is pressed.
When horizontal this switch
is off. When tilted 10° from
horizontal the tilt switch is on.
This two position miniature slide
switch allows LEDs to be turned
on or off in textiles projects.
The specially designed coin cell holder has large
connection points for the conductive thread and are
marked to show the battery
polarity. It is available on
its own, to incorporate into
your own designs.
Code
Code Code
CodeCode
Code
2711
2718 2708
27102709
2701
10+
1+ 10+
10+10+
10+1+
1+
1+1+
1+
SWITCHED COIN CELL HOLDER
MINIATURE COIN CELL HOLDER SEWABLE PUSH SWITCH
SEWABLE TILT SWITCHSEWABLE SLIDE SWITCH
SEWABLE COIN CELL HOLDER
Accepts CR2032 battery. Accepts CR2032 battery.
Dimensions: L44 x W20 x H4.5mm.
Dimensions: L18 x W8.5 x H6mm.
Dimensions: L26 x W6.5 x H7mm.
Dimensions: L34 x W20 x H4.5mm.
Dimensions: L18 x W8.5 x H4mm.
Description Code
3V CR2032 - 200mA/h - 5 pack
3V CR1220 - 40mA/h - 5 pack
2262
2269
1+ 10+
LITHIUM 3V COIN CELLS
Accepts CR1220 battery.
Dimensions: L22 x W12.5 x H4mm.
Electro-Fashion
Textiles & Craft
Description
Colour
Colour Code
Code
LED board - 10 pack
Red
LED board - 10 pack
Yellow
LED board - 10 pack
Red
White
Sakuru (lilac)
2712
3538
2714
3540
2726
2713
3539
2723
3545
10+
LED board - 10 pack
Green
LED board - 10 pack
Blue
Blue
Green
SEWABLE PCB LEDS
5MM FLASHING LED
FREE TO DOWNLOAD RESOURCES
These ultra slim, pre-mounted LEDs are illuminated continuously. They
have connections to which the conductive thread can be connected.
These are clearly marked with ‘+’ and ‘-’ to indicate which is the
positive and which is the negative connection.
The PCBs are double sided making the thread connection very reliable.
They are supplied on a small panel and the LEDs can easily be
removed by snapping them out.
These flashing LEDs can be used with the Electro-Fashion coin cell
power boards. 5mm flashing LEDs in red, green, yellow and blue. The
LEDs flash at around 2Hz when connected to a 5V supply.
Dimensions: L15 x W6.5 x H3mm.
100+
1+
10+1+ 1000+
To help people new to Electro-Fashion get started we have worked with Julie Boyd to develop some
free online resources. These give detailed step by step explanations of how to make a product.
There are guides on adding an LED to a hat (both a standard LED and a slim line LED), making a
zippi doll with light up eyes & adding three LEDs to a bag. We are always working on more resources
so it’s worth keeping an eye on the website.
www.kitronik.co.uk/fashionresources