DA-70156 User Manual 规格书
' DIGITUS®Z
USB - SERIAL
CONVERTER
User Manual
DA-70156 Rev.5
mm”! .H
HI; and Lu;
Shutaww '7‘
Adwsl you! {ampuler 5 sewing:
Q
@-
Syslem and Senm'ly
a. m (mm x nun;
mm ”mm“,
mm: ~ Mm
Ntlwork and Imam
”mummy“.
My ”Miamrmm
um. «WW 1p m mm, mm,
Nardwave and Sound
m a. mmgpmn
m . mu:
Proglims
w mm . mum
@1333
m :77 2mm .
use! means and Facility Saiay
' mmmmgumu
9% .p :mmnm-mm wev
Appuum and Fusmallzauon
(mg. m mime
mug. em: “(mm
lawn so." use wan
Clock Language, and Region
mug. knbcrus m a” m. mama;
0mm“ mun-an
Ease 0! Access
mwawmwmmg.
cm 1mm my
Windows 7/8/8.1 Installation Guide
Step 1: Insert CD Driver of this product to the CD-ROM. Connect the device to a spare
USB port on your PC.
Step 2: If there is an available Internet connection, Windows 7/8/8.1 will silently connect
to the Windows Update website and install any suitable driver it finds for the device.
If the automatic installation takes place there is no need to continue with the procedure
outlined below. If no suitable driver is automatically found then the following procedure
should be followed.
Press the Windows start button to bring up the start menu and select “Control Panel”.
Step 3: From the Control Panel window select Hardware and Sound
(- 0 new (cum.
(mm-4mm / E , mini
3 “an, mum Mdipnml mm W
mmlm m mm
, was.“ mmumsmgsmmwm.‘ nmmumm...mmm
"my: w Sound
0” “My Ad‘msymmvulume mmgqmmm mummiu
”"1 \. pmropums
Ant-um.“ Chingemrmngunmgs (hmgtmiuhemvbmmda
W mu. -mwu¢wmmmmmwu (Mnoewhelmewmpmuleeps (mamuplln
MWHMMM Di by
59
WA“- I “www.mmm.“ “,unmmm (munmmw
Mawln:wmmnnlndklw(tdmhrnd
I SulndEdelmnagu
wean—mm.
«Mullahs
43H: -
ppm-pm
palm-ma
rim-hows
pummm
vulrmwmnm
p imam-mm
vmw
p 8 mmlmp‘vfingdei‘a
vim-I'm
> imam
4 flow—swim
mfiuufiriiQ-m
. wmxcoumm
1 'MMKM)
[NIP-Dun
> ( mummy-mm
bflw‘eks
. j WWI-m
; 6 wwmummm
1.9 Wmmummm
‘ 6 wwmmm
HO wwwmm
o mum-29.0mm
Ir 9 mum:
‘ I “ml-unfit '
Step 4: At the next screen select Device Manager:
Step 5: In the Device Manager window there will be a device under Other Devices with a
yellow warning symbol to indicate a problem ie no driver installed. The text next to this
device will depend on the device attached. In this example the devices was “USB Serial
Cable” devices.
>qll‘l‘lAVMc-ulnlus
>70 rumour-am
>QW
> nmmmmm
>IW
> Quack-hymn
. i
. cu
.qr
yam
> 4 Sun-him“
)flspundaiw mama-gs
. 5mm...
3 WW M
.7 O WmmuvsuonCo-MI-
0 Wop-museum
'i wwmmm
C ”HM-whiz
0 um»...
I mm»
Imuwmmvmr—uwm
How do you want to search for driver software?
0 Seard'i automatically for updated driver software
Windows will search your (nmplfle! um (Nahum: forth: Iatat driver may:
in! your dam; unussyou've disabled mi: (martin your am: installation
settings.
0 Browse my computer for driver software
Locate and install my Wm MMIM'Y.
Step 6: Right click on the other device to bring up a menu as shown below. From the
displayed menu select “Update Driver Software…” This then displays the
option for an automatic search or a manual search.
Step 7: Select the second option to browse manually.
fit. as“, 1.95.1:
Bmwsefordfiversofiwamonyourmpum
mMfi-MHMW
— ' IE]
.hdudum
O lampidfromnlistofdevioedriversonmympwer
maummmmmmmmmmm
Mhmmmnmm
E-
lnstalling driver software-
E
Step 8: click “Browse” and choose the corresponding OS driver in CD. Click “Next” to
continue
Step 9: When the installation has finished a completion screen is displayed.
Step 10: Press Close to close this window and go back to the Device Manager Window.
mm has successfully updmd your drive: software
mmmmmmmmmmm:
USISaiIICm
J
Dali!
5.”. Vi- Min
*Wl-lfllfl‘a
» Dammnwunaiu:
» qntAn/nmmuus
o i mmmmmm
0 DW
. 0 wwum z
.i Mmmmmwmm
,1 Mmmmwmmm
a meoan
”.0 mmwnmmm
' O mung-apnea.
>70 Ins-mp»
i mum“
a mum
finance
Emanuel,
«wlllalllllmlnmas
.\ a mama:
> 3 Marina
> f Nmkmm
4 b Mum-s
fi usual-l P
> D; Hmnimalueualius
.» q DE AVA/AUDI wrlrolux
> 0 minimums-mum
> ,5 Mk: nu ma pointing dukes
4 w vmxomlu
. W Comm-am
4' I Pmuswrs
> i mum-n
n 4! Syfllm Min:
4 O Univuulsdul
6 swam (n
USB Root Hub
USE Root Huh
053 Run Hub
USB Root Null
(acaccnccu
um om sum-n.
Disable
Unml
hmnummnga
Pup-r-
. O sunam Enhanced Paw use No: Carmella
» O swam own use No: Curmollu
O sand-n1 owluco use Hm Connolly
uss Muss Swrlge Dnic:
USB Suhl Convene!
Launch: he Update Drive 500w: Ward lwflu idea“ duke.
The Device Manager will still show a device under Other Devices but in addition to this
there is a new entry under Universal Serial Bus Controllers indicated in the screenshot
above as the USB Serial Converter. This indicates the bus layer of the driver is installed.
Installing the Virtual Com Port layer of the driver is almost a repeat of the last few steps.
Step 11: Right click on the other device to bring up a menu as shown below. From the
displayed menu select “Update Driver Software…” This then displays the option for an
automatic search or a manual search.
Step 12: Select the second option to browse manually.
Haw do you want to search for d-iver software?
0 Search automaticaily for updated driver soflwave
Wmdaws wil suvch your campus: and mmmm Mast driver soflwlr:
'01 your devicg unless you‘ve distlad his tenure in your duke installation
settings
0 Browse my computer for driver software
Loam Ind ins-l dl'lvu sonny: mutually.
Browse for driver software on your computer
Search [or drive sunny: 'mfllis locxion:
— vlm
hclude subfoldas
9 Let me pid: frum a listafdevice driverson my computer
ThisIiiflmimlkdmmucnmpafikwfllm:dwk&mflfiv¢r
sofiwareinlheslmn mguvyaslhedeviu.
GE:-
Step 13: click “Browse” and choose the corresponding OS driver in CD. Click “Next”
to continue
Installing driver sofiware.
E
Step 14: When the installation has finished a completion screen is displayed.
Step 15: Press Close to close this window and go back to the Device Manager Window.
Windows has successfully updated your driver software
Wmdaws his finished inmling the driver my: “(this device
USS Sail! Pan
er
p Q Displ-y um: .
p O: Hun-«Me Devic:
» q n: AYA/AI‘ADI mullahs
p i mmWMm-muas
p :- Keybouds
p 8 Mice .m an... pointing mica
» g Mm'mm
p ,1 Wad-plus
. V pomcoum-
' - Wamkl‘iwlst _,
_
p I . ‘.
,, :1 Mum-Mymcmm
» ,- Symmdevm
4 i Umls‘uiuummlss
6 Standard [Named PCIWUSBHM (om-Mk:
i sums-m hum-mt namussumcmmllu
n 6 swam own use Hm Cmmllu
5 Standard Opal-cl) us: HmOommllu
n 6 mummy-gem:
mi 058mm!)
,, 6 What»
m5 mmmb
' v-: Huh
.1 USESeliMEomemu
12-: mt mummy: ccnmuus
E b Kayboads
- "ca and othev pmhg demos
I 3 WMMKOMI)
‘ ,y CWMMKOMZ)
1 PIMHMQPTI)
- Sound, Video end can: mmolers
System demos
Univasd Said as canola;
Stmd Wand PC] to USB m CWDH
Stmdld “Mal PC] to USB Host Control:
Slmd Um“ PC] to USB ms: Cfl'tmh
Skmdld LHvusd PC! to USB Host CurtrOIev
USE! Root Hub
Ufi Root Hub
U58 Root Hub
This time the Device Manager does not have a USB <->Serial Cable entry under Other
Devices but does show entries under Universal Serial Bus Controllers and Ports (COM &
LPT). The above screen shot displays a correct installation. The device is now ready to
use on COM3.
NOTE: Not all devices will install to COM3. The COM port allocation is determined by the
installation wizard on the basis of the next free com port as designated in the PC registry.
Remarks:
After installation if you can see “USB Serial Converter” from the “Device Manager”, but
can’t see “USB Serial Port (COM3)” , please continue next steps.
. h Human Intuface Devkes
lg IDE ATAIMAPI wntmlevs
I» Keyboards
" Mice md other Doint‘ng devices
other deltas
9 Ports (com & L")
3/ Cwnmmbms Pat (com)
y (mammataons Put (COMZ)
,y Plintu Put(LP11)
‘ Processovs
0' Stand. now and game :urimllers
System devlces
Universal Serial ms cumulus
Standad Unwevsd PCI to use Host Controller
Sandald Univarsal m to use Hug controller
Standard Umevsal PCI to use Host Controller
Stand-d Universal PCI to use Host Controller
.l.
Il‘v,
ll~w~
USS Root Ht
use not Huh
U58 Root HI)
use Root an:
Update Dliver. ..
Disable
Ur'mstal
Scan for hardware changes
Ilsli wnnl ( “mane: “mpg-m X
GWdJ Advanced LPM MW_ Dnvelr
e. IJSB Smd Cantata
Weber:
Use ":5: mm: m override mml dew: may.
W Load VEP
Step A: Right click “USB Serial Converter”, then click “Properties”.
Step B: Select “Load VCP” in the “Advanced”, click “OK”
USB Serial Lonvcncr Properties
Gar-ad MUM PowerMmagemeri‘L; Dnvov]
9 USB 5&deva
-Configxah'on
Uulleuewu‘lutloovenflemmddwiuewm
”LoadVCP
Step C: Move out USB 2.0 TO RS232 on your computer. Connect the device to an old
USB port on your PC again, now it’s ok , please refer to the following chart:
W h Human More Devices
a Q IDE ATAIAIAPI controllers
b Keyboards
{a " Mcemmummm
m ow dates
a Puts (comm)
3 Cmmlhtims Pat(COMl)
j Cumnuatm pmmmz)
.9
E Sound. vita and we crawlers
LE system «an;
a Unlversd 59ml Bus tannins
swan was! KIN) USB M Comm
SIM Wand PC] to USB M Cuticle!
Stankd Lhmrsal PG ho USE Hufi Cottmler
SIAM-Id Mid PG m USE HM (mule:
USE Rod Huh
USB am Huh
USE Root Hub
ml nuu
USB Saul Converbu
usa Saul M 90143;.
i
M'YmnMIomlD-mhmmm Him-Mbmflhhhww.
Emmmmhmm Ihhhfl—lhflm‘
EIE V WE]
Uninstalling FTDI Devices
With the release of Microsoft Windows 7/8/8.1, the FTDI uninstaller has been rendered
unusable due to Windows Resource Protection preventing the executable from deleting
driver files and associated registry values. Windows 7/8/8.1 will only allow the system
itself to modify files and registry values in these locations.
Devices can be removed using the Device Manager by simply right-clicking on the
mouse and selecting "Uninstall”. This will delete the associated registry entries for that
device only. Windows 7/8/8.1 provides an automatic method to delete driver files via a
check box to "Delete the driver software for this device" on the uninstall dialog box.
.0 Found New Hardware W
usb serial converter
Welcome to the Found New
Hardware Wizard
Windows will search In! cunent and updated software by
looking on you! computer, on the havdwale mslallallon CD, or on
the Windows Update Web site [With you! permission]
El. lll
Can Windows connect to Windows Update to search fol
software?
Ies, this time only
Yes, now and gvevy tlmel connect a dewce
Click Next to continue.
Windows XP Installation Guide
Step 1: Insert CD Driver of this product to the CD-ROM
Step 2: Connect the device to a free USB port on your PC, and find new hardware wizard,
please refer to the following chart:
Found New Hardware Wizard
This wrzard helps you Install soltware for
usb serial converter
1 -) ll your hardware came with an inslallatiun ED
\y or lloppy disk, insert it now.
What do you want the wrzard to do7
0 Install the soltware automallcally [Recommended]
(9 Install from a list or specrlrc location [Advanced]
Click Next to continue
Found New Hardware Wizard
Please choose your search and installalion oplions.
I
$
® Search lor the best driver in these locations
Use the check boxes below to limit or expand the delault search. which includes local
paths and removable media. The best driver lound wil be installed.
Search removable media [Howl CD-RDM...)
D Include this location in the search'
0 Don't search. I will choose the driver to install,
Choose this option to select the device driver lrom a list. Windows does not guarantee that
the driver you choose will be the best match for your hardware.
Step 3: Select “No, not this time“, click “Next” to continue.
Step 4: Select “Install from a list or specific location (Advanced)”, click “Next” to continue.
Found New Hardware Wizard
Please wail while Ihe wizard searches...
g usb aerial nonverbal
Please selecQ the besl malch let your hadwale lmm [he isl below.
E USE Salial Emulate!
D uiplion l Vaden‘ Haulachuet‘ Location
E'USB Sena Convevtev 2.2 4 U FTDI l usb 2,0 to 1:232 cable\wm2£
g >
E This dive! i: w tigned.
Tell me w driversi ' is im Kant
Step 5: Select “Search removable media (floppy, CD-ROM…)”, click “Next” to continue.
Step 6: Auto search for the corresponding driver in the CD.
Found New Hardware Wizard
Please wail while the wizard install: the software... \~
6 USB Serial Convener
('3
is? El
llexxfil
To C:\WINDDWS\syswuwl54
Found New Hardware Wizard
Completing the Found New
Hardware Wizard
The wuzard has finished instalhng |he soflwale for
G USB Serial Convener
Click Fimsh to close the wizard
Step 7: You will find two types of hardware wizard, one is for USB 2.0 - RS232 Converter,
another one is for USB 2.0 TO RS232 cable. Please choose the corresponding driver
according to your product, click “Next” to continue.
Step 8: The wizard has started installation and copy file to your system
j) Found New Hardware x
USB Serial Port
FvUiidilai.-"rl:iii' , .211 ml
Welcome to the Found New
‘k‘ H ardware Wizard
‘ Windows Will Search i0. cuiient and updated soltwaie by
looking on your computer, on the haidwaie installation CD, oi on
the Window: Update Web Site [wilh your permisxion]
Can Windows connect to Windows Update to seaich lor
soltwaie?
; Yes, thi: time only
Yesl now and eveiy time l connect a dew-ice
c No, not this time
Click Nexl to continue
Step 9: Click “Finish” to close the wizard.
Step 10: Find new com port.
| Found New Hardware Wizard
This wrzard helps you Install soltware lor
USB Serial Port
‘ ll your hardware carne vrilh an installation CD
W or floppy a , insert it now.
What do you wanl lhe Wizard to do?
0 Install the soltware automatically [Recommended]
@ Install from a list or specific location [Advanced]
Click Next to continue
l1‘rlr‘41
Please choose your search and installation options. .
(9 Search lor the best driver in these locations.
Use the check boxes below to limit or expand the default search, which includes local
paths and removable media. The best driver lound will be installed.
Search removable media "loopy, CD‘HOM...]
El Include this location in the search:
0 Don‘t search. I will choose the driver to instal,
Choose this option to select the device driver lrom a list. Windows does not guarantee that
the driver you choose wil be the best match for your hardware.
Step 11: Select “No, not this time“, click “Next” to continue.
Step 12: Select “Install from a list or specific location (Advanced), click “Next” to
continue.
Please wait while the wizard searches...
g usa Serial Port
—wT J
I Found New Hardware Wizard
Please select lhe besl match for you hardware from the list below‘
(3 USE Sari! Purl
Descriplim I Varsiun‘ Mmulaeluu‘ Locuion
fi Tiisdriverisddalveimed
I . . . ..
Step 13: Select “Search removable media (floppy,CD-ROM…)”,click “Next” to continue.
Step 14: Auto search for the corresponding driver in the CD.
I Found New Hardware Wizard
Please wail while the wizard install: the sullwarem
lg USB Seriad Poll
‘7
V ,/
FT Langdll
T o C:\WIN DDWS \system32
—
:m, [,7. ,,u,,
I Found New Hardware Wizard
Completing the Found New
Hardware Wizard
The wrzard has brushed Installing |he soltware for
1:? USE Serial Port
\
Click Frmsh tu dose |he wrzavd
Step 15: Choose one type of the driver for your product, click “Next” to continue.
Step 16: The wizard has started installation and copy file to your system .
jg Found New Hardware x
Your new hardware is installed and ready to use.
D
[umurnents
Open
Explore
Search. . .
Manage
Map Network Drive.
Disconnect Network Drive...
Create Shortcut
Delete
Rename
Step 17: Installation completed, click “Finish” to close the wizard.
Step 18: Your new hardware is installed and ready to use.
System Pm parties
Q
Device Manager
DllVelS'
Restore Automatic U ates
Computer Name Hardware Advanced
The Device Manager list: all the hardware devices installed
on your computer. Use the Device Manager to change the
properties of any device.
Driving Signing lets you make sure that 'nstaled drivers are
compatible with Windows. Windows Updae lets you set up
how Window: connect: to Windows Update for divers.
Winamum
Hardware Profiles
Hardware prolies provide a way for you to set up and store
dilerent hardware configurations.
Hardware Profiles
Step 19: If you want to see it, right click “my computer”, and then click “Properties”.
31 E Human Interface Devices
.i g IDE ATAIAYAPI controllas
.‘i ’0 KEybuards
"' Mce and other Wntll’b; dewces
other devices
Parts (coM & LPT)
5 (cmmcaticns Part (com)
; (ummcatmns Part (com)
e 0,, Sound, video and game cunlrollers
,vl System devites
, Universal Serial Bus controllers
standard Universal Pct tn usB Host Cnntrnller
Standard universal PCI ta USB Host Cnnmzller
Standard Universal PEI ta USB Host canvaller
Standard Universal PCI to USE Host controller
LISE Root Huh
USB Rout Hub
USB Root Hub
USB Serial Corwerkev
E Q IDE ATNATAPI controllers
e a; Keybuards
*' Mice and other pointing devices
other themes
. 5 COM & LPT)
3 Communications Part (com)
5 Communications Port (COMZ)
._ Printer Port (LPn)
i,+ g Processor
E 0, Sound, vldeo and game controllers
e System devices
l— universal Serial Bus controlers
Standard Unlversal PC) to USB Host Controller
Standard universal PCI to USB Host Cmtrnuer
Starliard Universal PCI to USB ”35C Cmtmfler
Standard Universal PC) to USB Host Controller
USE Ruut l'IJb
USE RUDE Hub
USE Root Hub
|Knn cue
Step 20: Select “Device Manager” in the “Hardware” of the interface “System Properties”,
click it, you can see the hardware devices installed on your computer, please refer to the
following chart:
Step 21: Installation finished.
Remarks:
After installation, if you can see “USB Serial Converter” from the “Device Manager”, but
can’t see “USB Serial Port (COM3)”, please continue next steps.
e & Human Interface Devices
l * g [DE ATAIATAPI controllers
l? by Keyboards
e "' MIZB and other pointrng devtces
le other devices
r ,y Ports (COM & LPT)
,9} Communications Port (com)
"y Communications Port (COMZ)
,y Printer Povt(LPT|)
l; a Processors
l 0, Sound. video ard game controllers
l: System devltes
l’ Universal Serial Bus controllers
standard Universal PCI to use Host Controller
standard Universal pcx to use Host Controller
Standard Unlversal PC] to use Host Controller
standard Universal PCI to use Host Controller
use Rout Hub
use Root Hub
U58 Root Hub
use Rout Hub
9
w
Update Driver. .,
Dlsable
Uninstall
Scan for hardware changes
Proper es
er
[Converter proper es
‘ Genelal Advanced Power Mataoemenl l Driver l
l
4 I USE Salialflunvatet
*Eunllgulaliorl'
Use these selling: to Wernde riolmal device conliaualon
['7 Load VEP
Step A: Right click “USB Serial Converter”, and then click “Properties”.
7 fi Human Interface emu-s
@ IDE ATA/ATAPI tomdlers
‘9 Keyboard;
" We and other pointing devices
other devkes
Puts (com e LPT)
5 Cummumanuns Purt (com)
3 Cummumanuns Pelt (com)
:. '.v ‘1 4
rr
T Q Sound, vwdea and game (nntrdlers
.7 System dewtes
a g Unwevsal Sellal Bus :untmlers
Standard Universal PC] to use Host Cumoflev
Standavd UnwersaA PCI to use Host Cumoflev
Standavd Unwsa PCI to use flea Cumoflev
Standavd Unwsa PC] to use Host tumouw
use Ruot Hub
Use Root Hub
use Rent Hub
mm mm
USB Semi‘ Converter
driverWSB 20 TU P5232 Convertefldnverwl'tlun
"mum!
ummun frugr;
FTHI Ltd
Step B: Select “Load VCP” in the “Advanced”, click “OK”.
Step C: Move out the USB - RS232 converter on your computer. Connect the device to
an old USB port on your PC again, now it is ok, please refers to the following chart:
Congratulations, installation is successful.
Remove Driver
1, Open the drivers of this product, please refer to the below chart :
2, Double click “FTClen.exe”, it appears the following interface
VID [Hex]
FTD‘ v
FID [Hex]
Status: Ready
FTDI
Chip
: Clean Sys|em
Em
qum Unhr ‘1 u
FTDI
PID [Hex]
V’lndnwi >
3, click “Clean System”, it appears the following interface:
I, You is flint! tn “WIRE“ it FVDI mm: fDV VID UXMUS and i“ VIDS‘
q) nu m m to mm:
FTD‘
PID [Hex]
mm: W
Status: Ready
WDI .
FID [Hex]
Wm: M:
Status: Ready
PID [Hex]
Exit
Windows)?
Status: System clean completed
4, Disconnect USB 2.0 To rs232 device from the pc,click “ok” it appears the following
interface, then click „Yes”
5, please click “No” to uninstall driver
6, When Uninstall is completed, please click “Exit” to terminate the uninstall application.
. O 0 Install FTDlUSISerIalDrlver Kernel Extenslon
Wekome to the F‘I'DIUSISerialDriver Kernel Extension Installer
Welcome to the Mac OS X Installation Program. You will be
guided through the steps necessary to install this software
\
O lnstallaflon Type
0 Installing
O leSh Up
Mac OS X Installation Guide
1 Welcome to the Mac OS X Installation Guide
This document describes the procedure for installing the Mac OS X FTDIUSBSerial
driver for FTDI's FT2232C, FT232BM, FT245BM, FT8U232AM and FT8U245AM
devices. The driver is available for free download from the Drivers section of the FTDI
web site.
2 Installing FTDIUSBSerialDriver
Download the driver from the Drivers section of the FTDI web site and save it to the hard
disk.The driver is now available in disk image (.dmg) format. Run the installer by double
clicking on the FTDIUSBSerialDriver.dmg icon.
Click Continue to proceed with the installation and follow the instructions on
screen. When the installation is complete, reboot the computer.
O 0 0 Install FTDIUSlSeriaIDriver Kernel Extension
Install Software
,/ ,
B lroductlon
8 Re C] Me
GSeIe Destination
6 Installhlm TYpe
a lnstalllng The software was successfully installed
arm-shun —
Click Restart to finish installing the software.
When the computer has rebooted, plug in the device. If the device is installed properly,
you will see entries in the /dev directory:
/dev/cu.usbserial-xxxxxxxx
/dev/tty.usbserial-xxxxxxxx
where xxxxxxxx is either the device's serial number or, for unserialized devices, a
location string that depends on which USB port your device is connected to. Note that for
FT2232C devices port A is denoted by the serial number appended with "A" and port B is
designated by the serial number appended with "B"./dev can be accessed through the
Terminal application. The Terminal application can be launched by selecting Go >
Applications > Utilities > Terminal. Type the following lines in the Terminal
window to produce the file list:
cd /dev
ls-l
If you run the application System Preferences and select Network (Go > Applications >
System Preferences > Network), you should see the text "New Port Detected".
. New Port Detected
B . A new network port has been detected:
usbserial-IBZZ
Please verify that it is configured correctly. then
press Apply Now to activate it.
V
O O 0 Network (I)
W M Q 8
ShowAIl Displays Sound Network Startup Disk
Location: Automatic 3
Show: Network Port Configurations 3
Check a configuration to make it active.
Drag configurations into the order you want to try them when
connecting to a network.
On Port Configurations
a Internal Modem
i Built—in Ethernet
GD
d Cllck the lock to prevent further changes. Apply Now
Click OK and select Network Port Configurations from the Show list. The new port can be
enabled from this screen by checking the On box and clicking Apply Now.
At this point, it is possible to exit Network and use the device as a COM port. If you wish
to set the device up a modem for an Internet connection, select the new port from the
Show list to display the window below. Please note that the FT2232C device has two
ports available and these must be configured separately.
V O . 0 Network
:[CJQGI
ShowAIl Displays Sound Network StanupDisk
Location: Automatic 3
Show: ushserial-IBZZ S
TCP/IP Proxies Modern
Service Provider: — (Outlay-3|)
Account Name:
Password:
Telephone Number:
Alternate Number: (Optional)
D Save password
Checking this box allows all users of this computer to
aceess this Internet account without entering a password.
} ,
i Click the lock to prevent further (flanges. Apuly Now ‘
Entries for this screen are specific to the Internet account for each user. If you do not
know the required details, contact your Internet service provider.
3 Uninstalling FTDIUSBSerialDriver
To remove the drivers from Mac OS X, the user must be logged on as root. Root is a
reserved username that has the privileges required to access all files.
Start a Terminal session (Go > Applications > Utilities > Terminal) and enter the following
commands at the command prompt:
cd /System/Library/Extensions
rm -r FTDIUSBSerialDriver.kext
The driver will then be removed from the system.
To remove the port from the system, run the application SystemPreferences and select
Network. Selecting Network Port Configurations from the Show menu will display the
port as greyed out.
Select the uninstalled port and click Delete. Confirm the deletion to remove the port.
O o 0 Network
1EQ8I
ShowAIl Displays Sound Network Stanup Disk
Location: Auiomaiic S
Show: Network For! Configurations :
Check a configuration [0 make it active.
Drag configurations into the order you want to try them when
connecting to a network.
On Pen Configurations
usbseriaI-lBZZ
lmernal Modern
Built—in Ethernet
IlllLl‘
‘ Duplicate
®
] —
a Click the lock to prevenr further changes. Appiy Now i
4 How do I know what my deviceID is?
Launch the System Profiler utility, or Apple System Profiler for earlier versions of OS X.
This can be accessed by going to the Finder and selecting Applications from the Go
menu, then open the Utilities folder.
Select USB under Hardware in the pane to the left and then select the appropriate device
from the USB Device Tree. In the screen shot below (from OS 10.3), the device has a
deviceID given by:
Vendor Name: FTDI
Prioduct ID: 24577 ($6001)
A Vendor Name of FTDI is equivalent to a Vendor ID of 1027 ($0403).
0”
imam Ml:
loin/Inns 05:37
Anst aux
Columns USI Devlu TIE \
v namware us: lus
Memory 7 us: ms
PEI/AG! cm; vHub In Anpl: mended :maru
An —_
SCSI A0 a 0mm usa Mouse
us. Appln manned usa nybnam
r mm us: lus
Aimm Card use High—Spud nus
Madems
VSaflwav:
bflinlims
Emma-u u“ <_) mm:="" mm="" lngx="" .="" vendor="" name:="" rrm="" speed:="" up="" m="" 12="" mhlsu:="" mam="" id:="" 2457756001)="" bus="" pmm="" (ma):="" )on="">
If the device does not work after installing the driver, it is likely to be because the PID is
not supported by the driver. If this is the case, contact FTDI Support with the PID that
needs to be added to the driver. If the VID is not 0x0403, it is likely that the device is not
an FTDI device and we cannot support it.
Windows CE Installation Guide
1 Welcome to the Windows CE Installation Guide
The purpose of this MANUAL is to provide users of USB 2.0 To RS232 with a simple
procedure for installing drivers for their devices on PDAs and targets running Windows
CE 4.2 and later.
2 Installing Devices
The VCP drivers emulate a standard COM port. These can be communicated with in
the same manner as any other COM port on the PC.
_ ftdi_ser.dll - the VCP driver file
_ FTDIPORT.inf - user changeable file to allow devices with custom VID and PID
combinations to be installed
_ Copy all of the unzipped files to the \\Windows directory on the PDA.
_ If the PDA requires a host adaptor (e.g. USB host cable, presentation pack or
Compact
Unldzntlhed USED .7 1x [2:04
G Sunday, June 01,20fl3
Enter the name of the devnce
dlIVQI f0: ms OGVICQ‘ Fa
info: matuon. SEE the devnte
manufactwev‘s documentation.
HIE
12311|2|314|51617|8119|0 - «-
Iaquleelrlt] YLui] iIoIp [.U
CAP a 5 df
9h kl
wmflflflflflflfllll
Ctléu \ $ + «——»
IE‘
Flash host card), make sure that it is connected and installed before proceeding.
_ Connect the RS232 device to a host USB port on the PDA. This will provide a dialog
box to direct Windows CE to the driver files.
_ Type the full name of the VCP driver file into the dialog box as shown below. If the file
name is incorrect, the driver will not be found and the device will not function.
_ The device installation is now complete.
_ The device installation is now complete.
www.assmann.com
ASSMANN Electronic GmbH
Auf dem Schüffel 3
58513 Lüdenscheid
Germany