SHARP/Socle Technology 的 GP2Y1026AU0F Specification 规格书
SHARP
SPEC N0. ED“17G00lA
ISSUE : Jan 11, 2018
T0 :
Product Name Dust Sensor
ModelNo. GP 2Y1 O 2 6AUOF
These specifications contain 14 pages including the cover and appendix.
This specification sheets and attached sheets shall be both side copy.
After confirmation of the contents, please be sure to send back 1 copy of the
Specifications with approving signature on each‘
If you have any objections, please contact us before issuing purchasing orderi
Accepted by:
Sharp Corporation
By :
Name I BY 1 C . hp
Title : Name : T. Ichinose,
Date : Title : Division Manager,
Development Division. V
By : Semiconductor Business Unit
Name : Electronic Components and Devices BU
Title: Date: Q? n’. Jo/o‘
Date :
Reviewed by 1 Prepared by :
WWW By MM»;
Name 2%. Yamaguchi Name : M. Okami
Title 2 Associate Manager Title : Supervisor
Date 1);” ,// Mu» Dave 2 Jam //,za/f
REFERENCE
SHARP
2 / 14
1. These specification sheets include materials protected under copyright of Sharp Corporation ("Sharp").
Please handle with great cares and do not reproduce or cause anyone to reproduce them without Sharp's consent.
2. When using this Sharp product, please observe the absolute maximum ratings, other conditions and instructions for use
described in the specification sheets, as well as the precautions mentioned below.
Sharp assumes no responsibility for any damages resulting from use of the product which does not comply with absolute
maximum ratings, other conditions and instructions for use included in the specification sheets, and the precautions
mentioned below.
(Precautions)
(1) In making catalogue or instruction manual based on the specification sheets, please verify the validity of the catalogue
or instruction manuals after assembling Sharp products in customer's products at the responsibility of customer.
(2) This Sharp product is designed for use in the following application areas ;
• Computers • OA equipment • Telecommunication equipment (Terminal) • Measuring equipment
• Tooling machines ・Audio visual equipment • Home appliances
If the use of the Sharp product in the above application areas is for equipment listed in paragraphs (3) or (4),
please be sure to observe the precautions given in those respective paragraphs.
(3) Appropriate measures, such as fail-safe design and redundant design considering the safety design of the overall
system and equipment, should be taken to ensure reliability and safety when Sharp product is used for equipment
in responsibility of customer which demands high reliability and safety in function and precision, such as ;
• Transportation control and safety equipment (aircraft, train, automobile etc.)
• Traffic signals • Gas leakage sensor breakers • Rescue and security equipment
• Other safety equipment
(4)Sharp product is designed for consumer goods and controlled as consumer goods in production and quality.
Please do not use this product for equipment which require extremely high reliability and safety in function and
precision, such as ;
• Space equipment • Telecommunication equipment (for trunk lines)
• Nuclear power control equipment • Medical equipment
(5) Please contact and consult with a Sharp sales representative if there are any question regarding interpretation of
the above four paragraphs.
3. Disclaimer
The warranty period for Sharp product is one (1) year after shipment.
During the period, if there are any products problem, Sharp will repair (if applicable), replace or refund.
Except the above, both parties will discuss to cope with the problems.
The failed Sharp product after the above one (1) year period will be coped with by Sharp, provided that both parties
shall discuss and determine on sharing responsibility based on the analysis results thereof subject to the above scope
of warranty.
The warranty described herein is only for Sharp product itself which are purchased by or delivered to customer.
Damages arising from Sharp product malfunction or failure shall be excepted.
Sharp will not be responsible for the Sharp product due to the malfunction or failures thereof which are caused by:
(1) storage keep trouble during the inventory in the marketing channel.
(2) intentional act, negligence or wrong/poor handling.
(3) equipment which Sharp products are connected to or mounted in.
(4) disassembling, reforming or changing Sharp products.
(5) installation problem.
(6) act of God or other disaster (natural disaster, fire, flood, etc.)
(7) external factors (abnormal voltage, abnormal electromagnetic wave, fire, etc.)
(8) special environment (factory, coastal areas, hotspring area, etc.)
(9) phenomenon which cannot be foreseen based on the practical technologies at the time of shipment.
(10) the factors not included in the product specification sheet.
4. Please contact and consult with a Sharp sales representative for any questions about Sharp product.
REFERENCE
3 / 14
1. Application
This specification applies to the outline and characteristics of Model No. GP2Y1026AU0F (Dust sensor).
2. Outline
Refer to the attached drawing No. CY15345i02.
3. Ratings and characteristics
Refer to the attached sheet, Page 7 to 9.
4. Reliability
Refer to the attached sheet, Page 10.
5. Outgoing inspection
Refer to the attached sheet, Page 11.
6. Supplements
6-1 Dust density characteristics[Example]:
Refer to the attached sheet, Page 12.
6-2 This product shall not contain the following materials.
Also, the following materials shall not be used in the production process for this product.
Materials for ODS : CFCS, Halon, Carbon tetrachloride, 1.1.1-Trichloroethane (Methylchloroform)
6-3 Specified brominated flame retardants
Specified brominated flame retardants (PBB and PBDE) are not used in this device at all.
6-4 Product mass : Approx. 17g
6-5 Packaging specification : Refer to the attached sheet, Page 13.
6-6 Compliance with each regulation
6.6.1 The RoHS directive(2011/65/EU)
This product complies with the RoHS directive(2011/65/EU) .
Object substances: mercury, lead, cadmium, hexavalent chromium, polybrominated biphenyls(PBB)
and polybrominated diphenyl ethers(PBDE)
6.6.2 Content of six substances specified in Management Methods for Control of Pollution Caused by Electronic
Information Products Regulation (Chinese : 电子信息产品污染控制管理办法).
Marking Styles for the Names and Contents of the Hazardous Substances
Category
Hazardous Substances
Lead
(Pb)
Mercury
(Hg)
Cadmium
(Cd)
Hexavalent
chromium
(Cr6+)
Polybrominated
biphenyls
(PBB)
Polybrominated
diphenyl ethers
(PBDE)
Dust sensor × ○ ○ ○ ○ ○
This table is prepared in accordance with the provisions of SJ/T 11364.
○:Indicates that said hazardous substance contained in all of the homogeneous materials for this part is
below the limit requirement of GB/T 26572
×:Indicates that said hazardous substance contained in at least one of the homogeneous materials used
for this part is above the limit requirement of GB/T 26572
Lead in glass of electronic components (designated by “×” in the above table) are exempt from the RoHS
directive (2011/65/EC) , because there is no effective way to eliminate or substitute them by present scientific technology.
REFERENCE
4 / 14
7. Notes
7-1 Connection of case and GND
Case material use conductive resin as cover case (printed model No.) and metal (test terminal side)
as bottom cover. The metal case connects with GND in sensor.
7-2 Cleaning
Please don’t do cleaning, because there is a case that this device is not satisfied with its
characteristics by cleaning.
7-3 Dust Adhesion
There is a case that this product does not detect the dust density correctly, since the dust adhered to the inside
of the dust through hole may project into the detecting space which consist of emitter and detector
light axis. Please take the structure and mechanism of the equipment into consideration to avoid the
influence of adhered dust. And when the dust is adhered. Please consider the maintenance such as vacuuming
or blowing off the dust by air.
In addition, in case the foreign substance such as dust is attached to the optical system consist of light emitting
diode, light detector, lens and so on, and the inner portion of case, there is a variation in output at no dust of this sensor.
Please make allowance for the error in dust detection based on initial output at no dust of this sensor.
7-4 Light output
In circuit designing, make allowance for the degradation of the light emitting diode output that results
from long continuous operation. (50% degradation/5years)
7-5 Sensitivity adjustment VR
VR for sensitivity adjustment is set up at shipping from Sharp.
Please do not touch the VR or Electro-optical characteristics specified on the specification will be invalid.
7-6 Resolution
Please do not disassemble the device such as removing a tapping screw and so on.
Even if the device is reassembled, it may not satisfy the specification.
7-7 Application to fire alarm
Please do not use this device for a fire alarm application. When using this device to application other
than air purifying and equipment with air purifying function, please inform us before usage.
7-8 Noise influence
If the sensor is located close to noise source (ex. Electric dust collector, etc.).
The sensor output may be affected by leaded noise.
On top of that noise from power supply line also may affect the sensor output.
When designing the system, please consider the effect from noise.
7-9 Vibration influence
The sensor may change its output value under mechanical oscillation.
Before usage, please make sure that the device works normally in the application.
7-10 Incident light influence
There is a case that the sensor output may be affected when outer-light comes through dust through hole on printed side.
In order to avoid any influence from outer-light, please locate the printed side of the sensor facing to
inside of the application.
REFERENCE
5 / 14
7-11 Dewing
When inside of the sensor is moisturized, this product does not keep its proper function.
Please design the application so that moisturization of the sensor does not happen.
7-12 NC pin handling
Without connecting about a NC terminal for a sensor, please use as an OPEN terminal.
REFERENCE
E
46
(3-0)
*3].— N
n
/\ Marking
3 \ porslon 5;
n \,
vi
U « _—.
20 $9105 2 N
2243 Dust llwough hole
Connector arrangement
No Pinnome
'—
M 8 l GND
7‘? ,,,~ A 2 Vcc
2 _ v :1 NC
I I] ...... V 4 N
—l Rx
© ® TxD
(34.8) Connector
Made by JCTC 11501W90-6P—S-HF
28.l
22.5
R2
1.4
(5)
[Marking portion]
Production dole
( 2 dg'ns)
Producn'on mom}-
(1 lo 9- )(IOcl. Y:ch. 2202:)
Q'}
14.3
0 0
Production year
(Last rigil 0! [reduction yea)
Compmy name Model No.
4—. _ _
"2‘; 1510]
O
(s) ‘1» 5
(WEE-n)
lel underl'ne : Producl is made in China‘
(5)
Dual thrwyu hole Hole for sensitivity r”
ud‘uslment volume L__:lCarved seal
C _ 3am
1) Unspecified tolerance shall be £0.3mm. N GP2Y1026AUOF
( ) :Reference value ome Outline Dimennsions
Unit;mm Drawing No CY15345i02
6 / 14
2. Outline
REFERENCE
lfm \/ IT?)
W1 e :
/0x
00 0
OOO
7 / 14
3. Ratings and characteristics
3-1 Constitution diagram
3-2 Absolute maximum ratings
(Ta=25℃)
Parameter Symbol Rating Unit Remark
Supply voltage Vcc -0.3 to +6 V -
Input terminal voltage VRXD -0.3 to Vcc V -
Operating temperature Topr -10 to +65 ℃ -
Storage temperature Tstg -20 to +80 ℃ -
3-3 Operating Supply Voltage
Symbol Rating Unit Remark
Vcc 5±0.2 V -
発光
素子
駆動
回路
受光
素子
増幅
回路
増幅
回路
増幅
回路
③ NC
⑤ RXD
⑥
TXD
Gain
adjust
Dust or
Smoke particle
マイコン
①GND
② Vcc
④ NC
LED
Light
detector
Amp.
circuit
Drivinng
circuit Microcomputer
Amp.
circuit
Amp.
circuit
REFERENCE
8 / 14
3-4 Electro-optical Characteristics (Ta=25℃, Vcc=5V)
Parameter Symbol Conditions Min. Typ. Max. Unit
Sensitivity K (*1)(*2) 0.29 0.35 0.41 V /
(0.1mg/㎥)
Sensitivity
Output at no dust ⊿Vo
(*1)(*2)
0 - - V
Output terminal
voltage
Txdh
Output voltage
at High-level
(Ioh=1.5mA)
4.35 - - V
Txdl
Output voltage
at Low-level
(Ioh=1.5mA)
- - 0.8 V
Average
supply current ICC Vcc=5V - 15 20 mA
(*1) Dust density shall be measured the density of MEVIUS (made by Japan Tobacco Inc.) by using a digital
dust indicator P-5L2 (made by SIBATA SCIENTIFIC TECHNOLOGY LTD.).
Sensitivity : K shall be specified about output change when dust density is changed 0.1mg/㎥
(*2) Connection circuit example.
*)Without connecting about a RXD terminal for a sensor, please use as an OPEN terminal.
GND ①
RXD ⑤
TXD ⑥
Vcc ②
NC ③
NC ④
GND
RXD
Vcc
GP2Y1026AU0F MCU
REFERENCE
Vout (I I)
Vout (L)
9 / 14
3-4 The detail of Serial output
1) Transmission rate:2400 bit/s
2) 1 byte transmits every 10ms(The 7 bytes output in total)(Checksum=Vout(H)+ Vout(L)+Vref(H)+
Vref(L));
3) Data transmission format:
Start Vout(H)
Vout(L)
Vref
(H)
Vref
(L) Checksum End
0xaa Ex:
0x01
Ex:
0x3a
Ex:
0x00
Ex:
0x7a
Ex:
0xb5 0xff
4) Data handling:
Calculating formula of output voltage Vout :Vout=(Vout(H)*256+Vout(L))/1024*5
Ex:Vout(H)=0x01,Decimal number 1;
Vout(L)=0x3a, Decimal number 58;
Vout=(1*256+58)/1024*5=1.533V; (Vout is data update every approximately one second)
REFERENCE
No.
Dcfccli» C(C]
m M
10 / 14
4. Reliability
The reliability of products shall be satisfied with items listed below. Confidence level : 90%
LTPD : 20 or 30
No. Test Items Test Conditions Failure Judgment
Criteria
Samples (n)
Defective(C)
Temperature cycling
Icc>U×1.2
U : Upper specification limit
L : Lower specification limit
<The appearance>
Appearance
defect that
affect the
electrical
optical
characteristic.
n=11,c=0
2 High temp. and high
humidity storage
+60℃, 90%RH, 500h
n=11,c=0
3 High temp. and high
humidity operation
+60℃, 90%RH, VCC=5V, 500h
n=11,c=0
4 High temp. storage +80℃, 500h n=11,c=0
5 High temp. operation 65℃, Vcc=5V, 500h n=11,c=0
6 Low temp. storage -20℃, 500h n=11,c=0
7 Low temp. operation -10℃, Vcc=5V, 500h n=11,c=0
8 Mechanical shock 1000m/s2, 6.0ms
3times/±X, ±Y, ±Z direction
n= 8,c=0
9 Variable frequency
Vibration
5 to 55 to 5Hz/1min.
overall amplitude : 1.5mm
2h/X, Y, Z direction
n= 8,c=0
*1 Test conditions are according to 3-4 Electro-optical characteristics.
*2 After test, measurement shall be done after leaving under the normal
temperature and the normal humidity for 2h. And there should be no dew.
*3 These test results are sampling examples from a specific lot for reference purpose only,
and do not constitute any warranty or assurance in connection with the products.
10min or more
10min or more
30min 30min
20 cycle
+8
0
℃
-2
0
℃
REFERENCE
11 / 14
5. Outgoing inspection
(1) Inspection lot
Inspection shall be carried out per each delivery lot.
(2) Inspection method
A single sampling plan, normal inspection level II based on ISO 2859 shall be adopted.
Defect Inspection item AQL (%)
Major defect Electro-optical characteristics defect
(In para. 3-4) 0.4
Minor defect Defect on appearance and dimension
※ Split, chip, scratch, stain 1.0
※ Split, chip, scratch, stain
One which affects the characteristics of para. 3-4 shall be defect.
※ Rust shall not be defect.
REFERENCE
12 / 14
6-1 Dust density characteristics[Example]
Test conditions are according to 3-4 Electro-optical characteristics.
0
0.5
1
1.5
2
0 0.1 0.2 0.3 0.4 0.5
Output Voltage[V]
dust density[mg/m3]
REFERENCE
Non chemically-charged bug
(The mouth of the bag is folded
back on itself.) /Pad (Plastic)
Tray put products
/ (S-Tmy/case)
Product
Packing case
Kmft tape
Tray (Plastic)
Product
Tmy section
\
H17»: Ta
/ xiii L
Indication
Fig.3
13 / 14
6-5 Packaging specification
Fig.1 Top row only Lower row only with pad.
5 stacks (stack rotated by 180 ° per stage. Inverted product storage direction)
REFERENCE
14 / 14
1. Store 50 products in tray. (The storage method is shown in the figure.)
While stacking the product, turn the tray 180 degrees and stack it in 5 rows.
Pads are put only on the top and bottom.(Fig.1)
2. Store trays containing products that are stacked in five layers in a non electrically-charged bag. (Fig.2)
3. Put them (5 trays) in the packing box.
The mouth of the bug shall be put one on top of another.
4. Seal the packing box with kraft tape.
Put a label with Model No., Quantity, Lot No. on it. (Fig.3)
5. Indication items
The contents of the carton indication conforms to EIAJ C-3 and the following items are indicated.
Model No., Internal production control name, Quantity, Packing date,
Corporate name, Country of origin
(250pcs/a packing box)
(Formal packed mass : Approximately 5.6kg)
Packaging method
REFERENCE