TE Connectivity AMP Connectors 的 AMP-LATCH Novo Receptacles for Ribbon Cable 规格书
-.'CTE
annecrivily
—
brackets
1 1 1
No Polarization
This End 01 10
Application Specification
AMP- LATCH* Novo Receptacles for
Ribbon Cable with Conductors Having 114--40005
LOC B
1of 9
E2011 Tyco Electronics Corporation, a TE Connectivity Ltd. Company
All Rights Reserved
*Trademark
TE Connectivity, TE connectivity (logo), and TE (logo) are trademarks. Other logos, product and/or Company names may be trademarks of their respective owners.
TOO LING ASSISTANCE CENTER 1--800-- 722--1111
PRODUCT INFORMATION 1--800--522--6752
This controlled document is subject to change.
For latest revision and Regional Customer Service,
visit our website at www.te.com
1.27 mm [.050 in.] Centerlines 15 APR 11 Rev H
All numerical values are in metric units [with U.S. customary units in brackets]. Dimensions are in millimeters [and
inches]. Unless otherwise specified, dimensions have a tolerance of +0.13 [+.005] and angles have a tolerance of +2_.
Figures and illustrations are for identification only and are not drawn to scale.
1. INTRODUCTION
This specification covers the requirements for application of the AMP--LATCH Novo line of receptacle
connectors. The receptacles are available in sizes of 10, 14, 16, 20, 24, 26, 30, 34, 40, 50, 60, and 64
positions.
The contacts housed in these receptacles are of the insulation displacement connection (IDC) type. They
accept mating headers or other pin connectors having 0.64 [.025]--square pins or 0.64 [.025]--diameter round
pins 6.1 [.240] nominal length. Intermateability limitations and available polarization features are detailed in
Paragraph 3.2.
When corresponding with TE Connectivity representatives, use the terminology provided in this specification to
facilitate your inquiry for information. Basic terms and features of the connectors and contacts are provided in
Figure 1. Accessories and their identifying features are described in Paragraph 3.4 and shown in Figure 5.
Figure 1
Typical Novo
Contact
With
Dual Polarization
With Military
Polarization
With Center and
Military Polarization
Position 1 Index
Slot on This End
No Polarization Bar on
This End of 10--Position
Receptacles
No Polarization Slot on
This End of 10-- and
14--Position Receptacles
Typical Cover
No Polarization Slot on
This End of 10-- and
14--Position Receptacles
End Wall
NOTE
i
-.' TE
conn-cuv/tv
Document Number Document T
114- 40005
Rev H2 of 9
2. REFERENCE MATERIAL
2.1. Revision Summary
This paragraph is reserved for a revision summary of changes and additions made to this specification. The
following changes were made for this revision.
SUpdated document to corporate requirements.
2.2. Customer Assistance
Reference Part Number 746285 and Product Code 5754 are representative numbers of the AMP--LATCH line
of receptacle connectors. Use of these numbers will identify the product line and expedite your inquiries
through a service network established to help you obtain product and tooling information. Such information can
be obtained through a local TE Representative (Field Sales Engineer, Field Applications Engineer, etc.) or,
after purchase, by calling the Product Information number on the bottom of page 1.
2.3. Drawings
Customer Drawings for each product part number are available from the service network. The information
contained in Customer Drawings takes priority if there is a conflict with this specification or with any technical
documentation supplied by TE.
2.4. Specifications
Product Specification108--40000 for AMP--LATCH Novo and Novo Stackable Receptacles covers test data and
performance requirements.
2.5. Instructional Material
The following list includes available instruction sheets (408--series) that provide assembly procedures for
product, operation, maintenance and repair of tooling, as well as setup and operation procedures of
applicators; and customer manuals (409--series) that provide setup, operation, and maintenance of machines.
Document Number Document Title
408--6732 Pneumatic Auto--Cycle Unit
408--7763 Pneumatic Applicator Frame Assembly
408--7777 Manual Arbor Frame Assembly
408--9828 AMP--LATCH Universal Tooling Kit
408--9831 AMP--LATCH Receptacle Connector--Specific Kits
409--5725 R--CAM 2A Cable Terminating Machine 760700--6
409--5794 R--CAM 3A Cable Terminating Machine 761900--[ ]
3. REQUIREMENTS
3.1. Storage
A. Ultraviolet Light
Prolonged exposure to ultraviolet light may deteriorate the chemical composition used in the housing
material.
B. Shelf Life
Each connector is packaged and shipped in an individual antistatic tube container. To prevent damage to
the housings and contacts, the connectors should remain in the container until ready for installation. Also,
to prevent possible storage contamination, the connectors should be used on a first in, first out basis.
C. Chemical Exposure
Do not store product near any of the following chemicals as they may cause stress corrosion.
Alkalies Ammonia Citrates Phosphates Citrates Sulfur Compounds
Amines Carbonates Nitrites Sulfides Nitrites Tartrates
Where the above environmental conditions exist, phosphor--bronze contacts are recommended instead of brass if
available.
NOTE
i
-.' TE
com-cm!”
.W
Standard Planar
Slranded N Solid
n m [1,37]
[To
Mound-"W" Min-w 1)
114- 40005
Rev H 3 of 9
3.2. Cable Selection and Preparation
The IDC contacts in AMP--LATCH receptacles are designed to accept PVC--insulated cable wires with 26 or 28
AWG conductors. Insulation materials other than standard PVC must be submitted to TE Engineering for
evaluation before use. The types of cables that can be used are shown in Figure 2. Also shown is the initial cut
to be made, regardless of the cable type, using a guillotine--type cutting tool. Contact your TE representative
for current tool recommendations for cutting and notching of cables.
Initial Cable Cut
(For All Cable Types)
-- A --
0.25 [.010] A
CABLE CONDUCTOR DIMENSION
C
A
B
L
E
TYPE SIZE (AWG) TYPE “A” “B”
Standard Planar 26
S
t
r
a
n
d
e
d
o
r
S
o
l
i
d
0
9
4
[
0
3
7
]
S
t
a
n
d
a
r
d
P
l
a
n
a
r
or Ribbon 28
S
tran
d
e
d
or
S
o
l
i
d
0.94
[
.037
]
Woven (Discrete Wire) 28 Stranded or Solid 0.79 [.031] (Total Number
o
f
C
o
n
d
u
c
t
o
r
s
M
i
n
u
s
1
)
All Shielded Types 28 Stranded or Solid 0.81 [.032]
o
f
C
on
d
uctors
M
i
nus 1
)
x 1.27 [.050]
Jacketed Flat 28 Stranded or Solid 0.86 [.034]
Twisted--Pair FLat 28 Stranded 1.09 [.043]
Figure 2 (cont’d)
-.'. TE
mummy
with 34
H
|+
114- 40005
Rev H4 of 9
Figure 2 (end)
12.7
[.500]
(Min)
44.45
[1.750]
B+(See Note 1)
[.050+.003]
0.64+0.18
[.025+.007]
(Typ)
1.27+0.08
A+0.13
[+.005]
A+0.13
[+.005]
0.64+0.18
[.025+.007]
(Typ)
A+0.13
[+.005]
43.18
[1.70]
(Min)
B+(See Note 1)
[.050+.003]
1.27+0.08
A+0.13
[+.005]
B+(See Note 1)
0.64+0.18
[.025+.007]
(Typ)
[.050+.003]
1.27+0.08
60.32
[2.375]
11.18
[.44]
(Min)
Woven Cable
(Discrete Wire)
Jacketed Flat Cable
Twisted-Pair Flat Cable
Shielded Cable
B+(See Note 1)
0.64+0.18
[.025+.007]
(Typ)
1.27+0.08
[.050+.003]
0.64+0.18
[.025+.007]
(Typ)
B+(See Note 1)
1.27+0.08
[.050+.003]
A+0.13
[+.005]
A+0.13
[+.005]
Standard Planar Cable
Ribbon Cable
(See Note 2)
Notes: 1.Cumulative tolerance for cables with 1--34 conductors is +0.25 [+.010];
for cables with 40--64 conductors is +0.38 [+.015].
2.Ground plane and shielded cable must be notched as shown.
Cable Types
mu :::::::::
114- 40005
Rev H 5 of 9
3.3. Product Selection
The specific acceptable pin length range for AMP--LATCH Novo Receptacles is 4.44--6.22 [.175--.245].
Figure 3 shows relationships between available receptacles and the connectors that will mate with them.
MATING POLARIZATION OPTIONS
M
A
T
I
N
G
CONNECTOR TYPES MILITARY CENTER AND MILITARY DUAL
Pin Connector with or without Mounting Ears XXX
Pin Connector with or without Mounting Ears
and with Detent Windows
XXX
Bulkhead Pin Connector X-- -- -- X
Universal Ejection Style Pin Header XXX
Military Ejection Style Header X X -- -- --
Low--Profile Pin Header XXX
High Temperature Universal
Ejection Style Pin Header
XXX
Universal Ejection Style Pinless Header XXX
Stacked Headers XXX
AMPMODU* HeadersUX-- -- -- X
UOnly headers that have a 3.81 [.150] end dimension will mate.
Figure 3
A. Polarization and Strain Relief
Polarization has been designed into the housings of Novo receptacles.
B. Military, Center, and Dual Polarization
Receptacles with military polarization can be used in all header and plug connectors. Those with a
combination of military and center polarization, and those with dual polarization can only be used with
header or plug connectors that have the respective type of center or dual polarization.
C. Receptacle Cover Options
Covers are designed for either feed--through or end--of--line applications.
3.4. Terminated Receptacle Requirements
Prepared cable shall be terminated according to the procedures given in the applicable tooling instructions.
See Paragraph 2.3, for details on tooling options and instructional materials. Figure 4 shows criteria for
acceptable terminations.
Reasonable care should be taken by tooling operators to provide undamaged terminations. An improper termination in
any of the IDC contacts will be reason to discard the entire receptacle. Contacts are designed for one--time
termination, and cannot be replaced, repaired, or re--used.
NOTE
i
.7
114- 40005
Rev H6 of 9
Figure 4
All Contact Latching Ears Must
Be Latched into Cover
0.13 [.005] (Max) Gap
Between Housing and
Cover (Typ Both Ends)
No Air Gaps Between
Wire Insulation And
Adjacent Contacts
0.51 [.020]
Protrusion (Ref)
0.89 [.035]
(Max) Recess
Side View of Application
Conductor Strands Will Be
Exposed and Deformed on
Both Sides
All Conductor
Strands Must Be
Below Tapered
Transition
Typical Cross- Section
Termination Requirements
3.5. Accessories (Figure 5)
A. Strain Relief
Strain relief may be added to any application.
B. Keying Plugs
Keying plugs are designed to be hand inserted directly into the contact cavities. Corresponding pins must
be removed from the mating connector.
C. Pull Loops
Flexible pull loops may be permanently assembled. The loop is installed between the strain relief and the
cover in strain--relieved applications. An unattached, insertion type of pull tab is also available for
receptacles not employing strain relief.
114- 40005
Rev H 7 of 9
Figure 5
Flexible Pull Loop
(For Receptacles
and Pin Connectors
Snap--In Pull Tab (For
Receptacles Without
Strain Relief)
Pull Tabs
Strain--Relief Cover
Keying Plug
Cable Dress for Receptacles
Using Strain--Relief Cover
Keying Plugs
Strain Relief
Recess on
This Side
Polarization Bar
Strain Relief Components
Accessories
Flexible Pull--Tab
Housing
Locking
Latch
3.6. Testing
Completed cable assemblies should be tested for continuity using a CIRRIS TesterD, or similar equipment.
The automatic cable assembly machines described in Paragraph 5.3, contain their own test equipment,
and should be operated according to the documentation supplied with them.
4. QUALIFICATIONS
AMP--LATCH Novo Receptacles for Ribbon Cable are Recognized under the Component Recognition Program
by Underwriters Laboratories Inc. (UL) under Electrical File Number E--28476. They are also Certified by the
Canadian Standards Association (CSA) under File Number LR--7189.
DManufactured by CIRRIS Systems Corp.
114- 40005
Rev H8 of 9
5. TOOLING
This section provides a selection of tools for various application requirements. They include hand tools for
manual application of product, and semi--automatic and automatic machines for power assist application
product. Modified designs and additional tooling concepts may be available to meet other application
requirements. For additional information, contact one of the service groups at the bottom of page 1. A listing of
tooling recommendations covering the full product range is provided in Figure 6.
AMP--LATCH Receptacle Connectors for ribbon cable having 1.27 [.050] centerlines can be attached to the
cable with hand application tooling and arbor frame assemblies for small volume prototype and repair
applications, or cable--making machines for complete cable assemblies in higher volume production
requirements.
SHand Application Tooling: A typical guillotine--type cutting tool used to cut ribbon cable for
AMP--LATCH receptacles is shown in Figure 6. The components needed for hand tool application will
consist of a hand tool, tooling assembly, and a connector--specific kit. After the hand tool and tooling
assembly are set up, they will accept the connector--specific kit with no further adjustments. The
connector--specific kit is designed for both the hand tool and the arbor frame assembly.
SArbor Frame Assemblies: There are manually operated and pneumatically operated (auto--cycle and foot
pedal actuated) arbor frame assemblies designed for bench mounted operation. They accept
standardized upper/lower tooling assemblies that have been designed for the AMP--LATCH
Connector--Specific Kit. Instruction sheets covering tool setup and operation are packaged with the
tooling. See Figure 6.
SCable Making Machines: There are two high production automatic machines designed to make cable
assemblies using standard planar ribbon cable described in Figure 2. One is the R--CAM 2A for
terminating up to four connectors to a cable assembly (one connector on the leading end and three on
the trailing end of the cable assembly), and the other is the R--CAM 3A for terminating up to two
connectors (one on the leading end and one on the trailing end). Both machines can accommodate
variations of the AMP--LATCH Ribbon Cable Connectors. A customer manual for setup and operation
will be supplied for each machine. Both machines test the cable assemblies for continuity and short
circuits as they are being processed. See Figure 8 for typical R--CAM 2A machine design.
Figure 6
Manual Arbor Frame
Assembly 91085--2
(408--7777)
Pneumatic Arbor Frame
Assemblies 91112--2
(408--7763); and --3
408--6732)
Connector--Specific
Kit 768341--1
(408--9831)
Tooling Assembly
768338--1 (408--9827)
Guillotine--Type Cable Cutter
(Customer--Supplied)
Hand Tool
Subassembly
768942--1
(408--9846)
Tooling Assembly
768339--1 (408--9826)
R--CAM 2A
Machine
760700--6
(409--5725)
R--CAM 3A
Machine
761900--[ ]
(409--5794)
'-' TE
114- 40005
Rev H 9 of 9
6. VISUAL AID
Figure 7 is to be used by production personnel to ensure a properly applied product. The views shown suggest
requirements for all similar applications. Applications NOT visually correct should be inspected using the
information in the main body of this document and in the instructional materials shipped with the product or
tooling.
FIGURE 7. VISUAL AID
TWO CONTACT
TIPS VISIBLE IN EACH
WINDOW
CABLE AND COVER
RIDGES MUST ALIGN WITH
EACH OTHER
CONTACT LATCHING EARS
MUST BE LATCHED INTO
COVER
NOTE: SMALL FISSURES IN THE END WALLS WHICH DO NOT RESULT IN MATERIAL
SEPARATION ARE ACCEPTABLE AND DO NOT AFFECT CONNECTOR FUNCTIONALITY.