TDK-Lambda 的 QM7, QS7 Series Install Manual 规格书
0M7 AND 087 HANDBOOK TDK-Lambda
A
Page 1 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
General Safety Instructions:
READ SAFETY INSTRUCTIONS
Servicing:
These products are not customer serviceable. TDK-Lambda UK LTD. and their authorised agents only are
permitted to carry out repairs.
Critical Components:
These products are not authorised for use as critical components in nuclear control systems, life support
systems or equipment for use in hazardous environments without the express written approval of the
Managing Director of TDK-Lambda EMEA.
Product Usage:
These products are designed for use within a host equipment which restricts access to authorised competent
personnel.
This product is a component power supply and is only to be installed by qualified persons within other
equipment and must not be operated as a stand-alone product.
This product is for sale to business to business customers and can be obtained via distribution channels.
It is not intended for sale to end users.
This product is a component power supply and does not fall within the scope of the EMC directive.
Compliance with the EMC directive must be considered in the final installation. Please contact your local
TDK-Lambda office
Environmental:
These products are IPX0, and therefore chemicals/solvents, cleaning agents and other liquids must not be
used.
Environment:
This power supply is a switch mode power supply for use in applications within a Pollution Degree 2,
overvoltage category II environment. Material Group IIIb PCB’s are used within it.
Output Loading:
The output power taken from the power supply must not exceed the rating stated on the power supply label,
except as stated in the product limitations in this handbook.
Input Parameters:
This product must be operated within the input parameters stated in the product limitations in this handbook.
End of Life Disposal:
The unit contains components that require special disposal. Make sure that the unit is properly disposed of at
the end of its service life and in accordance with local regulations.
RISK OF ELECTRIC SHOCK
High Voltage Warning:
Dangerous voltages are present within the power supply. The professional installer must protect service
personnel from inadvertent contact with these dangerous voltages in the end equipment.
0M7 AND 087 HANDBOOK
TDK-Lambda
Page 2 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
WARNING: When installed in a Class I end equipment, this product must be reliably earthed and
professionally installed.
The (+) or (-) output(s) can be earthed or left floating.
The unit cover(s)/chassis must not be made user accessible.
CAUTION: DOUBLE POLE/NEUTRAL FUSING (Option D)
The mains input connector is not acceptable for use as field wiring terminals.
Do not use mounting screws, which penetrate the unit more than 4.5mm.
Special earthing screws are used on these products which connect the cover to the chassis. They must not
be removed. If they are removed by mistake, they must be replaced with new ones and the product tested for
earth bonding.
An internal fuse protects the unit and must not be replaced by the user. In case of internal defect, the unit
must be returned to TDK-Lambda UK LTD or one of their authorised agents.
A suitable mechanical, electrical and fire enclosure must be provided by the end use equipment for
mechanical, electric shock and fire hazard protection.
Energy Hazards:
Certain modules are capable of providing hazardous energy (240VA) according to output voltage setting.
Final equipment manufacturers must provide protection to service personnel against inadvertent contact with
these module output terminals. If set such, that hazardous energy can occur, then the module terminals or
connections must not be user accessible.
HOT SURFACE
External Hot Surfaces:
In accordance with local regulations for Health and Safety at work, manufacturers have an obligation to
protect service engineers as well as users. In order to comply with this, a label must be fitted to these
products which is clearly visible to service personnel accessing the overall equipment, and which legibly
warns that surfaces of these products may be hot and must not be touched when the products are in
operation.
The unit may be mounted in any orientation except inverted (mounted on its top) or vertical with the airflow
downwards.
The ventilation openings on these products must not be impeded. Ensure that there is at least 50mm spacing
between any obstruction and the ventilation openings.
The unit cover/chassis is designed to protect skilled personnel from hazards. They must not be used as part
of the external covers of any equipment where they may be accessible to operators, since under full load
conditions, part or parts of the unit chassis may reach temperatures in excess of those considered safe for
operator access.
0M7 AND 087 HANDBOOK TDK-Lambda
A
Page 3 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
DEUTSCH
Allgemeine Sicherheitsvorschriften:
LESEN SIE DIE SICHERHEITSVORSCHRIFTEN
Wartung:
Diese Produkte können nicht durch den Kunden gewartet werden. Nur TDK-Lambda UK LTD. und deren
zugelassene Vertriebshändler sind zur Durchführung von Reparaturen berechtigt.
Kritische Komponenten:
Diese Produkte sind nicht für die Verwendung als kritische Komponenten in nuklearen Kontrollsystemen,
Lebenserhaltungssystemen oder Geräten in gefährlichen Umgebungen geeignet, sofern dies nicht
ausdrücklich und in Schriftform durch den Geschäftsführer von TDK-Lambda EMEA genehmigt wurde.
Produktverwendung:
Diese Produkte sind zur Verwendung innerhalb von Host-Anlagen gedacht, die einen auf das Fachpersonal
beschränkten Zugang haben.
Dieses Produkt ist eine Stromversorgungs-Komponente und sie darf nur von qualifiziertem Personal in
andere Geräte eingebaut werden und sie darf NICHT als eigenständiges ("Stand-Alone") Gerät betrieben
werden.
Dieses Produkt ist für den Verkauf an Geschäftskunden entwickelt worden und es kann über
Distributionskanäle bezogen werden.
Es ist NICHT für den Verkauf an Endkunden gedacht und konzipiert.
Dieses Produkt ist eine Stromversorgungsbaugruppe und sie fällt NICHT in den Bereich der EMV Direktive.
Die Konformität mit der EMV Richtlinie muss in der finalen Gesamtinstallation betrachtet werden.
Bitte kontaktieren Sie Ihr regionales TDK-Lambda Vertriebsbüro im Falle von Rückfragen.
Umwelt:
Diese Produkte sind IPX0, aus diesem Grund dürfen keine Chemikalien/Lösungsmittel, Reinigungsmittel und
andere Flüssigkeiten verwendet werden.
Umgebung:
Dieses Netzteil ist ein Schaltnetzteil zur Verwendung in einer Umgebung mit einem Verschmutzungsgrad 2,
Überspannungskategorie II. Materialgruppe IIIb mit darin verwendeten PCBs.
Ausgangsstrom:
Der Ausgangsstrom des Netzteiles darf die Leistung, die auf dem Label des Netzteiles vermerkt ist, nur dann
überschreiten, wenn dies in den Produktgrenzen dieses Handbuches ausgezeichnet ist.
Eingangsparameter:
Dieses Produkt muss innerhalb der Eingangsparameter, die in den Produktgrenzen dieses Handbuches
angegeben sind, betrieben werden.
Entsorgung am Ende der Betriebszeit:
Das Gerät enthält Komponenten die unter Sondermüll fallen. Das Gerät muss am Ende der Betriebszeit
ordnungsgemäß und in Übereinstimmung mit den regionalen Bestimmungen entsorgt werden.
GEFAHR DURCH ELEKTRISCHEN SCHLAG
Hochspannungswarnung:
Innerhalb des Netzteiles gibt es gefährliche Spannungen. Der Elektroinstallateur muss das
Wartungspersonal vor versehentlichem Kontakt mit den gefährlichen Spannungen im Endgerät schützen.
0M7 AND 087 HANDBOOK
TDK-Lambda
Page 4 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
WARNUNG! Falls Sie unser Netzgerät in eine Anwendung mit Schutzklasse 1 eingebaut haben, stellen Sie
sicher, dass es fachgerecht installiert und zuverlässig geerdet ist.
Die (+) oder (-) Ausgänge können geerdet werden oder unangeschlossen bleiben.
Die Abdeckung des Gerätes/das Gehäuse darf für den Benutzer nicht zugänglich sein.
ACHTUNG: ZWEIPOLIGE/NEUTRALE SICHERUNG (Option D)
Der Haupteingangsanschluss ist nicht für die Verwendung als Feldverdrahtungsanschluss geeignet.
Verwenden Sie keine Befestigungsschrauben, die mehr als 4.5mm in das Gerät eindringen.
Zur Befestigung der Abdeckung am Gehäuse werden für diese Produkte spezielle Erdungsschrauben
verwendet. Diese dürfen nicht entfernt werden. Sollten sie versehentlich entfernt werden, müssen sie durch
neue ersetzt und das Produkt auf Erdschluss geprüft werden.
Eine interne Sicherung schützt das Gerät und darf durch den Benutzer nicht ausgetauscht werden. Im Fall
von internen Defekten muss das Gerät an TDK-Lambda UK LTD oder einen der autorisierten
Vertriebshändler zurückgeschickt werden.
Ein geeignetes mechanisches, elektrisches und brandgeschütztes Gehäuse muss als Schutz vor der Gefahr
von mechanischen Risiken, Stromschlägen und Brandschutz in dem Endgerät vorgesehen werden.
Gefahren durch elektrische Energie:
Von bestimmten Modulen kann je nach Einstellung der Ausgangsspannung gefährliche elektrische Energie
ausgehen (240 VA). Die Endgerätehersteller müssen einen Schutz für Servicepersonal vor unbeabsichtigtem
Kontakt mit den Ausgangsanschlüssen dieser Module vorsehen. Kann aufgrund der Einstellung gefährliche
elektrische Energie auftreten, dürfen die Modulanschlüsse für den Benutzer nicht zugänglich sein.
HEISSE OBERFLÄCHEN
Äußere heiße Oberflächen:
In Übereinstimmung mit den regionalen Bestimmungen für Gesundheit und Sicherheit bei der Arbeit ist der
Hersteller für den Schutz von Wartungspersonal und Benutzern verantwortlich. Um diesen Bestimmungen
gerecht zu werden, muss auf den Produkten ein Label angebracht werden, das deutlich sichtbar für das
Wartungspersonal mit Zugriff auf die gesamte Anlage ist, und das gut lesbar auf die eventuell heiße
Oberfläche des Gerätes hinweist und das Berühren des Produktes in Betrieb untersagt.
Das Gerät darf in jeder Position befestigt werden, mit Ausnahme über Kopf (umgekehrt) oder vertikal mit dem
Luftstrom abwärts.
Die Belüftungsöffnungen an diesem Produkt dürfen nicht blockiert werden. Achten Sie darauf, dass
mindestens 50 mm Abstand zwischen Hindernissen und den Belüftungsöffnungen bleibt.
Die Geräteabdeckung/das Gehäuse ist so entworfen, dass das Fachpersonal vor Gefahren geschützt wird.
Sie dürfen nicht als Teil der externen Abdeckung für Geräte verwendet werden, die für den Betreiber
zugänglich sein müssen, da Teile oder das gesamte Gerätegehäuse unter voller Auslastung übermäßige
Temperaturen erreichen kann, die für den Zugang des Betreibers nicht mehr als sicher betrachtet werden.
0M7 AND 087 HANDBOOK
TDK-Lambda
A
Page 5 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
FRANÇAIS
Consignes générales de sécurité:
LIRE LES CONSIGNES DE SECURITE
Entretien:
Ces produits ne peuvent pas être réparés par l’utilisateur. Seuls, TDK-Lambda UK LTD et ses agents agréés
sont autorisés à effectuer des réparations.
Composants critiques:
Ces produits ne doivent pas être utilisés en tant que composants critiques dans des systèmes de commande
nucléaire, dans des systèmes de sauvetage ou dans des équipements utilisés dans des environnements
dangereux, sans l'autorisation écrite expresse du directeur général de TDK-Lambda EMEA.
Utilisation du produit:
Ces produits sont conçus pour être utilisés dans un équipement hôte dont l'accès n'est autorisé qu'aux
personnes compétentes.
Ce produit est une alimentation considérée comme un composant devant être installé par des personnes
qualifiées, dans un autre équipement. Il ne doit pas être utilisé en tant que produit fini.
Ce produit est destiné à la vente entre entreprises et peut être obtenu via des canaux de distribution.
Il n’est pas prévu à la vente pour les particuliers.
Ce produit est une alimentation considérée comme un composant, il ne relève pas du champ d’application de
la directive CEM. Le respect de la directive CEM doit être pris en compte dans l’installation finale. Veuillez
contacter votre bureau TDK-Lambda le plus proche.
Environnement:
Ces produits sont IPX0, et donc on ne doit pas utiliser des produits chimiques/solvants, des produits de
nettoyage et d'autres liquides.
Environnement fonctionnel:
Cette alimentation fonctionne en mode commutation pour utilisation dans des applications fonctionnant dans
un environnement avec Degré de Pollution 2 et catégorie de surtension II. Elle utilise des cartes des circuits
imprimés (PCB) de Groupe IIIb.
Intensité soutirée:
L'intensité soutirée de l'alimentation ne doit pas dépasser l'intensité nominale marquée sur la plaque
signalétique, sauf indications contraires dans les limitations du produit décrit dans ce manuel."
Paramètres d'entrée:
Ce produit doit être utilisé à l'intérieur des paramètres d'entrée indiqués dans les limitations du produit dans
ce manuel.
Elimination en fin de vie:
L'alimentation contient des composants nécessitant des dispositions spéciales pour leur élimination. Vérifiez
que cette alimentation est mise au rebut correctement en fin de vie utile et conformément aux
réglementations locales en vigueur."
RISQUE DE CHOC ELECTRIQUE
Attention-Danger haute tension:
Des tensions dangereuses sont présentes dans l'alimentation. L'installateur doit protéger le personnel
d'entretien contre un contact involontaire avec ces tensions dangereuses dans l'équipement final.
0M7 AND 087 HANDBOOK
TDK-Lambda
Page 6 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
AVERTISSEMENT: Si ce produit est installé dans un équipement final de classe I, il doit être mis à la terre de
manière fiable et installé par un professionnel averti.
Les sorties (+) ou (-) peuvent être raccordées à la terre ou laissées flottantes.
Le couvercle/châssis de l'alimentation ne doit pas être accessible à l'utilisateur.
ATTENTION : FUSIBLE BIPOLAIRE/NEUTRE (Option D)
Le connecteur d'entrée d'alimentation principale ne doit pas être utilisé comme borne de raccordement.
N'utilisez pas de vis pénétrant dans le module sur une profondeur supérieure à 4.5mm.
Des vis de terre spéciales sont utilisées sur ces produits pour raccorder le couvercle au châssis. Elles ne
doivent pas être enlevées. Si elles sont enlevées par erreur, elles doivent être remplacées et le produit doit
être testé pour vérifier que le raccordement à la terre est correct.
Un fusible interne protège le module et ne doit pas être remplacé par l'utilisateur. En cas de défaut interne, le
module doit être renvoyé à TDK-Lambda UK LTD ou l'un de ses agents agréés.
Une enceinte appropriée doit être prévue par l'utilisateur final pour assurer la protection contre les chocs
mécaniques, les chocs électriques et l'incendie.
Energies dangereuses:
Certains modules peuvent générer une énergie dangereuse (240 VA) selon le réglage de tension de sortie.
Le fabricant de l'équipement final doit assurer la protection des techniciens d'entretien contre un contact
involontaire avec les bornes de sortie de ces modules. Si une telle tension dangereuse risque de se produire,
les bornes ou les connexions du module ne doivent pas être accessibles par l'utilisateur.
SURFACE CHAUDE
Surfaces chaudes extérieures:
Conformément aux réglementations locales concernant la santé et la sécurité sur les lieux de travail, les
fabricants doivent protéger les techniciens d'entretien et les utilisateurs. Pour cela, une plaque signalétique
doit être installée sur ces produits, et cette plaque doit être bien visible pour les techniciens d'entretien
intervenant sur l'équipement, et elle doit indiquer de manière bien visible par les surfaces de ces produits
peuvent être chaudes et qu'elles ne doivent pas être touchées lorsque les produits fonctionnent.
Le module peut être monté suivant une orientation quelconque, sauf en position inversée (monté sur son
sommet) ou en position verticale avec écoulement d'air descendant.
Les orifices de ventilation sur ces produits ne doivent pas être obstrués. Vérifiez qu'il y a un espace libre d'au
moins 50 mm entre une obstruction et les orifices de ventilation.
Le couvercle et le châssis du module sont conçus pour protéger des personnels expérimentés. Ils ne doivent
pas être utilisés comme couvercles extérieurs d'un équipement, accessible aux opérateurs car en condition
de puissance maximum, des parties du châssis peuvent atteindre des températures considérées comme
dangereuses pour l'opérateur.
0M7 AND 087 HANDBOOK TDK-Lambda
A
Page 7 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
ITALIANO
Norme generali di sicurezza:
SI PREGA DI LEGGERE LE NORME DI SICUREZZA
Manutenzione:
Il cliente non può eseguire alcuna manutenzione su questi prodotti. L'esecuzione delle eventuali riparazioni è
consentita solo a TDK-Lambda UK LTD e ai suoi agenti autorizzati.
Componenti critici:
Non si autorizza l'uso di questi prodotti come componenti critici all'interno di sistemi di controllo nucleari,
sistemi necessari alla sopravvivenza o apparecchiature destinate all'impiego in ambienti pericolosi, senza
l'esplicita approvazione scritta dell'Amministratore Delegato di TDK-Lambda EMEA.
Uso dei prodotti:
Questi prodotti sono progettati per l'uso all'interno di un'apparecchiatura ospite che limiti l'accesso al solo
personale competente e autorizzato.
Questo prodotto è da considerarsi come un alimentatore professionale componente e come tale deve essere
installato da personale qualificato all'interno di altre apparecchiature e non può essere utilizzato come
prodotto indipendente.
Questo prodotto non è inteso per la vendita al dettaglio o agli utilizzatori finali.
Questo alimentatore è da considerarsi come un componente e come tale non è assogettato dagli scopi della
direttiva EMC. Conformità alla direttiva EMC deve essere considerata nell'installazione finale di utilizzo. Gli
uffici di TDK-Lambda Sas Succursale Italiana sono a vostra disposizione per ulteriori ragguagli.
Condizioni ambientali:
Questi prodotti sono classificati come IPX0, dunque non devono essere utilizzati sostanze chimiche/solventi,
prodotti per la pulizia o liquidi di altra natura.
Ambiente:
Questo prodotto è un alimentatore a commutazione, destinato all'uso in applicazioni rientranti in ambienti con
le seguenti caratteristiche: Livello inquinamento 2, Categoria sovratensione II. Questo prodotto contiene
schede di circuiti stampati in materiali di Gruppo IIIb.
Carico in uscita:
La potenza in uscita ottenuta dall'alimentatore non deve superare la potenza nominale indicata sulla targhetta
dell'alimentatore, fatto salvo dove indicato nei limiti per i prodotto specificati in questo manuale.
Parametri di alimentazione:
Questo prodotto deve essere utilizzato entro i parametri di alimentazione indicati nei limiti per il prodotto,
specificati in questo manuale."
Smaltimento:
L'unità contiene componenti che richiedono procedure speciali di smaltimento. Accertarsi che l'unità venga
smaltita in modo corretto al termine della vita utile e nel rispetto delle normative locali.
RISCHIO DI SCOSSA ELETTRICA
Avvertimento di alta tensione:
All'interno dell'alimentatore sono presenti tensioni pericolose. Gli installatori professionali devono proteggere
il personale di manutenzione dal rischio di contatto accidentale con queste tensioni pericolose all'interno
dell'apparecchiatura finale.
ATTENZIONE: Se installato in un’attrezzatura di classe I, questo prodotto deve essere collegato a terra in
modo affidabile ed installato in modo professionale.
0M7 AND 087 HANDBOOK
TDK-Lambda
Page 8 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Le uscite (+) o (-) possono essere messa a terra o lasciate isolate.
I coperchi/il telaio dell'unità non devono essere accessibili da parte dell'utente.
ATTENZIONE: PROTEZIONE CON FUSIBILE BIPOLARE/NEUTRO (Opzione D)
Il connettore dell'alimentazione principale non può essere utilizzato come terminale di collegamento di
campo.
Non utilizzare viti che penetrano nell'unità per più di 4.5mm.
Per questi prodotti vengono usate viti speciali di messa a terra, che collegano il coperchio al telaio. Tali viti
non devono essere rimosse. Se le viti vengono tolte per errore, vanno sostituite con nuove viti ed occorre
testare il prodotto per verificarne il collegamento a massa.
Un fusibile interno protegge l'unità e non deve essere sostituito dall'utente. Nell'eventualità di un difetto
interno, restituire l'unità a TDK-Lambda UK LTD o a uno dei suoi agenti autorizzati.
L'apparecchiatura finale deve includere una recinzione meccanica, elettrica e antincendio per proteggere dai
pericoli di natura meccanica, dalle scosse elettriche e dai pericoli di incendio.
Pericoli energetici:
Alcuni moduli sono in grado di erogare energia pericolosa (240 VA) a seconda della tensione in uscita
impostata. I produttori delle apparecchiature finali sono tenuti a proteggere il personale di manutenzione dal
rischio di contatto accidentale con questi terminali dei moduli di uscita. Se impostati su livelli che non
escludono l'erogazione di energia pericolosa, questi terminali o collegamenti non devono risultare accessibili
da parte dell'utente.
SUPERFICIE CALDA
Superfici esterne calde:
Coerentemente con le norme locali in materia di salute & sicurezza professionali, i produttori sono tenuti a
salvaguardare i tecnici di manutenzione, e inoltre gli utenti. Per far fronte a tali obblighi, i prodotti devono
presentare una targhetta, chiaramente visibile al personale di manutenzione che accede all'apparecchiatura
nel complesso e che risulti inoltre leggibile e avverta gli addetti del rischio che le superfici di questi prodotti
possono scottare e non vanno toccate con i prodotti in funzione.
L'unità può essere installata in qualunque orientamento, ma non in posizione capovolta o in posizione
verticale con il flusso dell'aria rivolto verso il basso.
Le griglie di ventilazione su questi prodotti non devono essere ostruite. Verificare che vi sia una distanza
minima di 50 mm fra le griglie di ventilazione e qualsiasi eventuale ostruzione.
Il coperchio/telaio dell'unità è realizzato per proteggere il personale esperto dai pericoli. Non deve essere
usato come parte degli involucri esterni di qualsiasi apparecchiatura, se risulta accessibile da parte degli
addetti, poiché è possibile che in condizioni di pieno carico una o più parti del telaio dell'unità
giunga/giungano a temperature superiori ai limiti considerati sicuri per l'accesso da parte degli addetti.
0M7 AND 087 HANDBOOK TDK-Lambda
A
Page 9 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
ESPAÑOL
Instrucciones generales de seguridad:
LEA LAS INSTRUCCIONES DE SEGURIDAD
Servicio:
Estos productos no pueden ser reparados por los clientes. TDK-Lambda UK LTD. y sus agentes autorizados
son los únicos que pueden llevar a cabo las reparaciones.
Componentes fundamentales:
Estos productos no pueden ser utilizados como componentes fundamentales en sistemas de control nuclear,
sistemas de soporte vital o equipos a utilizar en entornos peligrosos sin el consentimiento expreso por escrito
del Director General de TDK-Lambda EMEA.
Uso de los productos:
Estos productos han sido diseñados para ser utilizados en un equipo central que restrinja el acceso al
personal cualificado autorizado.
Este producto es una fuente de alimentación y sólo puede ser instalado por personal cualificado dentro de
otros equipos y no debe ser tratado como un producto independiente. Este producto debe ser vendido entre
empresas profesionales y solo puede obtenerse a través de los canales de distribución .No está destinado
para la venta a usuarios finales
Este producto es una fuente de alimentación y no se ve afectada por la directiva EMC . El cumplimiento de la
directiva EMC se debe considerar en la instalación final . Por favor, póngase en contacto con su oficina local
de TDK - Lambda
Medioambiental:
Estos productos son IPX0 y, por tanto, no pueden utilizarse sustancias químicas/disolventes, agentes de
limpieza ni otros líquidos.
Medio ambiente:
Esta fuente de alimentación es una fuente de alimentación de modo conmutado a utilizar en aplicaciones
dentro de un entorno con un Grado de contaminación 2 y una Categoría de sobretensión II. En él se utilizan
policloruros de bifenilo del Grupo de materiales IIIb.
Carga de salida:
La potencia de salida tomada de la fuente de alimentación no puede sobrepasar el valor nominal indicado en
la etiqueta de la fuente de alimentación, excepto en los casos indicados en las limitaciones del producto en
este manual.
Parámetros de entrada:
Este producto debe ser utilizado dentro de los parámetros de entrada indicados en las limitaciones del
producto en este manual.
Desecho de la unidad:
La unidad contiene componentes que deben ser desechados de una manera especial. Asegúrese de
desechar correctamente la unidad al final de su vida útil y conforme a las normas locales vigentes.
PELIGRO DE DESCARGAS ELÉCTRICAS
Advertencia de alta tensión:
En esta fuente de alimentación hay tensiones peligrosas. El instalador profesional debe proteger al personal
de servicio contra cualquier contacto accidental con estas tensiones peligrosas en el equipo final.
0M7 AND 087 HANDBOOK
TDK-Lambda
Page 10 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
ADVERTENCIA: La instalación de este producto en un equipo de clase I la deben llevar a cabo profesionales
y el producto debe estar conectado a tierra.
La salida o salidas (+) o (-) pueden conectarse a tierra o se las puede dejar flotando.
Debe impedirse el acceso de los usuarios a la cubierta o cubiertas y al chasis de la unidad.
PRECAUCIÓN: PROTECCIÓN POR FUSIBLES BIPOLAR/NEUTRA (Opción D)
El conector de entrada de la red no es apto para ser utilizado a modo de bornes de cableado de campo.
No utilice tornillos de montaje susceptibles de penetrar en la unidad más de 4.5 mm.
Con estos productos se utilizan unos tornillos de puesta a tierra especiales que conectan la cubierta al
chasis. No se deben quitar en ningún caso. En caso de quitarlos por error, hay que reemplazarlos por unos
nuevos y comprobar la conexión a tierra del producto.
Un fusible interno protege la unidad y este no debe ser nunca reemplazado por el usuario. En caso de existir
algún defecto interno, la unidad debe ser enviada a TDK-Lambda UK LTD o a uno de sus agentes
autorizados.
El equipo de uso final debe constituir un recinto de protección mecánica, eléctrica y contra incendios de
protección mecánica, contra descargas eléctricas y contra el peligro de incendios.
Peligros de energía:
Algunos módulos pueden generar energía peligrosa (240VA) dependiendo de la configuración de la tensión
de salida. Los fabricantes de equipos finales deben proteger al personal de servicio contra un contacto
accidental con estos bornes de salida de los módulos. Si se configura de modo que pueda generarse energía
peligrosa, hay que evitar que el usuario pueda acceder a los bornes o conexiones del módulo.
SUPERFICIE CALIENTE
Superficies externas calientes:
Según las normas locales relativas a la Salud y Seguridad en el trabajo, los fabricantes están obligados a
proteger a los ingenieros de servicio además de a los usuarios. Para que esto se cumpla, debe colocarse
una etiqueta en estos productos que pueda ser vista claramente por el personal de servicio que accede al
equipo general, y con advertencias legibles de que las superficies de estos productos pueden estar calientes
y no deben tocarse cuando los productos se encuentran en funcionamiento.
La unidad se puede montar en cualquier orientación excepto invertida (montada sobre su parte de arriba) o
vertical con los orificios para el flujo de aire mirando hacia abajo.
Las aberturas de ventilación de estos productos no deben obstruirse jamás. Asegúrese de que quede una
separación de 50 mm por lo menos entre cualquier obstrucción y las aberturas de ventilación.
La cubierta/chasis de la unidad ha sido diseñada para que proteja a las personas cualificadas de los peligros.
No deben ser utilizadas como parte de las cubiertas externas de cualquier equipo al que pueden acceder los
operarios, ya que bajo unas condiciones de carga completa, la pieza o piezas del chasis de la unidad pueden
alcanzar temperaturas superiores a las consideradas seguras para el acceso de los operarios.
0M7 AND 087 HANDBOOK TDK-Lambda
A
Page 11 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
PORTUGUÊS
Instruções gerais de segurança:
LEIA AS INSTRUÇÕES DE SEGURANÇA
Manutenção:
Estes produtos não são podem ser submetidos a manutenção por parte do cliente. Apenas a TDK-Lambda
UK LTD e os seus agentes autorizados têm permissão para realizar reparações.
Componentes essenciais:
Não é autorizada a utilização destes produtos como componentes essenciais de sistemas de controlo
nuclear, sistemas de suporte de vida ou equipamento para utilização em ambientes perigosos sem a
expressa autorização por escrito do Director-Geral da TDK-Lambda EMEA.
Utilização do produto:
Estes produtos foram concebidos para utilização dentro de um equipamento de alojamento que apenas
permita o acesso a pessoal qualificado autorizado.
Este produto é uma alimentaçao considerado com um componente para ser instalado por pessoas
qualificadas, em outros equipamentos. Não deve ser usado como um produto acabado.
Este produto é destinado para venda entre as empresas e pode ser obtido através de canais de distribuição.
Não se destina à venda aos particulares
Este produto é uma alimentaçao considerado com um componente, não é dentro do appliquation âmbito da
directiva CEM.
Conformidade com a directiva CEM devem ser considerados na instalação final.
Entre em contacto com seu escritório TDK-Lambda mais próximo.
Ambiental:
Estes produtos são IPX0 e, como tal, não se devem utilizar químicos/solventes, agentes de limpeza e outros
líquidos.
Ambiente:
Esta fonte de alimentação é uma fonte de alimentação do modo de comutação para utilização em aplicações
com um Nível de Poluição 2 e ambientes da categoria de sobretensão II. São utilizadas placas de circuitos
impressos do grupo de materiais IIIb.
Carga de saída:
A potência de saída extraída da fonte de alimentação não deve exceder a classificação assinalada na
etiqueta da fonte de alimentação, excepto quando indicado nas limitações do produto neste guia.
Parâmetros de entrada:
Este produto deve ser utilizado dentro dos parâmetros de entrada indicados nas limitações do produto neste
guia.
Eliminação no fim de vida:
A unidade contém componentes que necessitam de procedimentos especiais de eliminação. Certifique-se de
que a unidade é devidamente eliminada no fim da sua vida útil e que tal é feito em conformidade com os
regulamentos locais.
RISCO DE CHOQUE ELÉCTRICO
Aviso de alta tensão:
Estão presentes tensões perigosas dentro da fonte de alimentação. O profissional que realizar a instalação
deve proteger o pessoal de assistência contra contactos inadvertidos com estas tensões perigosas do
equipamento final.
0M7 AND 087 HANDBOOK
TDK-Lambda
Page 12 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
AVISO: Quando instalado num equipamento de Classe I, este produto deve ser ligado à terra de forma fiável
e instalado por um profissional.
As saídas (+) e (-) podem ser ligadas à terra ou deixadas soltas.
O chassis/cobertura(s) da unidade não deve estar acessível ao utilizador.
CUIDADO: LIGAÇÃO DE FUSÍVEIS DE DOIS PÓLOS/NEUTRA (Opção D)
O conector de entrada de alimentação não deve ser utilizado como terminal de cablagens no local.
Não utilize parafusos de montagem, uma vez que estes penetrarão na unidade em mais do que 4.5mm.
Nestes produtos utilizam-se parafusos especiais de ligação à terra, que ligam a cobertura ao chassis. Não
devem ser removidos. Se forem removidos por engano, deverão ser substituídos por parafusos novos,
devendo-se testar a ligação à terra do produto.
Existe um fusível interno que protege a unidade e que não deve ser substituído pelo utilizador. Em caso de
defeito interno, a unidade deve ser devolvida à TDK-Lambda UK LTD ou a um dos seus agentes autorizados.
O equipamento de utilização final deve fornecer um bastidor com protecção mecânica, eléctrica e contra
incêndios adequada.
Perigos de energia:
Alguns módulos tem a capacidade de fornecer energia perigosa (240 VA), de acordo com a configuração da
tensão de saída. O equipamento final do fabricante deve garantir que o pessoal de assistência está protegido
contra contactos inadvertidos com estes terminais de saída do módulo. Se essa energia perigosa for
produzida, as ligações e os terminais do módulo não devem ser acessíveis pelos utilizadores.
SUPERFÍCIE QUENTE
Superfícies quentes externas:
Segundo com os regulamentos locais sobre saúde e segurança no local de trabalho, os fabricantes têm a
obrigação de proteger os técnicos de manutenção, bem como os utilizadores. De forma a respeitar este
regulamento, estes produtos deverão ter uma etiqueta que seja facilmente visível ao pessoal de assistência
que aceda ao equipamento em geral, e que alerte, de forma legível, para o facto de as superfícies destes
produtos poderem estar quentes, não devendo ser tocadas quando os produtos estão em funcionamento.
A unidade pode ser instalada em qualquer posição, excepto invertida (montada sobre a parte superior), ou na
posição vertical, com o fluxo de ar dirigindo-se para baixo.
As aberturas de ventilação destes produtos não devem ser obstruídas. Certifique-se de que existe um
espaçamento de pelo menos 50 mm entre qualquer obstrução e as aberturas de ventilação.
O chassis/cobertura da unidade está concebido de forma a proteger o pessoal especializado de perigos. Não
devem ser utilizados como parte das coberturas externas de qualquer equipamento em que possam estar
acessíveis aos operadores, uma vez que em condições de carga máxima, algumas peças do chassis da
unidade podem atingir temperaturas superiores às consideradas seguras para o acesso do operador.
0M7 AND 087 HANDBOOK
TDK-Lambda
Page 13 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Special Instructions for medical applications
IEC/EN 60601-1 2nd Edition
UL 60601-1 1st Edition
CSA-C22.2 No. 601.1-M90
IEC/EN 60601-1 3rd Edition
ANSI/AAMI ES 60601-1
CSA C22.2 No 60601-1
These products are designed for continuous operation within an overall enclosure, and must be mounted
such that access to the mains terminals is restricted.
These products are NOT suitable for use in the presence of flammable anaesthetic mixtures with air or with
oxygen, or with nitrous oxide.
For IEC60601-1, EN60601-1 and UL/CSA 60601-1 (Second Edition standards), the QM and QS range
provide Reinforced insulation between input and outputs, and Basic insulation between Input and Earth and
from outputs to earth.
For IEC 60601-1, EN 60601-1, ANSI/AAMI ES 60601-1, CSA 22.2 No 60601-1 (Third Edition standards) the
QM and QS range provide reinforced insulation between input and outputs (2 MOPPs) and Basic insulation (1
MOPP) between Input and Earth and from Output to Earth.
These products are classed as ordinary equipment and are not protected against the ingress of water (IPX0).
Reference should be made to local regulations concerning the disposal of these products at the end of their
useful life.
Where any part of this product is made accessible to the operator in the end use equipment, the operator
must not touch this part and the patient at the same time.
WARNING: No modification of this product is allowed.
Special instructions:
Whilst all individual outputs are classed as SELV outputs in accordance with the standard
IEC/EN/UL/CSA60950-1 (<60Vdc or 42.4V peak), seriesed combinations of these outputs may exceed these
values and become Non-SELV output voltages.
In addition, for IEC/EN/UL/CSA 60601-1 approved products. Series connected outputs with an output voltage
between 60Vdc and up to 160Vdc may increase the working voltages across safety barriers. This may reduce
one level of protection (1 MOPP) between primary and secondary circuits.
For IEC/EN/UL/CSA 60950-1 approved products, safety barriers are maintained with series connected
outputs up to 160Vdc.
0M7 AND 087 HANDBOOK TDK-Lambda
Page 14 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Environmental Specifications:
Description
Operation
Storage
Use
Indoor
-
Temperature
0°C - +70°C (derating at 2.5%/°C above 50°C)
-40°C - +70°C
Humidity
5 - 95% RH, non-condensing
5 - 95% RH, non-condensing
Altitude
-200m - 5000m
-200m - 5000m
Pressure
54kPa - 106kPa
54kPa - 106kPa
Orientation
Horizontal with chassis lowest, on either side or
vertical with the input lowest
ALL
Material Group
IIIb
Pollution Degree
2
Overvoltage Category
II
Class
I
Weight
3.2Kg Max
IP Rating
IPX0
Level of Insulation:
Dielectric Strength testing is carried out as follows:
Primary mains circuit to earth: 2.774kVdc
*Primary mains circuits to secondary: 6.782kVDC.
Secondary circuits to earth: 2.121kVdc
*Important Note: This test is not possible with Y capacitors fitted to the unit as damage to these capacitors
may occur.
Safety Approvals:
UL60950-1 and CSA22.2 No.60950-1 - UL Recognised. C-UL for Canada.
IEC / EN60950-1 - CE mark.
IEC/EN60950-1 and/or IEC/EN60601-1 - CB Report and Certificate.
CE marking when applied to any QM and QS product indicates compliance with the Low Voltage Directive in
that it complies with EN60950-1 and with ROHS Directive.
UL/CSA 60601-1 - UL + C -UL approval
Fusing: Internal fuses (F1): Dual fuses in the L and N line or single fuse in the live line, F25AH, 250V,
6.35x32mm.
Symbols:
AC EARTH N – Neutral L – Live
If the earth terminal of the QM or QS PSU is connected to the main incoming earth conductor of the end
equipment, the installer must cover the earth symbol with a label bearing the earth symbol of IEC60417-5019.
N
L
Page 15 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Nomenclature:
QM models as described below:
Unit Configuration Code:
QMshabcdefghklm for modular configurations
Where:
s
=
7 for QM7 models
h
=
Hold Up Option:
Blank for none fitted
H for Extended Hold Up
a
=
Cooling:
C for Customer air
F for Variable speed, forward air fan.
R for Variable speed, reverse air fan
b
=
Input connector:
S for screw
F for faston
c
=
Input fuse:
D for dual AC fuses
E for single AC fuse in the live line
d
=
Leakage option:
S for 3.5mA (60950-1 only)
L for 300 µA
R for 150 µA
T for 60 µA
e
=
Primary option:
Blank for none fitted
E for global enable
T for global inhibit
P for PMBus
Q for PMBus with individual module enable (KQM700HJx model only, where x can be any letter
for non-safety related differences)
f
=
Standby supply:
Blank for none fitted
5 for 5V/2A (Primary option Q or P only)
5H for 5V/2A (Primary option E or T only)
5L for 5V/0.25A (Primary option E or T only)
12 for 12V/1A (Primary option Q or P only)
12H for 12V/1A (Primary option E or T only)
g
=
Blank if Primary option P or Q not fitted
H for Input Power Present
C for Control Pin Active High
D for Control Pin Active Low
F for PMBus™ and Control Pin Active High
G for PMBus™ and Control Pin Active Low
J for Individual output control, followed by two hexadecimal numbers specifying which modules
are on/off (for ‘Q’ type PMBus option only)
h
=
Blank or C for Industrial leakage, output Y capacitors up to 100nF (Leakage option S only)
May be followed by:
TDK-Lambda
Page 16 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Single output modules
vMcde
Where:
v
=
Output voltage
M
=
Module name: SB or SC
c
=
S for screw terminal output, F for faston
d
=
N for no signals, omit for standard signals
e
=
‘C’ for Industrial Leakage, omit for standard leakage (60950 only)
Optionally followed by ‘Dxxx’ where xxx is the number of mV of droop. Droop option available by Non-
Standard request only.
Dual output modules
v1/v2DHcde
Where:
v1
=
CH1 output voltage
v2
=
CH2 output voltage
DH
=
Module name: DH
c
=
S for screw terminal output, F for faston
d
=
N for no signals, omit for standard signals
e
=
‘C’ for Industrial Leakage, omit for standard leakage (60950 only)
v1/v2DMcde
Where:
v1
=
CH1 output voltage
v2
=
CH2 output voltage
DM
=
Module name: DM
c
=
S for screw terminal output, F for faston
d
=
N for no signals, omit for standard signals
e
=
‘C’ for Industrial Leakage, omit for standard leakage (60950 only)
Blanking plates
B/S
Where:
B/S
=
Blanking plate
Parallel combinations
vZxcde
Where:
v
=
Output voltage
Z
=
Paralleled output module comprising SB or SC modules
x
=
Number of slots. (See Parallel and Series combinations Table below)
c
=
S for screw terminal output, F for faston
d
=
N for no signals, omit for standard signals
e
=
‘C’ for Industrial Leakage, omit for standard leakage (60950 only)
TDK-Lambda
Page 17 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Series combinations
vYxcde
Where:
v
=
Output voltage
Y
=
Series output module comprising SB, SC or DH modules
x
=
Number of slots. (See Parallel and Series combinations Table below)
c
=
S for screw terminal output, F for faston
d
=
N for no signals, omit for standard signals
e
=
‘C’ for Industrial Leakage, omit for standard leakage (60950 only)
Series connected parallel modules
vHxcde
Where:
v
=
Output voltage
H
=
Series connected parallel SB or SC modules
x
=
Number of slots. (See Parallel and Series combinations Table below)
c
=
S for screw terminal output, F for faston
d
=
N for no signals, omit for standard signals
e
=
‘C’ for Industrial Leakage, omit for standard leakage (60950 only)
Combined DM modules – Sereies channel 1 only.
vMxcde
Where:
v
=
Output voltage
M
=
Series Channel 1 output comprising DM modules.
x
=
Number of slots. (See Parallel and Series combinations Table below)
c
=
S for screw terminal output, F for faston
d
=
N for no signals, omit for standard signals
e
=
‘C’ for Industrial Leakage, omit for standard leakage (60950 only)
klm
Where
klm
=
Blank for standard output settings, may be three numbers
from 0 to 9 (Preceded by - ) which denotes various output
voltage/current settings within the specified ranges of each
output for a particular unit. (May define non-safety related
parameters/features, e.g reduced primary current limit,
reduced OVP)
0M7 AND 087 HANDBOOK
TDK-Lambda
Page 18 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
QS models as described below:
Unit Configuration Code:
QS[Number of available slots][Hold Up Option]-[Power]-[Voltage][Output Terminal][Standby/Signals][Unit
Options]-[non safety related]
Number of available slots = 7
Hold Up Option = Blank for none fitted, H for Extended Hold Up
Power (max) = 1080 or 1200 from QS Output Parameters table below
Voltage = Output Voltage from the Vout range in the QS Output Parameters
table below
Output Terminal = Blank for Screw terminal, F for Faston terminal
Standby/Signals = Blank or –E5H, -E5L, -T5H, -T5L, -E12H, -T12H, -P5H or
-P12H
Where: E = Enable, T = Inhibit and P = PMBus
5H is 5V/2A, 5L is 5V/0.25A and 12H is 12V/1A
Followed by: (P option only)
H for Input Power Present
C for Control Pin Active High
D for Control Pin Active Low
F for PMBus™ and Control Pin Active High
G for PMBus™ and Control Pin Active Low
Unit Options = Blank for defaults or all of -[cooling][input connector][input fuse][leakage option]
Where [cooling] = F for Variable speed, forward air fan (default), R for Variable speed, reverse air fan
[Input Connector] = S for screw (default), F for Faston
[Input Fuse] = D for dual AC fuses (default), E for single AC fuse in the live line
[Leakage Option] = S for 3.5mA (60950 Only), L for 300 µA (default), R for 150 µA, T for 60 µA
[Non-safety related] = optional ‘-‘ followed by any number of characters indicating non-safety related model
differences.
QS Output Parameters
Model Note Power Vout Current Hazardous Modules used
(max) (range) (max) Energy
QS7 - 1080 12-12.8V 90A Yes 1 x ZF Module
- - 1200 24-26.4V 50A Yes 1 x YF Module
- - 1200 48-52.8V 25A Yes 1 x YF Module
- - 1200 96-105.6V 12.5A Yes 1 x YF Module
0M7 AND 087 HANDBOOK
TDK-Lambda
Page 19 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Parallel and Series combinations Table
Series connection number of slots
Qty of modules
SB
SC
DH
Name
Slots
Name
Slots
Name
Slots
1
SB
1
SC
2
YB
1
2
YC
2
YF
4
YP
2
3
YD
3
YM
6
YQ
3
4
YG
4
-
-
YR
4
5
YH
5
-
-
YS
5
6
YJ
6
-
-
YT
6
7
YK
7
-
-
YV
7
Limitations of use:
1. Output voltage is the combined seriated modules voltage.
2. Module limitations apply to seriated modules.
Parallel connection number of slots
Number of modules in parallel
Slots
SB
SC
Name
2
2
0
ZC
3
1
1
ZD
4
0
2
ZF
6
0
3
ZH
3
3
0
ZT
4
4
0
ZV
See ratings in Module output ratings table below
Series connection of parallel connected modules
Module
Qty
Slots
Name
ZC
2
4
HC
ZD
2
6
HD
ZF
2
8
HF
ZT
2
6
HT
ZC
3
6
HW
Limitations of use:
1. Output voltage is the combined seriated modules voltage.
2. Module limitations apply to seriated/parallel modules.
0M7 AND 087 HANDBOOK
TDK-Lambda
Page 20 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
DH outputs in series but split to create extra outputs.
Qty of modules
Split after output x (first output is 1)
Name
2
1
CB
2
3
CD
3
1
FB
3
3
FD
3
5
FG
4
1
GB
4
3
GD
4
5
GG
4
7
GJ
5
1
JB
5
3
JD
5
5
JG
5
7
JJ
5
9
JL
6
1
KB
6
3
KD
6
5
KG
6
7
KJ
6
9
KL
6
11
KN
7
1
LB
7
3
LD
7
5
LG
7
7
LJ
7
9
LL
7
11
LN
7
13
LQ
0M7 AND 087 HANDBOOK
TDK-Lambda
Page 21 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Combined DM modules – seriesed Channel 1 only.
Number of
Nomenclature
Modules
Outputs
2
3
v1/v2/v3MC
3
4
v1/v2/v3/v4MD
4
5
v1/v2/v3/v4/v5MF
5
6
v1/v2/v3/v4/v5/v6MG
6
7
v1/v2/v3/v4/v5/v6/v7MH
7
8
v1/v2/v3/v4/v5/v6/v7/v8MJ
Input Parameters:
Input parameters
Standard
60601-1
60950-1
Nominal input voltage
100-240Vac
100-240Vac
Input voltage range
90-264Vac
(150-264Vac)*
90-264Vac
(150-264Vac)*
Input frequency range
47-63
47-440Hz
Maximum input current
19Arms
19Arms
*Input for 1500W models
Input Connections:
3 way Terminal block: 8.25mm spacing between screw head centres. M3 screws, 0.5Nm torque, 20A/300V
MAX.
Faston: 6.3 x 0.8mm, Tin plated brass, rated 22A.
0M7 AND 057 HANDBOOK
TDK-Lambda
Page 22 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
QM7 Output Parameters:
Module output ratings table.
Module
Note
Slots
Output
Channel
Vout Nom
(V)
Adjustment
range
Output
current
(A)
Output
power
(W)
Hazardous
energy
DM
5,8
1
CH1
12
11.9 to 16.1
10
120
Yes
DM
2
1
CH1
17
16 to 21.6
7.5
120
Yes
DM
4,5
1
CH1
24
20.8 to 28.2
5
120
Yes
DM
-
1
CH2
3.3
2.8 to 3.8
10
33
No
DM
-
1
CH2
5
4.25 to 5.75
10
50
No
DM
-
1
CH2
8
7 to 9.5
10
95
No
DM
3,8
1
CH2
14
11.9 to 16.1
8.3
100
No
DM
3
1
CH2
24
23.5 to 24.5
4.16
100
No
DH
1
1
CH1
12
10.2 to 13.8
10
120
Yes
DH
1
1
CH1
15
12.75 to 17.25
8
120
Yes
DH
1
1
CH1
24
20.4 to 27.6
5
120
Yes
DH
1
1
CH1
27
23 to 31
4.4
120
Yes
DH
2
1
CH2
12
10.2 to 13.8
10
120
Yes
DH
2
1
CH2
15
12.75 to 17.25
8
120
Yes
DH
2
1
CH2
24
20.4 to 27.6
5
120
Yes
DH
2
1
CH2
27
23 to 31
4.4
120
Yes
SB
-
1
CH1
3.3
3.3 to 3.63
37
122
No
SB
7
1
CH1
3.4
3.2 to 3.6
37
126
No
SB
-
1
CH1
5
5 to 5.5
30
150
No
SB
-
1
CH1
8.1
8 to 8.8
25
200
Yes
SB
-
1
CH1
12
12 to 13.2
25
300
Yes
SB
-
1
CH1
15
15 to 16.5
20
300
Yes
SB
-
1
CH1
18
18 to 19.8
16.7
300
Yes
SB
-
1
CH1
20
20 to 22
15
300
Yes
SB
-
1
CH1
48
48 to 52.8
6.25
300
Yes
SB
-
1
CH1
24
24 to 26.4
12.5
300
Yes
SB
-
1
CH1
28
28 to 30.8
10.7
300
Yes
SC
6
2
CH1
5
5 to 5.5
60
300
Yes
SC
-
2
CH1
12
12 to 13.2
50
600
Yes
SC
-
2
CH1
17
17 to 18.7
35.29
600
Yes
SC
-
2
CH1
24
24 to 26.4
25
600
Yes
SC
-
2
CH1
30
30 to 33
20
600
Yes
SC
-
2
CH1
48
48 to 52.8
12.5
600
Yes
ZC
-
2
CH1
15
15 to 16
36
540
Yes
ZC
-
2
CH1
18
18 to 19.2
30
540
Yes
ZC
-
2
CH1
28
28 to 30
19.3
540
Yes
ZD
-
3
CH1
5
5 to 5.3
80
400
Yes
ZD
-
3
CH1
12
12 to 12.8
65
780
Yes
ZD
-
3
CH1
24
24 to 25.6
30
720
Yes
ZD
-
3
CH1
48
48 to 51.2
15
720
Yes
ZF
6
4
CH1
5
5 to 5.3
110
550
Yes
ZF
-
4
CH1
12
12 to 12.8
90
1080
Yes
ZF
9
4
CH1
17
17 to 18.19
63.5
1080
Yes
ZH
10
6
CH1
24
24 to 25.6
62.4
1200
Yes
ZT
-
3
CH1
15
15 to 16
50
750
Yes
ZV
-
4
CH1
15
15 to 16
66.4
996
Yes
Note 1: CH1 limited to 80W when CH2 at 120W. Maximum of 200W across module.
Note 2: CH2 Limited to 80W when CH1 at 120W. Maximum of 200W across module.
Note 3: CH2 has a maximum of 100W. Maximum of 200W across the module.
Note 4: CH1 (24V) has a reduced adjustment range when CH2 is 24V. Reduced adjustment range is 21.6V
to 28.8V.
0M7 AND 087 HANDBOOK
TDK-Lambda
Page 23 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Note 5: CH1 limited to 100W when CH2 at 100W. Maximum of 200W across module. Achievable if the
ambient temperature is reduced to 40°C.
Note 6: Please see Further De-ratings Table below
Note 7: KQM5001V-x model only
Note 8: 12/12DM Module limited to 180W in slot 2 or 45°C ambient. (QM8 only)
Note 9: 67A for 10 seconds
Note 10: 1500W at high-line
Cooling options QM7
Cooling option
Input voltage
(Vnom)
Output power
(W)
Ambient
°C
F (Forward air, variable speed)
100-240
166.7-240
1200
1500
50
50
C (Customer air)
100-240
166.7-240
1200
1500
50
50
R (Reverse air, variable speed
fan)
100-240
1200
40
Output Limitations:
Adjusting output voltage beyond the stated range may cause overvoltage protection (OVP) to operate,
whereby the output will latch off. To reset for normal operation simply adjust the potentiometer to reduce the
output voltage to within its range and cycle the input off then on.
For SB and SC modules, all outputs are SELV except under the following circumstance: Outputs connected in
series are non-SELV if the total output voltage + 35% of the nominal rated output voltage of the output with
the highest rated adjustment range voltage exceeds 60Vdc (the 35% addition allows for a single fault in any
one individual channel).
For DH modules, all outputs are SELV except under the following circumstance: Outputs connected in series
are non-SELV if the total output voltage + 35% of each rated nominal output voltage of the highest rated
adjustment range voltage exceeds 60Vdc (the 35% addition allows for a single fault in any one individual
channel).
If the total voltage of outputs connected in series exceeds the 60Vdc SELV limit then all outputs must be
considered non-SELV.
Non-SELV outputs are hazardous and must not be made user accessible. Consideration must be given to
service engineers making inadvertent contact with the output terminals in the end equipment.
Cooling for unit
Component temperatures, for customer air cooled models, must be monitored in the end use application as
described in the “Cooling for Unit Temperature Table” below.
The following method must be used for determining the safe operation of PSUs.
The components listed in the following table must not exceed the temperatures given. To determine the
component temperatures the heating tests must be conducted in accordance with the requirements of the
standard in question. Consideration should also be given to the requirements of other safety standards.
Test requirements include: PSU to be fitted in its end-use equipment and operated under the most adverse
conditions permitted in the end-use equipment handbook/specification and which will result in the highest
temperatures in the PSU. To determine the most adverse conditions consideration should be given to the end
use equipment maximum operating ambient, the PSU loading and input voltage, ventilation, end use
equipment orientation, the position of doors & covers, etc. Temperatures should be monitored using type K
fine wire thermocouples (secured with cyanoacrylate adhesive or similar) placed on the hottest part of the
component (out of any direct airflow) and the equipment should be run until all temperatures have stabilised.
0M7 AND 087 HANDBOOK TDK-Lambda
Page 24 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Cooling for Unit Temperature Table:
Higher temperature limits (in brackets) may be used but product life may be reduced.
Circuit Ref.
Description
Max. Temperature (°C)
PFC
-
-
QM7
-
-
L2
Common Mode Choke
115 (140)
L3
Boost choke
125
C2
Electrolytic Capacitors
71 (105)
C10
Electrolytic Capacitors
64 (105)
C7
Electrolytic Capacitors
64 (105)
C8
Electrolytic Capacitors
73 (105)
C11
Electrolytic Capacitors
77 (105)
C3, C14,
X Capacitor
100
C12
Y Capacitors
105
TX1
Fly back Transformer
120
D1
Diode bridge
114 (130)
D3
PFC diode
130
U4
Opto-coupler
100
U3
Voltage regulator
120 (130)
Q2
Boost FETS
130
Low Power Options
-
-
U6
Opto-couplers
100
High Power Options
-
-
C6
Electrolytic Capacitors
73 (105)
XU3
Opto-couplers
100
TX1
Transformer Class F
130
‘Q’ PMbus
XU3
Opto-couplers
100
DM/DH Modules
-
-
C206
Y Capacitors
105
C207
Electrolytic Capacitors
84 (105)
U8
Opto-couplers
100
Q1
Primary FET
120 (130)
D201
Output diode
124 (130)
TX1
Transformer Class B
110
SC module Modules
-
-
C206
Electrolytic Capacitors
83 (105)
C209
Y Capacitors
105
U1
Opto-couplers
100
TX1
Transformer Class B
110
TX1 (12V)
Transformer Class F
130
Q1
Primary FET
127 (130)
Q203
Secondary FET
130
SB module Modules
-
-
C206
Electrolytic Capacitors
83 (105)
C209
Y Capacitors
105
U1
Opto-couplers
100
TX1
Transformer Class B
110
Q1
Primary FET
127 (130)
Q203
Secondary FET
130
0M7 AND 087 HANDBOOK
TDK-Lambda
Page 25 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Output Connections:
Module/Option
Connector
Housing
Crimp pin
Output
screw size
and torque
Fast-on terminals
Global Option.
J1 Option connector
(Molex)
51110-1060
(Molex)
50394-8051
-
-
PMbus
J5 Option connector
(Molex)
51110-1260
(Molex)
50394-8051
-
-
DM module
J206 Option connector
(Molex)
51110-1260
(Molex)
50394-8051
-
-
DM module
J202, J203, J204, J205
Power connectors
-
-
M3
0.5 – 0.6Nm
Four 6.35mm
fast-ons. Each rated
18 Amps
DH module
J206 Option connector
(Molex)
51110-1060
(Molex)
50394-8051
-
-
DH module
J202, J203, J204, J205
Power connectors
-
-
M3
0.5 – 0.6Nm
Four 6.35mm
fast-ons. Each rated
18 Amps
SB module
J204 Option connector
(Molex)
51110-1060
(Molex)
50394-8051
-
-
SB module
J202, J203
Power connectors
-
-
M5
2.4 -2.6Nm
Four 9.5mm fast-ons.
Each rated 32 Amps
SC module
J204 Option connector
(Molex)
51110-1060
(Molex)
50394-8051
-
-
SC module
J202, J203
Power connectors
-
-
M5
2.4 -2.6Nm
Four 9.5mm fast-ons.
Each rated 32Amps
0M7 AND 087 HANDBOOK TDK-Lambda
270 MAX (INCLUDVNG ENDCAP}
2: go : 175.00 :
:n H Elfi m: w
__—_—_—7_ V X
< 1="" e="" ‘="" ‘="" m="" \="" 1="" m="" f—'—'—'—'er9\="" "="" ‘="" an}:="" 'x="" l‘="" va="" off="" side="" hx‘ngs="" are="" secondary="" flx‘ngs="" and="" should="" be="" used="" in="" conjunction="" with="" other="" f‘xings="" supports="" 21="" 20="" 2c5="" 00="" 1:,="" ‘l="" a="" 9="" '="" '="" '="" ‘="" ‘="" 9="" a:="" 0‘="" m="" g="" in“:="" w="" ’:="" a="" ‘="" e="" ,="" c="" g="" i;="" ‘="" .="" u="" g="" d="" a:="" \u="" e="" ‘="" %="" .="" rm="" %="" i="" eiifiiiiiiiiio="" i="" '31]="" %="" customer="" fixings‘="" 8="" holes="" m4.="" max="" thread="" penefrafio="">
Page 26 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Mechanical Outline Drawings:
Customer fixing points
Maximum torque 1.1 to 1.3Nm
0M7 AND 087 HANDBOOK TDK-Lambda
T76 MAX
A
V
= a
= g
4-,alfl
TERMINAL COVER REMOVED
PRESS BOTH TABS THEN
LEVER FORWARD TO
REMOVE. REVERSE TO
RE-FIT
ACCESS TO SCREW ‘
TERMINALS
BY REMOVING COVER
Page 27 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
0M7 AND 087 HANDBOOK
TDK-Lambda
8. 8r
0 d
a
l I
139m
268 MA) :
. 7b MAX
173,09 21.30
:1 HF“ um i 1
i’*’*’*’* i? D
x z :
‘ ‘ m ,
\ 77777777 \ g g n
33:, WERE 7 ;
AOFFSIDEHX‘NGSARESECONDARYHX‘NGSANDSHOULE} L N J,— u
BE USED \N CONJUNCHON WHH OIHER HX‘NGS / SUPPORTS
205 00 _
Cus10mer Fixings.
8 holes M4.
Max thread penetrationz- 4.5mm
SCREW TERM‘NALS/
Page 28 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Customer air
Maximum torque 1.1 to 1.3Nm
0M7 AND 087 HANDBOOK
TDK-Lambda
SB MODULE
DH MODULE
DM MODULE
SC MODUL
C MODULE
STANDBY / SIGNALS
PMBU?GLOBAL
OPTION
I 2
I I I I 12
DETAIL C DETAIL L
GLOBAL OPTION
I. H PMBUSTM
Pin OUTPUTS OUTPUTS OUTPUTS
I NC STANDBY 2 + STANDBY 2 +
2 NC STANDBY 2 - STANDBY 2 -
3 STANDBY I + STANDBY I + N/C
4 STANDBY I - STANDBY I - FAN FAIL OUT
5 PSU ON/OFF + PSU ON/OFF + PMBUSTM ADDRESS 0
6 PSU ON/OFF — PSU ON/OFF — PMBUSTM ADDRESS I
7 AC FAIL OUT AC FAIL OUT PMBUSm ADDRESS 2
8 AC FAIL RTN AC FAIL RTN I‘i’MBUSTM ADDRESS 3
9 NC INPUT LOGIC~ 0 SCL — CLOCK
I0 NC INPUT LOGIC~ I SDA - DATA
I I N/A N/A F’MBUSTM CONTROL LINE IN
I2 N/A N/A GND
Page 29 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Option Pin Outs
0M7 AND 057 HANDBOOK
DM MODULE (1 SLOT, 2 OUTPUT)
CH1 +
E J
I C)
m CH1 0v
C)
12\E H
< ch1="" 3="" ::="" v="" adj="" z="" '="" '="" 8h2="" 2a="" @9="" 1="" adj="" e="" ch2="" +="" e="" —="" c)="" ch2="" ov="" pin="" output="" 1="" ch2="" sense="" +="" 2="" ch2="" sense="" —="" 3="" ch2="" inhibit="" anode="" 4="" ch2="" inhibit="" cathode="" 5="" ch2="" good="" collector="" 6="" ch2="" good="" emitter="" 7="" ch1="" good="" collector="" 8="" ch1="" good="" emitter="" 9="" module="" inhibit="" anode="" 10="" module="" inhibit="" cathode="" 11="" chi="" sense="" +="" 12="" ch1="" sense="" —="" tdk-lambda="">
Page 30 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Secondary Option Pin Out
TDK-Lambda
0M7 AND 087 HANDBOOK
DH MODULE I SLOT, 2 OUTPUT)
E h CHI +
: @ CHI 0v
Io\‘
‘ = v ADJ
Z I
2/ I
a: CH2 +
E 469
CH2 0v
PIN OUTPUT
I NC.
2 NC.
3 MODULE GOOD COLLECTOR
4 MODULE GOOD EMITTER
5 MODULE INHIBIT ANODE
6 MODULE INHIBIT CATHODE
7 NC.
8 NC.
9 NC.
10
N.C.
Page 31 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
0M7 AND 037 HANDBOOK TDK-Lambda
SB MODULE
(1 SLOT, 1 OUTPUT)
CHI +
Cl H
I
E3 3 CHI OV
V ADJ
OUTPUT
N.C.
N.C.
MODULE GOOD COLLECTOR
MODU LE GOOD EMITTER
MODULE INHIBIT ANODE
MODULE INHIBIT CATHODE
REMOTE SENSE +
REMOTE SENSE -
N.C.
_. 'U
Oomwomgwm—z
N.C.
Page 32 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
0M7 AND 037 HANDBOOK TDK-Lambda
W
(2 SLOT, 1 OUTPUT)
IE
1:1 nnn
O
I
III
IO\
ITII'IYAII
OUTPUT
N.C.
N.C.
MODULE GOOD COLLECTOR
MODULE GOOD EMITTER
MODULE INHIBIT ANODE
MODULE INHIBIT CATHODE
REMOTE SENSE +
REMOTE SENSE —
N.C.
N.C.
_. 'U
O‘OOOVOUW-Ikwwfiz
Page 33 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
0M7 AND 057 HANDBOOK TDK-Lambda
TDK-Lambda
www.uk.ldkrlambda.com
Page 34 of 34 260297-4 Apr 2018
QM7 AND QS7 HANDBOOK
Slot order
TDK-Lambda UK Ltd
Kingsley Avenue, Ilfracombe
Devon, EX34 8ES
Telephone - Sales and Service +44 (0)1271 856666
Head Office and Works +44 (0)1271 856600
Facsimile +44 (0)1271 864894
WEBSITE: www.uk.tdk-lambda.com