Texas Instruments 的 CC3220 Out-of-Box Appl Quick Start Guide 规格书
l TEXAS
INSTRUMENTS
1
SWRU470–February 2017
Submit Documentation Feedback Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
Quick Start Guide
SWRU470–February 2017
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
This quick start guide details the out-of-box experience for the CC3220 LaunchPad™ Development Kit
from Texas Instruments™.
The CC3220 device is part of the SimpleLink™ microcontroller (MCU) platform which consists of Wi-Fi®,
Bluetooth®low energy, Sub-1 GHz and host MCUs, which all share a common, easy-to-use development
environment with a single core software development kit (SDK) and rich tool set. A one-time integration of
the SimpleLink platform enables you to add any combination of the portfolio’s devices into your design,
allowing 100 percent code reuse when your design requirements change. For more information, visit
www.ti.com/simplelink.
Contents
1 Introduction ................................................................................................................... 2
2 Download and Installation .................................................................................................. 2
3 Building the Setup ........................................................................................................... 7
4 Getting Started With the Out-of-Box Demonstration .................................................................... 9
5 Troubleshooting ............................................................................................................ 18
6 Limitations and Known Issues............................................................................................ 20
Trademarks
LaunchPad, Texas Instruments, SimpleLink, SmartConfig are trademarks of Texas Instruments.
Bluetooth is a registered trademark of Bluetooth SIG, Inc.
iOS is a trademark of Cisco.
iOS is a trademark of Cisco Systems.
Android is a trademark of Google.
Wi-Fi is a registered trademark of Wi-Fi Alliance.
All other trademarks are the property of their respective owners.
l TEXAS
INSTRUMENTS
Introduction
www.ti.com
2SWRU470–February 2017
Submit Documentation Feedback
Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
1 Introduction
This quick start guide details the out-of-box (OOB) experience for the CC3220 LaunchPad Development
Kit from Texas Instruments.
The focus is on using the SimpleLink Wi-Fi Starter Pro application (available both on iOS™ and
Android™). It is also possible to run the demo using any browser. In the later method, web pages stored
on the serial flash are loaded on the browser and provide the same functionality as the mobile application
does. Working with the on-chip web pages is described in detail in the SimpleLink™ Wi-Fi® CC3220 Out-
of-Box Application Quick Start Guide.
The following features are highlighted:
• Easy connection to the CC3220 LaunchPad using SimpleLink Wi-Fi Starter Pro application. Users can
use AP provisioning or SmartConfig™ provisioning for fast connection. Once the device is provisioned
and connected to an access point in station mode, the profile is stored on the local file system so that
any reset to the CC3220 automatically makes it connect to the access point.
• Over-the-air update, demonstrating an update of a full image. OTA service enables in-system update
of the MCU application, CC3220 firmware releases (also known as Service Pack) made available by
Texas Instruments and other vendor files. Update procedure executed in a full system integrity fashion,
that is, failure in upgrading any of the image components would lead to rolling back to the previous
valid version.
• Easy access to the CC3220 device demonstrates configuring and reading onboard sensors.
This quick start guide is intended for basic level users who would like to experience the OOB image as is.
This quick start guide also assumes that the OOB is already programmed on the CC3220 LaunchPad. If
this is not the case, please see SimpleLink™ Wi-Fi® CC3220 Out-of-Box Application User's Guide. The
guide is structured chronologically starting from required downloads and installations, then building the
setup, and experiencing the demo.
2 Download and Installation
In an effort to make the out-of-box guide as self-contained as possible, all download and installation steps
are described in detail here.
2.1 UniFlash
The UniFlash utility lets the developer download the application image, service pack, and other files on the
serial flash of the CC3220 device. Follow these steps to install UniFlash.
1. Download UniFlash for CC3x20. If UniFlash is not available online, use the offline version (v4.x or
later).
2. Run the installer by double clicking on it.
3. Read and accept the license agreement to proceed.
4. Choose the desired path to place the package (otherwise the default is chosen).
5. Proceed with the installation, and click the Finish button when done.
l TEXAS
INSTRUMENTS
-ms-~ may WW. ..
k wm sunny") 0
s‘mpwemkwwm' mm
m
5mm
rm; ‘nswmms s‘mp‘mw
mm Svanev _ L
www.ti.com
Download and Installation
3
SWRU470–February 2017
Submit Documentation Feedback Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
2.2 SimpleLink™ Wi-Fi®Starter Pro Mobile Application
This application can be downloaded and installed through the application store. It is available on both
iOS™ and Android. Look for SimpleLink Wi-Fi Starter Pro (see Figure 1).
Figure 1. SimpleLink™ Wi-Fi Starter Pro
2.3 Serial Terminal
Many sample applications come with UART support for printing the debug information, or status of any
operation. Some applications require user input through the UART, so TI advises installing a serial
terminal application. Tera Term is used for demonstration here, but the Code Composer Terminal may
also be used. Follow these steps to instal Tera Term:
1. Download Tera Term, and install as per the instructions.
2. Run the Tera Term application.
l TEXAS
INSTRUMENTS
- Teva Term , [dwsnonnedsd] VT K
TCPIlP luyhugt example mm
may
mm
55 mm
other
uNsvtc v
a Serim Pon room: >anary Data Po J
’COMS XDSI In Class Auxmary Data Pan [coma]
0K
2mm VevaTsvmVT \mEW-I-
mg gm gm cw“ MN m
com
m m m
wmaw
Fm
Klyhnard
W m
puny
55>»
55>» Aulhznnanun
$3?» meavflwq
$9» mummy
ch/Iv
Germ-3‘
Addmmm 52““ng
SN: 5( up
Res are sum)
saw mum
ma key map
Download and Installation
www.ti.com
4SWRU470–February 2017
Submit Documentation Feedback
Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
3. Select the Serial Port shown as XDS110 Class Application/User UART (see Figure 2).
Be sure to install the XDS110 drivers for the PC to enumerate these ports for the serial terminal. Refer
to Section 2.4 for installation of the XDS110 drivers.
Figure 2. Tera Term New Connection Window
4. Go to Setup →Serial port (see Figure 3).
Figure 3. Tera Term Serial Port Tab
l TEXAS
INSTRUMENTS
Eon: com .
fiaud rate: 115200 .
Data: 3 hit
Parlly:
Etop:
flow control:
Transmit delay
(I mseclghar msedlme
ISemp
Sewn -x|)snu Mmdlivels
Welcome to m: xDsno Windows drivers Setup szald.
m m. ‘
www.ti.com
Download and Installation
5
SWRU470–February 2017
Submit Documentation Feedback Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
5. Configure the settings as per Figure 4.
Figure 4. Tera Term Serial Port Settings
2.4 XDS110 Driver Installation
XDS110 drivers must be installed before using the debugger or image creator. The drivers also enumerate
the serial terminal port, which can be used for printing the debug messages over the UART. The XDS
drivers can be obtained through the XDS110 driver installation.
Follow these steps for the installation:
1. Run the installer in Administrator mode, and click the Next button (Figure 5).
Figure 5. XDS110 Driver Setup Wizard
l TEXAS
INSTRUMENTS
muse Mleelnem
"ease lead the Mowing meme AgreemenL You must accept the tam“ ol nu: agreement
befure continuing wimlhe Installation
Texas mrmnc: [nmrpozacea A
lacunae Ian—2n: E
mum, , u of Hatch um, 2am)
momma mus: mm m mamm; LICENSE mm“ mm. ms 15
A Item! mums mm”. Ami You mn mu ”can: 1511mm, You
mu. m nsx‘zn mmn You mm um mm m :12 runs 01: nus means:
mm. m m cum 1 mw: mm Mn mam wuss: 0) mm
manna» 10 mm m m2 M m nuns 0? ms 11mm: mum on
“my 0E yoansua mm mm mm.- um (2) you 1mm) 70 zmn mm m V
a ‘1 new «.2 agreenmg
Do you accept mus llceme? ,
,1 [do rm ucepnhe zgreemem
Insulation Dim-y
Ham specify the dummy where XDSllD Windows drivers will be Imallcd.
Installation Dummy (A m
Download and Installation
www.ti.com
6SWRU470–February 2017
Submit Documentation Feedback
Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
2. Read and accept the license agreement, and click the Next button (see Figure 6).
Figure 6. XDS110 Driver License Agreement
3. Specify the installation path (default is c:\ti\), and proceed with the installation (see Figure 7).
Figure 7. XDS110 Driver Installation Directory
l TEXAS
INSTRUMENTS
ISemp
Insulin
Installing
\ 1m
Pleas: wan wmlc Setup "mus xmuo Windows drivers on ymlr computer.
Unpachng mmxdsuo duvemDPlnstélgye
Next ,
www.ti.com
Building the Setup
7
SWRU470–February 2017
Submit Documentation Feedback Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
4. Click the Finish button after the installation is done (Figure 8).
Figure 8. XDS110 Driver Installation Complete
3 Building the Setup
The following components are required:
• A CC3220 LaunchPad flashed with the out-of-box package with the jumpers set correctly. See Figure 9
for reference when powering from USB. J5 is not mandatory
• Micro USB cable
• Mobile or tablet with SimpleLink Wi-Fi Starter Pro application installed. An internet connection is
required for the OTA procedure, because the software package is retrieved from the cloud.
• Local access point
» TEXAS
INSTRUMENTS
...
000
000
.
II "I
III-
.
.u...
..
'oo.
Ico-
....
once
coco
a...
loo-
Building the Setup
www.ti.com
8SWRU470–February 2017
Submit Documentation Feedback
Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
To power up the CC3220 LaunchPad, connect it to the PC or to any USB power supply. The CC3220
LaunchPad out of the box should already contain the application, so there is no need to flash it; that is,
flashing the OOB project paragraph is not required.
Figure 9. CC3220 Default Jumpers Settings
l TEXAS
INSTRUMENTS
, LJP44020P2m
www.ti.com
Getting Started With the Out-of-Box Demonstration
9
SWRU470–February 2017
Submit Documentation Feedback Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
4 Getting Started With the Out-of-Box Demonstration
4.1 Returning to Factory Image
The out-of-box application enables users to go back to the factory image. Factory image means that the
original image stored on the serial flash is extracted, erasing all content from the serial flash. This
assumes that an out-of-box image resides on the serial flash; otherwise, users must reprogram the
CC3220 using the UniFlash utility. Returning to the factory image is equivalent to reprogramming an
image from scratch.
One scenario where users must return to the factory image is if a profile exists and must be replaced by
another one.
Returning to the factory image is an embedded feature, and is not application-dependent.
The procedure is described in the Restore to Factory by Using the SOP section of the SimpleLink™ Wi-
Fi® and Internet of Things CC3120 and CC3220 Network Processor Programmer's Guide.
The procedure is as follows:
1. Set the SOP to 011 (SOP2 = 0, SOP1 = 1, SOP0 = 1), and perform power on reset (POR). Device
reset can be simply done by pressing SW1 Reset switch. See Figure 10 for reference of SOP jumpers.
Figure 10. SOP Jumpers Configuration
2. The device is initiated in Restore to Factory phase, set the SOP jumpers to 000 (SOP2 = 0, SOP1 = 0,
SOP0 = 0).
3. At this point, returning to the factory image occurs because the image is large, and the entire file
system is recreated, which may take up to 1 minute to complete. Upon successful completion, the
default OOB application executes.
• The terminal message should instruct the user to perform POR.
• Because the application is initiated, the red LED starts flashing once every second.
4. The OOB application requests the user perform POR. Manual reset is mandatory in this case.
5. The user performs POR and the default OOB application is executed.
At this point, the device is returning to the factory image. Because the image is large and the entire file
system is recreated, it may take up to a minute to complete. Upon successful completion, the default out-
of-box application should execute.
l TEXAS
INSTRUMENTS
w my q. mm,
SEY'HNGS
(name Smavl Cur-Mg n n
Enab‘e DR Reader fl ‘77
momma u m
Show Secumy Key n w
Open \n Dances Screen fl 4
Show \amnk m n m
WW Dow 60
mm a. use so
mg: gm
Hem
Getting Started With the Out-of-Box Demonstration
www.ti.com
10 SWRU470–February 2017
Submit Documentation Feedback
Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
4.2 Connecting to the CC3220
Connection to the CC3220 device can be applied either by provisioning it or by direct connection when the
CC3220 is set as an access point.
Because this document describes provisioning only, access point mode is not described. Working with the
CC3220 in access point mode is described in detail in the CC3220 SimpleLink™ Wi-Fi® Out-of-Box User's
Guide.
Using SimpleLink Wi-Fi Starter Pro, the user can start AP or SmartConfig provisioning for a fast
connection. During this procedure, the access point credentials are decoded by the CC3220, and a profile
is stored on the serial flash for future connection.
By default, the out-of-box application starts in provisioning mode. It is reflected by a blinking red led
(labeled D7) once every 2 seconds. Terminal can also be used for extra debug messages. A Waiting to be
provisioned message appears when the device is ready to be provisioned.
The provisioning procedure for SmartConfig is described as follows.
1. Open the application and navigate to the Settings tab. Ensure the Enable Smart Config setting is set to
ON (Smart Config is the preferred provisioning method, see Figure 11).
Figure 11. Wi-Fi Starter Settings Tab
l TEXAS
INSTRUMENTS
unx .- 4 Isu v ”mm 7.
Oanfigurzfian Page
Nmuwmu a ccazznrooa
mumkuum u
NeMorkName B mmmmuz «
mmumm fl
sum coNHr amen
wax-‘4 Isu w mm 7.
Oanfigurzfian Page
Nmuwmu a ccazznrooa
mumkuum u
NeMorkName B mmmmuz «
%)
5mm nu mk (awn-Amman mummy Smash"
sum conmunmon
www.ti.com
Getting Started With the Out-of-Box Demonstration
11
SWRU470–February 2017
Submit Documentation Feedback Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
2. Navigate to the provisioning tab to configure the AP credentials. Click on the START
CONFIGURATION button to start the process (see Figure 12).
Figure 12. Wi-Fi Starter Provisioning Tab
3. Successful provisioning is indicated on the mobile application as shown in Figure 13,Figure 14, and
Figure 15. On the LaunchPad, the red Led (D7) turns solid on.
Figure 13. Wi-Fi Starter Provisioning Process (1/3) Figure 14. Wi-Fi Starter Provisioning Process (2/3)
l TEXAS
INSTRUMENTS
—_m v 155a “mm
stwcss :
fl] ccmoroou
Getting Started With the Out-of-Box Demonstration
www.ti.com
12 SWRU470–February 2017
Submit Documentation Feedback
Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
Figure 15. Wi-Fi Starter Provisioning Process (3/3)
Additional LAN and OTA tabs are applicable only to the OOB and automatically open after provisioning is
successfully completed. If these tabs do not show up, navigate to the Devices tab and select the device by
pressing and holding it.
4.3 Use the Mobile Application
One way to control the CC3220 running the out-of-box demo is by using SimpleLink Wi-Fi Starter Pro.
This application can be downloaded and installed through the application stores. Look for Wi-Fi Starter
Pro.
4.3.1 Connect to the CC3220
The application includes the following tabs: Provisioning, Devices, and Settings. Additional LAN and OTA
tabs are applicable to out-of-box only, and are automatically opened after provisioning is successfully
completed.
NOTE: If these tabs do not appear, navigate to the Devices tab and select the device by holding the
button down.
If the device has never been provisioned, refer to Section 4.2. If the device has already been provisioned,
it should automatically connect to an access point so that users can start playing with LAN and OTA
demonstrations. If the access point credentials have not been provisioned by SimpleLink Wi-Fi Starter Pro,
or if SimpleLink Wi-Fi Starter Pro was started while the device was already provisioned and connected to
the access point, the user must bind the application to the desired device. In this case, navigate to the
Devices tab and select the device by long-pressing it.
l TEXAS
INSTRUMENTS
www.ti.com
Getting Started With the Out-of-Box Demonstration
13
SWRU470–February 2017
Submit Documentation Feedback Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
4.3.2 Local Network Demo
On this tab and screen, the user can control and get the state of the onboard sensors. These sensors
include the red LED (D7) and the accelerometer. Device-specific information can also be fetched. The list
of HTTP methods is described in Table 1.
Table 1. HTTP Server Methods
Service Operation Description
Device Get Fetches MAC address, IP address, and SSID of the access point the CC3220 server is
connected to. If the CC3220 is in access point mode, the SSID is the name of the
CC3220 device.
Light Get/Post Fetches and updates the state of the onboard red LED (labeled D7)
Sensor Get Fetches the value of X/Y/Z accelerometer axis
Ota Put Uploads the over-the-air image to the CC3220 web server
Ota Get Fetches the current over-the-air version
Figure 16 shows device information, status of the onboard red LED (D7), and periodic accelerometer
readings of the CC3220 LaunchPad board.
Figure 16. Mobile App LAN Tab
To change the state of the red LED (D7), tap on the LED icon.
To show board movement, move the CC3220 board. The update rate is once every second.
4.3.3 Over-the-Air Update
On this tab and screen, the user can see the current software version running on the CC3220 out-of-box
application. Users can check for a new software version by clicking the Check for software update button.
The application then connects to a cloud server where the software version is stored, and downloads it.
Users may modify this link by long-tapping the download icon next to Check for software update label, and
filling the new URL. The procedure is monitored by an upload progress bar, which gets feedback from the
CC3220 device itself during the process.
The over-the-air update is adapted to the out-of-box application. If the user either programed other
examples or modified the out-of-box application, they must program an official out-of-box again. Refer to .
l TEXAS
INSTRUMENTS
6 check hr snflware update
nu mm Me mg
«4.: WWW
:]
“1100303”
PROGRAM
Getting Started With the Out-of-Box Demonstration
www.ti.com
14 SWRU470–February 2017
Submit Documentation Feedback
Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
The procedure is as follows:
1. Click the Check for software update button to test whether a new software version exists. As shown in
Figure 17, Current software version shows that no version file exists on the device, and New software
version shows that no file has been downloaded from a data store server. If the device is updated, an
appropriate informative message pops up asking for the user to manually approve it if desired.
Figure 17. Mobile App OTA Tab
In Figure 18, clicking the Check for software update triggers a new software version download from a
data store server, as indicated by New software version.
Figure 18. Mobile App Check for Software Update Completed
TEXAS
INSTRUMENTS
Developer made
m" yourmm mm m . m m.
\—
Cancel 0K
w zmosum
PROGRAM
Upmaumg
(M) E 7 m I
w zmosum
PROGRAM
\u
Upluadmg 4m;
(M) E 7 m I
www.ti.com
Getting Started With the Out-of-Box Demonstration
15
SWRU470–February 2017
Submit Documentation Feedback Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
Alternatively, the user may modify this link by long-tapping the download icon next to the Check for
software update label, and filling the new URL, as shown in Figure 19.
Figure 19. Mobile App Private OTA Repository
2. If a new software version has been downloaded, start the software update by clicking the Program
button, as shown in Figure 20 and Figure 21.
Figure 20. Mobile App OTA Started Figure 21. Mobile App OTA in Progress
l TEXAS
INSTRUMENTS
zmamw
[mommy 1
PROGRAM
Getting Started With the Out-of-Box Demonstration
www.ti.com
16 SWRU470–February 2017
Submit Documentation Feedback
Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
An upload progress bar should appear with the following messages:
• Download started
– Uploading new software version
– Extracting archive file
– Writing to serial flash
• Download done
– Rebooting…
– Testing new software version
• Verdict
– When successful →“Done”
– When failed →“OTA Update failed”
After a successful update, the new version should appear under the New software version section, as
shown in Figure 22. An Upload finished! message appears on the bottom of the screen, and the screen is
enabled again.
Figure 22. Mobile App OTA Done
l TEXAS
INSTRUMENTS
www.ti.com
Getting Started With the Out-of-Box Demonstration
17
SWRU470–February 2017
Submit Documentation Feedback Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
Table 2 lists some abnormal behaviors of the over-the-air procedure.
Table 2. OTA Abnormal Behavior From Mobile App
Behavior Cause Solution
Progress bar does not start Client is not able to open
connection to the CC3220
report server
Usually, it is harmless. Users should probe the red LED (D7),
terminal messages, and the mobile application for more
information.
After a successful process, the red LED (D7) should stop its rapid
blinking, turn solid momentarily, and follow local network
connection procedure, as described under Red LED legend.
Terminal messages should indicate a successful OTA update
process, as described under Terminal messages.
The mobile application should show no error message, and the
current software version field should be updated to the new
version.
The user can then navigate to the Demo tab and continue with the
demonstration.
Progress bar is stuck Client is not able to
communicate with the report
server, or some error
occurred during the process
If the client is not able to communicate, the over-the-air procedure
may still finish successfully. In this case, the same applies as for
when the progress bar does not start (follow the above item on this
table).
If errors occur, the red LED (D7) should stop its rapid blinking and
turn solid off. Users can restart OTA.
4.3.4 Local OTA When CC3220 is in Access Point Mode
When the CC3220 device is set in access point mode, the mobile application can communicate to it as if
both were connected though a local access point. The only use case that requires clarification is the over-
the-air feature, because the image for updates resides on a cloud server and, as the mobile application is
connected to the CC3220, it cannot fetch and download the image.
Follow the steps below to upgrade the image:
1. Set the CC3220 LaunchPad as an access point.
2. Go to Wireless Settings, locate the SSID of the CC3220 LaunchPad, and connect to it (it should start
with a mysimplelink prefix). At this point, the terminal should display a printout stating a device has
been connected.
3. Open SimpleLink Wi-Fi Starter Pro and navigate to the Devices tab. The connected CC3220 with the
MAC address as a prefix on the list should be displayed.
4. Long-press the icon until a pop up message with the IP address, LAN, and OTA tabs appears.
5. Return to Wireless Settings, and connect to an access point with an internet connection.
6. Return to SimpleLink Wi-Fi Starter Pro and navigate to the OTA tab. Click the Check for software
update, and the image should be downloaded.
7. Go to Wireless Settings, locate the SSID of the CC3220 LaunchPad, and connect to it.
8. Return to SimpleLink Wi-Fi Starter Pro and navigate to the OTA tab. The version can now be
upgraded.
l TEXAS
INSTRUMENTS
Troubleshooting
www.ti.com
18 SWRU470–February 2017
Submit Documentation Feedback
Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
5 Troubleshooting
5.1 Red LED Legend
This section lists all the state options of the red LED (D7). Red LED (D7) indication helps the user to both
understand the application flow and debug cases where the application does not behave as expected.
Only the red LED (D7) is used for status indication, and as such, similar indications may be applied in
more than one occasion. To distinguish similar indications, be aware of the executed procedure.
Table 3 lists all options.
Table 3. LED Indication Legend
Red LED Indication Procedure Interpretation
Blinking once in 2 seconds Provisioning The CC3220 is being provisioned.
Solid on Provisioning Connection to the access point is up.
Solid off Provisioning Connection to the access point is down.
Blinking once a second Local network connection For station mode, connection to the access point is in
progress. For access point mode, initialization is in progress.
Solid on Local network connection For station mode, connection to the access point is up. For
access point mode, initialization is done.
Solid off Local network connection Applies in station mode only. Connection to the access point
is down.
Blinking 5 times a second Over-the-air update Over-the-air update of the CC3220 is in progress.
Solid on Over-the-air update Over-the-air update of the CC3220 succeeded.
Solid off Over-the-air update Over-the-air update of the CC3220 failed.
5.2 Terminal Messages
Terminal can also be used for debugging messages. The default configuration is 115200bps, 8 bits, no
parity, and 1 stop bit. Most of the debug messages are self-explained.
For better tracking, each message is preceded with square parentheses that include the task and module
generating the message.
Table 4 lists some common messages to help users track the application status.
Table 4. Terminal Messages
Message Meaning
[Provisioning task] Provisioning Started.
Waiting to be provisioned..!! The CC3220 is in provisioning mode. The user should use SimpleLink Wi-Fi Starter
Pro to provision the device.
[ProvisioningEvent] Connection to AP
succeeded During provisioning, the CC3220 managed to decode the access point credentials
and connect to it successfully.
[ProvisioningEvent] Confirmation Success! During provisioning, the CC3220 managed to feedback SimpleLink Wi-Fi Starter Pro.
[Provisioning task] Provisioning completed
successfully..! Provisioning process completed successfully
[ProvisioningEvent] Provisioning stopped Provisioning is stopped. May indicate the following:
• Successful provisioning
• Inactivity timeout elapsed
• Upon general error
[Provisioning task] committing new ota
download... Upon end of an OTA procedure, indicates a new software package is being
committed.
[Provisioning task] commit succeeded New OTA software package committed successfully.
[Provisioning task] Rollback error sl_FsCtl New OTA software package failed its validation testing (connect to AP while in
station mode or initialize while in access point mode), reverting to previous software
package.
l TEXAS
INSTRUMENTS
www.ti.com
Troubleshooting
19
SWRU470–February 2017
Submit Documentation Feedback Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
Table 4. Terminal Messages (continued)
Message Meaning
[Provisioning task] failed to commit new
download, reverting to previous copy by
reseting the device
New OTA software package failed to commit, reverting to previous software
package.
Return To Factory Image successful, Do a
power cycle(POR) of the device using switch
SW1-Reset
After a return-to-factory is triggered and the device is up, a manual reset is required
from the user to complete the operation
Connection Success (feedback to
Smartphone app failed) During provisioning, the CC3220 connected to the access point successfully but
failed to feedback SimpleLink Wi-Fi Starter Pro.
[Link local task] HTTP GET Request Indicates client HTTP GET request. For details, refer to HTTP server methods.
[Link local task] characteristic is: During HTTP request, indicates the relevant resource.
[Link local task] HTTP POST Request Indicates client HTTP POST request. For details, refer to HTTP server methods.
[Link local task] value is: During HTTP request, indicates the value of the resource.
[Link local task] HTTP PUT Request Indicates client HTTP PUT request. For details, refer to HTTP server methods.
[Link local task] Received OTA filename Archive filename received during over-the-air update. Filename and file size should
follow.
[Link local task] OTA filename should be in
*.tar format Archive filename received during over-the-air update is not in tar format.
[Link local task] ota bundle version file does
not exist OTA version file does not exist on file system. This is informative, not an error.
[OtaArchive_CheckVersion] accept the new
version OTA version file does not exist on file system. New version is accepted. Version
number should follow.
[ OtaArchive_CheckVersion] newer version
update New OTA version is newer than the stored version.
[ OtaArchive_CheckVersion] older version
update New OTA version is older than the stored version.
[OtaArchive_RunParseTar] Create/Open for
write file File is updated on file system during an over-the-air update. Filename should follow.
[OtaArchive_RunParseTar] Downloading
File Completed File has been downloaded and updated on file system successfully during an over-
the-air update.
[ota report task] OTA progress Progress bar in percentages during an over-the-air update.
[Link local task] sl_extLib_OtaRun: ----
Download file completed Over-the-air procedure completed successfully.
[Link local task] sl_NetAppRecv error Error in communication with client during an over-the-air update. Error code should
follow.
[Link local task] OtaArchive error Error in archive module during an over-the-air update. Error code should follow. For
details, refer to OtaArchive.h header file.
[Control task] switching to AP mode The CC3220 is switching to access point mode.
[Control task] device not started in AP role Configuring the CC3220 as an access point failed.
[Control task] device started in AP role,
rebooting device... Switching to access point mode succeeded, rebooting application.
[Control task] device cannot start in AP
mode, please reset the board Switching to access point mode failed. Manual reset is required.
[ERROR] - FATAL ERROR Fatal error occurred. Manual reset is required.
l TEXAS
INSTRUMENTS
Limitations and Known Issues
www.ti.com
20 SWRU470–February 2017
Submit Documentation Feedback
Copyright © 2017, Texas Instruments Incorporated
SimpleLink™ Wi-Fi®CC3220 Out-of-Box Application
6 Limitations and Known Issues
• Up to20 non-default files can be updated during over-the-air updates. Default files include files that are
non-secured, part of a bundle, failsafe, and with the size of the original file.
• Maximal file length inside tar archive is 100 bytes. It is the full path as appears in the tar file itself
(including all directories from root). This is a limitation in the uncompressed tar format.
• Rarely, after provisioning is completed, the LAN and OTA tabs do not appear. If these tabs do not
appear, navigate to the Devices tab and select the device by long-pressing it.
• Rarely, the progress bar does not start or starts but freezes in the middle, even if the over-the-air
update procedure is successful. In these cases, the red LED (labeled D7) indication and terminal
printouts show the true status of the procedure, and the Web client or mobile application should
eventually indicate a successful process.
IMPORTANT NOTICE FOR TI DESIGN INFORMATION AND RESOURCES
Texas Instruments Incorporated (‘TI”) technical, application or other design advice, services or information, including, but not limited to,
reference designs and materials relating to evaluation modules, (collectively, “TI Resources”) are intended to assist designers who are
developing applications that incorporate TI products; by downloading, accessing or using any particular TI Resource in any way, you
(individually or, if you are acting on behalf of a company, your company) agree to use it solely for this purpose and subject to the terms of
this Notice.
TI’s provision of TI Resources does not expand or otherwise alter TI’s applicable published warranties or warranty disclaimers for TI
products, and no additional obligations or liabilities arise from TI providing such TI Resources. TI reserves the right to make corrections,
enhancements, improvements and other changes to its TI Resources.
You understand and agree that you remain responsible for using your independent analysis, evaluation and judgment in designing your
applications and that you have full and exclusive responsibility to assure the safety of your applications and compliance of your applications
(and of all TI products used in or for your applications) with all applicable regulations, laws and other applicable requirements. You
represent that, with respect to your applications, you have all the necessary expertise to create and implement safeguards that (1)
anticipate dangerous consequences of failures, (2) monitor failures and their consequences, and (3) lessen the likelihood of failures that
might cause harm and take appropriate actions. You agree that prior to using or distributing any applications that include TI products, you
will thoroughly test such applications and the functionality of such TI products as used in such applications. TI has not conducted any
testing other than that specifically described in the published documentation for a particular TI Resource.
You are authorized to use, copy and modify any individual TI Resource only in connection with the development of applications that include
the TI product(s) identified in such TI Resource. NO OTHER LICENSE, EXPRESS OR IMPLIED, BY ESTOPPEL OR OTHERWISE TO
ANY OTHER TI INTELLECTUAL PROPERTY RIGHT, AND NO LICENSE TO ANY TECHNOLOGY OR INTELLECTUAL PROPERTY
RIGHT OF TI OR ANY THIRD PARTY IS GRANTED HEREIN, including but not limited to any patent right, copyright, mask work right, or
other intellectual property right relating to any combination, machine, or process in which TI products or services are used. Information
regarding or referencing third-party products or services does not constitute a license to use such products or services, or a warranty or
endorsement thereof. Use of TI Resources may require a license from a third party under the patents or other intellectual property of the
third party, or a license from TI under the patents or other intellectual property of TI.
TI RESOURCES ARE PROVIDED “AS IS” AND WITH ALL FAULTS. TI DISCLAIMS ALL OTHER WARRANTIES OR
REPRESENTATIONS, EXPRESS OR IMPLIED, REGARDING TI RESOURCES OR USE THEREOF, INCLUDING BUT NOT LIMITED TO
ACCURACY OR COMPLETENESS, TITLE, ANY EPIDEMIC FAILURE WARRANTY AND ANY IMPLIED WARRANTIES OF
MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, AND NON-INFRINGEMENT OF ANY THIRD PARTY INTELLECTUAL
PROPERTY RIGHTS.
TI SHALL NOT BE LIABLE FOR AND SHALL NOT DEFEND OR INDEMNIFY YOU AGAINST ANY CLAIM, INCLUDING BUT NOT
LIMITED TO ANY INFRINGEMENT CLAIM THAT RELATES TO OR IS BASED ON ANY COMBINATION OF PRODUCTS EVEN IF
DESCRIBED IN TI RESOURCES OR OTHERWISE. IN NO EVENT SHALL TI BE LIABLE FOR ANY ACTUAL, DIRECT, SPECIAL,
COLLATERAL, INDIRECT, PUNITIVE, INCIDENTAL, CONSEQUENTIAL OR EXEMPLARY DAMAGES IN CONNECTION WITH OR
ARISING OUT OF TI RESOURCES OR USE THEREOF, AND REGARDLESS OF WHETHER TI HAS BEEN ADVISED OF THE
POSSIBILITY OF SUCH DAMAGES.
You agree to fully indemnify TI and its representatives against any damages, costs, losses, and/or liabilities arising out of your non-
compliance with the terms and provisions of this Notice.
This Notice applies to TI Resources. Additional terms apply to the use and purchase of certain types of materials, TI products and services.
These include; without limitation, TI’s standard terms for semiconductor products http://www.ti.com/sc/docs/stdterms.htm), evaluation
modules, and samples (http://www.ti.com/sc/docs/sampterms.htm).
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2017, Texas Instruments Incorporated