TPI (Test Products Int) 的 505 Instruction Manual 规格书
copyright © 2006, Test Products International, Inc
The Value LeaderTM
www.tpi-thevalueleader.com
Test Products International, Inc.
9615 SW Allen Blvd
Beaverton, OR 97005-4814 USA
Ph: 503-520-9197 Fax: 503-520-1225
Test Product International Ltd.
342 Bronte Street South, Unit 9
Milton, Ontario L9T 5B7
Ph: 905-693-8558 Fax: 905-693-0888
Test Products International UK Ltd.
Longley House, East Park
Crawley, West Sussex RH10 6AP
Ph: +44 (0) 1293 561212 Fax: +44 (0) 1293 813465
505 Instruction Manual
505
PHOTO / CONTACT
TACHOMETER
Instruction Manual
@619
WARNING
Read instructions before operating:
Be sure these instructions accompany the tool
when passed from one user to a new or inex-
perienced user.
Rotating equipment can cause flying particles
Wear Safety Goggles (User and bystanders).
Flying particles can cause eye injury.
Keep yourself, clothing and test equipment
clear of moving parts.
Note: To zero previous readings on all tach
operations, Press and hold the START
button then press the desired function
button. If a stored value appears,
release START button until the display
goes off. Then press the START button
immediately and a zero reading will be
displayed until the unit is used for mea-
suring RPM or the START button is
released.
2
OPERATION SPECIFICATIONS
Function Range Accuracy
Photo Tach 6 - 30,000 RPM ± 0.1% of FS + 1 digit
Contact Tach 6 - 20,000 RPM ± 0.1% of FS + 1 digit
Surface Speed 0.9 - 3,046 m/min ± 0.1% of FS + 1 digit
2.0 - 9,990 ft/min ± 0.1% of FS + 1 digit
GENERAL SPECIFICATIONS
Display 5 Digit LCD
Operating Temperature: 32°to 122°F
0°to 50°C
Operating Humidity: 80% Max. R.H.
Power Supply: AA Alkaline Bat.
(2 each)
7
BATTERY REPLACEMENT
Measurement Procedure:
1. Remove the screw holding the battery compart-
ment cover in place on the back of the 505.
2. Slide the cover off of the unit.
3. Remove the 2 each “AA” alkaline batteries and
replace with the same type.
4. Replace the cover and screw.
STANDARD ACCESSORIES
Reflective Tape . . . . . . . . . . . . . . . . . . . . . . .A501
Contact RPM Adapter (screw on) . . . . . . . . .A502
RPM Adapter (Cone Type) . . . . . . . . . . . . . .A503
RPM Adapter (Funnel Type) . . . . . . . . . . . . .A504
Surface Speed Test Wheel . . . . . . . . . . . . . .A505
(O.D. 48.7 mm exactly)
Carrying case . . . . . . . . . . . . . . . . . . . . . . . .A915
6
PHOTO TACH OPERATION
Measurement Procedure:
1. Unscrew contact collar from optical end of
505 (if attached).
2. Attach a piece of reflectIive tape on the rotating
object to be measured.
3. Depress and hold the START button and then
press the Photo button (lower right) on the
505.
4. With the start button depressed, point the
optical end at the rotating surface so the
relective tape passes the lens every rotation.
5. Read the RPM on the LCD display.
Memory Recall
Note: The memory resets itself once the START
button is depressed and stable measurements
are displayed for 10 seconds or 12 revolutions
(whichever is longer). The values are stored
when the START button is released.
1. When you are finished taking measurements,
release the START button.
2. Depress the MEMORY button once, the LAST
reading will be displayed
3. Press the MEMORY button twice, the MAX
reading will be displayed.
4. Press the MEMORY button three times, the MIN
reading will be displayed.
Unit will auto power off after 5 seconds.
3
CONTACT TACH OPERATION
Measurement Procedure:
1. Screw the shaft assembly to the optical end of
the 505.
2. Insert the cone or concave wheel that more
closely matches the end of the component to
be measured on the shaft assembly.
3. Press and hold the START button and then
press the Contact button (lower left) on the
505.
4. While pressing the START button, hold the
wheel against the end of the rotating shaft..
5. Read the RPM on the LCD.
Memory Recall
Note: The memory resets itself once the START
button is depressed and stable measurements
are displayed for 10 seconds or 12 revolutions
(whichever is longer). The values are stored
when the START button is released.
1. When you are finished taking measurements,
release the START button.
2. Depress the MEMORY button once, the LAST
reading will be displayed
3. Press the MEMORY button twice, the MAX
reading will be displayed.
4. Press the MEMORY button three times, the MIN
reading will be displayed.
Unit will power off after 5 seconds.
4
SURFACE SPEED OPERATION
Measurement Procedure:
1. Screw the shaft assembly to the optical end of
the 505.
2. Insert the large wheel to the end of the shaft
assembly.
3. Press and hold the START button and then
press the ft/min (feet per minute) or m/min
(meters per minute) on the 505.
4. While pressing the START button, hold the
wheel against the moving surface.
5. Read the speed on the LCD.
Memory Recall
Note: The memory resets itself once the START
button is depressed and stable measurements
are displayed for 10 seconds or 12 revolutions
(whichever is longer). The values are stored
when the START button is released.
1. When you are finished taking measurements,
release the START button.
2. Depress the MEMORY button once, the LAST
reading will be displayed
3. Press the MEMORY button twice, the MAX
reading will be displayed.
4. Press the MEMORY button three times, the MIN
reading will be displayed.
Unit will power off after 5 seconds.
5
CONTACT TACH OPERATION
Measurement Procedure:
1. Screw the shaft assembly to the optical end of
the 505.
2. Insert the cone or concave wheel that more
closely matches the end of the component to
be measured on the shaft assembly.
3. Press and hold the START button and then
press the Contact button (lower left) on the
505.
4. While pressing the START button, hold the
wheel against the end of the rotating shaft..
5. Read the RPM on the LCD.
Memory Recall
Note: The memory resets itself once the START
button is depressed and stable measurements
are displayed for 10 seconds or 12 revolutions
(whichever is longer). The values are stored
when the START button is released.
1. When you are finished taking measurements,
release the START button.
2. Depress the MEMORY button once, the LAST
reading will be displayed
3. Press the MEMORY button twice, the MAX
reading will be displayed.
4. Press the MEMORY button three times, the MIN
reading will be displayed.
Unit will power off after 5 seconds.
4
SURFACE SPEED OPERATION
Measurement Procedure:
1. Screw the shaft assembly to the optical end of
the 505.
2. Insert the large wheel to the end of the shaft
assembly.
3. Press and hold the START button and then
press the ft/min (feet per minute) or m/min
(meters per minute) on the 505.
4. While pressing the START button, hold the
wheel against the moving surface.
5. Read the speed on the LCD.
Memory Recall
Note: The memory resets itself once the START
button is depressed and stable measurements
are displayed for 10 seconds or 12 revolutions
(whichever is longer). The values are stored
when the START button is released.
1. When you are finished taking measurements,
release the START button.
2. Depress the MEMORY button once, the LAST
reading will be displayed
3. Press the MEMORY button twice, the MAX
reading will be displayed.
4. Press the MEMORY button three times, the MIN
reading will be displayed.
Unit will power off after 5 seconds.
5
BATTERY REPLACEMENT
Measurement Procedure:
1. Remove the screw holding the battery compart-
ment cover in place on the back of the 505.
2. Slide the cover off of the unit.
3. Remove the 2 each “AA” alkaline batteries and
replace with the same type.
4. Replace the cover and screw.
STANDARD ACCESSORIES
Reflective Tape . . . . . . . . . . . . . . . . . . . . . . .A501
Contact RPM Adapter (screw on) . . . . . . . . .A502
RPM Adapter (Cone Type) . . . . . . . . . . . . . .A503
RPM Adapter (Funnel Type) . . . . . . . . . . . . .A504
Surface Speed Test Wheel . . . . . . . . . . . . . .A505
(O.D. 48.7 mm exactly)
Carrying case . . . . . . . . . . . . . . . . . . . . . . . .A915
6
PHOTO TACH OPERATION
Measurement Procedure:
1. Unscrew contact collar from optical end of
505 (if attached).
2. Attach a piece of reflectIive tape on the rotating
object to be measured.
3. Depress and hold the START button and then
press the Photo button (lower right) on the
505.
4. With the start button depressed, point the
optical end at the rotating surface so the
relective tape passes the lens every rotation.
5. Read the RPM on the LCD display.
Memory Recall
Note: The memory resets itself once the START
button is depressed and stable measurements
are displayed for 10 seconds or 12 revolutions
(whichever is longer). The values are stored
when the START button is released.
1. When you are finished taking measurements,
release the START button.
2. Depress the MEMORY button once, the LAST
reading will be displayed
3. Press the MEMORY button twice, the MAX
reading will be displayed.
4. Press the MEMORY button three times, the MIN
reading will be displayed.
Unit will auto power off after 5 seconds.
3
WARNING
Read instructions before operating:
Be sure these instructions accompany the tool
when passed from one user to a new or inex-
perienced user.
Rotating equipment can cause flying particles
Wear Safety Goggles (User and bystanders).
Flying particles can cause eye injury.
Keep yourself, clothing and test equipment
clear of moving parts.
Note: To zero previous readings on all tach
operations, Press and hold the START
button then press the desired function
button. If a stored value appears,
release START button until the display
goes off. Then press the START button
immediately and a zero reading will be
displayed until the unit is used for mea-
suring RPM or the START button is
released.
2
OPERATION SPECIFICATIONS
Function Range Accuracy
Photo Tach 6 - 30,000 RPM ± 0.1% of FS + 1 digit
Contact Tach 6 - 20,000 RPM ± 0.1% of FS + 1 digit
Surface Speed 0.9 - 3,046 m/min ± 0.1% of FS + 1 digit
2.0 - 9,990 ft/min ± 0.1% of FS + 1 digit
GENERAL SPECIFICATIONS
Display 5 Digit LCD
Operating Temperature: 32°to 122°F
0°to 50°C
Operating Humidity: 80% Max. R.H.
Power Supply: AA Alkaline Bat.
(2 each)
7
copyright © 2006, Test Products International, Inc
The Value LeaderTM
www.tpi-thevalueleader.com
Test Products International, Inc.
9615 SW Allen Blvd
Beaverton, OR 97005-4814 USA
Ph: 503-520-9197 Fax: 503-520-1225
Test Product International Ltd.
342 Bronte Street South, Unit 9
Milton, Ontario L9T 5B7
Ph: 905-693-8558 Fax: 905-693-0888
Test Products International UK Ltd.
Longley House, East Park
Crawley, West Sussex RH10 6AP
Ph: +44 (0) 1293 561212 Fax: +44 (0) 1293 813465
505 Instruction Manual
505
PHOTO / CONTACT
TACHOMETER
Instruction Manual