Adafruit Industries LLC 的 Adding a Real Time Clock to Raspberry Pi 规格书
- adafruit learning system
Adding a Real Time Clock to Raspberry Pi
Created by lady ada
Last updated on 2019-05-19 07:22:10 AM UTC
* adafruit learning system
I. II... I'lll
II III-- III-
“N, CZ
.I I
_I. I
_- I
_- I
.I l
_- I
_. I
_- I
.I I
_n I
“Hm&UM69L9§vEZ
.. II... .I-I'
Overview
The Raspberry Pi is designed to be an ultra-low cost computer, so a lot of things we are used to on a computer have
been left out. For example, your laptop and computer have a little coin-battery-powered 'Real Time Clock' (RTC)
module, which keeps time even when the power is off, or the battery removed. To keep costs low and the size small,
an RTC is not included with the Raspberry Pi. Instead, the Pi is intended to be connected to the Internet via Ethernet or
WiFi, updating the time automatically from the global ntp (nework time protocol) servers
For stand-alone projects with no network connection, you will not be able to keep the time when the power goes out.
So in this project we will show you how to add a low cost battery-backed RTC to your Pi to keep time!
This tutorial requires a Raspberry Pi running a kernel with the RTC module and DS1307 module included.
Current Raspbian distros have this, but others may not!
© Adafruit Industries https://learn.adafruit.com/adding-a-real-time-clock-to-raspberry-pi Page 3 of 14
* adafruit learning system
Wiring the
RTC
To keep costs low, the Raspberry Pi does not include a Real Time Clock module. Instead, users are expected to have it
always connected to WiFi or Ethernet and keep time by checking the network. Since we want to include an external
module, we'll have to wire one up.
We have three different RTC we suggest, PCF8523 is inexpensive, DS1307 is most common, and DS3231 is most
precise. Any of them will do!
While the DS1307 is historically the most common, its not the best RTC chipset, we've found!
Adafruit PiRTC - PCF8523 Real Time Clock for Raspberry Pi
$5.95
IN STOCK
ADD TO CART
Adafruit PCF8523 Real Time Clock Assembled Breakout
Board
$4.95
IN STOCK
ADD TO CART
Adafruit DS1307 Real Time Clock Assembled Breakout
Board
$7.50
IN STOCK
ADD TO CART
© Adafruit Industries https://learn.adafruit.com/adding-a-real-time-clock-to-raspberry-pi Page 4 of 14
Don't forget to also install a CR1220 coin cell. In particular the DS1307 wont work at all without it and none of the RTCs
will keep time when the Pi is off and no coin battery is in place.
Wiring is simple:
1. Connect VCC on the breakout board to the 5.0V pin of the Pi (if using DS1307)
Connect VCC on the breakout board to the 3.3V pin of the Pi (if using PCF8523 or DS3231)
2. Connect GND on the breakout board to the GND pin of the Pi
3. Connect SDA on the breakout board to the SDA pin of the Pi
4. Connect SCL on the breakout board to the SCL pin of the Pi
Adafruit DS3231 Precision RTC Breakout
$13.95
IN STOCK
ADD TO CART
CR1220 12mm Diameter - 3V Lithium Coin Cell Battery
$0.95
IN STOCK
ADD TO CART
© Adafruit Industries https://learn.adafruit.com/adding-a-real-time-clock-to-raspberry-pi Page 5 of 14
.nmeu
mxnm .22 m u mu
_ Hue M: m w. A w m.
.
m m w
JaPEaH w
© Adafruit Industries https://learn.adafruit.com/adding-a-real-time-clock-to-raspberry-pi Page 6 of 14
* adafrult learning system
VEI SeliaerOM7 , SecureCRT
Mew Ojnons Dansfev 2:ku Tunis unduw new
EQE Qty-‘35
llRuws, 53cm; xterm
Set Up & Test
I2C
Set up I2C on your Pi
You'll also need to set up i2c on your Pi, to do so, run sudo raspi-config and under Advanced select I2C and turn it on.
For more details, check out our tutorial on Raspberry Pi i2c setup and testing at http://learn.adafruit.com/adafruits-
raspberry-pi-lesson-4-gpio-setup/configuring-i2c (https://adafru.it/aTI)
Reboot once you've done that with sudo reboot
Verify Wiring (I2C scan)
Verify your wiring by running
sudo apt-get install python-smbus i2c-tools
to install the helper software and then sudo i2cdetect -y 1 at the command line, you should see ID #68 show up -
that's the address of the DS1307, PCF8523 or DS3231!
If you have a much older Pi 1, you will have to run sudo i2cdetect -y 0 as the I2C bus address changed from 0 to 1
Once you have the Kernel driver running, i2cdetect will skip over 0x68 and display UU instead, this means its
working!
© Adafruit Industries https://learn.adafruit.com/adding-a-real-time-clock-to-raspberry-pi Page 7 of 14
3% anafrult \enming system
(boot/conflv . cn
Set RTC
Time
Now that we have the module wired up and verified that you can see the module with i2cdetect, we can set up the
module.
Raspbian Jessie (Systemd)
Thanks to kd8twg for the hints! (https://adafru.it/ne3)
You can add support for the RTC by adding a device tree overlay. Run
sudo nano /boot/config.txt
to edit the pi configuration and add whichever matches your RTC chip:
dtoverlay=i2c-rtc,ds1307
or
dtoverlay=i2c-rtc,pcf8523
or
dtoverlay=i2c-rtc,ds3231
to the end of the file
Save it and run sudo reboot to start again. Log in and run sudo i2cdetect -y 1 to see the UU show up where
0x68 should be
Don't forget to set up I2C in the previous step!
© Adafruit Industries https://learn.adafruit.com/adding-a-real-time-clock-to-raspberry-pi Page 8 of 14
@(OMB-PJ’V ‘ I - .. - - 7 &
g p‘i'azpbevrypv .
L9 Cows m
nm/uaev/nuclocx-sec ‘
Disable the "fake hwclock" which interferes with the 'real' hwclock
sudo apt-get -y remove fake-hwclock
sudo update-rc.d -f fake-hwclock remove
sudo systemctl disable fake-hwclock
Now with the fake-hw clock off, you can start the original 'hardware clock' script.
Run sudo nano /lib/udev/hwclock-set and comment out these three lines:
#if [ -e /run/systemd/system ] ; then
# exit 0
#fi
© Adafruit Industries https://learn.adafruit.com/adding-a-real-time-clock-to-raspberry-pi Page 9 of 14
"Q
g cows- MW
CM'IE , PuTTV
Also comment out the two lines
/sbin/hwclock --rtc=$dev --systz --badyear
and
/sbin/hwclock --rtc=$dev --systz
Sync time from Pi to RTC
When you first plug in the RTC module, it's going to have the wrong time because it has to be set once. You can
always read the time directly from the RTC with sudo hwclock -D -r
You can see, the date at first is invalid! You can set the correct time easily. First run date to verify the time is correct.
Plug in Ethernet or WiFi to let the Pi sync the right time from the Internet. Once that's done, run sudo hwclock -w to
write the time, and another sudo hwclock -r to read the time
Once the time is set, make sure the coin cell battery is inserted so that the time is saved. You only have to set the time
once
© Adafruit Industries https://learn.adafruit.com/adding-a-real-time-clock-to-raspberry-pi Page 10 of 14
7C0M7 , SecureCRT
Ele gum wew Qatmns Ivansfer :mpt Ian‘s Mndow Help
:33: $1 0. g 5 g 3% 1
31:3 ’Hm, um,
WW: I ‘»
3:14: run, .
up): u
Ready 52va cow 5, 19 )2Rnw5, 65 Cal; Xtevm
That's it! Next time you boot the time will automatically be synced from the RTC module
Raspbian Wheezy or other pre-systemd Linux
First, load up the RTC module by running
sudo modprobe i2c-bcm2708
sudo modprobe i2c-dev
sudo modprobe rtc-ds1307
Then, as root (type in sudo bash) run
echo ds1307 0x68 > /sys/class/i2c-adapter/i2c-1/new_device
If you happen to have an old Rev 1 Pi, type in
echo ds1307 0x68 > /sys/class/i2c-adapter/i2c-0/new_device
You can then type in exit to drop out of the root shell.
Then check the time with sudo hwclock -r which will read the time from the DS1307 module. If this is the first time the
module has been used, it will report back Jan 1 2000, and you'll need to set the time
First you'll need to get the right time set on the Pi, the easiest way is to connect it up to Ethernet or Wifi - it will
automatically set the time from the network. Once the time is correct (check with the date command), run sudo
hwclock -w to write the system time to the RTC
You can then verify it with sudo hwclock -r
© Adafruit Industries https://learn.adafruit.com/adding-a-real-time-clock-to-raspberry-pi Page 11 of 14
El SeriaerOMI , SecureCRT
EH2 m wew thans Dansfer :cnpt Yen‘s Maw help
Mn . ”Hwy
3,! pieraspbenypi ~
in; gdm W Wm
Q 23 E
ENLI mam 2.2.5
Q E 5 [3% Q
, w m 1W
, "u Multm
H5 JL
senalzcom m 19 11Rows,3uco\s Xtemu NUM
[Iansfav 2mm Yanls Wm fie‘p
QB 5Q%!1
me: /2‘.1:/rmdules "Dawes
sshz Assam 13, 9 zunows, 91cm; xuvm MJM
Next, you'll want to add the RTC kernel module to the /etc/modules list, so its loaded when the machine boots. Run
sudo nano /etc/modules and add rtc-ds1307 at the end of the file (the image below says rtc-1307 but its a typo)
Older pre-Jessie raspbian is a little different. First up, you'll want to create the DS1307 device creation at boot, edit
/etc/rc.local by running
sudo nano /etc/rc.local
and add:
echo ds1307 0x68 > /sys/class/i2c-adapter/i2c-0/new_device
(for v1 raspberry pi)
echo ds1307 0x68 > /sys/class/i2c-adapter/i2c-1/new_device
(for v2 raspberry pi)
sudo hwclock -s
(both versions)
before exit 0 (we forgot the hwclock -s part in the screenshot below)
© Adafruit Industries https://learn.adafruit.com/adding-a-real-time-clock-to-raspberry-pi Page 12 of 14
Ev SeriaerOMi , SecureCRT
Ede m wew gym: [vansfer icupt tools wmnw Help
3333 E EQ E S Lg X ?
GNJ ham 2 2.6 Fue' late/re local
y_1p“
Ready senalzcom 5,1 24Rows,aucols Xtemu NUM
That's it! Next time you boot the time will automatically be synced from the RTC module
© Adafruit Industries https://learn.adafruit.com/adding-a-real-time-clock-to-raspberry-pi Page 13 of 14
© Adafruit Industries Last Updated: 2019-05-19 07:22:10 AM UTC Page 14 of 14