Arduino 的 A000093 规格书
9G5
ARDUINO
g .
U
k Own-mo“
ARDUINOMICROWITHOUT
HEADERS
Code:A000093
ArduinoMicroisthesmallestboardofthefamily,easytointegrateit
ineverydayobjectstomaketheminteractive.TheMicroisbasedon
theATmega32U4microcontrollerfeaturingabuilt‐inUSBwhich
makestheMicrorecognisableasamouseorkeyboard.
The Micro is a microcontroller board based on the ATmega32U4 (datasheet), developed in
conjunction with Adafruit. It has 20 digital input/output pins (of which 7 can be used as PWM
outputs and 12 as analog inputs), a 16 MHz crystal oscillator, a micro USB connection, an ICSP
header, and a reset button. It contains everything needed to support the microcontroller; simply
connect it to a computer with a micro USB cable to get started. It has a form factor that enables
it to be easily placed on a breadboard.
The Micro board is similar to the Arduino Leonardo in that the ATmega32U4 has built-in USB
communication, eliminating the need for a secondary processor. This allows the Micro to appear
to a connected computer as a mouse and keyboard, in addition to a virtual (CDC) serial / COM
port. It also has other implications for the behavior of the board; these are detailed on
the getting started page.
MicrocontrollerATmega32U4
OperatingVoltage5V
InputVoltage(recommended)7‐12V
InputVoltage(limit)6‐20V
DigitalI/OPins20
PWMChannels7
AnalogInputChannels12
DCCurrentperI/OPin20mA
DCCurrentfor3.3VPin50mA
FlashMemory32KB(ATmega32U4)ofwhich4KBusedbybootloader
SRAM2.5KB(ATmega32U4)
EEPROM1KB(ATmega32U4)
ClockSpeed16MHz
LED_BUILTIN13
Length48mm
Width18mm
Weight13g
OSH:Schematics,ReferenceDesign,Boardsize
Arduino / Genuino Micro is open-source hardware! You can build your own board using the
follwing files:
https://www.arduino.cc/en/uploads/Main/arduino‐micro‐reference‐design.zip
https://www.arduino.cc/en/uploads/Main/arduino‐micro‐schematic.pdf
http://arduino.cc/documents/dimensioniMicro.dxf
Programming
The Micro board can be programmed with the Arduino Software (IDE). Select "Arduino/Genuino
Micro from the Tools > Board menu. For details, see the reference and tutorials.
The ATmega32U4 on the Micro comes preprogrammed with a bootloader that allows you to
upload new code to it without the use of an external hardware programmer. It communicates
using the AVR109 protocol.
You can also bypass the bootloader and program the microcontroller through the ICSP (In-
Circuit Serial Programming) header using Arduino ISP or similar; see these instructions for
details. https://www.arduino.cc/en/Hacking/Programmer
Warnings
The Micro has a resettable polyfuse that protects your computer's USB ports from shorts and
overcurrent. Although most computers provide their own internal protection, the fuse provides
an extra layer of protection. If more than 500 mA is applied to the USB port, the fuse will
automatically break the connection until the short or overload is removed.
Power
The Micro can be powered via the micro USB connection or with an external power supply. The
power source is selected automatically.
External (non-USB) power can come either from a DC power supply or battery. Leads from a
battery or DC power supply can be connected to the Gnd and Vin pins.
The board can operate on an external supply of 6 to 20 volts. If supplied with less than 7V,
however, the 5V pin may supply less than five volts and the board may become unstable. If
using more than 12V, the voltage regulator may overheat and damage the board. The
recommended range is 7 to 12 volts.
The power pins are as follows:
VI.TheinputvoltagetotheMICROboardwhenit'susinganexternalpowersource(as
opposedto5voltsfromtheUSBconnectionorotherregulatedpowersource).Youcan
supplyvoltagethroughthispin.
5V.Theregulatedpowersupplyusedtopowerthemicrocontrollerandothercomponents
ontheboard.ThiscancomeeitherfromVINviaanon‐boardregulator,orbesuppliedby
USBoranotherregulated5Vsupply.
3V.A3.3voltsupplygeneratedbytheon‐boardregulator.Maximumcurrentdrawis50mA.
GND.Groundpins.
Memory
The ATmega32U4 has 32 KB (with 4 KB used for the bootloader). It also has 2.5 KB of SRAM
and 1 KB of EEPROM (which can be read and written with the EEPROM library).
https://www.arduino.cc/en/Main/en/Reference/EEPROM
InputandOutput
See the mapping between Arduino pins and ATmega 32U4 ports, and the Pin Mapping of the
Arduino Micro:
nomebottonehttps://www.arduino.cc/en/Hacking/PinMapping32u4
nomebottonehttps://www.arduino.cc/en/uploads/Main/ArduinoMicro_Pinout3.png
Each of the 20 digital i/o pins on the Micro can be used as an input or output,
using pinMode(),digitalWrite(), and digitalRead() functions. They operate at 5 volts. Each pin
can provide or receive 20 mA as recommended operating condition and has an internal pull-up
resistor (disconnected by default) of 20-50 k ohm. A maximum of 40mA is the value that must
not be exceeded to avoid permanent damage to the microcontroller.
In addition, some pins have specialized functions:
Serial:0(RX)and1(TX).Usedtoreceive(RX)andtransmit(TX)TTLserialdatausingthe
ATmega32U4hardwareserialcapability.NotethatontheMicro,theSerialclassrefersto
USB(CDC)communication;forTTLserialonpins0and1,usetheSerial1class.
TWI:2(SDA)and3(SCL).SupportTWIcommunicationusingtheWirelibrary.
ExternalInterrupts:0(RX),1(TX),2,3and7.Thesepinscanbeconfiguredtotriggeran
interruptonalowvalue,arisingorfallingedge,orachangeinvalue.See
theattachInterrupt()functionfordetails.
PWM:3,5,6,9,10,11and13.Provide8‐bitPWMoutputwiththeanalogWrite()function.
SPI:ontheICSPheader.ThesepinssupportSPIcommunicationusingtheSPIlibrary.Note
thattheSPIpinsarenotconnectedtoanyofthedigitalI/OpinsastheyareontheUno,
theyareonlyavailableontheICSPconnectorandonthenearbypinslabelledMISO,MOSI
andSCK.
RX_LED/SSThisisanadditionalpincomparedtotheLeonardo.Itisconnectedtothe
RX_LEDthatindicatestheactivityoftransmissionduringUSBcommunication,butiscan
alsousedasslaveselectpin(SS)inSPIcommunication.
LED:13.Thereisabuilt‐inLEDconnectedtodigitalpin13.WhenthepinisHIGHvalue,the
LEDison,whenthepinisLOW,it'soff.
AnalogInputs:A0‐A5,A6‐A11(ondigitalpins4,6,8,9,10,and12).TheMicrohasatotal
of12analoginputs,pinsfromA0toA5arelabelleddirectlyonthepinsandtheotherones
thatyoucanaccessincodeusingtheconstantsfromA6troughA11aresharedrespectively
ondigitalpins4,6,8,9,10,and12.AllofwhichcanalsobeusedasdigitalI/O.Eachanalog
inputprovide10bitsofresolution(i.e.1024differentvalues).Bydefaulttheanaloginputs
measurefromgroundto5volts,thoughisitpossibletochangetheupperendoftheir
rangeusingtheAREFpinandtheanalogReference()function.
There are a couple of other pins on the board:
AREF.Referencevoltagefortheanaloginputs.UsedwithanalogReference().
Reset.BringthislineLOWtoresetthemicrocontroller.Typicallyusedtoaddaresetbutton
toshieldswhichblocktheoneontheboard.
Communication
The Micro has a number of facilities for communicating with a computer, another board of the
Arduino & Genuino family, or other microcontrollers. The 32U4 provides UART TTL (5V)
serial communication, which is available on digital pins 0 (RX) and 1 (TX). The ATmega32U4
also allows for serial (CDC) communication over USB and appears as a virtual com port to
software on the computer. The chip also acts as a full speed USB 2.0 device, using standard USB
COM drivers. On Windows, a .inf file is required . The Arduino Software (IDE) includes a serial
monitor which allows simple textual data to be sent to and from the board. The RX and TX
LEDs on the board will flash when data is being transmitted via the USB connection to the
computer (but not for serial communication on pins 0 and 1).
A SoftwareSerial library allows for serial communication on other Micro's digital pins.
The ATmega32U4 also supports I2C (TWI) and SPI communication. The Arduino Software
(IDE) includes a Wire library to simplify use of the I2C bus; see the documentation for details.
https://www.arduino.cc/en/Reference/Wire For SPI communication, use the SPI library.
https://www.arduino.cc/en/Reference/SPI
The Micro appears as a generic keyboard and mouse, and can be programmed to control these
input devices using the Keyboard and Mouse classes.
PhysicalCharacteristics
The maximum length and width of the Micro PCB are 4.8cm and 1.77cm respectively, with the
USB connector extending beyond the former dimension. The layout allows for easy placement on
a solderless breadboard..
Automatic(Software)ResetandBootloaderInitiation
Rather than requiring a physical press of the reset button before an upload, the Micro board is
designed in a way that allows it to be reset by software running on a connected computer. The
reset is triggered when the Micro's virtual (CDC) serial / COM port is opened at 1200 baud and
then closed. When this happens, the processor will reset, breaking the USB connection to the
computer (meaning that the virtual serial / COM port will disappear). After the processor resets,
the bootloader starts, remaining active for about 8 seconds. The bootloader can also be initiated
by pressing the reset button on the Micro. Note that when the board first powers up, it will jump
straight to the user sketch, if present, rather than initiating the bootloader.
Because of the way the Micro handles reset it's best to let the Arduino Software (IDE) try to
initiate the reset before uploading, especially if you are in the habit of pressing the reset button
before uploading on other boards. If the software can't reset the board, you can always start the
bootloader by pressing the reset button on the board.
https://store.arduino.cc/usa/arduino‐micro‐without‐headers12‐6‐17