Analog Devices Inc./Maxim Integrated 的 DS1982 规格书
F3 MicroCan
mus
mm
2‘ "mm umnmn
+ .e
'\
97 » "09
00003392355
flywvww
mam
/
um
mm
lVI/JXI/VI
rs illE
“Moms
1/ 09 ‘
ODDCUGFBIBBS
HMve'j <37 m="" ,="" mm="" zzzusfiv/="" um="" mun="">37>
SPECIAL FEATURES
1024 bits Electrically Programmable Read-
Only Memory (EPROM) communicates with
the economy of one signal plus ground
EPROM partitioned into four 256-bit pages for
randomly accessing packetized data
Each memory page can be permanently write-
protected to prevent tampering
Device is an “add only” memory where
additional data can be programmed into
EPROM without disturbing existing data
Architecture allows software to patch data by
superseding an old page in favor of a newly
programmed page
Reduces control, address, data, power, and
programming signals to a single data pin
8-bit family code specifies DS1982
communications requirements to reader
Reads over a wide voltage range of 2.8V to
6.0V from -40°C to +85°C; programs at 11.5V
to 12.0V from -40°C to +50°C
ORDERING INFORMATION
DS1982-F3+ F3 MicroCan
DS1982-F5+ F5 MicroCan
+Denotes a lead(Pb)-free/RoHS-compliant product.
EXAMPLES OF ACCESSORIES
DS9096P Self-Stick Adhesive Pad
DS9101 Multi-Purpose Clip
DS9093RA Mounting Lock Ring
DS9093F Snap-In Fob
DS9092 iButton Probe
F3 MicroCan
COMMON iButton FEATURES
Unique, factory-lasered and tested 64-bit
registration number (8-bit family code + 48-bit
serial number + 8-bit CRC tester) assures
absolute traceability because no two parts are
alike
Multidrop controller for MicroLAN
Digital identification and information by
momentary contact
Chip-based data carrier compactly stores
information
Data can be accessed while affixed to object
Economically communicates to bus master
with a single digital signal at 16.3kbps
Standard 16mm diameter and 1-Wire® protocol
ensure compatibility with iButton® family
Button shape is self-aligning with cup-shaped
probes
Durable stainless steel case engraved with
registration number withstands harsh
environments
Easily affixed with self-stick adhesive backing,
latched by its flange, or locked with a ring
pressed onto its rim
Presence detector acknowledges when reader
first applies voltage
F5 MicroCan
DS1982
1Kb Add-Only iButton
19-4891; Rev 8/09
iButton and 1-Wire are registered trademarks of Maxim Integrated Products, Inc.
Page 1 of 24
DS1982
Page 2 of 24
iButton DESCRIPTION
The DS1982 1Kb Add-Only iButton is a rugged read/write data carrier that identifies and stores relevant
information about the product or person to which it is attached. This information can be accessed with
minimal hardware, for example, a single port pin of a microcontroller. The DS1982 consists of a factory-
lasered registration number that includes a unique 48-bit serial number, an 8-bit CRC, and an 8-bit Family
Code (09h) plus 1Kb of EPROM that is user-programmable. The power to program and read the DS1982
is derived entirely from the 1-Wire communication line. Data is transferred serially via the 1-Wire
protocol that requires only a single data lead and a ground return. The entire device can be programmed
and then write-protected if desired. Alternatively, the part may be programmed multiple times with new
data being appended to, but not overwriting, existing data with each subsequent programming of the
device. Note: Individual bits can be changed only from a logical 1 to a logical 0, never from a logical 0 to
a logical 1. A provision is also included for indicating that a certain page or pages of data are no longer
valid and have been replaced with new or updated data that is now residing at an alternate page address.
This page address redirection allows software to patch data and enhance the flexibility of the device as a
standalone database. The 48-bit serial number that is factory-lasered into each DS1982 provides a
guaranteed unique identity that allows for absolute traceability. The durable MicroCan package is highly
resistant to harsh environments such as dirt, moisture, and shock. Its compact button-shaped profile is
self-aligning with cup-shaped receptacles, allowing the DS1982 to be used easily by human operators or
automatic equipment. Accessories permit the DS1982 to be mounted on printed circuit boards, plastic key
fobs, photo-ID badges, ID bracelets, and many other objects. Applications include work-in-progress
tracking, electronic travelers, access control, storage of calibration constants, and debit tokens.
OVERVIEW
The block diagram in Figure 1 shows the relationships between the major control and memory sections of
the DS1982. The DS1982 has three main data components: 1) 64-bit lasered ROM, 2) 1024-bit EPROM,
and 3) EPROM Status Bytes. The device derives its power for read operations entirely from the 1-Wire
communication line by storing energy on an internal capacitor during periods of time when the signal line
is high and continues to operate off of this “parasite” power source during the low times of the 1-Wire
line until it returns high to replenish the parasite (capacitor) supply. During programming, 1-Wire
communication occurs at normal voltage levels and then is pulsed momentarily to the programming
voltage to cause the selected EPROM bits to be programmed. The 1-Wire line must be able to provide 12
volts and 10 milliamperes to adequately program the EPROM portions of the part. Whenever
programming voltages are present on the 1-Wire line a special high voltage detect circuit within the
DS1982 generates an internal logic signal to indicate this condition. The hierarchical structure of the 1-
Wire protocol is shown in Figure 2. The bus master must first provide one of the four ROM function
commands: 1) Read ROM, 2) Match ROM, 3) Search ROM, 4) Skip ROM. These commands operate on
the 64-bit lasered ROM portion of each device and can singulate a specific device if many are present on
the 1-Wire line as well as indicate to the bus master how many and what types of devices are present. The
protocol required for these ROM function commands is described in Figure 9. After a ROM function
command is successfully executed, the memory functions that operate on the EPROM portions of the
DS1982 become accessible and the bus master may issue any one of the five memory function commands
specific to the DS1982 to read or program the various data fields. The protocol for these memory function
commands is described in Figure 6. All data is read and written least significant bit first.
DS1982
3 of 24
64-BIT LASERED ROM
Each DS1982 contains a unique ROM code that is 64 bits long. The first 8 bits are a 1-Wire family code.
The next 48 bits are a unique serial number. The last 8 bits are a CRC of the first 56 bits (see Figure 3).
The 64-bit ROM and ROM Function Control section allow the DS1982 to operate as a 1-Wire device and
follow the 1-Wire protocol detailed in the section “1-Wire Bus System.” The memory functions required
to read and program the EPROM sections of the DS1982 are not accessible until the ROM function
protocol has been satisfied. This protocol is described in the ROM functions flow chart (Figure 9). The
1-Wire bus master must first provide one of four ROM function commands: 1) Read ROM, 2) Match
ROM, 3) Search ROM, or 4) Skip ROM. After a ROM function sequence has been successfully executed,
the bus master may then provide any one of the memory function commands specific to the DS1982
(Figure 6).
The 1-Wire CRC of the lasered ROM is generated using the polynomial X8 + X5 + X4 + 1. Additional
information about the Maxim 1-Wire Cyclic Redundancy Check is available in the Book of DS19xx
iButton Standards. The shift register acting as the CRC accumulator is initialized to 0. Then starting with
the least significant bit of the family code, 1 bit at a time is shifted in. After the 8th bit of the family code
has been entered, then the serial number is entered. After the 48th bit of the serial number has been
entered, the shift register contains the CRC value. Shifting in the 8 bits of CRC should return the shift
register to all 0s.
1—Wl RE
BUS :
PARASITE POWER
flag
a
DATA
1~W|RE FUNCTION 64_BIT LASERED
CONTROL ROM
PROGRAM MEMORY B—BIT
VOLTAGE FUNCTION 0
DETECT CONTROL SCHATCHPAD
Han CRC
GENERATOR
1024—5” EPROM
(4 PAGES 0F 32 BVTES) .———._—.
EPROM STATUS
BYTES
DS1982
Page 4 of 24
DS1982 BLOCK DIAGRAM Figure 1
>
LEVEL: COMMANDS: AFFECTED:
\IVRITE STATUS BYTE
READ MEMORY
READ STATUS BYTE
( 6) READ DATA/GENERATE
XVBIT CRC
64-BIT LASERED ROM Figure 3
S—Bit CRC Code 48- Bit Serial Number 8- Bi
MSB LSB MSB LSB MSB
1-WIRE CRC GENERATOR Figure 4
{NPUY
» +® -@ + * @
(MSB) use)
Page 5 of 24
DS1982
Page 5 of 24
HIERARCHICAL STRUCTURE FOR 1-WIRE PROTOCOL Figure 2
64-BIT LASERED ROM Figure 3
8-Bit CRC Code 48- Bit Serial Number 8- Bit Family Code (09h)
MSB LSB MSB LSB MSB LSB
1-WIRE CRC GENERATOR Figure 4
BUS
MASTER
OTHER
DEVICES
DS 1982
COMMAND AVAILABLE DATA FIELD
LEVEL: COMMANDS: AFFECTED:
READ ROM 64-BIT ROM
MATCH ROM 64-BIT ROM
SEARCH ROM 64-BIT ROM
SKIP ROM N/A
WRITE MEMORY 1024-BIT EPROM
WRITE STATUS BYTE EPROM STATUS BYTES
READ MEMORY 1024-BIT EPROM
READ STATUS BYTE EPROM STATUS BYTES
READ DATA/GENERATE 1024-BIT EPROM
8-BIT CRC
1-WIRE ROM FUNCTION
COMMANDS (SEE FIGURE 9)
DS1982-SPECIFIC
MEMORY FUNCTION
COMMANDS
(
SEE FIGURE 6
)
DS1982
Page 6 of 24
1024-BIT EPROM
The memory map in Figure 5 shows the 1024-bit EPROM section of the DS1982 that is configured as
four pages of 32 bytes each. The 8-bit scratchpad is an additional register that acts as a buffer when
programming the memory. Data is first written to the scratchpad and then verified by reading an 8-bit
CRC from the DS1982 that confirms proper receipt of the data. If the buffer contents are correct, a
programming voltage should be applied and the byte of data will be written into the selected address in
memory. This process ensures data integrity when programming the memory. The details for reading and
programming the 1024-bit EPROM portion of the DS1982 are given in the "Memory Function
Commands" section.
EPROM STATUS BYTES
In addition to the 1024 bits of data memory the DS1982 provides 64 bits of status memory accessible
with separate commands.
The EPROM Status Bytes can be read or programmed to indicate various conditions to the software
interrogating the DS1982. The first byte of the EPROM status memory contains the Write-Protect Page
bits that inhibit programming of the corresponding page in the 1024-bit main memory area if the
appropriate write protection bit is programmed. Once a bit has been programmed in the Write-Protect
Page byte, the entire 32-byte page that corresponds to that bit can no longer be altered but may still be
read.
The next 4 bytes of the EPROM Status Memory contain the Page Address Redirection Bytes that indicate
if one or more of the pages of data in the 1024-bit EPROM section have been invalidated and redirected
to the page address contained in the appropriate redirection byte. The hardware of the DS1982 makes no
decisions based on the contents of the Page Address Redirection Bytes. These additional bytes of status
EPROM allow for the redirection of an entire page to another page address, indicating that the data in the
original page is no longer considered relevant or valid. With EPROM technology, bits within a page can
be changed from a logical 1 to a logical 0 by programming, but cannot be changed back. Therefore, it is
not possible to simply rewrite a page if the data requires changing or updating, but with space permitting,
an entire page of data can be redirected to another page within the DS1982 by writing the one’s
complement of the new page address into the Page Address Redirection Byte that corresponds to the
original (replaced) page.
This architecture allows the user’s software to make a “data patch” to the EPROM by indicating that a
particular page or pages should be replaced with those indicated in the Page Address Redirection Bytes.
If a Page Address Redirection Byte has a FFH value, the data in the main memory that corresponds to that
page is valid. If a Page Address Redirection Byte has some other hex value, the data in the page
corresponding to that redirection byte is invalid, and the valid data can now be found at the one’s
complement of the page address indicated by the hex value stored in the associated Page Address
Redirection Byte. A value of FDH in the redirection byte for page 1, for example, would indicate that the
updated data is now in page 2. The details for reading and programming the EPROM status memory
portion of the DS1982 are given in the Memory Function Commands section.
0020
EPROM STATUS BYTES
ADDRESS: 0007b 0006h 000511
(MSB)
7 6 5 4 3 2 I
FAUI’ORVA RESERVED FOR PM! ADDRE§ PAGE m PAGE WRESS PAGE ADDRESS
momma) mung wmsm museum Rmmscnon magnum ammzcrm
nu. mg m 3va ma an; m m; m
M; 3 mg way We
|
BIT o
BIT l
BIT 2
BIT 3
BlT4
DS1982
Page 7 of 24
MEMORY FUNCTION COMMANDS
The “Memory Function Flow Chart” (Figure 6) describes the protocols necessary for accessing the
various data fields within the DS1982. The Memory Function Control section, 8-bit scratchpad, and the
Program Voltage Detect circuit combine to interpret the commands issued by the bus master and create
the correct control signals within the device. A 3-byte protocol is issued by the bus master. It is comprised
of a command byte to determine the type of operation and 2 address bytes to determine the specific
starting byte location within a data field. The command byte indicates if the device is to be read or
written. Writing data involves not only issuing the correct command sequence but also providing a 12-
volt programming voltage at the appropriate times. To execute a write sequence, a byte of data is first
loaded into the scratchpad and then programmed into the selected address. Write sequences always occur
a byte at a time. To execute a read sequence, the starting address is issued by the bus master and data is
read from the part beginning at that initial location and continuing to the end of the selected data field or
until a reset sequence is issued. All bits transferred to the DS1982 and received back by the bus master
are sent least significant bit first.
DS1982 MEMORY MAP Figure 5
PAGE 0
32 BYTES
PAGE 1
32 BYTES
PAGE 2
32 BYTES
PAGE 3
32 BYTES
EPROM STATUS BYTES
ADDRESS: 0007h 0006h 0005h 0004h 0003h 0002h 0001h 0000h
(MSB) (LSB)
BIT 0 WRITE PROTECT PAGE 0
BIT 1 WRITE PROTECT PAGE 1
BIT 2 WRITE PROTECT PAGE 2
BIT 3 WRITE PROTECT PAGE 3
BIT 4-7 BITMAP OF USED PAGES (RESERVED FOR TMEX)
8-BIT SCRATCHPAD
1024-BIT
EPROM
STARTING
ADDRESS
0000h
00
2
0
h
0040h
0060h
MASTER r MEMORY
FUNC‘noN ND
Mn N
v
BUS MASTER TX BUS MASTER TX
TM (17:10) TM (17-11))
BUS MASTER TX BUS MASTER TX
TAZ min) TA2 mszm
BUS MASTER RX B—BIT CFC BUS MASTER fix HW ONE
OF COMMAND AND ADDRESS OF COMMAND AND ADDRESS
CFC N N CK:
consign MAHSETSEERT 1x ~——@
v v
BUS MASTER Rx BUS MASTER Rx
DATA FROM DATA FROM
DATA MEMORY STATUS MEMORY
051m '1
ADDRESS COUNTER
BUSMASTERR
Lemma): A
y
M MASTER
TX Rsssr
7
N
Bus MASTER
BUS MASTER
1x agsn
051982 WEMENTS
ADDRESS omen
EUS MASTER Rx
5-8” cm: 0F
STATus DATA
Hus MASTER
TX RESET
aus MASTER
Rx 1'5
Rx 1‘s
D31982 1'
PRESENCE P LSE
DS1982
Page 8 of 24
MEMORY FUNCTION FLOW CHART Figure 6
can
READ DATA N
A GENERATE
s—aflvcnc
if v
Bus MASTER TX
TA| (T7:TD)
T
BUS MASTER TX
TA2 msmn
T
BUS MASTER Rx B—EIT CHC
0F COMMAND AND ADDRESS
cac N
CORRECT
7
v
Eus MASTER
>
To WRITE COMMANDS
BUS MASTER Rx
DATA FROM
DATA MEMORY
Dsmzz NcREMENTs
ADDRESS
COUNTER
aus MASTER
TX RESET
N
LEGEND:
<>
DECEDN MADE
BY THE MASTER
<>
DECSIDN MADE
BY mum
TX RESET
BUS MASTER R B—aIT cm
OF PRECEDING P GE OF DATA
BUS MASTER
Rx 1‘5
Bus MASTER
Tx RESET
V
051932 T
PRESENCE? LSE
DS1982
Page 9 of 24
MEMORY FUNCTION FLOW CHART (cont’d) Figure 6
FROM
READ COMMANDS
aus MASTER Tx
TAT mm
T
BUS MASTER TX
TA2 mam
EUS MASTER TX
DATA BYTE (mm)
6
Eus MASTER Rx B—E‘T
CR4: DF COMMAND. ADDRESS.
DATA (15' PASS)
cRc OF ADDRESS, DATA
(SusSEauENT PASSES)
N CRC
CORRECT
v
BUS MASTER Tx
PROGRAM PULSE
T
051982 wHES
SCRATCHPAD
To DATA EPROM
&
aus MASTER Rx
BYTE FROM EPHOM
osum monEuEN-rs
ADDRESS COUNTER
i
DSIM LOADS LE OF
MASTER TX
L‘ RESET
new ADDRESS mo
CRC GBIERATOR
I
Bus MASTER TK
TAT (T7:Tn)
T
BUS MASTER TX
TA2 (Tlsm
BUS MASTER TX
DATA EVTE (D71DD)
T
cRc OF OOMMAND, ADDRESS
Eus MASTER Rx B—EIT
DATA (15' PASS)
we OF ADDRESS, DATA
(SUBSEOLIENT PASSES)
N cm
MASTER Tx
RESET
CORRECT
v
BUS MASTER TX
PROGRAM PULSE
T
D5198: COPES
SCRATum
To STATUS EPRDM
&
EUS MASTER Rx
BVTE FROM EPROM
Dsme mREMENTS
ADDRESS oouNTER
T
as 1992 LOADS [SE OF
NEW ADDR-s NI'D
CK: GETERATOR
aus MASTER
Ix RESET
l__.
D3198? T
vRESENcE P6
DS1982
Page 10 of 24
MEMORY FUNCTION FLOW CHART (cont’d) Figure 6
DS1982
Page 11 of 24
READ MEMORY [F0h]
The Read Memory command is used to read data from the 1024-bit EPROM data field. The bus master
follows the command byte with a 2-byte address (TA1=(T7:T0), TA2=(T15:T8)) that indicates a starting
byte location within the data field. An 8–bit CRC of the command byte and address bytes is computed by
the DS1982 and read back by the bus master to confirm that the correct command word and starting
address were received. If the CRC read by the bus master is incorrect, a Reset Pulse must be issued and
the entire sequence must be repeated. If the CRC received by the bus master is correct, the bus master
issues read time slots and receives data from the DS1982 starting at the initial address and continuing
until the end of the 1024-bit data field is reached or until a Reset Pulse is issued. If reading occurs
through the end of memory space, the bus master may issue eight additional read time slots and the
DS1982 will respond with an 8-bit CRC of all data bytes read from the initial starting byte through the
last byte of memory. After the CRC is received by the bus master, any subsequent read time slots will
appear as logical 1s until a Reset Pulse is issued. Any reads ended by a Reset Pulse prior to reaching the
end of memory will not have the 8-bit CRC available.
Typically a 16-bit CRC would be stored with each page of data to ensure rapid, error-free data transfers
that eliminate having to read a page multiple times to determine if the received data is correct or not. (See
Book of DS19xx iButton Standards, Chapter 7 for the recommended file structure to be used with the
1-Wire environment.) If CRC values are imbedded within the data, a Reset Pulse may be issued at the end
of memory space during a Read Memory command.
READ STATUS [AAh]
The Read Status command is used to read data from the EPROM Status data field. The bus master
follows the command byte with a two-byte address (TA1=(T7:T0), TA2=(T15:T8)) that indicates a
starting byte location within the data field. An 8–bit CRC of the command byte and address bytes is
computed by the DS1982 and read back by the bus master to confirm that the correct command word and
starting address were received. If the CRC read by the bus master is incorrect, a Reset Pulse must be
issued and the entire sequence must be repeated. If the CRC received by the bus master is correct, the bus
master issues read time slots and receives data from the DS1982 starting at the supplied address and
continuing until the end of the EPROM Status data field is reached. At that point the bus master will
receive an 8-bit CRC that is the result of shifting into the CRC generator all of the data bytes from the
initial starting byte through the final factory-programmed byte that contains the 00h value.
This feature is provided since the EPROM Status information may change over time making it impossible
to program the data once and include an accompanying CRC that will always be valid. Therefore, the
Read Status command supplies an 8-bit CRC that is based on and always is consistent with the current
data stored in the EPROM Status data field.
After the 8-bit CRC is read, the bus master will receive logical 1s from the DS1982 until a Reset Pulse is
issued. The Read Status command sequence can be exited at any point by issuing a Reset Pulse.
READ DATA/GENERATE 8-BIT CRC [C3h]
The Read Data/Generate 8-bit CRC command is used to read data from the 1024-bit EPROM memory
field. The bus master follows the command byte with a two-byte address (TA1=(T7:T0), TA2=(T15:T8))
that indicates a starting byte location within the data field. An 8-bit CRC of the command byte and
address bytes is computed by the DS1982 and read back by the bus master to confirm that the correct
command word and starting address were received. If the CRC read by the bus master is incorrect, a
Reset Pulse must be issued and the entire sequence must be repeated. If the CRC received by the bus
master is correct, the bus master issues read time slots and receives data from the DS1982 starting at the
DS1982
Page 12 of 24
initial address and continuing until the end of a 32-byte page is reached. At that point the bus master will
send eight additional read time slots and receive an 8-bit CRC that is the result of shifting into the CRC
generator all of the data bytes from the initial starting byte to the last byte of the current page. Once the
8-bit CRC has been received, data is again read from the 1024-bit EPROM data field starting at the next
page. This sequence will continue until the final page and its accompanying CRC are read by the bus
master. Thus each page of data can be considered to be 33 bytes long, the 32 bytes of user-programmed
EPROM data and an 8-bit CRC that gets generated automatically at the end of each page.
This type of read differs from the Read Memory command that simply reads each page until the end of
address space is reached. The Read Memory command only generates an 8-bit CRC at the end of memory
space that often might be ignored, since in many applications the user would store a 16-bit CRC with the
data itself in each page of the 1024-bit EPROM data field at the time the page was programmed. The
Read Data/Generate 8-bit CRC command provides an alternate read capability for applications that are
“bit-oriented” rather than “page-oriented” where the 1024-bit EPROM information may change over time
within a page boundary, making it impossible to program the page once and include an accompanying
CRC that will always be valid. Therefore, the Read Data/Generate 8-Bit CRC command concludes each
page with the DS1982 generating and supplying an 8-bit CRC that is based on and therefore is always
consistent with the current data stored in each page of the 1024-bit EPROM data field. After the 8-bit
CRC of the last page is read, the bus master will receive logical 1s from the DS1982 until a Reset Pulse is
issued. The Read Data/Generate 8-Bit CRC command sequence can be exited at any point by issuing a
Reset Pulse.
WRITE MEMORY [0Fh]
The Write Memory command is used to program the 1024–bit EPROM data field. The bus master will
follow the command byte with a two byte starting address (TA1=(T7:T0), TA2=(T15:T8)) and a byte of
data (D7:D0). An 8-bit CRC of the command byte, address bytes, and data byte is computed by the
DS1982 and read back by the bus master to confirm that the correct command word, starting address, and
data byte were received.
The highest starting address within the DS1982 is 007FH. If the bus master sends a starting address
higher than this, the nine most significant address bits are set to 0 by the internal circuitry of the chip.
This will result in a mismatch between the CRC calculated by the DS1982 and the CRC calculated by the
bus master, indicating an error condition.
If the CRC read by the bus master is incorrect, a Reset Pulse must be issued and the entire sequence must
be repeated. If the CRC received by the bus master is correct, a programming pulse (12 volts on the 1-
Wire bus for 480 s) is issued by the bus master. Prior to programming, the entire unprogrammed
1024-bit EPROM data field will appear as logical 1s. For each bit in the data byte provided by the bus
master that is set to a logical 0, the corresponding bit in the selected byte of the 1024–bit EPROM will be
programmed to a logical 0 after the programming pulse has been applied at that byte location.
After the 480 s programming pulse is applied and the data line returns to a 5-volt level, the bus master
issues eight read time slots to verify that the appropriate bits have been programmed. The DS1982
responds with the data from the selected EPROM address sent least significant bit first. This byte contains
the logical AND of all bytes written to this EPROM data address. If the EPROM data byte contains 1s in
bit positions where the byte issued by the master contains 0s, a Reset Pulse should be issued and the
current byte address should be programmed again. If the DS1982 EPROM data byte contains 0s in the
same bit positions as the data byte, the programming was successful and the DS1982 will automatically
increment its address counter to select the next byte in the 1024-bit EPROM data field. The least
DS1982
Page 13 of 24
significant byte of the new 2-byte address will also be loaded into the 8-bit CRC generator as a starting
value. The bus master will issue the next byte of data using eight write time slots.
As the DS1982 receives this byte of data into the scratchpad, it also shifts the data into the CRC generator
that has been preloaded with the LSB of the current address, and the result is an 8-bit CRC of the new
data byte and the LSB of the new address. After supplying the data byte, the bus master will read this
8-bit CRC from the DS1982 with eight read time slots to confirm that the address incremented properly
and the data byte was received correctly. If the CRC is incorrect, a Reset Pulse must be issued and the
Write Memory command sequence must be restarted. If the CRC is correct, the bus master will issue a
programming pulse and the selected byte in memory will be programmed.
Note that the initial pass through the Write Memory flow chart will generate an 8-bit CRC value that is
the result of shifting the command byte into the CRC generator, followed by the 2 address bytes, and
finally the data byte. Subsequent passes through the Write Memory flow chart due to the DS1982
automatically incrementing its address counter will generate an 8-bit CRC that is the result of loading (not
shifting) the LSB of the new (incremented) address into the CRC generator and then shifting in the new
data byte.
For both of these cases, the decision to continue (to apply a program pulse to the DS1982) is made
entirely by the bus master, since the DS1982 will not be able to determine if the 8-bit CRC calculated by
the bus master agrees with the 8-bit CRC calculated by the DS1982. If an incorrect CRC is ignored and a
program pulse is applied by the bus master, incorrect programming could occur within the DS1982. Also
note that the DS1982 will always increment its internal address counter after the receipt of the eight read
time slots used to confirm the programming of the selected EPROM byte. The decision to continue is
again made entirely by the bus master; therefore if the EPROM data byte does not match the supplied
data byte but the master continues with the Write Memory command, incorrect programming could occur
within the DS1982. The Write Memory command sequence can be exited at any point by issuing a Reset
Pulse.
WRITE STATUS [55h]
The Write Status command is used to program the EPROM Status data field. The bus master will follow
the command byte with a 2-byte starting address (TA1=(T7:T0), TA2=(T15:T8)) and a byte of status data
(D7:D0). An 8-bit CRC of the command byte, address bytes, and data byte is computed by the DS1982
and read back by the bus master to confirm that the correct command word, starting address, and data
byte were received.
If the CRC read by the bus master is incorrect, a Reset Pulse must be issued and the entire sequence must
be repeated. If the CRC received by the bus master is correct, a programming pulse (12 volts on the 1-
Wire bus for 480 s) is issued by the bus master. Prior to programming, the first 7 bytes of the EPROM
Status data field will appear as logical 1s. For each bit in the data byte provided by the bus master that is
set to a logical 0, the corresponding bit in the selected byte of the EPROM Status data field will be
programmed to a logical 0 after the programming pulse has been applied at that byte location. The 8th
byte of the EPROM status byte data field is factory-programmed to contain 00h.
After the 480 s programming pulse is applied and the data line returns to a 5-volt level, the bus master
issues eight read time slots to verify that the appropriate bits have been programmed. The DS1982
responds with the data from the selected EPROM Status address sent least significant bit first. This byte
contains the logical AND of all bytes written to this EPROM Status Byte address. If the EPROM Status
Byte contains 1s in bit positions where the byte issued by the master contained 0s, a Reset Pulse should
be issued and the current byte address should be programmed again. If the DS1982 EPROM Status Byte
DSleXj
DS1982
Page 14 of 24
contains 0s in the same bit positions as the data byte, the programming was successful and the DS1982
will automatically increment its address counter to select the next byte in the EPROM Status data field.
The least significant byte of the new 2-byte address will also be loaded into the 8-bit CRC generator as a
starting value. The bus master will issue the next byte of data using eight write time slots.
As the DS1982 receives this byte of data into the scratchpad, it also shifts the data into the CRC generator
that has been preloaded with the LSB of the current address and the result is an 8-bit CRC of the new data
byte and the LSB of the new address. After supplying the data byte, the bus master will read this 8-bit
CRC from the DS1982 with eight read time slots to confirm that the address incremented properly and the
data byte was received correctly. If the CRC is incorrect, a Reset Pulse must be issued and the Write
Status command sequence must be restarted. If the CRC is correct, the bus master will issue a
programming pulse and the selected byte in memory will be programmed.
Note that the initial pass through the Write Status flow chart will generate an 8-bit CRC value that is the
result of shifting the command byte into the CRC generator, followed by the 2 address bytes, and finally
the data byte. Subsequent passes through the Write Status flow chart due to the DS1982 automatically
incrementing its address counter will generate an 8-bit CRC that is the result of loading (not shifting) the
LSB of the new (incremented) address into the CRC generator and then shifting in the new data byte.
For both of these cases, the decision to continue (to apply a program pulse to the DS1982) is made
entirely by the bus master, since the DS1982 will not be able to determine if the 8-bit CRC calculated by
the bus master agrees with the 8-bit CRC calculated by the DS1982. If an incorrect CRC is ignored and a
program pulse is applied by the bus master, incorrect programming could occur within the DS1982. Also
note that the DS1982 will always increment its internal address counter after the receipt of the eight read
time slots used to confirm the programming of the selected EPROM byte. The decision to continue is
again made entirely by the bus master, therefore if the EPROM data byte does not match the supplied
data byte but the master continues with the Write Status command, incorrect programming could occur
within the DS1982. The Write Status command sequence can be ended at any point by issuing a Reset
Pulse.
1-WIRE BUS SYSTEM
The 1-Wire bus is a system which has a single bus master and one or more slaves. In all instances, the
DS1982 is a slave device. The bus master is typically a microcontroller. The discussion of this bus system
is broken down into three topics: hardware configuration, transaction sequence, and 1-Wire signaling
(signal type and timing). A 1-Wire protocol defines bus transactions in terms of the bus state during
specified time slots that are initiated on the falling edge of sync pulses from the bus master. For a more
detailed protocol description, refer to Chapter 4 of the Book of DS19xx iButton Standards.
Hardware Configuration
The 1-Wire bus has only a single line by definition; it is important that each device on the bus be able to
drive it at the appropriate time. To facilitate this, each device attached to the 1-Wire bus must have an
open drain connection or 3-state outputs. The DS1982 is an open drain part with an internal circuit
equivalent to that shown in Figure 7. The bus master can be the same equivalent circuit. If a bidirectional
pin is not available, separate output and input pins can be tied together.
The bus master requires a pullup resistor at the master end of the bus, with the bus master circuit
equivalent to the one shown in Figures 8a and 8b. The value of the pullup resistor should be
approximately 5 kfor short line lengths.
DS1982
Page 15 of 24
A multidrop bus consists of a 1-Wire bus with multiple slaves attached. The 1-Wire bus has a maximum
data rate of 16.3kbps. If the bus master is also required to perform programming of the EPROM portions
of the DS1982, a programming supply capable of delivering up to 10 milliamps at 12 volts for 480 s is
required. The idle state for the 1-Wire bus is high. If, for any reason, a transaction needs to be suspended,
the bus MUST be left in the idle state if the transaction is to resume. If this does not occur and the bus is
left low for more than 120 s, one or more of the devices on the bus may be reset.
TRANSACTION SEQUENCE
The sequence for accessing the DS1982 via the 1-Wire port is as follows:
Initialization
ROM Function Command
Memory Function Command
Read/Write Memory/Status
INITIALIZATION
All transactions on the 1-Wire bus begin with an initialization sequence. The initialization sequence
consists of a Reset Pulse transmitted by the bus master followed by a presence pulse(s) transmitted by the
slave(s).
The presence pulse lets the bus master know that the DS1982 is on the bus and is ready to operate. For
more details, see the “1-Wire Signaling” section.
ROM FUNCTION COMMANDS
Once the bus master has detected a presence, it can issue one of the four ROM function commands. All
ROM function commands are 8 bits long. A list of these commands follows (refer to flowchart in Figure
9):
Read ROM [33h]
This command allows the bus master to read the DS1982’s 8-bit family code, unique 48-bit serial
number, and 8-bit CRC. This command can be used only if there is a single DS1982 on the bus. If more
than one slave is present on the bus, a data collision will occur when all slaves try to transmit at the same
time (open drain will produce a wired-AND result).
Match ROM [55h]
The match ROM command, followed by a 64–bit ROM sequence, allows the bus master to address a
specific DS1982 on a multidrop bus. Only the DS1982 that exactly matches the 64-bit ROM sequence
will respond to the subsequent memory function command. All slaves that do not match the 64-bit ROM
sequence will wait for a Reset Pulse. This command can be used with a single or multiple devices on the
bus.
100(2
MOSFET
Data (inner surface)
Ground (outer rim)
@—
i7
. 12V
A) Open Drain
M VDD
I BUS MASTER
10 in
035000 on 3051 EQUIVALENT VP83£OL
5 kn 1° “9 s vpoagsNa
D
o 9“ gram _I_ 553110
on in
S D ,
H To data connection
Y 21300 ’ at Dsmsz
T D 470 pF
PGM S “‘
'—| Capacitor added to reduce
2N7000 coupling on data line due to
$ prognamming signal switching
2N7000
B) Standard TTL
1&3
BUS MASTER 12V
VDD (10 mA min.)
5 k9
TTL—Equivalent PROGRAMMING PULSE
Port Pins
To data connection
0! DS1 982
DS1982
Page 16 of 24
DS1982 EQUIVALENT CIRCUIT Figure 7
BUS MASTER CIRCUIT Figure 8
MASTER 7X
RESET PULSE
DSIBBZ TX
PRESENCE
PULSE
I
MASTER TX ROM
FUNCTION COMMAND
33h
READ ROM
55h
FUN
CCh N
MATCH ROM SEARCH ROM SKIP ROM
COMMAND COMMAND COMMAND COMMAND
y
D31982 TX BIT o
DSIQEégBEFAMILV MASTER TX BIT o uswsez 1x Wu
1 BYTE MASTER TX BIT o
BIT o N N
MATCH? /—’
I V '
uswez TX BIT 1
051982 TX 7
SERIAL NUMBER MASTER 1x 5m ns'sez TX am
6 “ES MASTER TX am
I
DSISBZ T a” ‘ N N
x
CRC BYTE MATCH?
V v
T 031952 TX BIT as
MASTER TX BIT 68 051932 Tx FT 53
MASTER TX BIT 53
BIT as N
MATCH?
v
I
MASTER TX MEMORV
FUNCTION COMMAND
DS1982
Page 17 of 24
ROM FUNCTIONS FLOW CHART Figure 9
DS1982
Page 18 of 24
Skip ROM [CCh]
This command can save time in a single-drop bus system by allowing the bus master to access the
memory functions without providing the 64-bit ROM code. If more than one slave is present on the bus
and a read command is issued following the Skip ROM command, data collision will occur on the bus as
multiple slaves transmit simultaneously (open drain pull–downs will produce a wired-AND result).
Search ROM [F0h]
When a system is initially brought up, the bus master might not know the number of devices on the 1-
Wire bus or their 64-bit ROM codes. The search ROM command allows the bus master to use a process
of elimination to identify the 64-bit ROM codes of all slave devices on the bus. The ROM search process
is the repetition of a simple, three-step routine: read a bit, read the complement of the bit, then write the
desired value of that bit. The bus master performs this simple, three-step routine on each bit of the ROM.
After one complete pass, the bus master knows the contents of the ROM in one device. The remaining
number of devices and their ROM codes may be identified by additional passes. See Chapter 5 of the
Book of DS19xx iButton Standards for a comprehensive discussion of a ROM search, including an actual
example.
1-Wire Signaling
The DS1982 requires strict protocols to ensure data integrity. The protocol consists of five types of
signaling on one line: Reset Sequence with Reset Pulse and Presence Pulse, Write 0, Write 1, Read Data
and Program Pulse. All these signals except presence pulse are initiated by the bus master. The
initialization sequence required to begin any communication with the DS1982 is shown in Figure 10. A
Reset Pulse followed by a presence pulse indicates the DS1982 is ready to accept a ROM command. The
bus master transmits (TX) a Reset Pulse (tRSTL , minimum 480 s). The bus master then releases the line
and goes into receive mode (RX). The 1-Wire bus is pulled to a high state via the pullup resistor. After
detecting the rising edge on the 1-Wire line, the DS1982 waits (tPDH , 15-60 s) and then transmits the
presence pulse (tPDL , 60-240 s).
Read/Write Time Slots
The definitions of write and read time slots are illustrated in Figure 11. All time slots are initiated by the
master driving the data line low. The falling edge of the data line synchronizes the DS1982 to the master
by triggering a delay circuit in the DS1982. During write time slots, the delay circuit determines when the
DS1982 will sample the data line. For a read data time slot, if a 0 is to be transmitted, the delay circuit
determines how long the DS1982 will hold the data line low overriding the 1 generated by the master. If
the data bit is a 1, the device will leave the read data time slot unchanged.
PROGRAM PULSE
To copy data from the 8-bit scratchpad to the EPROM Data or Status Memory, a program pulse of 12
volts is applied to the data line after the bus master has confirmed that the CRC for the current byte is
correct. During programming, the bus master controls the transition from a state where the data line is
idling high via the pullup resistor to a state where the data line is actively driven to a programming
voltage of 12 volts providing a minimum of 10 mA of current to the DS1982. This programming voltage
(Figure 12) should be applied for 480 s, after which the bus master returns the data line to an idle high
state controlled by the pullup resistor. Note that due to the high voltage programming requirements for
any 1-Wire EPROM device, it is not possible to multidrop non-EPROM based 1-Wire devices with the
DS1982 during programming. An internal diode within the non-EPROM based 1-Wire devices will
attempt to clamp the data line at approximately 8 volts and could potentially damage these devices.
including 0
Standards.
INITIALI
VPULLUP
VPUL P MIN
IH MIN
VlL MAX
0V
MASTE
DSIQXZ
~11. order no; to mmA mm m,” Wynn/m}: In
‘PDH
<— ipdl="" —="">
—>
DS1982
Page 19 of 24
CRC GENERATION
The DS1982 has an 8-bit CRC stored in the most significant byte of the 64-bit ROM. The bus master can
compute a CRC value from the first 56 bits of the 64-bit ROM and compare it to the value stored within
the DS1982 to determine if the ROM data has been received error-free by the bus master. The equivalent
polynomial function of this CRC is: X8 + X5 + X4 + 1.
Under certain conditions, the DS1982 also generates an 8-bit CRC value using the same polynomial
function shown above and provides this value to the bus master to validate the transfer of command,
address, and data bytes from the bus master to the DS1982. The Memory Function Flow Chart of Figure
6 indicates that the DS1982 computes an 8-bit CRC for the command, address, and data bytes received
for the Write Memory and the Write Status commands and then outputs this value to the bus master to
confirm proper transfer. Similarly the DS1982 computes an 8–bit CRC for the command and address
bytes received from the bus master for the Read Memory, Read Status, and Read Data/Generate 8-Bit
CRC commands to confirm that these bytes have been received correctly. The CRC generator on the
DS1982 is also used to provide verification of error-free data transfer as each page of data from the 1024-
bit EPROM is sent to the bus master during a Read Data/Generate 8-bit CRC command, and for the 8
bytes of information in the status memory field.
In each case where a CRC is used for data transfer validation, the bus master must calculate a CRC value
using the polynomial function given above and compare the calculated value to either the 8-bit CRC
value stored in the 64-bit ROM portion of the DS1982 (for ROM reads) or the 8-bit CRC value computed
within the DS1982. The comparison of CRC values and decision to continue with an operation are
determined entirely by the bus master. There is no circuitry on the DS1982 that prevents a command
sequence from proceeding if the CRC stored in or calculated by the DS1982 does not match the value
generated by the bus master. Proper use of the CRC as outlined in the flow chart of Figure 6 can result in
a communication channel with a very high level of integrity. For more details on generating CRC values
including example implementations in both hardware and software, see the Book of DS19xx iButton
Standards.
INITIALIZATION PROCEDURE “RESET AND PRESENCE PULSES” Figure 10
480 s tRSTL < *
480 s tRSTH < (includes recovery time)
15 s tPDH < 60 s
60 s tPDL < 240 s
*In order not to mask interrupt signaling by other devices on the 1-Wire bus, tRSTL + tR should always be less than 960
s.
RESISTOR
MASTER
DS1982
MASTER T
X
"RESET PULSE" MASTER R
X
"RESET PULSE"
READ
Write-
‘SLOT
VPULLUP
VPULLUF MIN
VIII MIN 031952
VIL MAX SAMPLING wmuow
W W 7 7, ,
Write-
[REC
¢ ‘sm'r . .4
VPULLU P (
VPULVJP MIN \\ ,_
IH MIN
DS1962 \
VIL MAX SAMPLING wmoow \
0V
15 gé
‘—’*‘ 60 p5 #—p
DS1982
Page 20 of 24
READ/WRITE TIMING DIAGRAM Figure 11
Write-1 Time Slot
60 s tSLOT < 120 s
1 s tLOW1 < 15 s
1 s tREC <
Write-0 Time Slot
60 s tLOW0 < tSLOT < 120 s
1 s tREC <
RESISTOR
MASTER
DS1982
‘SLDY ‘nEc -—
VPuLLuP
Vmuup Mm \\
m um
MASTER SAMPLING \
VIL W WINDOW __ \
0v ——— '
—> Igu‘
I a 'RELEASE
—- W F’
«— ‘RDV ————u
PROGR
v” __—I—-—--—-———————-——————-
VPULLIJP V
—— ‘— (R, 1n: —> 4—
END
NORMALI—era >5 III Mp5 >5 us NORMALl-Vflre
COMMUNICATION ENDS < communication="" resumes="" «up="" i»="" cum="" line="" tvpe="" legend:="" —="" ——="" bus="" master="" active="" high="" (12v="" 0="" io="" ma)="" hasislnr="" pull-up="">
DS1982
Page 21 of 24
Read-data Time Slot
60 s tSLOT < 120 s
1 s tLOWR < 15 s
0 tRELEASE < 45 s
1 s tREC <
tRDV = 15 s
tSU < 1 s
PROGRAM PULSE TIMING DIAGRAM Figure 12
RESISTOR
MASTER
DS1982
VPUP
CN OUT
VPUP
DS1982
Page 22 of 24
ABSOLUTE MAXIMUM RATINGS*
Voltage on any Pin Relative to Ground –0.5V to +12.0V
Operating Temperature –40°C to +85°C
Storage Temperature –55°C to +125°C
This is a stress rating only and functional operation of the device at these or any other conditions
outside those indicated in the operation sections of this specification is not implied. Exposure to
absolute maximum rating conditions for extended periods of time may affect reliability.
DC ELECTRICAL CHARACTERISTICS (VPUP=2.8V to 6.0V; -40C to +85C)
PARAMETER SYMBOL MIN TYP MAX UNITS NOTES
Logic 1 VIH 2.2 V 1, 6
Logic 0 VIL -0.3 +0.8 V 1, 11
Output Logic Low @ 4 mA VOL 0.4 V 1
Output Logic High VOH V
PUP 6.0 V 1, 2
Input Load Current IL 5 A 3
Operating Charge QOP 30 nC 7, 8
Programming Voltage @ 10 mA VPP 11.5 12.0 V
CAPACITANCE (TA = 25C)
PARAMETER SYMBOL MIN TYP MAX UNITS NOTES
Data (1-Wire) CIN/OUT 800 pF 9
AC ELECTRICAL CHARACTERISTICS (VPUP=2.8V to 6.0V; -40C to +85C)
PARAMETER SYMBOL MIN TYP MAX UNITS NOTES
Time Slot tSLOT 60 120 s
Write 1 Low Time tLOW1 1 15 s
Write 0 Low Time tLOW0 60 120 s
Read Data Valid tRDV exactly 15
s
Release Time tRELEASE 0 15 45 s
Read Data Setup tSU 1 s 5
Recovery Time tREC 1 s
Reset Time High tRSTH 480 s 4
Reset Time Low tRSTL 480 s
Presence Detect High tPDHIGH 15 60 s
Presence Detect Low tPDLOW 60 240 s
Delay to Program tDP 5 s 10
Delay to Verify tDV 5 s 10
Program Pulse Width tPP 480 5000 s 10,12
Program Voltage Rise Time tRP 0.5 5.0 s 10
Program Voltage Fall Time tFP 0.5 5.0 s 10
DS1982
Page 23 of 24
NOTES:
1. All voltages are referenced to ground.
2. VPUP = external pullup voltage.
3. Input load is to ground.
4. An additional reset or communication sequence cannot begin until the reset high time has expired.
5. Read data setup time refers to the time the host must pull the 1-Wire bus low to read a bit. Data is
guaranteed to be valid within 1 s of this falling edge and will remain valid for 14 s minimum. (15
s total from falling edge on 1-Wire bus.)
6. VIH is a function of the external pullup resistor and the pullup voltage.
7. 30 nanocoulombs per 72 time slots @ 5.0V.
8. At VCC =5.0V with a 5 k pullup to VCC and a maximum time slot of 120 s.
9. Capacitance on the data pin could be 800 pF when power is first applied. If a 5 k resistor is used to
pull up the data line to VCC , 5 ms after power has been applied the parasite capacitance will not affect
normal communications.
10. Maximum 1-Wire voltage for programming parameters is 11.5V to 12.0V; temperature range is -40°C
to +50°C.
11. Under certain low voltage conditions VILMAX may have to be reduced to as much as 0.5V to always
guarantee a presence pulse.
12. The accumulative duration of the programming pulses for each address must not exceed 5 ms.
DS1982
24 of 24
Maxim cannot assume responsibility for use of any circuitry other than circuitry entirely embodied in a Maxim product. No circuit patent licenses are implied. Maxim
reserves the right to change the circuitry and specifications without notice at any time.
Maxim Integrated Products, 120 San Gabriel Drive, Sunnyvale, CA 94086 408-737-7600
© 2009 Maxim Integrated Products Maxim is a registered trademark of Maxim Integrated Products, Inc.
REVISION HISTORY
REVISION
DATE DESCRIPTION PAGES
CHANGED
7/08 Updated the F3 MicroCan and F5 MicroCan face brands with the latest
per PCN H020201. 1
8/09
Added plus signs (+) to the Ordering Information to reflect the
conversion to a lead-free product.
Deleted the UL bullet from the Features section.
1