Adafruit Industries LLC 的 Pulse Sensor Getting Started Guide 规格书
Hook Dots
Pulse Sensor
Ear Clip
3 Pln Male
Connector
Vinyl Stickers
VEICFO Tape 24" Color Coded Cable
Pulse Sensor Getting Started Guide
Introduction:
Pulse Sensor is a well-designed plug-and-play heart-rate sensor for Arduino. It can be used by
students, artists, athletes, makers, and game & mobile developers who want to easily incorporate live heart-
rate data into their projects. The sensor clips onto a fingertip or earlobe and plugs right into Arduino with some
jumper cables. It also includes an open-source monitoring app that graphs your pulse in real time.
The Pulse Sensor Kit includes:
1) A 24-inch Color-Coded Cable, with (male) header connectors. You'll find this makes it easy to embed the
sensor into your project, and connect to an Arduino. No soldering is required.
2) An Ear Clip, perfectly sized to the sensor. We searched many places to find just the right clip. It can be hot-
glued to the back of the sensor and easily worn on the earlobe.
3) 2 Velcro Dots. These are 'hook' side and are also perfectly sized to the sensor. You'll find these velcro dots
very useful if you want to make a velcro (or fabric) strap to wrap around a finger tip.
4) Velcro strap to wrap the Pulse Sensor around your finger.
4) 3 Transparent Stickers. These are used on the front of the Pulse Sensor to protect it from oily fingers and
sweaty earlobes.
5) The Pulse Sensor has 3 holes around the outside edge which make it easy to sew it into almost anything.
Let’s get started with Pulse Sensor Anatomy
The front of the sensor is the pretty side with the Heart logo. This is the side that makes contact with
the skin. On the front you see a small round hole, which is where the LED shines through from the back, and
there is also a little square just under the LED. The square is an ambient light sensor, exactly like the one used
in cellphones, tablets, and laptops, to adjust the screen brightness in different light conditions. The LED shines
light into the fingertip or earlobe, or other capillary tissue, and sensor reads the light that bounces back. The
back of the sensor is where the rest of the parts are mounted. We put them there so they would not get in the
way of the of the sensor on the front. Even the LED we are using is a reverse mount LED. For more about the
circuit functionality, check out the Hardware page.[needs link]
The cable is a 24” flat color coded ribbon cable with 3 male header connectors.
RED wire = +3V to +5V
BLACK wire = GND
PURPLE wire = Signal
The Pulse Sensor can be connected to arduino, or plugged into a breadboard. Before we get it up and
running, we need to protect the exposed circuitry so you can get a reliable heart beat signal.
Preparing the Pulse Sensor
Before you really start using the sensor you want to insulate the board from your (naturally) sweaty/oily
fingers. The Pulse Sensor is an exposed circuit board, and if you touch the solder points, you could short the
board, or introduce unwanted signal noise. We will use a thin film of vinyl to seal the sensor side. Find the
small page of four clear round stickers in your kit, and peel one off. Then center it on the Pulse Sensor. It
should fit perfectly.
When you are happy with the way it’s lined up, squeeze it onto the face all at once! The sticker (made
of vinyl) will kind of stretch over the sensor and give it a nice close fit. If you get a wrinkle, don’t worry, just
press it down really hard and it should stick. We gave you 4, so you can replace it if necessary.
That takes care of the front side. The vinyl sticker offers very good protection for the underlying circuit,
and we rate it ‘water resistant’. meaning: it can stand to get splashed on, but don’t throw it in the pool!
If this is your first time working with Pulse Sensor, you’re probably eager to get started, and not sure if
you want to use the ear-clip or finger-strap (or other thing). The back of the Pulse Sensor has even more
exposed contacts than the front, so you need to make sure that you don’t let it touch anything conductive or
wet.
duino- x
ped
e httg:l/puIsesensor.com/downloadsl
ing-xx
The easiest and quickest way to protect the back side from undesireable shorts or noise is to simply
stick a velcro dot there for now. The dot will keep your parts away from the Pulse Sensor parts enough for you
to get a good feel for the sensor and decide how you want to mount it. You’ll find that the velcro dot comes off
easily, and stores back on the little strip of plastic next to the other one.
Notice that the electrical connections
are still exposed! We only recommend
this as a temporary setup so you can
get started. We show you how to better
seal the Pulse Sensor later in this
document.
Running The Pulse Sensor Code
Get the latest Arduino and Processing Pulse Sensor software here http :// pulsesensor . com / downloads /
Arduino code is called “PulseSensorAmped_Arduino-xx”
The Processing code is called “PulseSensorAmped_Processing-xx”
We strongly advise that you DO NOT connect the Pulse Sensor to your body while your computer or arduino is
being powered from the mains AC line. That goes for charging laptops and DC power supplies. Please be safe
and isolate yourself from from the power grid, or work under battery power.
Connect the Pulse Sensor to: +V (red), Ground (black), and Analog Pin 0 (purple) on your favorite Arduino, or
Arduino compatible device, and upload the ‘PulseSensoAmped_Arduino-xx’ sketch.
note: If you want to power Pulse Sensor Amped
with low voltage (3.3V for example), make sure
you have this line of code in the setup()
analogReference(EXTERNAL);
Also, make sure that you apply the lower voltage
to the Arduino Aref pin (next to pin 13).
After it’s done uploading, you should see Arduino pin 13 blink in time with your heartbeat when you hold the
sensor on your fingertip. If you grip the sensor too hard, you will squeeze all the blood out of your fingertip and
there will be no signal! If you hold it too lightly, you will invite noise from movement and ambient light. Sweet
Pulse Sensor Amped Visualizer 1.0
Heart beats
with your pulse!
Pulse window
with live
heartbeat
waveform Heart rate
window
updates
every beat
Use scrollbar
to scale the Time between
Pulse window pu|se Window Scale o_75 — — HRV 907ms heartbeats
www.arduino.cc www.grocessing.org
Spot pressure on the Pulse Sensor will give a nice clean signal. You may need to play around and try different
parts of your body and pressures. If you see an intermittent blink, or no blink, you might be a zombie or a robot.
To view the heartbeat waveform and check your heart rate, you can use the Processing sketch that we
made. Start up Processing on your computer and run the ‘PulseSensorAmped_Processing-xx’ sketch. This is
our data visualization software, and it looks like this.
note: If you get an error when starting this code, you may need to make sure you are selecting the right
serial port. Check the Troubleshooting section below..
The large main window shows a graph of raw sensor data over time. The Pulse Sensor Data Window can be
scaled using the scrollbar at the bottom if you have a very large or very small signal. At the right of the screen,
a smaller data window graphs heart rate over time. This graph advances every pulse, and the Beats Per
Minute is updated every pulse as a running average of the last ten pulses. The big red heart in the upper right
also pulses to the time of your heartbeat. When you hold the Pulse Sensor to your fingertip or earlobe or (fill in
body part here) you should see a nice heartbeat waveform like the one above. If you don’t, and you’re sure
you’re not a zombie, try the sensor on different parts of your body that have capillary tissue. We’ve had good
results on the side of the nose, middle of the forehead, palm, and lower lip. We’re all different, original
organisms. Play around and find the best spot on you and your friends. As you are testing and getting used to
the sensor. You may find that some fingers or parts of fingers are better than others. For example, I find that
when I position the sensor so that the edge of the PCB is at the bottom edge of my earlobe I get an awesome
signal. Also, people with cold hands or poor circulation may have a harder time reading the pulse. Run your
hands under warm water, or do some jumping-jacks!
Arduino and Processing programming environments available for download here:
www . arduino . cc www . processing . org
Sealing the Back Side of Pulse Sensor
Basic protection for the back of the Pulse Sensor
and prep for attaching Velcro Dot.
It’s really important to protect the exposed Pulse Sensor circuitry so the sweat of your fingertips or earlobe (or
wherever) doesn’t cause signal noise or a short circuit. This How-To uses hot glue, which can be removed
easily or re-worked if you want to change where you’ve stuck your Pulse Sensor. We love hot glue!
The other things you’ll need are:
Hot Glue Gun
Blue Tape (any tape should do ok)
Nail Trimmers (or your favorite trimming device. Flush-cut wire snips work well too)
Read these instructions all the way through before you start!
First, attach the clear vinyl sticker to the front of your Pulse Sensor, as shown above. Then put a blob of
hot glue on the back, right over the circuit. Size can be difficult to judge sometimes. What I meant was put a
hot glue blob about the size of a kidney bean on the back side of the Pulse Sensor.
Then, while the glue is still very hot, press the Pulse Sensor glue-side-down onto the sticky side of a piece of
blue tape (I believe that blue tape has magical properties, but if you don’t have blue tape other kinds of tape
will work just as well).
note: The tallest thing on the back of the Pulse Sensor is
the green LED housing right in the middle. Use it to make
the hot-glue seal thin and strong. When you press evenly
until the back of the LED touches, all the conductive parts
will be covered with hot glue. If the glue doesn’t ooze out
all around, let it cool down, then peel if from the Pulse
Sensor and try again. Once the glue has cooled down and
has some body, you can peel it off easily. Here’s some
pics of hot glue ‘impressions’ that I took during the making
of this guide.
Next put a small dab of hot glue on the front
of the cables, where they attach to the Pulse
Sensor circuit board. This will bond to the other
glue that’s there and act as a strain-relief for the
cable connection. This is important because the
cable connection can wear out over time.
Once the hot glue has cooled (wait for it!)
the blue tape will peel off very easily. Check
your work to make sure that there are not
exposed electrical connections!
Next is trimming. I find the easiest way is to
use nail clippers. Flush cutting wire snips work
too. Take care not to clip the wires!!!
And leave enough around the cable to act
as a good strain-relief
This is the basic Pulse Sensor Hot Glue Seal, It’s also got the clear vinyl sticker on the front face. We’re calling
this ‘Water Resistant’, ready to be handled and passed around from fingers to earlobes or whatever. It is not
advised to submerge or soak the Pulse Sensor with this basic seal.
Now you can stick on the velcro dot (included) and make a finger strap with the velcro tape (included)!
Attaching the Ear Clip
We looked all over, and were lucky enough to find an ear clip that fits the Pulse Sensor perfectly. The
earlobe is a great place to attach Pulse Sensor. Here’s some instruction on how to do it.
It is important to apply some strain relief to the cable connection where it meets the Pulse Sensor PCB.
The little wire connections can wear out and break (or short on something) over time. We can do this with hot
glue, like we did in the previous example.
First, attach a clear vinyl sticker to the front of the Pulse Sensor if you have not already. Then, put a
small dab of hot glue on the front of the cables right where they meet the PCB. Get some on the edge of the
PCB too, that will help. Remember, if you don’t like the blob you’ve made for any reason, it’s easy to remove
once it cools down.
Next place the Pulse Sensor face down, and put a dab of glue about the size of a kidney bean on the
back as illustrated above. Center the round part of the ear clip on the sensor and press it into the hot glue. The
tallest component on the back is the plastic body of the reverse mount LED, and if you press it evenly it will
help keep the metal of the ear clip from contacting any of the component connections.
Allow the hot glue to ooze out around the ear clip. That will ensure good coverage. Take care not to let
the hot glue cover around the ear clip hinge, as that could get in the way of it working. Trimming is easy with
nail clippers (as above) or your trimming tool of choice. Don’t trim the wires by mistake!!!
Take a good look at your work with a magnifying glass to be sure that you haven't made contact with any of
the solder joints, then plug it in and test it. Hot glue is also great because it is easy to remove or re-work if you
need to.
Troubleshooting:
}11t|r11.(serlal.l
1)):
port = new Serialvthls, Serial.llff[) [0], 115200);
—-
pmt.clear()
port . bufferUntll (' H);
o ht‘lp:l/Drecessinq.orq/reference/libraries/serial/indexhtml
Processing Sketch gives me a COM port error at startup.
Make sure you are plugged into an Arduino board, that it is working correctly, and running our firmware.
Check to see if you have the right serial port. The code underlined in red should match the correct port
number in the terminal window at the bottom of Processing IDE.
Processing gives an RXTX mismatch warning, then nothing happens
The RXTX mismatch problem can be resolved by making sure you are running the latest version of
Processing and Arduino.
If you’re still having trouble, go to http :// processing . org / reference / libraries / serial / index . html for more info.