3M 的 DP88(05, 10, 25)NS Green Series 规格书
DP8805NS Green 0 DP881ONS Green 0 DP8825NS Green
Technical Da‘a Sheet May 2019
Scotch-Weld™
Low Odor Acrylic Adhesives
Page 1 of 7
DP8805NS Green • DP8810NS Green • DP8825NS Green
Technical Data Sheet
May 2019
Product Description
3M™ Scotch-Weld™ Low Odor Acrylic Adhesives are high performance, two-
part acrylic adhesives that offer excellent shear, peel, and impact performance.
These toughened products provide improved adhesion to many plastics and
metals, including those with slightly oily surfaces. These durable products
feature a fast rate of strength build, providing structural strength in minutes.
Their low odor and non-flammability feature also makes them easier to
incorporate into a manufacturing process.
Review UL File QOQW2. MH17478 and Sign Components Manual (SAM) File
E464624 for certification of these adhesive systems in electrical equipment.
DP8810NS Green has been tested for surface flammability, smoke, toxic gas
generation, and caloric content per ASTM E162, ASTM E662, ASTM E1354,
Bombardier SMP 800-C, and Boeing BSS 7239 test methods. DP8805NS
Green and DP8825NS Green should yield similar results.
Product Features
• Toughened
• Excellent shear strength
• High peel and impact strength
• 10:1 mix ratio
• Variety of open times available
• Increased cure speed with applied heat
• Contain glass beads (0.010" diameter) to
control bond line thickness
Note: Unless otherwise indicated, all properties measured at 72°F (22°C).
Typical Uncured
Physical Properties
Note: The following technical information and data should be considered representative or typical
only and should not be used for specification purposes.
Property
3M™ Scotch-Weld™ Low Odor Acrylic Adhesive
DP8805NS Green
DP8810NS Green
DP8825NS Green
Color
Base (B)
Accelerator (A)
Off-White
Blue
Viscosity
1
Base (B)
Accelerator (A)
45,000 cP
15,000 cP
45,000 cP
15,000 cP
40,000 cP
15,000 cP
Density
2
Base (B)
Accelerator (A)
1.06 g/cm3
1.08 g/cm3
1.06 g/cm3
1.08 g/cm3
1.12 g/cm3
1.08 g/cm3
Mix ratio
By volume
10 Parts B : 1 Part A
By weight
10 Parts B : 1 Part A
Note: Cure times are approximate and depend on adhesive temperature.
Work life3
3–5 minutes
8–12 minutes
22–24 minutes
Open time4
4–6 minutes
8–12 minutes
20–22 minutes
Time to handling strength5
6–8 minutes
16–20 minutes
42–46 minutes
Time to structural strength6
8–10 minutes
19–23 minutes
50–56 minutes
dheswes. Therefcle. any exposed
3M™ Scotch-Weld™ Low Odor Acrylic Adhesives
DP8805NS Green • DP8810NS Green • DP8825NS Green
Page 2 of 7
1. Viscosity measured using cone-and-plate viscometer; reported viscosity at 3.8 sec-1 shear rate.
2. Density measured using pycnometer.
3. Maximum time that adhesive can remain in a static mixing nozzle and still be expelled without undue force on the applicator.
4. Maximum time allowed after applying a small amount of adhesive to one substrate before bond must be closed and fixed in place.
5. Minimum time required to achieve 50 psi of overlap shear strength.
6. Minimum time required to achieve 1,000 psi of overlap shear strength.
Typical Mixed
Physical Properties
Note: The following technical information and data should be considered representative or typical
only and should not be used for specification purposes.
Property
3M™ Scotch-Weld™ Low Odor Acrylic Adhesive
DP8805NS Green
DP8810NS Green
DP8825NS Green
Color
Blue-Green
Full cure time
24 hours
Viscosity
45,000 cP
45,000 cP
40,000 cP
Density
1.06 g/cm
3
1.06 g/cm
3
1.12 g/cm
3
Typical Cured
Physical Properties
Note: The following technical information and data should be considered representative or typical only
and should not be used for specification purposes.
Overlap Shear (psi)7
Substrate
3M™ Scotch-Weld™ Low Odor Acrylic Adhesive
DP8805NS Green
DP8810NS Green
DP8825NS Green
Aluminum
3,900 CF
3,600 CF
3,100 CF
Stainless steel
3,500 CF
3,400 CF
2,700 CF
PVC
2,000 SF
1,800 SF
1,400 SF
ABS
1,200 SF
1,200 SF
1,300 SF
Acrylic
1,100 SF
1,100 SF
1,000 SF
Polycarbonate
800 AF
1,000 CF
900 CF
Polystyrene
400 AF
550 AF
550 AF
Polyester (fiber-reinforced)
650 AF
1,000 AF
900 AF
Epoxy resin (fiber-reinforced)
3,300 CF
3,400 CF
2,700 CF
Aluminum (tested at -40°F)
800 AF
900 AF
1,000 AF
Aluminum (tested at 180°F)
900 CF
900 CF
700 CF
7. Overlap shear values measured using ASTM D1002; 1 min open time; adhesive allowed to cure for 24 hours at room temperature; 1/2"
overlap; 0.010" bond line thickness; samples pulled at 0.1 in/min for metals and 2 in/min for plastics; all surfaces prepared with light
abrasion and solvent clean; substrates used were 1/16" thick metals and 1/8" thick plastics; failure modes:
AF: adhesive failure CF: cohesive failure SF: substrate failure
Note: Environmental aging tests have shown that these adhesives may accelerate the corrosion of
certain bare metals (such as cold rolled steel, copper, brass, and bronze), leading to low bond strength
values and early bond failure. These adhesives also have relatively low adhesion to low surface energy
plastics (such as polypropylene, polyethylene, TPO, and PTFE). Applications involving any of these
materials should be carefully evaluated by the end user for suitability.
Note: The presence of oxygen inhibits the cure of acrylic structural adhesives. Therefore, any exposed
surfaces of the mixed adhesive will cure much more slowly than adhesive contained within the bond
line. With methyl methacrylate (MMA) acrylic adhesives, any uncured adhesive on the surface flashes
off immediately, leaving a surface that feels dry to the touch. With these low odor acrylic adhesives,
uncured adhesive on exposed surfaces does not evaporate away quickly, leaving a wet film of partially
cured material. For manufacturing processes that need a dry surface quickly, such as for subsequent
sanding or painting operations, consider instead the standard acrylic adhesives (DP8405NS Green,
DP8410NS Green, DP8425NS Green, and Metal Bonder DP8407NS Green).
nly
3M™ Scotch-Weld™ Low Odor Acrylic Adhesives
DP8805NS Green • DP8810NS Green • DP8825NS Green
Page 3 of 7
Typical Cured
Physical Properties
(continued)
Note: The following technical information and data should be considered representative or typical only
and should not be used for specification purposes.
Mechanical Properties8
Property
3M™ Scotch-Weld™ Low Odor Acrylic Adhesive
DP8805NS Green
DP8810NS Green
DP8825NS Green
Tensile modulus (psi)
140,000
125,000
Not tested
Tensile strength (psi)
1,800
1,650
Not tested
Tensile strain at break (%)
8.5
6.5
Not tested
8. Tensile properties measured using ASTM D638; adhesives allowed to cure for 2 weeks at room temperature; 1/8" thick Type I test
specimens; samples pulled at 0.2 in/min.
Environmental Resistance9
Condition
Substrate
3M™ Scotch-Weld™ Low Odor Acrylic Adhesive
DP8805NS Green
DP8810NS Green
DP8825NS Green
300°F (149°C)
Aluminum
100%
100%
100%
-40°F (-40°C)
100%
95%
95%
120°F (49°C) +
80% relative humidity
70%
65%
75%
150°F (66°C) +
80% relative humidity
65%
70%
70%
185°F (85°C) +
85% relative humidity
50%
50%
30%
Water
70%
75%
60%
90°F (32°C) Water
55%
55%
45%
120°F (49°C) Water
35%
35%
35%
Salt water
(5 wt% in water)
75%
75%
75%
Diesel fuel
95%
90%
95%
Motor oil
100%
95%
100%
Antifreeze
(50 wt% in water)
85%
90%
95%
Isopropyl alcohol
60%
50%
65%
Bleach
(10 wt% in water)
65%
65%
75%
1- wide sampxgs
3M™ Scotch-Weld™ Low Odor Acrylic Adhesives
DP8805NS Green • DP8810NS Green • DP8825NS Green
Page 4 of 7
Typical Cured
Physical Properties
(continued)
Note: The following technical information and data should be considered representative or typical
only and should not be used for specification purposes.
Condition
Substrate
3M™ Scotch-Weld™ Low Odor Acrylic Adhesive
DP8805NS Green
DP8810NS Green
DP8825NS Green
-40°F (-40°C)
PVC
100%
100%
85%
120°F (49°C) +
80% relative humidity
100%
95%
90%
150°F (66°C) +
80% relative humidity
100%
100%
90%
185°F (85°C) +
85% relative humidity
95%
100%
85%
Water
100%
100%
100%
Salt water
(5 wt% in water)
100%
100%
100%
Hydrochloric acid
(16 wt% in water)
100%
95%
100%
Sodium hydroxide
(10 wt% in water)
90%
95%
65%
9. Values indicate overlap shear test performance retained after 1,000 hours of continuous exposure relative to a control sample left
at room temperature; samples conditioned for 24 hours at room temperature and 50% relative humidity prior to tests.
Note: Fully-cured structural adhesives can withstand short-term incidental contact with almost any
solvent, chemical, or environmental condition. However, long-term continuous exposure of these
Acrylic Adhesives to the following liquids should be avoided:
1. Elevated temperature (>100°F) water
2. Ketone-type solvents (acetone, MEK)
3. Gasoline and similar liquids
Floating Roller Peel (lb/inch width)10
Substrate
3M™ Scotch-Weld™ Low Odor Acrylic Adhesive
DP8805NS Green
DP8810NS Green
DP8825NS Green
Aluminum
25 CF
35 CF
30 CF
10. Floating roller peel values measured using ASTM D3167; adhesives allowed to cure for 24 hours at room temperature; 1" wide samples;
0.017" bond line thickness; samples pulled at 6 in/min; aluminum surfaces etched; substrates used were 1/16" thick and 0.020" thick
aluminum; failure modes: AF: adhesive failure CF: cohesive failure SF: substrate failure
Note: The data in this sheet were generated using the 3M™ EPX Applicator System equipped with an
EPX static mixer, according to manufacturer’s directions. Thorough hand-mixing will afford
comparable results.
3M™ Scotch-Weld™ Low Odor Acrylic Adhesives
DP8805NS Green • DP8810NS Green • DP8825NS Green
Page 5 of 7
Directions for Use
1. To obtain the highest strength structural bonds, paint, oxide films, oils, dust, mold
release agents, and all other surface contaminants must be completely removed.
The amount of surface preparation depends on the required bond strength and
environmental aging resistance desired by user. For suggested surface
preparations on common substrates, see the section on surface preparation.
2. Mixing For Duo-Pak Cartridges
Store cartridges with cap end up to allow any air bubbles to rise towards the
tip. To use, simply insert the cartridge into the EPX applicator and start the
plunger into the cylinders using light pressure on the trigger. Then remove
the cap and expel a small amount of adhesive to ensure material flows freely
from both sides of cartridge. For automatic mixing, attach an EPX mixing
nozzle to the cartridge and begin dispensing the adhesive. For hand mixing,
expel the desired amount of adhesive and mix thoroughly. Mix approximately
15 seconds after obtaining a uniform color.
Mixing For Bulk Containers
Mix thoroughly by weight or volume in the proportion specified on the
product label or in the typical uncured properties section. Mix approximately
15 seconds after obtaining a uniform color.
3. Apply adhesive and join surfaces within the open time listed for the specific
product. Larger quantities and/or higher temperatures will reduce this
working time.
4. The adhesive and all materials should be at 60°F (16°C) or above prior to
assembly. Allow adhesive to cure at 60°F (16°C) or above until completely
firm. Applying heat up to 150°F (66°C) will increase cure speed.
5. Keep parts from moving during cure. Apply contact pressure or fixture in
place if necessary. Optimum bond line thickness ranges from 0.005 to 0.020
inch; shear strength will be maximized with thinner bond lines, while peel
strength reaches a maximum with thicker bond lines.
6. Excess uncured adhesive can be cleaned up with ketone-type solvents.*
*Note: When using solvents, extinguish all ignition sources, including pilot lights, and follow the
manufacturer’s precautions and directions for use.
3M™ Scotch-Weld™ Low Odor Acrylic Adhesives
DP8805NS Green • DP8810NS Green • DP8825NS Green
Page 6 of 7
Surface Preparation
3M™ Scotch-Weld™ Low Odor Acrylic Adhesives are designed to be used on
painted or coated metals, most plastics, and some bare metals. The following
cleaning methods are suggested for common surfaces:
Painted/coated metals:
1. Wipe surface free of dust and dirt with clean cloth and pure
isopropyl alcohol.*
2. Sandblast or lightly abrade using clean fine grit abrasives. Do not completely
remove the paint layer or coating down to bare steel.
3. Wipe again with clean cloth and pure isopropyl alcohol to remove
loose particles.*
Aluminum/stainless steel:
1. Wipe surface free of dust and dirt with clean cloth and pure acetone.*
2. Sandblast or lightly abrade using clean fine grit abrasives.
3. Wipe again with clean cloth and pure acetone to remove loose particles.*
Plastics:
1. Wipe surface free of dust and dirt with clean cloth and pure
isopropyl alcohol.*
2. Lightly abrade using fine grit abrasives.
3. Wipe again with clean cloth and pure isopropyl alcohol to remove
loose particles.*
*Note: When using solvents, extinguish all ignition sources, including pilot lights, and follow the
manufacturer’s precautions and directions for use.
'0
-._.r—)>
Excem for me limiled remedy smee above, and ex
m be liable lcrany loss 0! damage arising ham 0
lndilec‘, special, lncidemal, or consequential (incl
opportunlly), regardless of the legal or equitable
warramy. contracl, negllgence, or 3mm llabilky.
Web
3M.cnm/ suucluralAcrylies
ISOQ 1
3M™ Scotch-Weld™ Low Odor Acrylic Adhesives
DP8805NS Green • DP8810NS Green • DP8825NS Green
Page 7 of 7
Storage
Store product at 80°F (27°C) or below. Refrigeration at 40°F (4°C) will help
extend shelf life. Do not freeze. Allow product to reach room temperature
prior to use.
Shelf Life
3M™ Scotch-Weld™ DP8805NS, DP8810NS and DP8825NS Low Odor
Acrylic Adhesives in Duo-Pak cartridges and 1 and 5 gallon pails have a shelf
life of 24 months from date of manufacture in unopened original containers
kept at recommended storage conditions. 55 gallon drums have a shelf life of
12 months from date of manufacture in unopened original containers kept at
recommended storage conditions.
Precautionary Information
Refer to Product Label and Material Safety Data Sheet for health and safety information before
using this product. For additional health and safety information, call 1-800-364-3577 or
(651) 737-6501.
Technical Information
The technical information, guidance, and other statements contained in this document or
otherwise provided by 3M are based upon records, tests, or experience that 3M believes to be
reliable, but the accuracy, completeness, and representative nature of such information is not
guaranteed. Such information is intended for people with knowledge and technical skills
sufficient to assess and apply their own informed judgment to the information. No license under
any 3M or third party intellectual property rights is granted or implied with this information.
Product Selection and Use
Many factors beyond 3M’s control and uniquely within user’s knowledge and control can affect the
use and performance of a 3M product in a particular application. As a result, customer is solely
responsible for evaluating the product and determining whether it is appropriate and suitable for
customer’s application, including conducting a workplace hazard assessment and reviewing all
applicable regulations and standards (e.g., OSHA, ANSI, etc.). Failure to properly evaluate, select,
and use a 3M product and appropriate safety products, or to meet all applicable safety regulations,
may result in injury, sickness, death, and/or harm to property.
Warranty, Limited Remedy
and Disclaimer
Unless a different warranty is specifically stated on the applicable 3M product packaging or
product literature (in which case such warranty governs), 3M warrants that each 3M product
meets the applicable 3M product specification at the time 3M ships the product. 3M MAKES
NO OTHER WARRANTIES OR CONDITIONS, EXPRESS OR IMPLIED, INCLUDING, BUT NOT
LIMITED TO, ANY IMPLIED WARRANTY OR CONDITION OF MERCHANTABILITY, FITNESS
FOR A PARTICULAR PURPOSE, OR ARISING OUT OF A COURSE OF DEALING, CUSTOM, OR
USAGE OF TRADE. If a 3M product does not conform to this warranty, then the sole and
exclusive remedy is, at 3M’s option, replacement of the 3M product or refund of the purchase
price.
Limitation of Liability
Except for the limited remedy stated above, and except to the extent prohibited by law, 3M will
not be liable for any loss or damage arising from or related to the 3M product, whether direct,
indirect, special, incidental, or consequential (including, but not limited to, lost profits or business
opportunity), regardless of the legal or equitable theory asserted, including, but not limited to,
warranty, contract, negligence, or strict liability.
This Industrial Adhesives and Tapes Division product was manufactured under a 3M quality system registered to ISO 9001 standards.
Industrial Adhesives and Tapes Division
3M Center, Building 225-3S-06
St. Paul, MN 55144-1000
Phone 800-362-3550
Fax 877-369-2923
Web 3M.com/StructuralAcrylics
3M and Scotch-Weld are trademarks of 3M Company.
© 3M 2016. All rights reserved.
ISO 9001