SparkFun Electronics 的 MCP4725 Hookup Guide 规格书
Page 1 of 9
MCP4725 Digital to Analog Converter Hookup
Guide
CONTRIBUTORS: JOELEB
To DAC, or Not to DAC...
When learning about the world of microcontrollers, you will come across
analog-to-digital converters quite frequently. These allows us to read in
signals from analog sensors and convert them into a digital language our
microcontrollers and other computational devices can understand.
However, what if you need to do the opposite? What if you need your
Arduino to speak the language of analog signals? Enter the MCP4725
Digital-toAnalog Converter Breakout.
This tiny IC allows you to do just that. By using the Arduino’s I C lines, you
can create a wide variety of analog waveforms on the other end.
Covered in This Tutorial
2
Page 1 of 9
Page 2 of 9
In this tutorial, we will overview the breakout and discuss additional
hardware details. Then an assembly section will discuss how to connect
this breakout to a microcontroller. Last, the firmware will be broken down to
help you understand how the digital to analog conversion happens.
Suggested Reading
• Analog vs Digital
• Logic Levels
• Pull-up Resistors
• Analog to Digital Conversion (ADC)
•IC
• How to Use an Oscilloscope
Board Overview
Before we discuss hooking up the breakout, let’s go over some of the
features of this board.
Pinout
The first thing to point out is the pinout on this breakout now conforms to
the standard I C pinout we’ve started using on most devices that use the
two-wire interface. Thus, it is easy to solder some headers on the breakout
and plug it directly into an Arduino with the same pinout for the I C pins.
There is also the signal out and a GND pin grouped together to connect to
an oscilloscope or whatever other device you’re hooking up to the breakout.
Power
The breakout can be powered anywhere between 2.7V to 5.5V, making it
great for both 5V and 3.3V microcontrollers.
2
2
2
Page 2 of 9
Page 3 of 9
' E (LUT.
12c -*
PULLupsmio .
I C Communication
A few features have been added to this breakout to give the user more
flexibility with the IC, particularly when it comes to adding multiple DACs to
one bus. First, we’ve broken out the address selection pin (A0) to a jumper
pad. By default, this pin is pulled LOW to GND. To change the address of
your other device, simply de-solder the jumper and add a blob of solder to
the middle pad and the Vcc pad.
If you’re going to have more than one MCP4725 on a bus, you’ll also want
to disable the pull-up resistors on all but one breakout. To make this
easier, we’ve added another jumper on the back of the board. The pull-ups
are enabled by default. If you need to disable them, you’ll need to cut the
traces on the jumper pad with an Xacto knife. If you ever need to re-enable
the pull-ups, simply solder the three pads back together.
2
Page 3 of 9
Page 4 of 9
Last, there are two mounting holes to mount this board inside the enclosure
of your choice.
Hooking it Up
To use the MCP4725, all you’ll need is some male headers, a SparkFun
RedBoard or other microcontroller, and a means to see your signal. Using
an oscilloscope will be the easiest way to get started.
First, solder the headers onto your breakout. We recommend using a 4-pin
header facing downward for the power and communication connections and
using a 2-pin header facing up for the Out and GND pins. See the below
image for an example.
Most Arduino boards have the I C on the A4 and A5 pins. Then, in the
firmware we’ll uplaod in the next section, we can set pins A2 and A3 as
GND and Vcc respectively to power the breakout. If you prefer to wire
everything to a breadboard, you can solder a 6-pin header and connect
everything with some jumper wires.
2
Page 4 of 9
Page 5 of 9
Last, it’s time to connect the MCP4725 to whatever device you’ll be sending
analog signals. In this tutorial, we’ll be visualizing the signal with an
oscilloscope. Using the o-scope probes, you could connect to the headers
directly, or you could use some jumper wires. Make sure to not mix up the
Out and GND pins.
Firmware
With everything hooked up, it’s time to upload some code to the Arduino
that will allow the breakout to send analog signals. In this example, the
code will generate a simple sine wave.
Open up the Arduino IDE, and copy in this snippet of code:
Page 5 of 9
Page 6 of 9
/*************************************************************
*****************
MCP4725ExampleWaveformSketch
JoelBartlett
SparkFunElectronics
Sept.11,2014
https://github.com/sparkfun/MCP4725_Breakout
Thissketchtakesdatafromalookuptabletoprovide
waveformstobegeneratedbytheMCP4725DAC.
Developmentenvironmentspecifics:
Arduino1.0+
HardwareVersionV14
Thiscodeisbeerware;ifyouseeme(oranyotherSparkFunem
ployee)atthelocal,
andyou'vefoundourcodehelpful,pleasebuyusaround!
Distributedasis;nowarrantyisgiven.
ThiscodebuildsoffthesketchwrittenbyMarkVandeWetterin
g,whichcanbefoundhere:
http://brainwagon.org/2011/02/24/arduinomcp4725breakoutboar
d/
*/
#include<Wire.h>//IncludetheWirelibrarytotalkI2C
//ThisistheI2CAddressoftheMCP4725,bydefault(A0pulle
dtoGND).
//PleasenotethatthisbreakoutisfortheMCP4725A0.
#defineMCP4725_ADDR0x60
//FordeviceswithA0pulledHIGH,use0x61
//SinewaveTablesweregeneratedusingthiscalculator:
//http://www.daycounter.com/Calculators/SineGeneratorCalcula
tor.phtml
int lookup= 0;//varaiblefornavigatingthroughthetables
int sintab2[512]=
{
2048,2073,2098,2123,2148,2174,2199,2224,
2249,2274,2299,2324,2349,2373,2398,2423,
2448,2472,2497,2521,2546,2570,2594,2618,
2643,2667,2690,2714,2738,2762,2785,2808,
Page 6 of 9
Page 7 of 9
2832,2855,2878,2901,2924,2946,2969,2991,
3013,3036,3057,3079,3101,3122,3144,3165,
3186,3207,3227,3248,3268,3288,3308,3328,
3347,3367,3386,3405,3423,3442,3460,3478,
3496,3514,3531,3548,3565,3582,3599,3615,
3631,3647,3663,3678,3693,3708,3722,3737,
3751,3765,3778,3792,3805,3817,3830,3842,
3854,3866,3877,3888,3899,3910,3920,3930,
3940,3950,3959,3968,3976,3985,3993,4000,
4008,4015,4022,4028,4035,4041,4046,4052,
4057,4061,4066,4070,4074,4077,4081,4084,
4086,4088,4090,4092,4094,4095,4095,4095,
4095,4095,4095,4095,4094,4092,4090,4088,
4086,4084,4081,4077,4074,4070,4066,4061,
4057,4052,4046,4041,4035,4028,4022,4015,
4008,4000,3993,3985,3976,3968,3959,3950,
3940,3930,3920,3910,3899,3888,3877,3866,
3854,3842,3830,3817,3805,3792,3778,3765,
3751,3737,3722,3708,3693,3678,3663,3647,
3631,3615,3599,3582,3565,3548,3531,3514,
3496,3478,3460,3442,3423,3405,3386,3367,
3347,3328,3308,3288,3268,3248,3227,3207,
3186,3165,3144,3122,3101,3079,3057,3036,
3013,2991,2969,2946,2924,2901,2878,2855,
2832,2808,2785,2762,2738,2714,2690,2667,
2643,2618,2594,2570,2546,2521,2497,2472,
2448,2423,2398,2373,2349,2324,2299,2274,
2249,2224,2199,2174,2148,2123,2098,2073,
2048,2023,1998,1973,1948,1922,1897,1872,
1847,1822,1797,1772,1747,1723,1698,1673,
1648,1624,1599,1575,1550,1526,1502,1478,
1453,1429,1406,1382,1358,1334,1311,1288,
1264,1241,1218,1195,1172,1150,1127,1105,
1083,1060,1039,1017,995,974,952,931,
910,889,869,848,828,808,788,768,
749,729,710,691,673,654,636,618,
600,582,565,548,531,514,497,481,
465,449,433,418,403,388,374,359,
345,331,318,304,291,279,266,254,
242,230,219,208,197,186,176,166,
156,146,137,128,120,111,103,96,
88,81,74,68,61,55,50,44,
39,35,30,26,22,19,15,12,
10,8,6,4,2,1,1,0,
0,0,1,1,2,4,6,8,
10,12,15,19,22,26,30,35,
39,44,50,55,61,68,74,81,
88,96,103,111,120,128,137,146,
156,166,176,186,197,208,219,230,
Page 7 of 9
Page 8 of 9
242,254,266,279,291,304,318,331,
345,359,374,388,403,418,433,449,
465,481,497,514,531,548,565,582,
600,618,636,654,673,691,710,729,
749,768,788,808,828,848,869,889,
910,931,952,974,995,1017,1039,1060,
1083,1105,1127,1150,1172,1195,1218,1241,
1264,1288,1311,1334,1358,1382,1406,1429,
1453,1478,1502,1526,1550,1575,1599,1624,
1648,1673,1698,1723,1747,1772,1797,1822,
1847,1872,1897,1922,1948,1973,1998,2023
};
void setup()
{
Wire.begin();
//SetA2andA3asOutputstomakethemourGNDandVcc,
//whichwillpowertheMCP4725
pinMode(A2,OUTPUT);
pinMode(A3,OUTPUT);
digitalWrite(A2,LOW);//SetA2asGND
digitalWrite(A3,HIGH);//SetA3asVcc
}
//
void loop()
{
Wire.beginTransmission(MCP4725_ADDR);
Wire.write(64);//cmdtoupdatetheDAC
Wire.write(sintab2[lookup]>> 4);//the8mostsigni
ficantbits...
Wire.write((sintab2[lookup]& 15)<< 4);//the4leastsign
ificantbits...
Wire.endTransmission();
lookup= (lookup+1)&511;
}
Once the sketch is uploaded, fire up the o-scope, connect the probe, if you
haven’t yet, and you should be greeted with a nice looking sine wave.
Page 8 of 9
Page 9 of 9
https://leam.sparkthn.com/tutorials/mcp4725- ’
’tal-to-analog-converter-hookup-guidaja=l . 1074846761.. 2/12/2015
Resources and Going Further
With that, you should be able to get your MCP4725 working the way you’d
like and integrated into your next project. For more information on the
MCP4725, please visit the links below.
• MCP4725 on Brainwagon
• Sine Lookup Table Generator
• MCP4725 Datasheet
Need more? Check out these other SparkFun tutorials:
• Pulse-width Modulation
• Sound Detector Hookup Guide
• AD8232 Heart Rate Monitor Hookup Guide
• Hacking MindWave Mobile
Page 9 of 9
2
/
12
/
201
5
htt
p
s://learn.s
p
arkfun.com/tutorials/mc
p
472
5
-di
g
ita
l
-t
o
-analo
g
-converte
r
-hooku
p
-
g
uide?
_g
a=1.107484676.
7
...