Thomas Research Products 的 LVS Series Install Instr 规格书

sw‘ em HUBBELL' General Solu
070219
72-00405 D
Low Voltage Wall Switches
INSTALLATION INSTRUCTIONS
PRECAUTIONS
CAUTION: FOR USE WITH CLASS 2, LOW VOLTAGE SYSTEMS ONLY. DO NOT USE IN HIGH VOLTAGE APPLICATIONS.
Read and understand all instructions before beginning installation.
NOTICE: For installation by a licensed electrician in accordance with National and/or local Electrical Codes, the instructions of the system to be
interfaced with, and the following instructions.
NOTICE: For indoor use only.
CAUTION: USE COPPER CONDUCTOR ONLY.
Confirm device ratings are suitable for application prior to installation. Use of device in applications beyond its specified ratings or in applications
other than its intended use may cause an unsafe condition and will void manufacturer’s warranty.
NOTICE: Do not install if any damage to product is noticed.
SPECIFICATIONS
Electrical Ratings:
Each switch: 100mA @ 30VDC Max
Each pilot LED: 18 – 30VDC, internal 2.2kohm, ½ Watt resistor
1, 2, 3 and 4 button versions available with or without pilot LEDs
Available in either latching (sustained) or momentary versions
Accepts standard decorator style wall plate (Not Included)
Available in White or Ivory
Fits standard single gang wall box
Two-year warranty
DESCRIPTION
The LVS Series of Low Voltage Wall Switches are designed to provide a user interface and control of systems operating on Class 2, low voltage circuitry. With
a configuration that fits standard, single gang wall boxes and an architecturally pleasing appearance, these devices provide a solution for applications
where low voltage interface capabilities are required.
INSTALLATION
1. Prepare the installation site, as necessary, to install the LVS Wall Switch.
2. Route 18 AWG, Class 2 cable with a quantity of conductors sufficient for the version of LVS Wall Switch being used from the wall switch location to the
system control device. Maximum lead length must not exceed 750 feet. Note: Low voltage wiring must be isolated from line voltage wiring. Consult
National and Local Electrical Codes for conduit requirements.
3. Wire the LVS Wall Switch to the control device according to the instructions of the device and the appropriate Wiring Diagram below.
Note: Wiring Diagrams can also be found at www.hubbellcontrolsolutions.com.
4. Install the LVS Wall Switch into the wall box using the mounting screws provided. For LVS Wall Switches with multiple buttons, note proper “up
orientation as shown on the product label. Install decorator style wall plate (not included).
5. Perform system setup and/or programming activities as applicable in accordance with the instructions of the system control device.
6. Verify switch functionality by pressing the LVS Wall Switch button(s) and confirm proper system response.
WIRING DIAGRAMS
Wiring Diagram A – LVS 1-Button Latching or Momentary Switch, No Pilot
WIRING DIAGRAMS
Wiring Diagram A LVS 1-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram C LVS 2-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram E LVS 3-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram G LVS 4-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram B LVS 1-Button Latching or
Momentary Switch, with Pilot LED*
Wiring Diagram D LVS 2-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram F LVS 3-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram H LVS 4-Button Latching or
Momentary Switch, with Pilot LEDs*
*Note Pilot Polarity Marks
72-00405-D
701 Millennium Blvd. | Greenville, SC 29607 | (864) 678-1000 | (866) 898-0131 - fax www.hubbellcontrolsolutions.com
Copyright © 2019 Hubbell Control Solutions, a division of Hubbell Lighting, Inc. All rights reserved. All product and company names, logos and product
identifiers are trademarks ™ or registered trademarks ® of Hubbell Lighting, Inc. or their respective owners. Use of them does not necessarily imply any
affiliation with or endorsement by such respective owners.
N O B‘ur/Whuc Wan M mark/Winn: °—m. —°’ swv m rd °__A A A —H— Eluz’wmz mu :2 '6 mark/Wm» °__A A A —H— may/wrung mm: 0740/ o, m. w / mm ° Gmy 5w: ° o——04 Bun c M 94c EM :2 Red 5“ HIJBBELL~ Control Solu
070219
72-00405 D
Low Voltage Wall Switches
INSTALLATION INSTRUCTIONS
Wiring Diagram B – LVS 1-Button Latching or Momentary Switch, with Pilot LED*
Wiring Diagram C – LVS 2-Button Latching or Momentary Switch, No Pilot
Wiring Diagram D – LVS 2-Button Latching or Momentary Switch, with Pilot LEDs*
WIRING DIAGRAMS
Wiring Diagram A LVS 1-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram C LVS 2-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram E LVS 3-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram G LVS 4-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram B LVS 1-Button Latching or
Momentary Switch, with Pilot LED*
Wiring Diagram D LVS 2-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram F LVS 3-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram H LVS 4-Button Latching or
Momentary Switch, with Pilot LEDs*
*Note Pilot Polarity Marks
72-00405-D
WIRING DIAGRAMS
Wiring Diagram A LVS 1-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram C LVS 2-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram E LVS 3-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram G LVS 4-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram B LVS 1-Button Latching or
Momentary Switch, with Pilot LED*
Wiring Diagram D LVS 2-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram F LVS 3-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram H LVS 4-Button Latching or
Momentary Switch, with Pilot LEDs*
*Note Pilot Polarity Marks
72-00405-D
WIRING DIAGRAMS
Wiring Diagram A LVS 1-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram C LVS 2-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram E LVS 3-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram G LVS 4-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram B LVS 1-Button Latching or
Momentary Switch, with Pilot LED*
Wiring Diagram D LVS 2-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram F LVS 3-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram H LVS 4-Button Latching or
Momentary Switch, with Pilot LEDs*
*Note Pilot Polarity Marks
72-00405-D
WIRING DIAGRAMS
Wiring Diagram A LVS 1-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram C LVS 2-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram E LVS 3-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram G LVS 4-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram B LVS 1-Button Latching or
Momentary Switch, with Pilot LED*
Wiring Diagram D LVS 2-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram F LVS 3-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram H LVS 4-Button Latching or
Momentary Switch, with Pilot LEDs*
*Note Pilot Polarity Marks
72-00405-D
Wiring Diagram E – LVS 3-Button Latching or Momentary Switch, No Pilot
701 Millennium Blvd. | Greenville, SC 29607 | (864) 678-1000 | (866) 898-0131 - fax www.hubbellcontrolsolutions.com
Copyright © 2019 Hubbell Control Solutions, a division of Hubbell Lighting, Inc. All rights reserved. All product and company names, logos and product
identifiers are trademarks ™ or registered trademarks ® of Hubbell Lighting, Inc. or their respective owners. Use of them does not necessarily imply any
affiliation with or endorsement by such respective owners.
lua/W'Kfi 94c Blue 0/ my swzc Red ya Orange SW C Black 6 Fun I \\ rum 2\\ \ rum 4 sm H u BBELL' cam-o: Solutions
070219
72-00405 D
Low Voltage Wall Switches
INSTALLATION INSTRUCTIONS
Wiring Diagram F – LVS 3-Button Latching or Momentary Switch, with Pilot LEDs*
Wiring Diagram G – LVS 4-Button Latching or Momentary Switch, No Pilot
Wiring Diagram H – LVS 4-Button Latching or Momentary Switch, with Pilot LEDs*
*Note Pilot Polarity Marks
WIRING DIAGRAMS
Wiring Diagram A LVS 1-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram C LVS 2-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram E LVS 3-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram G LVS 4-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram B LVS 1-Button Latching or
Momentary Switch, with Pilot LED*
Wiring Diagram D LVS 2-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram F LVS 3-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram H LVS 4-Button Latching or
Momentary Switch, with Pilot LEDs*
*Note Pilot Polarity Marks
72-00405-D
WIRING DIAGRAMS
Wiring Diagram A LVS 1-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram C LVS 2-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram E LVS 3-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram G LVS 4-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram B LVS 1-Button Latching or
Momentary Switch, with Pilot LED*
Wiring Diagram D LVS 2-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram F LVS 3-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram H LVS 4-Button Latching or
Momentary Switch, with Pilot LEDs*
*Note Pilot Polarity Marks
72-00405-D
WIRING DIAGRAMS
Wiring Diagram A LVS 1-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram C LVS 2-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram E LVS 3-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram G LVS 4-Button Latching or
Momentary Switch, No Pilot
Wiring Diagram B LVS 1-Button Latching or
Momentary Switch, with Pilot LED*
Wiring Diagram D LVS 2-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram F LVS 3-Button Latching or
Momentary Switch, with Pilot LEDs*
Wiring Diagram H LVS 4-Button Latching or
Momentary Switch, with Pilot LEDs*
*Note Pilot Polarity Marks
72-00405-D
701 Millennium Blvd. | Greenville, SC 29607 | (864) 678-1000 | (866) 898-0131 - fax www.hubbellcontrolsolutions.com
Copyright © 2019 Hubbell Control Solutions, a division of Hubbell Lighting, Inc. All rights reserved. All product and company names, logos and product
identifiers are trademarks ™ or registered trademarks ® of Hubbell Lighting, Inc. or their respective owners. Use of them does not necessarily imply any
affiliation with or endorsement by such respective owners.