Using LED Driver Eval Boards to Optimize Retrofit Lighting Designs
投稿人:电子产品
2013-04-02
Lighting designers would do well to make judicious use of readily available evaluation boards or modules, both as a foundation for their lighting projects and to help accelerate the design cycle. In some cases, use of datasheets alone may not be sufficient to prepare you for the design challenges ahead, particularly, for example, if they lack all the data required to select the best LED driver solution for powering lighting systems such as LED retrofit bulbs and down-lighting applications.
Some of the trials lighting designers face include implementing dimming capabilities, achieving high efficiency, and choosing the right design tradeoffs, while simultaneously trying to squeeze all of the electronics into a small space. These reference design kits or evaluation boards focus on making it easier to solve some of these tasks so engineers can quickly implement LED driver ICs into their designs.
We will look at several evaluation boards for LED retrofit bulb projects, including A19, PAR30/38, PAR20, GU10, and candelabra-style bulbs. A range of reference design kits and evaluation boards is available on the DigiKey website from companies such as Maxim Integrated, Power Integrations, and Texas Instruments.
"LED lighting designs are really a balancing act," said Andrew Smith, product marketing manager at Power Integrations. "There are multiple different features and requirements in different geographical regions. If this is your first time trying to manage all of these competing variables, it is extremely daunting."
The role of a design evaluation board or reference design kit is to provide a design that is 75 percent completed, added Smith. "It makes it a lot easier to establish what you really need. You might have to modify a reference design, but you won't have to design it from scratch."
Smith noted that Power Integrations' reference design boards or kits offer a working, production-ready board. The idea is to give a designer something that looks like a real solution, which can be modified. The company's reference design kits include the board, schematics, Gerber files, complete bill of materials, blank boards to build a modified version of the circuit, and extra ICs to evaluate other devices in the same series, which typically provide a little more or less power. The included engineering test report also explains why specific trade-offs were made in the design.
"One of the challenges for LED drivers is that no two applications seem to have the same voltage, current, or form factor," said Smith. He added that “the other thing about reference designs is that they have to fit into very weird spaces so we spend a lot of time optimizing the layout to fit into the space required while not violating any of the design rules for good layout practice."
One of the key requirements for power supply design is to lay out the board properly, according to Smith. "If you're not familiar with how to lay out a power supply, it's a very difficult task."
Once you have decided to take advantage of the benefits provided by a reference design, a remaining challenge is choosing the right reference design for your application without having to do too many modifications. "The first retrofit bulbs were all isolated designs, but now we're seeing the market transition to non-isolated because it's lower cost and higher efficiency," said Smith.
As an example, Power Integrations offers a reference design kit for a basic bulb design that is a low cost and low component count solution. The RDK-131 reference design (Figure 1) board is a 3 W non-isolated constant current LED driver, using Power Integration's LinkSwitch-TN series (e.g., LNK306) for a small GU10 bulb socket. It uses a non-isolated buck converter configuration that enables the use of standard inductors, which reduces the cost of the design.

In another example, Texas Instruments Inc. also focuses on applications that require a small form factor with minimal external components, targeting high-power LED retrofit bulbs including A19, PAR30/38, and GU10. TI offers evaluation boards for its TPS92310 constant-current driver with primary side sensing and power factor correction. The evaluation boards are available for a 120 V flyback LED driver and 230 V flyback LED driver.
The TPS92310 module (Figure 2) PCB measures 22 (L) x 55 (W) x 19 (H) mm. The module can operate with an AC line input from 90 to 132 VRMS or 180 to 264 VRMS. It can supply 350 mA current into a single string of LEDs, with typically six to seven LEDs in series. The evaluation board is designed to comply with industrial EMC and safety requirements. The user guide, datasheet and application notes will help engineers design a board for their specific application.

Another challenge is which of the four topologies – flyback, buck, tapped buck or buck-boost – does a designer select for the LED bulb? Said Smith: "The problem is which one do I pick for my application, and unfortunately the combination of input and output, power factor (PF) and total harmonic distortion (THD) all influence those choices. It's not straightforward."
Power Integrations' RDK-268 reference design kit (Figure 3), as an example, does a good job balancing power factor and THD. The 1.1 W power-factor-corrected LED driver (non-isolated) using the LinkSwitch-PL driver IC, for a non-dimming candelabra lamp replacement design, delivers high power factor (>0.85), low THD (<25%), and low-harmonic content.

"The other thing that is critical for retrofit bulbs in down lighting is the thorny subject of triac dimming, which is a very iterative process to fix because there are many different triacs, and many different dimming circuits," said Smith. "What we tend to do with our reference designs is to specify a list of triac dimmers that this particular circuit will work with."
For instance, the RDK-193 reference design kit from Power Integrations (Figure 4) is a design for a 7 W TRIAC dimmable PAR20 LED driver, using the LinkSwitch-PH LNK403EG. The isolated flyback design delivers high efficiency (greater or equal to 81 percent), and high power factor (>0.90). It is a low cost and low component-count design.

For MR16 bulb applications, Maxim Integrated offers its MAX16820EVKIT+ evaluation kit for the MAX16840 LED driver with integrated MOSFET, which is compatible with most electronic transformers and cut-angle dimmers. The IC can be used in buck, boost, and buck-boost topologies.
Summary
LED lighting designers have a number of design tradeoffs to consider when selecting a LED driver for their retrofit bulb designs. Designers have to consider a number of specs including topology, temperature, THD, efficiency, power factor, input voltage range, surge ratings, type of heat sink, lifetime, and, of course, cost. All of these design criteria have an impact on the final design.
The good news is that many fundamental decisions are made right on the reference design or evaluation board, allowing the designer to concentrate on areas that are most important. A few examples include meeting a high thermal environment, or ensuring that the design will work over an extended voltage range.
免责声明:各个作者和/或论坛参与者在本网站发表的观点、看法和意见不代表 DigiKey 的观点、看法和意见,也不代表 DigiKey 官方政策。